aboutsummaryrefslogtreecommitdiffstats
Commit message (Collapse)AuthorAgeFilesLines
* iio: adc: hx711: Add DT binding for avia,hx711Andreas Klinger2017-10-082-0/+19
| | | | | | | | | | | | | [ Upstream commit ff1293f67734da68e23fecb6ecdae7112b8c43f9 ] Add DT bindings for avia,hx711 Add vendor avia to vendor list Signed-off-by: Andreas Klinger <ak@it-klinger.de> Acked-by: Rob Herring <robh@kernel.org> Signed-off-by: Jonathan Cameron <jic23@kernel.org> Signed-off-by: Sasha Levin <alexander.levin@verizon.com> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* drm: bridge: add DT bindings for TI ths8135Bartosz Golaszewski2017-10-081-0/+46
| | | | | | | | | | | | | | [ Upstream commit 2e644be30fcc08c736f66b60f4898d274d4873ab ] THS8135 is a configurable video DAC. Add DT bindings for this chip. Signed-off-by: Bartosz Golaszewski <bgolaszewski@baylibre.com> Reviewed-by: Laurent Pinchart <laurent.pinchart@ideasonboard.com> Acked-by: Rob Herring <robh@kernel.org> Signed-off-by: Archit Taneja <architt@codeaurora.org> Link: http://patchwork.freedesktop.org/patch/msgid/1481623759-12786-3-git-send-email-bgolaszewski@baylibre.com Signed-off-by: Sasha Levin <alexander.levin@verizon.com> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* sysctl: enable strict writesKees Cook2017-07-051-8/+7
| | | | | | | | | | | | | | | | | | | | | commit 41662f5cc55335807d39404371cfcbb1909304c4 upstream. SYSCTL_WRITES_WARN was added in commit f4aacea2f5d1 ("sysctl: allow for strict write position handling"), and released in v3.16 in August of 2014. Since then I can find only 1 instance of non-zero offset writing[1], and it was fixed immediately in CRIU[2]. As such, it appears safe to flip this to the strict state now. [1] https://www.google.com/search?q="when%20file%20position%20was%20not%200" [2] http://lists.openvz.org/pipermail/criu/2015-April/019819.html Signed-off-by: Kees Cook <keescook@chromium.org> Cc: "Eric W. Biederman" <ebiederm@xmission.com> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org> Cc: Sumit Semwal <sumit.semwal@linaro.org> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* mm: larger stack guard gap, between vmasHugh Dickins2017-06-261-0/+7
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | commit 1be7107fbe18eed3e319a6c3e83c78254b693acb upstream. Stack guard page is a useful feature to reduce a risk of stack smashing into a different mapping. We have been using a single page gap which is sufficient to prevent having stack adjacent to a different mapping. But this seems to be insufficient in the light of the stack usage in userspace. E.g. glibc uses as large as 64kB alloca() in many commonly used functions. Others use constructs liks gid_t buffer[NGROUPS_MAX] which is 256kB or stack strings with MAX_ARG_STRLEN. This will become especially dangerous for suid binaries and the default no limit for the stack size limit because those applications can be tricked to consume a large portion of the stack and a single glibc call could jump over the guard page. These attacks are not theoretical, unfortunatelly. Make those attacks less probable by increasing the stack guard gap to 1MB (on systems with 4k pages; but make it depend on the page size because systems with larger base pages might cap stack allocations in the PAGE_SIZE units) which should cover larger alloca() and VLA stack allocations. It is obviously not a full fix because the problem is somehow inherent, but it should reduce attack space a lot. One could argue that the gap size should be configurable from userspace, but that can be done later when somebody finds that the new 1MB is wrong for some special case applications. For now, add a kernel command line option (stack_guard_gap) to specify the stack gap size (in page units). Implementation wise, first delete all the old code for stack guard page: because although we could get away with accounting one extra page in a stack vma, accounting a larger gap can break userspace - case in point, a program run with "ulimit -S -v 20000" failed when the 1MB gap was counted for RLIMIT_AS; similar problems could come with RLIMIT_MLOCK and strict non-overcommit mode. Instead of keeping gap inside the stack vma, maintain the stack guard gap as a gap between vmas: using vm_start_gap() in place of vm_start (or vm_end_gap() in place of vm_end if VM_GROWSUP) in just those few places which need to respect the gap - mainly arch_get_unmapped_area(), and and the vma tree's subtree_gap support for that. Original-patch-by: Oleg Nesterov <oleg@redhat.com> Original-patch-by: Michal Hocko <mhocko@suse.com> Signed-off-by: Hugh Dickins <hughd@google.com> Acked-by: Michal Hocko <mhocko@suse.com> Tested-by: Helge Deller <deller@gmx.de> # parisc Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org> [wt: backport to 4.11: adjust context] [wt: backport to 4.9: adjust context ; kernel doc was not in admin-guide] [wt: backport to 4.4: adjust context ; drop ppc hugetlb_radix changes] Signed-off-by: Willy Tarreau <w@1wt.eu> [gkh: minor build fixes for 4.4] Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* arm64: documentation: document tagged pointer stack constraintsKristina Martsenko2017-05-251-15/+47
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | commit f0e421b1bf7af97f026e1bb8bfe4c5a7a8c08f42 upstream. Some kernel features don't currently work if a task puts a non-zero address tag in its stack pointer, frame pointer, or frame record entries (FP, LR). For example, with a tagged stack pointer, the kernel can't deliver signals to the process, and the task is killed instead. As another example, with a tagged frame pointer or frame records, perf fails to generate call graphs or resolve symbols. For now, just document these limitations, instead of finding and fixing everything that doesn't work, as it's not known if anyone needs to use tags in these places anyway. In addition, as requested by Dave Martin, generalize the limitations into a general kernel address tag policy, and refactor tagged-pointers.txt to include it. Fixes: d50240a5f6ce ("arm64: mm: permit use of tagged pointers at EL0") Reviewed-by: Dave Martin <Dave.Martin@arm.com> Acked-by: Will Deacon <will.deacon@arm.com> Signed-off-by: Kristina Martsenko <kristina.martsenko@arm.com> Signed-off-by: Catalin Marinas <catalin.marinas@arm.com> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* clk: sunxi: Add apb0 gates for H3Krzysztof Adamski2017-05-021-0/+2
| | | | | | | | | | | | | | | | | | | commit 6e17b4181603d183d20c73f4535529ddf2a2a020 upstream. This patch adds support for APB0 in H3. It seems to be compatible with earlier SOCs. apb0 gates controls R_ block peripherals (R_PIO, R_IR, etc). Since this gates behave just like any Allwinner clock gate, add a generic compatible that can be reused if we don't have any clock to protect. Signed-off-by: Krzysztof Adamski <k@japko.eu> [Maxime: Removed the H3 compatible from the simple-gates driver, reworked the commit log a bit] Signed-off-by: Maxime Ripard <maxime.ripard@free-electrons.com> Cc: Julia Lawall <julia.lawall@lip6.fr> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* mnt: Add a per mount namespace limit on the number of mountsEric W. Biederman2017-04-291-0/+7
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | commit d29216842a85c7970c536108e093963f02714498 upstream. CAI Qian <caiqian@redhat.com> pointed out that the semantics of shared subtrees make it possible to create an exponentially increasing number of mounts in a mount namespace. mkdir /tmp/1 /tmp/2 mount --make-rshared / for i in $(seq 1 20) ; do mount --bind /tmp/1 /tmp/2 ; done Will create create 2^20 or 1048576 mounts, which is a practical problem as some people have managed to hit this by accident. As such CVE-2016-6213 was assigned. Ian Kent <raven@themaw.net> described the situation for autofs users as follows: > The number of mounts for direct mount maps is usually not very large because of > the way they are implemented, large direct mount maps can have performance > problems. There can be anywhere from a few (likely case a few hundred) to less > than 10000, plus mounts that have been triggered and not yet expired. > > Indirect mounts have one autofs mount at the root plus the number of mounts that > have been triggered and not yet expired. > > The number of autofs indirect map entries can range from a few to the common > case of several thousand and in rare cases up to between 30000 and 50000. I've > not heard of people with maps larger than 50000 entries. > > The larger the number of map entries the greater the possibility for a large > number of active mounts so it's not hard to expect cases of a 1000 or somewhat > more active mounts. So I am setting the default number of mounts allowed per mount namespace at 100,000. This is more than enough for any use case I know of, but small enough to quickly stop an exponential increase in mounts. Which should be perfect to catch misconfigurations and malfunctioning programs. For anyone who needs a higher limit this can be changed by writing to the new /proc/sys/fs/mount-max sysctl. Tested-by: CAI Qian <caiqian@redhat.com> Signed-off-by: "Eric W. Biederman" <ebiederm@xmission.com> [bwh: Backported to 4.4: adjust context] Signed-off-by: Ben Hutchings <ben.hutchings@codethink.co.uk> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* netlink: remove mmapped netlink supportFlorian Westphal2017-03-221-332/+0
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | commit d1b4c689d4130bcfd3532680b64db562300716b6 upstream. mmapped netlink has a number of unresolved issues: - TX zerocopy support had to be disabled more than a year ago via commit 4682a0358639b29cf ("netlink: Always copy on mmap TX.") because the content of the mmapped area can change after netlink attribute validation but before message processing. - RX support was implemented mainly to speed up nfqueue dumping packet payload to userspace. However, since commit ae08ce0021087a5d812d2 ("netfilter: nfnetlink_queue: zero copy support") we avoid one copy with the socket-based interface too (via the skb_zerocopy helper). The other problem is that skbs attached to mmaped netlink socket behave different from normal skbs: - they don't have a shinfo area, so all functions that use skb_shinfo() (e.g. skb_clone) cannot be used. - reserving headroom prevents userspace from seeing the content as it expects message to start at skb->head. See for instance commit aa3a022094fa ("netlink: not trim skb for mmaped socket when dump"). - skbs handed e.g. to netlink_ack must have non-NULL skb->sk, else we crash because it needs the sk to check if a tx ring is attached. Also not obvious, leads to non-intuitive bug fixes such as 7c7bdf359 ("netfilter: nfnetlink: use original skbuff when acking batches"). mmaped netlink also didn't play nicely with the skb_zerocopy helper used by nfqueue and openvswitch. Daniel Borkmann fixed this via commit 6bb0fef489f6 ("netlink, mmap: fix edge-case leakages in nf queue zero-copy")' but at the cost of also needing to provide remaining length to the allocation function. nfqueue also has problems when used with mmaped rx netlink: - mmaped netlink doesn't allow use of nfqueue batch verdict messages. Problem is that in the mmap case, the allocation time also determines the ordering in which the frame will be seen by userspace (A allocating before B means that A is located in earlier ring slot, but this also means that B might get a lower sequence number then A since seqno is decided later. To fix this we would need to extend the spinlocked region to also cover the allocation and message setup which isn't desirable. - nfqueue can now be configured to queue large (GSO) skbs to userspace. Queing GSO packets is faster than having to force a software segmentation in the kernel, so this is a desirable option. However, with a mmap based ring one has to use 64kb per ring slot element, else mmap has to fall back to the socket path (NL_MMAP_STATUS_COPY) for all large packets. To use the mmap interface, userspace not only has to probe for mmap netlink support, it also has to implement a recv/socket receive path in order to handle messages that exceed the size of an rx ring element. Cc: Daniel Borkmann <daniel@iogearbox.net> Cc: Ken-ichirou MATSUZAWA <chamaken@gmail.com> Cc: Pablo Neira Ayuso <pablo@netfilter.org> Cc: Patrick McHardy <kaber@trash.net> Cc: Thomas Graf <tgraf@suug.ch> Signed-off-by: Florian Westphal <fw@strlen.de> Signed-off-by: David S. Miller <davem@davemloft.net> Cc: Shi Yuejie <shiyuejie@outlook.com> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* samples: move mic/mpssd example code from DocumentationShuah Khan2017-03-119-2428/+1
| | | | | | | | | | | | | | | | | | commit 6bee835dd54e279f3d3ae2eca92a9c394b4fd028 upstream. Move mic/mpssd examples to samples and remove it from Documentation Makefile. Create a new Makefile to build mic/mpssd. It can be built from top level directory or from mic/mpssd directory: Run make -C samples/mic/mpssd or cd samples/mic/mpssd; make Acked-by: Jonathan Corbet <corbet@lwn.net> Signed-off-by: Shuah Khan <shuahkh@osg.samsung.com> [backported to 4.4-stable as this code is broken on newer versions of gcc and we don't want to break the build for a Documentation sample. - gregkh] Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* x86/platform/goldfish: Prevent unconditional loadingThomas Gleixner2017-02-261-0/+4
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | commit 47512cfd0d7a8bd6ab71d01cd89fca19eb2093eb upstream. The goldfish platform code registers the platform device unconditionally which causes havoc in several ways if the goldfish_pdev_bus driver is enabled: - Access to the hardcoded physical memory region, which is either not available or contains stuff which is completely unrelated. - Prevents that the interrupt of the serial port can be requested - In case of a spurious interrupt it goes into a infinite loop in the interrupt handler of the pdev_bus driver (which needs to be fixed seperately). Add a 'goldfish' command line option to make the registration opt-in when the platform is compiled in. I'm seriously grumpy about this engineering trainwreck, which has seven SOBs from Intel developers for 50 lines of code. And none of them figured out that this is broken. Impressive fail! Fixes: ddd70cf93d78 ("goldfish: platform device for x86") Reported-by: Gabriel C <nix.or.die@gmail.com> Signed-off-by: Thomas Gleixner <tglx@linutronix.de> Acked-by: Linus Torvalds <torvalds@linux-foundation.org> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* ARM: dts: imx31: fix clock control module interrupts descriptionVladimir Zapolskiy2017-01-261-1/+1
| | | | | | | | | | | | | | | commit 2e575cbc930901718cc18e084566ecbb9a4b5ebb upstream. The type of AVIC interrupt controller found on i.MX31 is one-cell, namely 31 for CCM DVFS and 53 for CCM, however for clock control module its interrupts are specified as 3-cells, fix it. Fixes: ef0e4a606fb6 ("ARM: mx31: Replace clk_register_clkdev with clock DT lookup") Acked-by: Rob Herring <robh@kernel.org> Signed-off-by: Vladimir Zapolskiy <vz@mleia.com> Signed-off-by: Shawn Guo <shawnguo@kernel.org> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* KVM: PPC: Book3S HV: Save/restore XER in checkpointed register statePaul Mackerras2017-01-091-0/+1
| | | | | | | | | | | | | | | | | | | | | | | | commit 0d808df06a44200f52262b6eb72bcb6042f5a7c5 upstream. When switching from/to a guest that has a transaction in progress, we need to save/restore the checkpointed register state. Although XER is part of the CPU state that gets checkpointed, the code that does this saving and restoring doesn't save/restore XER. This fixes it by saving and restoring the XER. To allow userspace to read/write the checkpointed XER value, we also add a new ONE_REG specifier. The visible effect of this bug is that the guest may see its XER value being corrupted when it uses transactions. Fixes: e4e38121507a ("KVM: PPC: Book3S HV: Add transactional memory support") Fixes: 0a8eccefcb34 ("KVM: PPC: Book3S HV: Add missing code for transaction reclaim on guest exit") Signed-off-by: Paul Mackerras <paulus@ozlabs.org> Reviewed-by: Thomas Huth <thuth@redhat.com> Signed-off-by: Paul Mackerras <paulus@ozlabs.org> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* Revert "x86/mm: Expand the exception table logic to allow new handling options"Greg Kroah-Hartman2016-10-311-35/+0
| | | | | | | | | | | | | This reverts commit fcf5e5198b447969ed2a56ec335dae3c695a6b46 which is 548acf19234dbda5a52d5a8e7e205af46e9da840 upstream. Cc: Tony Luck <tony.luck@intel.com> Cc: Borislav Petkov <bp@suse.de> Cc: Linus Torvalds <torvalds@linux-foundation.org> Cc: Peter Zijlstra <peterz@infradead.org> Cc: Thomas Gleixner <tglx@linutronix.de> Cc: Ingo Molnar <mingo@kernel.org> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* x86/mm: Expand the exception table logic to allow new handling optionsTony Luck2016-10-311-0/+35
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | commit 548acf19234dbda5a52d5a8e7e205af46e9da840 upstream. Huge amounts of help from Andy Lutomirski and Borislav Petkov to produce this. Andy provided the inspiration to add classes to the exception table with a clever bit-squeezing trick, Boris pointed out how much cleaner it would all be if we just had a new field. Linus Torvalds blessed the expansion with: ' I'd rather not be clever in order to save just a tiny amount of space in the exception table, which isn't really criticial for anybody. ' The third field is another relative function pointer, this one to a handler that executes the actions. We start out with three handlers: 1: Legacy - just jumps the to fixup IP 2: Fault - provide the trap number in %ax to the fixup code 3: Cleaned up legacy for the uaccess error hack Signed-off-by: Tony Luck <tony.luck@intel.com> Reviewed-by: Borislav Petkov <bp@suse.de> Cc: Linus Torvalds <torvalds@linux-foundation.org> Cc: Peter Zijlstra <peterz@infradead.org> Cc: Thomas Gleixner <tglx@linutronix.de> Link: http://lkml.kernel.org/r/f6af78fcbd348cf4939875cfda9c19689b5e50b8.1455732970.git.tony.luck@intel.com Signed-off-by: Ingo Molnar <mingo@kernel.org> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* Input: i8042 - skip selftest on ASUS laptopsMarcos Paulo de Souza2016-10-281-1/+8
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | commit 930e19248e9b61da36c967687ca79c4d5f977919 upstream. On suspend/resume cycle, selftest is executed to reset i8042 controller. But when this is done in Asus devices, subsequent calls to detect/init functions to elantech driver fails. Skipping selftest fixes this problem. An easier step to reproduce this problem is adding i8042.reset=1 as a kernel parameter. On Asus laptops, it'll make the system to start with the touchpad already stuck, since psmouse_probe forcibly calls the selftest function. This patch was inspired by John Hiesey's change[1], but, since this problem affects a lot of models of Asus, let's avoid running selftests on them. All models affected by this problem: A455LD K401LB K501LB K501LX R409L V502LX X302LA X450LCP X450LD X455LAB X455LDB X455LF Z450LA [1]: https://marc.info/?l=linux-input&m=144312209020616&w=2 Fixes: "ETPS/2 Elantech Touchpad dies after resume from suspend" (https://bugzilla.kernel.org/show_bug.cgi?id=107971) Signed-off-by: Marcos Paulo de Souza <marcos.souza.org@gmail.com> Signed-off-by: Dmitry Torokhov <dmitry.torokhov@gmail.com> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* regulator: qcom_spmi: Update mvs1/mvs2 switches on pm8941Stephen Boyd2016-10-071-1/+1
| | | | | | | | | | | | | | | | | | | | commit 93bfe79b03365f410aa91caf04263173c008ecdf upstream. The mvs1 and mvs2 switches are actually called 5vs1 and 5vs2 on some datasheets. Let's rename them to match the datasheets and also match the RPM based regulator driver which calls these by their 5vs names (see qcom_smd-regulator.c). There aren't any users of these regulators so far, so there aren't any concerns of DT ABI breakage here. While we're here making updates to the switches, also mandate usage of the OCP irq for these switches too. Cc: Bjorn Andersson <bjorn.andersson@linaro.org> Fixes: e92a4047419c ("regulator: Add QCOM SPMI regulator driver") Signed-off-by: Stephen Boyd <stephen.boyd@linaro.org> Signed-off-by: Mark Brown <broonie@kernel.org> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* regulator: qcom_spmi: Add support for S4 supply on pm8941Stephen Boyd2016-10-071-2/+2
| | | | | | | | | | | | | | | | | commit c333dfe8dba7d3e47e97e1cee3c38123e19ae73c upstream. The S4 supply is sometimes called the boost regulator because it outputs 5V. Typically it's connected to the 5vs1 and 5vs2 switches for use in USB OTG and HDMI applications. Add support for this regulator which was mistakenly left out from the initial submission of this driver. Cc: Bjorn Andersson <bjorn.andersson@linaro.org> Fixes: e92a4047419c ("regulator: Add QCOM SPMI regulator driver") Signed-off-by: Stephen Boyd <stephen.boyd@linaro.org> Signed-off-by: Mark Brown <broonie@kernel.org> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* pinctrl: Flag strict is a field in struct pinmux_opsAndy Shevchenko2016-10-071-1/+1
| | | | | | | | | | | | | commit 7440926ed9623dceca3310c5f437d06c859dc02b upstream. Documentation incorrectly refers to struct pinctrl_desc, where no such flag is available. Replace the name of the struct. Fixes: commit 8c4c2016345f ("pinctrl: move strict option to pinmux_ops") Signed-off-by: Andy Shevchenko <andriy.shevchenko@linux.intel.com> Signed-off-by: Linus Walleij <linus.walleij@linaro.org> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* mpssd: fix buffer overflow warningMike Danese2016-09-241-2/+2
| | | | | | | | | | | | | | | | | | | | | commit 3610a2add39365a0f153154c60169a66c616d50f upstream. The compilation emits a warning in function ‘snprintf’, inlined from ‘set_cmdline’ at ../Documentation/mic/mpssd/mpssd.c:1541:9: /usr/include/x86_64-linux-gnu/bits/stdio2.h:64:10: warning: call to __builtin___snprintf_chk will always overflow destination buffer This was introduced in commit f4a66c204482 ("misc: mic: Update MIC host daemon with COSM changes") and is fixed by reverting the changes to the size argument of these snprintf statements. Cc: Ashutosh Dixit <ashutosh.dixit@intel.com> Signed-off-by: Mike Danese <mikedanese@google.com> Signed-off-by: Jonathan Corbet <corbet@lwn.net> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* iio: adc: rockchip_saradc: reset saradc controller before programming itCaesar Wang2016-09-241-0/+7
| | | | | | | | | | | | | | | | | | commit 543852af8e5902aee8f7c72c89e1513663e0f696 upstream. SARADC controller needs to be reset before programming it, otherwise it will not function properly. Signed-off-by: Caesar Wang <wxt@rock-chips.com> Cc: Jonathan Cameron <jic23@kernel.org> Cc: Heiko Stuebner <heiko@sntech.de> Cc: Rob Herring <robh+dt@kernel.org> Cc: linux-iio@vger.kernel.org Cc: linux-rockchip@lists.infradead.org Tested-by: Guenter Roeck <linux@roeck-us.net> Signed-off-by: Jonathan Cameron <jic23@kernel.org> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* proc: revert /proc/<pid>/maps [stack:TID] annotationJohannes Weiner2016-09-151-6/+3
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | [ Upstream commit 65376df582174ffcec9e6471bf5b0dd79ba05e4a ] Commit b76437579d13 ("procfs: mark thread stack correctly in proc/<pid>/maps") added [stack:TID] annotation to /proc/<pid>/maps. Finding the task of a stack VMA requires walking the entire thread list, turning this into quadratic behavior: a thousand threads means a thousand stacks, so the rendering of /proc/<pid>/maps needs to look at a million combinations. The cost is not in proportion to the usefulness as described in the patch. Drop the [stack:TID] annotation to make /proc/<pid>/maps (and /proc/<pid>/numa_maps) usable again for higher thread counts. The [stack] annotation inside /proc/<pid>/task/<tid>/maps is retained, as identifying the stack VMA there is an O(1) operation. Siddesh said: "The end users needed a way to identify thread stacks programmatically and there wasn't a way to do that. I'm afraid I no longer remember (or have access to the resources that would aid my memory since I changed employers) the details of their requirement. However, I did do this on my own time because I thought it was an interesting project for me and nobody really gave any feedback then as to its utility, so as far as I am concerned you could roll back the main thread maps information since the information is available in the thread-specific files" Signed-off-by: Johannes Weiner <hannes@cmpxchg.org> Cc: "Kirill A. Shutemov" <kirill@shutemov.name> Cc: Siddhesh Poyarekar <siddhesh.poyarekar@gmail.com> Cc: Shaohua Li <shli@fb.com> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org> Signed-off-by: Sasha Levin <alexander.levin@verizon.com> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* Documentation/module-signing.txt: Note need for version info if reusing a keyBen Hutchings2016-08-201-0/+6
| | | | | | | | | | | | | | commit b8612e517c3c9809e1200b72c474dbfd969e5a83 upstream. Signing a module should only make it trusted by the specific kernel it was built for, not anything else. If a module signing key is used for multiple ABI-incompatible kernels, the modules need to include enough version information to distinguish them. Signed-off-by: Ben Hutchings <ben@decadent.org.uk> Signed-off-by: Rusty Russell <rusty@rustcorp.com.au> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* x86/pat: Document the PAT initialization sequenceToshi Kani2016-08-161-0/+32
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | commit b6350c21cfe8aa9d65e189509a23c0ea4b8362c2 upstream. Update PAT documentation to describe how PAT is initialized under various configurations. Signed-off-by: Toshi Kani <toshi.kani@hpe.com> Reviewed-by: Thomas Gleixner <tglx@linutronix.de> Cc: Andrew Morton <akpm@linux-foundation.org> Cc: Andy Lutomirski <luto@amacapital.net> Cc: Borislav Petkov <bp@alien8.de> Cc: Borislav Petkov <bp@suse.de> Cc: Brian Gerst <brgerst@gmail.com> Cc: Denys Vlasenko <dvlasenk@redhat.com> Cc: H. Peter Anvin <hpa@zytor.com> Cc: Juergen Gross <jgross@suse.com> Cc: Linus Torvalds <torvalds@linux-foundation.org> Cc: Luis R. Rodriguez <mcgrof@suse.com> Cc: Peter Zijlstra <peterz@infradead.org> Cc: Toshi Kani <toshi.kani@hp.com> Cc: elliott@hpe.com Cc: konrad.wilk@oracle.com Cc: paul.gortmaker@windriver.com Cc: xen-devel@lists.xenproject.org Link: http://lkml.kernel.org/r/1458769323-24491-8-git-send-email-toshi.kani@hpe.com Signed-off-by: Ingo Molnar <mingo@kernel.org> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* scsi: fix race between simultaneous decrements of ->host_failedWei Fang2016-07-271-2/+6
| | | | | | | | | | | | | | | | | | | | | | | | | commit 72d8c36ec364c82bf1bf0c64dfa1041cfaf139f7 upstream. sas_ata_strategy_handler() adds the works of the ata error handler to system_unbound_wq. This workqueue asynchronously runs work items, so the ata error handler will be performed concurrently on different CPUs. In this case, ->host_failed will be decreased simultaneously in scsi_eh_finish_cmd() on different CPUs, and become abnormal. It will lead to permanently inequality between ->host_failed and ->host_busy, and scsi error handler thread won't start running. IO errors after that won't be handled. Since all scmds must have been handled in the strategy handler, just remove the decrement in scsi_eh_finish_cmd() and zero ->host_busy after the strategy handler to fix this race. Fixes: 50824d6c5657 ("[SCSI] libsas: async ata-eh") Signed-off-by: Wei Fang <fangwei1@huawei.com> Reviewed-by: James Bottomley <jejb@linux.vnet.ibm.com> Signed-off-by: Martin K. Petersen <martin.petersen@oracle.com> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* iio: proximity: as3935: correct IIO_CHAN_INFO_RAW outputMatt Ranostay2016-07-271-1/+1
| | | | | | | | | | | | commit 5138806f16c74c7cb8ac3e408a859c79eb7c9567 upstream. IIO_CHAN_INFO_RAW was returning processed data which was incorrect. This also adds the IIO_CHAN_INFO_SCALE value to convert to a processed value. Signed-off-by: Matt Ranostay <mranostay@gmail.com> Signed-off-by: Jonathan Cameron <jic23@kernel.org> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* pipe: limit the per-user amount of pages allocated in pipesWilly Tarreau2016-06-071-0/+23
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | commit 759c01142a5d0f364a462346168a56de28a80f52 upstream. On no-so-small systems, it is possible for a single process to cause an OOM condition by filling large pipes with data that are never read. A typical process filling 4000 pipes with 1 MB of data will use 4 GB of memory. On small systems it may be tricky to set the pipe max size to prevent this from happening. This patch makes it possible to enforce a per-user soft limit above which new pipes will be limited to a single page, effectively limiting them to 4 kB each, as well as a hard limit above which no new pipes may be created for this user. This has the effect of protecting the system against memory abuse without hurting other users, and still allowing pipes to work correctly though with less data at once. The limit are controlled by two new sysctls : pipe-user-pages-soft, and pipe-user-pages-hard. Both may be disabled by setting them to zero. The default soft limit allows the default number of FDs per process (1024) to create pipes of the default size (64kB), thus reaching a limit of 64MB before starting to create only smaller pipes. With 256 processes limited to 1024 FDs each, this results in 1024*64kB + (256*1024 - 1024) * 4kB = 1084 MB of memory allocated for a user. The hard limit is disabled by default to avoid breaking existing applications that make intensive use of pipes (eg: for splicing). Reported-by: socketpair@gmail.com Reported-by: Tetsuo Handa <penguin-kernel@I-love.SAKURA.ne.jp> Mitigates: CVE-2013-4312 (Linux 2.0+) Suggested-by: Linus Torvalds <torvalds@linux-foundation.org> Signed-off-by: Willy Tarreau <w@1wt.eu> Signed-off-by: Al Viro <viro@zeniv.linux.org.uk> Cc: Moritz Muehlenhoff <moritz@wikimedia.org> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* ARM: dts: imx35: restore existing used clock enumerationAlexander Kurz2016-06-071-0/+1
| | | | | | | | | | | | | | | | | | commit 3397c2c45b1b6f54834dfeae30a73046f33ca943 upstream. A new element got inserted into enum mx35_clks with commit 3713e3f5e927 ("clk: imx35: define two clocks for rtc"). This insertion shifted most nummerical clock assignments to a new nummerical value which in turn rendered most hardcoded nummeric values in imx35.dtsi incorrect. Restore the existing order by moving the newly introduced clock to the end of the enum. Update the dts documentation accordingly. Signed-off-by: Alexander Kurz <akurz@blala.de> Fixes: 3713e3f5e927 ("clk: imx35: define two clocks for rtc") Signed-off-by: Shawn Guo <shawnguo@kernel.org> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* Fix OpenSSH pty regression on closeBrian Bloniarz2016-06-011-3/+0
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | commit 0f40fbbcc34e093255a2b2d70b6b0fb48c3f39aa upstream. OpenSSH expects the (non-blocking) read() of pty master to return EAGAIN only if it has received all of the slave-side output after it has received SIGCHLD. This used to work on pre-3.12 kernels. This fix effectively forces non-blocking read() and poll() to block for parallel i/o to complete for all ttys. It also unwinds these changes: 1) f8747d4a466ab2cafe56112c51b3379f9fdb7a12 tty: Fix pty master read() after slave closes 2) 52bce7f8d4fc633c9a9d0646eef58ba6ae9a3b73 pty, n_tty: Simplify input processing on final close 3) 1a48632ffed61352a7810ce089dc5a8bcd505a60 pty: Fix input race when closing Inspired by analysis and patch from Marc Aurele La France <tsi@tuyoix.net> Reported-by: Volth <openssh@volth.com> Reported-by: Marc Aurele La France <tsi@tuyoix.net> BugLink: https://bugzilla.mindrot.org/show_bug.cgi?id=52 BugLink: https://bugzilla.mindrot.org/show_bug.cgi?id=2492 Signed-off-by: Brian Bloniarz <brian.bloniarz@gmail.com> Reviewed-by: Peter Hurley <peter@hurleysoftware.com> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* ata: ahci-platform: Add ports-implemented DT bindings.Srinivas Kandagatla2016-05-111-0/+4
| | | | | | | | | | | | | | | | | | | | | | | commit 17dcc37e3e847bc0e67a5b1ec52471fcc6c18682 upstream. On some SOCs PORTS_IMPL register value is never programmed by the firmware and left at zero value. Which means that no sata ports are available for software. AHCI driver used to cope up with this by fabricating the port_map if the PORTS_IMPL register is read zero, but recent patch broke this workaround as zero value was valid for NVMe disks. This patch adds ports-implemented DT bindings as workaround for this issue in a way that DT can can override the PORTS_IMPL register in cases where the firmware did not program it already. Fixes: 566d1827df2e ("libata: disable forced PORTS_IMPL for >= AHCI 1.3") Signed-off-by: Srinivas Kandagatla <srinivas.kandagatla@linaro.org> Acked-by: Tejun Heo <tj@kernel.org> Reviewed-by: Andy Gross <andy.gross@linaro.org> Signed-off-by: Tejun Heo <tj@kernel.org> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* pinctrl: pistachio: fix mfio84-89 function description and pinmux.Govindraj Raja2016-04-201-6/+6
| | | | | | | | | | | | | | | | | | | | | | | | | | | | commit e9adb336d0bf391be23e820975ca5cd12c31d781 upstream. mfio 84 to 89 are described wrongly, fix it to describe the right pin and add them to right pin-mux group. The correct order is: pll1_lock => mips_pll -- MFIO_83 pll2_lock => audio_pll -- MFIO_84 pll3_lock => rpu_v_pll -- MFIO_85 pll4_lock => rpu_l_pll -- MFIO_86 pll5_lock => sys_pll -- MFIO_87 pll6_lock => wifi_pll -- MFIO_88 pll7_lock => bt_pll -- MFIO_89 Cc: linux-gpio@vger.kernel.org Cc: devicetree@vger.kernel.org Cc: linux-mips@linux-mips.org Cc: James Hartley <James.Hartley@imgtec.com> Fixes: cefc03e5995e("pinctrl: Add Pistachio SoC pin control driver") Signed-off-by: Govindraj Raja <Govindraj.Raja@imgtec.com> Acked-by: Andrew Bresticker <abrestic@chromium.org> Acked-by: Rob Herring <robh@kernel.org> Signed-off-by: Linus Walleij <linus.walleij@linaro.org> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* USB: uas: Add a new NO_REPORT_LUNS quirkHans de Goede2016-04-201-0/+2
| | | | | | | | | | | | | | commit 1363074667a6b7d0507527742ccd7bbed5e3ceaa upstream. Add a new NO_REPORT_LUNS quirk and set it for Seagate drives with an usb-id of: 0bc2:331a, as these will fail to respond to a REPORT_LUNS command. Reported-and-tested-by: David Webb <djw@noc.ac.uk> Signed-off-by: Hans de Goede <hdegoede@redhat.com> Acked-by: Alan Stern <stern@rowland.harvard.edu> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* KVM: MMU: fix ept=0/pte.u=1/pte.w=0/CR0.WP=0/CR4.SMEP=1/EFER.NX=0 comboPaolo Bonzini2016-03-161-1/+2
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | commit 844a5fe219cf472060315971e15cbf97674a3324 upstream. Yes, all of these are needed. :) This is admittedly a bit odd, but kvm-unit-tests access.flat tests this if you run it with "-cpu host" and of course ept=0. KVM runs the guest with CR0.WP=1, so it must handle supervisor writes specially when pte.u=1/pte.w=0/CR0.WP=0. Such writes cause a fault when U=1 and W=0 in the SPTE, but they must succeed because CR0.WP=0. When KVM gets the fault, it sets U=0 and W=1 in the shadow PTE and restarts execution. This will still cause a user write to fault, while supervisor writes will succeed. User reads will fault spuriously now, and KVM will then flip U and W again in the SPTE (U=1, W=0). User reads will be enabled and supervisor writes disabled, going back to the originary situation where supervisor writes fault spuriously. When SMEP is in effect, however, U=0 will enable kernel execution of this page. To avoid this, KVM also sets NX=1 in the shadow PTE together with U=0. If the guest has not enabled NX, the result is a continuous stream of page faults due to the NX bit being reserved. The fix is to force EFER.NX=1 even if the CPU is taking care of the EFER switch. (All machines with SMEP have the CPU_LOAD_IA32_EFER vm-entry control, so they do not use user-return notifiers for EFER---if they did, EFER.NX would be forced to the same value as the host). There is another bug in the reserved bit check, which I've split to a separate patch for easier application to stable kernels. Cc: Andy Lutomirski <luto@amacapital.net> Reviewed-by: Xiao Guangrong <guangrong.xiao@linux.intel.com> Fixes: f6577a5fa15d82217ca73c74cd2dcbc0f6c781dd Signed-off-by: Paolo Bonzini <pbonzini@redhat.com> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* ARM: OMAP2+: hwmod: Introduce ti,no-idle dt propertyLokesh Vutla2016-03-161-0/+1
| | | | | | | | | | | | | | | | | | commit 2e18f5a1bc18e8af7031b3b26efde25307014837 upstream. Introduce a dt property, ti,no-idle, that prevents an IP to idle at any point. This is to handle Errata i877, which tells that GMAC clocks cannot be disabled. Acked-by: Roger Quadros <rogerq@ti.com> Tested-by: Mugunthan V N <mugunthanvnm@ti.com> Signed-off-by: Lokesh Vutla <lokeshvutla@ti.com> Signed-off-by: Sekhar Nori <nsekhar@ti.com> Signed-off-by: Dave Gerlach <d-gerlach@ti.com> Acked-by: Rob Herring <robh@kernel.org> Signed-off-by: Paul Walmsley <paul@pwsan.com> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* efi: Make efivarfs entries immutable by defaultPeter Jones2016-03-031-0/+7
| | | | | | | | | | | | | | | | | | | | | | | | commit ed8b0de5a33d2a2557dce7f9429dca8cb5bc5879 upstream. "rm -rf" is bricking some peoples' laptops because of variables being used to store non-reinitializable firmware driver data that's required to POST the hardware. These are 100% bugs, and they need to be fixed, but in the mean time it shouldn't be easy to *accidentally* brick machines. We have to have delete working, and picking which variables do and don't work for deletion is quite intractable, so instead make everything immutable by default (except for a whitelist), and make tools that aren't quite so broad-spectrum unset the immutable flag. Signed-off-by: Peter Jones <pjones@redhat.com> Tested-by: Lee, Chun-Yi <jlee@suse.com> Acked-by: Matthew Garrett <mjg59@coreos.com> Signed-off-by: Matt Fleming <matt@codeblueprint.co.uk> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* usb: core: lpm: fix usb3_hardware_lpm sysfs nodeLu Baolu2016-01-312-12/+15
| | | | | | | | | | | | | | | | | | | | commit bf5ce5bf3cc7136fd7fe5e8999a580bc93a9c8f6 upstream. Commit 655fe4effe0f ("usbcore: add sysfs support to xHCI usb3 hardware LPM") introduced usb3_hardware_lpm sysfs node. This doesn't show the correct status of USB3 U1 and U2 LPM status. This patch fixes this by replacing usb3_hardware_lpm with two nodes, usb3_hardware_lpm_u1 (for U1) and usb3_hardware_lpm_u2 (for U2), and recording the U1/U2 LPM status in right places. This patch should be back-ported to kernels as old as 4.3, that contains Commit 655fe4effe0f ("usbcore: add sysfs support to xHCI usb3 hardware LPM"). Signed-off-by: Lu Baolu <baolu.lu@linux.intel.com> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* Merge git://git.kernel.org/pub/scm/linux/kernel/git/davem/netLinus Torvalds2015-12-311-3/+3
|\ | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Pull networking fixes from David Miller: 1) Prevent XFRM per-cpu counter updates for one namespace from being applied to another namespace. Fix from DanS treetman. 2) Fix RCU de-reference in iwl_mvm_get_key_sta_id(), from Johannes Berg. 3) Remove ethernet header assumption in nft_do_chain_netdev(), from Pablo Neira Ayuso. 4) Fix cpsw PHY ident with multiple slaves and fixed-phy, from Pascal Speck. 5) Fix use after free in sixpack_close and mkiss_close. 6) Fix VXLAN fw assertion on bnx2x, from Yuval Mintz. 7) natsemi doesn't check for DMA mapping errors, from Alexey Khoroshilov. 8) Fix inverted test in ip6addrlbl_get(), from ANdrey Ryabinin. 9) Missing initialization of needed_headroom in geneve tunnel driver, from Paolo Abeni. 10) Fix conntrack template leak in openvswitch, from Joe Stringer. 11) Mission initialization of wq->flags in sock_alloc_inode(), from Nicolai Stange. * git://git.kernel.org/pub/scm/linux/kernel/git/davem/net: (35 commits) sctp: sctp should release assoc when sctp_make_abort_user return NULL in sctp_close net, socket, socket_wq: fix missing initialization of flags drivers: net: cpsw: fix error return code openvswitch: Fix template leak in error cases. sctp: label accepted/peeled off sockets sctp: use GFP_USER for user-controlled kmalloc qlcnic: fix a loop exit condition better net: cdc_ncm: avoid changing RX/TX buffers on MTU changes geneve: initialize needed_headroom ipv6: honor ifindex in case we receive ll addresses in router advertisements addrconf: always initialize sysctl table data ipv6/addrlabel: fix ip6addrlbl_get() switchdev: bridge: Pass ageing time as clock_t instead of jiffies sh_eth: fix 16-bit descriptor field access endianness too veth: don’t modify ip_summed; doing so treats packets with bad checksums as good. net: usb: cdc_ncm: Adding Dell DW5813 LTE AT&T Mobile Broadband Card net: usb: cdc_ncm: Adding Dell DW5812 LTE Verizon Mobile Broadband Card natsemi: add checks for dma mapping errors rhashtable: Kill harmless RCU warning in rhashtable_walk_init openvswitch: correct encoding of set tunnel action attributes ...
| * drivers: net: cpsw: fix RMII/RGMII mode when used with fixed-link PHYDavid Rivshin2015-12-181-3/+3
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Commit 1f71e8c96fc654724723ce987e0a8b2aeb81746d ("drivers: net: cpsw: Add support for fixed-link PHY") did not parse the "phy-mode" property in the case of a fixed-link PHY, leaving slave_data->phy_if with its default of PHY_INTERFACE_MODE_NA(0). This later gets passed to phy_connect() in cpsw_slave_open(), and eventually to cpsw_phy_sel() where it hits a default case that configures the MAC for MII mode. The user visible symptom is that while kernel log messages seem to indicate that the interface is set up, there is no network communication. Eventually a watchdog error occurs: NETDEV WATCHDOG: eth0 (cpsw): transmit queue 0 timed out Fixes: 1f71e8c96fc6 ("drivers: net: cpsw: Add support for fixed-link PHY") Signed-off-by: David Rivshin <drivshin@allworx.com> Signed-off-by: David S. Miller <davem@davemloft.net>
* | Merge branch 'for-linus' of ↵Linus Torvalds2015-12-191-1/+1
|\ \ | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | git://git.kernel.org/pub/scm/linux/kernel/git/dtor/input Pull input fixes from Dmitry Torokhov: "Just a few assorted driver fixes" * 'for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/dtor/input: Input: elants_i2c - fix wake-on-touch Input: elan_i2c - set input device's vendor and product IDs Input: sun4i-lradc-keys - fix typo in binding documentation Input: atmel_mxt_ts - add maxtouch to I2C table for module autoload Input: arizona-haptic - fix disabling of haptics device Input: aiptek - fix crash on detecting device without endpoints Input: atmel_mxt_ts - add generic platform data for Chromebooks Input: parkbd - clear unused function pointers Input: walkera0701 - clear unused function pointers Input: turbografx - clear unused function pointers Input: gamecon - clear unused function pointers Input: db9 - clear unused function pointers
| * | Input: sun4i-lradc-keys - fix typo in binding documentationKarsten Merker2015-12-121-1/+1
| | | | | | | | | | | | | | | | | | | | | | | | | | | Trivial typo fix ("mut" -> "must") in the sunxi LRADC-keys binding documentation. Signed-off-by: Karsten Merker <merker@debian.org> Acked-by: Rob Herring <robh@kernel.org> Acked-by: Chen-Yu Tsai <wens@csie.org> Signed-off-by: Dmitry Torokhov <dmitry.torokhov@gmail.com>
* | | Merge tag 'for-linus-20151217' of git://git.infradead.org/linux-mtdLinus Torvalds2015-12-181-1/+6
|\ \ \ | |_|/ |/| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Pull MTD fixes from Brian Norris: "I was holding out on this pull request for a bit, since there are a few other small issues being discussed that look like 4.4-rc regressions. Hopefully I can get those stabilized soon, but these are ready at any rate: - A little bit of a last-minute change for the device tree "fixed partition" binding. This is needed because we might want to reuse the 'partitions' subnode for other sorts of partitioning descriptions -- e.g., for describing which on-flash partition format(s) might be used on the system. - Also tone down a warning message, since it is probably going to show up on a lot of systems where it should just be ignored" * tag 'for-linus-20151217' of git://git.infradead.org/linux-mtd: doc: dt: mtd: partitions: add compatible property to "partitions" node mtd: ofpart: don't complain about missing 'partitions' node too loudly
| * | doc: dt: mtd: partitions: add compatible property to "partitions" nodeBrian Norris2015-12-081-1/+6
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | As noted here [1], there are potentially future conflicts if we try to use MTD's "partitions" subnode to describe anything besides just the fixed-in-the-device-tree partitions currently described in this document. Particularly, there was a proposal to use this node for the AFS parser too. It can pose a (small) problem to try to differentiate the following nodes: // using binding as currently specified partitions { #address-cells = <x>; #size-cells = <y>; partition@0 { ...; }; }; and // proposed future binding partitions { compatible = "arm,arm-flash-structure"; }; It's especially difficult if other uses of this node start having subnodes. So, since the "partitions" node is new in v4.4, let's fixup the binding before release so that it requires a compatible property, so it's much clearer to distinguish. e.g.: // proposed partitions { compatible = "fixed-partitions"; #address-cells = <x>; #size-cells = <y>; partition@0 { ...; }; }; [1] Subject: "mtd: create a partition type device tree binding" http://lkml.kernel.org/g/20151113220039.GA74382@google.com http://lists.infradead.org/pipermail/linux-mtd/2015-November/063355.html http://lists.infradead.org/pipermail/linux-mtd/2015-November/063364.html Cc: Michal Suchanek <hramrach@gmail.com> Signed-off-by: Brian Norris <computersforpeace@gmail.com> Acked-by: Rob Herring <robh@kernel.org>
* | | Merge git://git.kernel.org/pub/scm/linux/kernel/git/davem/netLinus Torvalds2015-12-171-14/+0
|\ \ \ | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Pull networking fixes from David Miller: 1) Fix uninitialized variable warnings in nfnetlink_queue, a lot of people reported this... From Arnd Bergmann. 2) Don't init mutex twice in i40e driver, from Jesse Brandeburg. 3) Fix spurious EBUSY in rhashtable, from Herbert Xu. 4) Missing DMA unmaps in mvpp2 driver, from Marcin Wojtas. 5) Fix race with work structure access in pppoe driver causing corruptions, from Guillaume Nault. 6) Fix OOPS due to sh_eth_rx() not checking whether netdev_alloc_skb() actually succeeded or not, from Sergei Shtylyov. 7) Don't lose flags when settifn IFA_F_OPTIMISTIC in ipv6 code, from Bjørn Mork. 8) VXLAN_HD_RCO defined incorrectly, fix from Jiri Benc. 9) Fix clock source used for cookies in SCTP, from Marcelo Ricardo Leitner. 10) aurora driver needs HAS_DMA dependency, from Geert Uytterhoeven. 11) ndo_fill_metadata_dst op of vxlan has to handle ipv6 tunneling properly as well, from Jiri Benc. 12) Handle request sockets properly in xfrm layer, from Eric Dumazet. 13) Double stats update in ipv6 geneve transmit path, fix from Pravin B Shelar. 14) sk->sk_policy[] needs RCU protection, and as a result xfrm_policy_destroy() needs to free policies using an RCU grace period, from Eric Dumazet. 15) SCTP needs to clone ipv6 tx options in order to avoid use after free, from Eric Dumazet. 16) Missing kbuild export if ila.h, from Stephen Hemminger. 17) Missing mdiobus_alloc() return value checking in mdio-mux.c, from Tobias Klauser. 18) Validate protocol value range in ->create() methods, from Hannes Frederic Sowa. 19) Fix early socket demux races that result in illegal dst reuse, from Eric Dumazet. 20) Validate socket address length in pptp code, from WANG Cong. 21) skb_reorder_vlan_header() uses incorrect offset and can corrupt packets, from Vlad Yasevich. 22) Fix memory leaks in nl80211 registry code, from Ola Olsson. 23) Timeout loop count handing fixes in mISDN, xgbe, qlge, sfc, and qlcnic. From Dan Carpenter. 24) msg.msg_iocb needs to be cleared in recvfrom() otherwise, for example, AF_ALG will interpret it as an async call. From Tadeusz Struk. 25) inetpeer_set_addr_v4 forgets to initialize the 'vif' field, from Eric Dumazet. 26) rhashtable enforces the minimum table size not early enough, breaking how we calculate the per-cpu lock allocations. From Herbert Xu. 27) Fix FCC port lockup in 82xx driver, from Martin Roth. 28) FOU sockets need to be freed using RCU, from Hannes Frederic Sowa. 29) Fix out-of-bounds access in __skb_complete_tx_timestamp() and sock_setsockopt() wrt. timestamp handling. From WANG Cong. * git://git.kernel.org/pub/scm/linux/kernel/git/davem/net: (117 commits) net: check both type and procotol for tcp sockets drivers: net: xgene: fix Tx flow control tcp: restore fastopen with no data in SYN packet af_unix: Revert 'lock_interruptible' in stream receive code fou: clean up socket with kfree_rcu 82xx: FCC: Fixing a bug causing to FCC port lock-up gianfar: Don't enable RX Filer if not supported net: fix warnings in 'make htmldocs' by moving macro definition out of field declaration rhashtable: Fix walker list corruption rhashtable: Enforce minimum size on initial hash table inet: tcp: fix inetpeer_set_addr_v4() ipv6: automatically enable stable privacy mode if stable_secret set net: fix uninitialized variable issue bluetooth: Validate socket address length in sco_sock_bind(). net_sched: make qdisc_tree_decrease_qlen() work for non mq ser_gigaset: remove unnecessary kfree() calls from release method ser_gigaset: fix deallocation of platform device structure ser_gigaset: turn nonsense checks into WARN_ON ser_gigaset: fix up NULL checks qlcnic: fix a timeout loop ...
| * \ \ Merge branch 'master' of ↵David S. Miller2015-12-051-14/+0
| |\ \ \ | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | git://git.kernel.org/pub/scm/linux/kernel/git/jkirsher/net-queue Jeff Kirsher says: ==================== Intel Wired LAN Driver Updates 2015-12-03 This series contains updates to ixgbe, i40e/i40evf, MAINTAINERS and e100.txt Alex provides a fix for ixgbe where enabling SR-IOV and then bringing the interface up was resulting in the PF MAC addresses getting into a bad state. The workaround for this issue is to bring up the interface first and then enable SR-IOV as this will trigger the reset in the existing code. I clean up legacy license stuff in the e100.txt documentation and then update the maintainers/reviewers list for our drivers. Jesse fixes an issue with the i40e/i40evf drivers, where if the driver were to happen to have a mutex held while the i40e_init_adminq() call was called, the init_adminq might inadvertently call mutex_init on a lock that was held which is a violation of the calling semantices. ==================== Signed-off-by: David S. Miller <davem@davemloft.net>
| | * | | e100.txt: Cleanup license info in kernel docJeff Kirsher2015-12-031-14/+0
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Apparently the e100.txt document contained a "License" section left over from days of old, which does not need to be in the kernel documentation. So clean it up.. CC: John Ronciak <john.ronciak@intel.com> Signed-off-by: Jeff Kirsher <jeffrey.t.kirsher@intel.com> Tested-by: Aaron Brown <aaron.f.brown@intel.com>
* | | | | Merge tag 'dmaengine-fix-4.4-rc6' of ↵Linus Torvalds2015-12-151-6/+4
|\ \ \ \ \ | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | git://git.infradead.org/users/vkoul/slave-dma Pull dmaengine fixes from Vinod Koul: "This has fixes spread thru driver, notably among them: - edma fixes for recent edma DT changes which went into 4.4 - odd fixes for at_hdmac - minor fixes on bc dma and mic dma" * tag 'dmaengine-fix-4.4-rc6' of git://git.infradead.org/users/vkoul/slave-dma: dmaengine: at_xdmac: fix at_xdmac_prep_dma_memcpy() dmaengine: edma: DT: Change reserved slot array from 16bit to 32bit type dmaengine: edma: DT: Change memcpy channel array from 16bit to 32bit type dmaengine: mic_x100: add missing spin_unlock dmaengine: bcm2835-dma: Convert to use DMA pool dmaengine: at_xdmac: fix bad behavior in interleaved mode dmaengine: at_xdmac: fix false condition for memset_sg transfers dmaengine: at_xdmac: fix macro typo
| * \ \ \ \ Merge branch 'fix/edma' into fixesVinod Koul2015-12-091-6/+4
| |\ \ \ \ \
| | * | | | | dmaengine: edma: DT: Change reserved slot array from 16bit to 32bit typePeter Ujfalusi2015-12-091-3/+2
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | This change makes the DT file to be easier to read since the reserved slots array does not need the '/bits/ 16' to be specified, which might confuse some people. Signed-off-by: Peter Ujfalusi <peter.ujfalusi@ti.com> Acked-by: Arnd Bergmann <arnd@arndb.de> Acked-by: Rob Herring <robh@kernel.org> Acked-by: Tony Lindgren <tony@atomide.com> Signed-off-by: Vinod Koul <vinod.koul@intel.com>
| | * | | | | dmaengine: edma: DT: Change memcpy channel array from 16bit to 32bit typePeter Ujfalusi2015-12-091-3/+2
| | | |_|/ / | | |/| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | This change makes the DT file to be easier to read since the memcpy channels array does not need the '/bits/ 16' to be specified, which might confuse some people. Signed-off-by: Peter Ujfalusi <peter.ujfalusi@ti.com> Acked-by: Arnd Bergmann <arnd@arndb.de> Acked-by: Rob Herring <robh@kernel.org> Acked-by: Tony Lindgren <tony@atomide.com> Signed-off-by: Vinod Koul <vinod.koul@intel.com>
* | | | | | Merge tag 'fixes-for-linus' of ↵Linus Torvalds2015-12-121-0/+4
|\ \ \ \ \ \ | |_|_|/ / / |/| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | git://git.kernel.org/pub/scm/linux/kernel/git/arm/arm-soc Pull ARM SoC fixes from Arnd Bergmann: "Here are a bunch of small bug fixes for various ARM platforms, nothing really sticks out this week, most of either fixes bugs in code that was just added in 4.4, or that has been broken for many years without anyone noticing. at91/sama5d2: - fix sama5de hardware setup of sd/mmc interface - proper selection of pinctrl drivers. PIO4 is necessary for sama5d2 berlin: - fix incorrect clock input for SDIO exynos: - Fix potential NULL pointer dereference in Exynos PMU driver. imx: - Fix vf610 SAI clock configuration bug which is discovered by the newly added master mode support in SAI audio driver. - Fix buggy L2 cache latency values in vf610 device trees, which may cause system hang when cpu runs at a higher frequency. ixp4xx: - fix prototypes for readl/writel functions ls2080a: - use little-endian register access for GPIO and SDHCI omap: - Fix clock source for ARM TWD and global timers on am437x - Always select REGULATOR_FIXED_VOLTAGE for omap2+ instead of when MACH_OMAP3_PANDORA is selected - Fix SPI DMA handles for dm816x as only some were mapped - Fix up mbox cells for dm816x to make mailbox usable pxa: - use PWM lookup table for all ezx machines s3c24xx: - Remove incorrect __init annotation from s3c24xx cpufreq driver structures. versatile: - fix PCI IRQ mapping on Versatile PB" * tag 'fixes-for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/arm/arm-soc: ls2080a/dts: Add little endian property for GPIO IP block dt-bindings: define little-endian property for QorIQ GPIO ARM64: dts: ls2080a: fix eSDHC endianness ARM: dts: vf610: use reset values for L2 cache latencies ARM: pxa: use PWM lookup table for all machines ARM: dts: berlin: add 2nd clock for BG2Q sdhci0 and sdhci1 ARM: dts: berlin: correct BG2Q's sdhci2 2nd clock ARM: dts: am4372: fix clock source for arm twd and global timers ARM: at91: fix pinctrl driver selection ARM: at91/dt: add always-on to 1.8V regulator ARM: dts: vf610: fix clock definition for SAI2 ARM: imx: clk-vf610: fix SAI clock tree ARM: ixp4xx: fix read{b,w,l} return types irqchip/versatile-fpga: Fix PCI IRQ mapping on Versatile PB ARM: OMAP2+: enable REGULATOR_FIXED_VOLTAGE ARM: dts: add dm816x missing spi DT dma handles ARM: dts: add dm816x missing #mbox-cells cpufreq: s3c24xx: Do not mark s3c2410_plls_add as __init ARM: EXYNOS: Fix potential NULL pointer access in exynos_sys_powerdown_conf
| * | | | | dt-bindings: define little-endian property for QorIQ GPIOLi Yang2015-12-111-0/+4
| |/ / / / | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | The GPIO block on different QorIQ chips could have registers in different endianess. Define the property to specify which endian is used by the hardware. Signed-off-by: Liu Gang <Gang.Liu@freescale.com> Acked-by: Rob Herring <robh@kernel.org> Signed-off-by: Li Yang <leoli@freescale.com> Signed-off-by: Kevin Hilman <khilman@linaro.org>