WM8962 audio CODEC This device supports I2C only. Required properties: - compatible : "wlf,wm8962" - reg : the I2C address of the device. Optional properties: - spk-mono: This is a boolean property. If present, the SPK_MONO bit of R51 (Class D Control 2) gets set, indicating that the speaker is in mono mode. - mic-cfg : Default register value for R48 (Additional Control 4). If absent, the default should be the register default. - gpio-cfg : A list of GPIO configuration register values. The list must be 6 entries long. If absent, no configuration of these registers is performed. And note that only the value within [0x0, 0xffff] is valid. Any other value is regarded as setting the GPIO register by its reset value 0x0. Example: codec: wm8962@1a { compatible = "wlf,wm8962"; reg = <0x1a>; gpio-cfg = < 0x0000 /* 0:Default */ 0x0000 /* 1:Default */ 0x0013 /* 2:FN_DMICCLK */ 0x0000 /* 3:Default */ 0x8014 /* 4:FN_DMICCDAT */ 0x0000 /* 5:Default */ >; };