/* * Timer/Counter Unit (TC) registers. * * This program is free software; you can redistribute it and/or modify * it under the terms of the GNU General Public License as published by * the Free Software Foundation; either version 2 of the License, or * (at your option) any later version. */ #ifndef ATMEL_TC_H #define ATMEL_TC_H #include #include /* * Many 32-bit Atmel SOCs include one or more TC blocks, each of which holds * three general-purpose 16-bit timers. These timers share one register bank. * Depending on the SOC, each timer may have its own clock and IRQ, or those * may be shared by the whole TC block. * * These TC blocks may have up to nine external pins: TCLK0..2 signals for * clocks or clock gates, and per-timer TIOA and TIOB signals used for PWM * or triggering. Those pins need to be set up for use with the TC block, * else they will be used as GPIOs or for a different controller. * * Although we expect each TC block to have a platform_device node, those * nodes are not what drivers bind to. Instead, they ask for a specific * TC block, by number ... which is a common approach on systems with many * timers. Then they use clk_get() and platform_get_irq() to get clock and * IRQ resources. */ struct clk; /** * struct atmel_tcb_config - SoC data for a Timer/Counter Block * @counter_width: size in bits of a timer counter register */ struct atmel_tcb_config { size_t counter_width; }; /** * struct atmel_tc - information about a Timer/Counter Block * @pdev: physical device * @regs: mapping through which the I/O registers can be accessed * @id: block id * @tcb_config: configuration data from SoC * @irq: irq for each of the three channels * @clk: internal clock source for each of the three channels * @node: list node, for tclib internal use * @allocated: if already used, for tclib internal use * * On some platforms, each TC channel has its own clocks and IRQs, * while on others, all TC channels share the same clock and IRQ. * Drivers should clk_enable() all the clocks they need even though * all the entries in @clk may point to the same physical clock. * Likewise, drivers should request irqs independently for each * channel, but they must use IRQF_SHARED in case some of the entries * in @irq are actually the same IRQ. */ struct atmel_tc { struct platform_device *pdev; void __iomem *regs; int id; const struct atmel_tcb_config *tcb_config; int irq[3]; struct clk *clk[3]; struct list_head node; bool allocated; }; extern struct atmel_tc *atmel_tc_alloc(unsigned block); extern void atmel_tc_free(struct atmel_tc *tc); /* platform-specific ATMEL_TC_TIMER_CLOCKx divisors (0 means 32KiHz) */ extern const u8 atmel_tc_divisors[5]; /* * Two registers have block-wide controls. These are: configuring the three * "external" clocks (or event sources) used by the timer channels; and * synchronizing the timers by resetting them all at once. * * "External" can mean "external to chip" using the TCLK0, TCLK1, or TCLK2 * signals. Or, it can mean "external to timer", using the TIOA output from * one of the other two timers that's being run in waveform mode. */ #define ATMEL_TC_BCR 0xc0 /* TC Block Control Register */ #define ATMEL_TC_SYNC (1 << 0) /* synchronize timers */ #define ATMEL_TC_BMR 0xc4 /* TC Block Mode Register */ #define ATMEL_TC_TC0XC0S (3 << 0) /* external clock 0 source */ #define ATMEL_TC_TC0XC0S_TCLK0 (0 << 0) #define ATMEL_TC_TC0XC0S_NONE (1 << 0) #define ATMEL_TC_TC0XC0S_TIOA1 (2 << 0) #define ATMEL_TC_TC0XC0S_TIOA2 (3 << 0) #define ATMEL_TC_TC1XC1S (3 << 2) /* external clock 1 source */ #define ATMEL_TC_TC1XC1S_TCLK1 (0 << 2) #define ATMEL_TC_TC1XC1S_NONE (1 << 2) #define ATMEL_TC_TC1XC1S_TIOA0 (2 << 2) #define ATMEL_TC_TC1XC1S_TIOA2 (3 << 2) #define ATMEL_TC_TC2XC2S (3 << 4) /* external clock 2 source */ #define ATMEL_TC_TC2XC2S_TCLK2 (0 << 4) #define ATMEL_TC_TC2XC2S_NONE (1 << 4) #define ATMEL_TC_TC2XC2S_TIOA0 (2 << 4) #define ATMEL_TC_TC2XC2S_TIOA1 (3 << 4) /* * Each TC block has three "channels", each with one counter and controls. * * Note that the semantics of ATMEL_TC_TIMER_CLOCKx (input clock selection * when it's not "external") is silicon-specific. AT91 platforms use one * set of definitions; AVR32 platforms use a different set. Don't hard-wire * such knowledge into your code, use the global "atmel_tc_divisors" ... * where index N is the divisor for clock N+1, else zero to indicate it uses * the 32 KiHz clock. * * The timers can be chained in various ways, and operated in "waveform" * generation mode (including PWM) or "capture" mode (to time events). In * both modes, behavior can be configured in many ways. * * Each timer has two I/O pins, TIOA and TIOB. Waveform mode uses TIOA as a * PWM output, and TIOB as either another PWM or as a trigger. Capture mode * uses them only as inputs. */ #define ATMEL_TC_CHAN(idx) ((idx)*0x40) #define ATMEL_TC_REG(idx, reg) (ATMEL_TC_CHAN(idx) + ATMEL_TC_ ## reg) #define ATMEL_TC_CCR 0x00 /* Channel Control Register */ #define ATMEL_TC_CLKEN (1 << 0) /* clock enable */ #define ATMEL_TC_CLKDIS (1 << 1) /* clock disable */ #define ATMEL_TC_SWTRG (1 << 2) /* software trigger */ #define ATMEL_TC_CMR 0x04 /* Channel Mode Register */ /* Both modes share some CMR bits */ #define ATMEL_TC_TCCLKS (7 << 0) /* clock source */ #define ATMEL_TC_TIMER_CLOCK1 (0 << 0) #define ATMEL_TC_TIMER_CLOCK2 (1 << 0) #define ATMEL_TC_TIMER_CLOCK3 (2 << 0) #define ATMEL_TC_TIMER_CLOCK4 (3 << 0) #define ATMEL_TC_TIMER_CLOCK5 (4 << 0) #define ATMEL_TC_XC0 (5 << 0) #define ATMEL_TC_XC1 (6 << 0) #define ATMEL_TC_XC2 (7 << 0) #define ATMEL_TC_CLKI (1 << 3) /* clock invert */ #define ATMEL_TC_BURST (3 << 4) /* clock gating */ #define ATMEL_TC_GATE_NONE (0 << 4) #define ATMEL_TC_GATE_XC0 (1 << 4) #define ATMEL_TC_GATE_XC1 (2 << 4) #define ATMEL_TC_GATE_XC2 (3 << 4) #define ATMEL_TC_WAVE (1 << 15) /* true = Waveform mode */ /* CAPTURE mode CMR bits */ #define ATMEL_TC_LDBSTOP (1 << 6) /* counter stops on RB load */ #define ATMEL_TC_LDBDIS (1 << 7) /* counter disable on RB load */ #define ATMEL_TC_ETRGEDG (3 << 8) /* external trigger edge */ #define ATMEL_TC_ETRGEDG_NONE (0 << 8) #define ATMEL_TC_ETRGEDG_RISING (1 << 8) #define ATMEL_TC_ETRGEDG_FALLING (2 << 8) #define ATMEL_TC_ETRGEDG_BOTH (3 << 8) #define ATMEL_TC_ABETRG (1 << 10) /* external trigger is TIOA? */ #define ATMEL_TC_CPCTRG (1 << 14) /* RC compare trigger enable */ #define ATMEL_TC_LDRA (3 << 16) /* RA loading edge (of TIOA) */ #define ATMEL_TC_LDRA_NONE (0 << 16) #define ATMEL_TC_LDRA_RISING (1 << 16) #define ATMEL_TC_LDRA_FALLING (2 << 16) #define ATMEL_TC_LDRA_BOTH (3 << 16) #define ATMEL_TC_LDRB (3 << 18) /* RB loading edge (of TIOA) */ #define ATMEL_TC_LDRB_NONE (0 << 18) #define ATMEL_TC_LDRB_RISING (1 << 18) #define ATMEL_TC_LDRB_FALLING (2 << 18) #define ATMEL_TC_LDRB_BOTH (3 << 18) /* WAVEFORM mode CMR bits */ #define ATMEL_TC_CPCSTOP (1 << 6) /* RC compare stops counter */ #define ATMEL_TC_CPCDIS (1 << 7) /* RC compare disables counter */ #define ATMEL_TC_EEVTEDG (3 << 8) /* external event edge */ #define ATMEL_TC_EEVTEDG_NONE (0 << 8) #define ATMEL_TC_EEVTEDG_RISING (1 << 8) #define ATMEL_TC_EEVTEDG_FALLING (2 << 8) #define ATMEL_TC_EEVTEDG_BOTH (3 << 8) #define ATMEL_TC_EEVT (3 << 10) /* external event source */ #define ATMEL_TC_EEVT_TIOB (0 << 10) #define ATMEL_TC_EEVT_XC0 (1 << 10) #define ATMEL_TC_EEVT_XC1 (2 << 10) #define ATMEL_TC_EEVT_XC2 (3 << 10) #define ATMEL_TC_ENETRG (1 << 12) /* external event is trigger */ #define ATMEL_TC_WAVESEL (3 << 13) /* waveform type */ #define ATMEL_TC_WAVESEL_UP (0 << 13) #define ATMEL_TC_WAVESEL_UPDOWN (1 << 13) #define ATMEL_TC_WAVESEL_UP_AUTO (2 << 13) #define ATMEL_TC_WAVESEL_UPDOWN_AUTO (3 << 13) #define ATMEL_TC_ACPA (3 << 16) /* RA compare changes TIOA */ #define ATMEL_TC_ACPA_NONE (0 << 16) #define ATMEL_TC_ACPA_SET (1 << 16) #define ATMEL_TC_ACPA_CLEAR (2 << 16) #define ATMEL_TC_ACPA_TOGGLE (3 << 16) #define ATMEL_TC_ACPC (3 << 18) /* RC compare changes TIOA */ #define ATMEL_TC_ACPC_NONE (0 << 18) #define ATMEL_TC_ACPC_SET (1 << 18) #define ATMEL_TC_ACPC_CLEAR (2 << 18) #define ATMEL_TC_ACPC_TOGGLE (3 << 18) #define ATMEL_TC_AEEVT (3 << 20) /* external event changes TIOA */ #define ATMEL_TC_AEEVT_NONE (0 << 20) #define ATMEL_TC_AEEVT_SET (1 << 20) #define ATMEL_TC_AEEVT_CLEAR (2 << 20) #define ATMEL_TC_AEEVT_TOGGLE (3 << 20) #define ATMEL_TC_ASWTRG (3 << 22) /* software trigger changes TIOA */ #define ATMEL_TC_ASWTRG_NONE (0 << 22) #define ATMEL_TC_ASWTRG_SET (1 << 22) #define ATMEL_TC_ASWTRG_CLEAR (2 << 22) #define ATMEL_TC_ASWTRG_TOGGLE (3 << 22) #define ATMEL_TC_BCPB (3 << 24) /* RB compare changes TIOB */ #define ATMEL_TC_BCPB_NONE (0 << 24) #define ATMEL_TC_BCPB_SET (1 << 24) #define ATMEL_TC_BCPB_CLEAR (2 << 24) #define ATMEL_TC_BCPB_TOGGLE (3 << 24) #define ATMEL_TC_BCPC (3 << 26) /* RC compare changes TIOB */ #define ATMEL_TC_BCPC_NONE (0 << 26) #define ATMEL_TC_BCPC_SET (1 << 26) #define ATMEL_TC_BCPC_CLEAR (2 << 26) #define ATMEL_TC_BCPC_TOGGLE (3 << 26) #define ATMEL_TC_BEEVT (3 << 28) /* external event changes TIOB */ #define ATMEL_TC_BEEVT_NONE (0 << 28) #define ATMEL_TC_BEEVT_SET (1 << 28) #define ATMEL_TC_BEEVT_CLEAR (2 << 28) #define ATMEL_TC_BEEVT_TOGGLE (3 << 28) #define ATMEL_TC_BSWTRG (3 << 30) /* software trigger changes TIOB */ #define ATMEL_TC_BSWTRG_NONE (0 << 30) #define ATMEL_TC_BSWTRG_SET (1 << 30) #define ATMEL_TC_BSWTRG_CLEAR (2 << 30) #define ATMEL_TC_BSWTRG_TOGGLE (3 << 30) #define ATMEL_TC_CV 0x10 /* counter Value */ #define ATMEL_TC_RA 0x14 /* register A */ #define ATMEL_TC_RB 0x18 /* register B */ #define ATMEL_TC_RC 0x1c /* register C */ #define ATMEL_TC_SR 0x20 /* status (read-only) */ /* Status-only flags */ #define ATMEL_TC_CLKSTA (1 << 16) /* clock enabled */ #define ATMEL_TC_MTIOA (1 << 17) /* TIOA mirror */ #define ATMEL_TC_MTIOB (1 << 18) /* TIOB mirror */ #define ATMEL_TC_IER 0x24 /* interrupt enable (write-only) */ #define ATMEL_TC_IDR 0x28 /* interrupt disable (write-only) */ #define ATMEL_TC_IMR 0x2c /* interrupt mask (read-only) */ /* Status and IRQ flags */ #define ATMEL_TC_COVFS (1 << 0) /* counter overflow */ #define ATMEL_TC_LOVRS (1 << 1) /* load overrun */ #define ATMEL_TC_CPAS (1 << 2) /* RA compare */ #define ATMEL_TC_CPBS (1 << 3) /* RB compare */ #define ATMEL_TC_CPCS (1 << 4) /* RC compare */ #define ATMEL_TC_LDRAS (1 << 5) /* RA loading */ #define ATMEL_TC_LDRBS (1 << 6) /* RB loading */ #define ATMEL_TC_ETRGS (1 << 7) /* external trigger */ #define ATMEL_TC_ALL_IRQ (ATMEL_TC_COVFS | ATMEL_TC_LOVRS | \ ATMEL_TC_CPAS | ATMEL_TC_CPBS | \ ATMEL_TC_CPCS | ATMEL_TC_LDRAS | \ ATMEL_TC_LDRBS | ATMEL_TC_ETRGS) \ /* all IRQs */ #endif