/* * include/linux/cpu.h - generic cpu definition * * This is mainly for topological representation. We define the * basic 'struct cpu' here, which can be embedded in per-arch * definitions of processors. * * Basic handling of the devices is done in drivers/base/cpu.c * * CPUs are exported via sysfs in the devices/system/cpu * directory. */ #ifndef _LINUX_CPU_H_ #define _LINUX_CPU_H_ #include #include #include struct device; struct device_node; struct attribute_group; struct cpu { int node_id; /* The node which contains the CPU */ int hotpluggable; /* creates sysfs control file if hotpluggable */ struct device dev; }; extern int register_cpu(struct cpu *cpu, int num); extern struct device *get_cpu_device(unsigned cpu); extern bool cpu_is_hotpluggable(unsigned cpu); extern bool arch_match_cpu_phys_id(int cpu, u64 phys_id); extern bool arch_find_n_match_cpu_physical_id(struct device_node *cpun, int cpu, unsigned int *thread); extern int cpu_add_dev_attr(struct device_attribute *attr); extern void cpu_remove_dev_attr(struct device_attribute *attr); extern int cpu_add_dev_attr_group(struct attribute_group *attrs); extern void cpu_remove_dev_attr_group(struct attribute_group *attrs); extern struct device *cpu_device_create(struct device *parent, void *drvdata, const struct attribute_group **groups, const char *fmt, ...); #ifdef CONFIG_HOTPLUG_CPU extern void unregister_cpu(struct cpu *cpu); extern ssize_t arch_cpu_probe(const char *, size_t); extern ssize_t arch_cpu_release(const char *, size_t); #endif struct notifier_block; /* * CPU notifier priorities. */ enum { /* * SCHED_ACTIVE marks a cpu which is coming up active during * CPU_ONLINE and CPU_DOWN_FAILED and must be the first * notifier. CPUSET_ACTIVE adjusts cpuset according to * cpu_active mask right after SCHED_ACTIVE. During * CPU_DOWN_PREPARE, SCHED_INACTIVE and CPUSET_INACTIVE are * ordered in the similar way. * * This ordering guarantees consistent cpu_active mask and * migration behavior to all cpu notifiers. */ CPU_PRI_SCHED_ACTIVE = INT_MAX, CPU_PRI_CPUSET_ACTIVE = INT_MAX - 1, CPU_PRI_SCHED_INACTIVE = INT_MIN + 1, CPU_PRI_CPUSET_INACTIVE = INT_MIN, /* migration should happen before other stuff but after perf */ CPU_PRI_PERF = 20, CPU_PRI_MIGRATION = 10, CPU_PRI_SMPBOOT = 9, /* bring up workqueues before normal notifiers and down after */ CPU_PRI_WORKQUEUE_UP = 5, CPU_PRI_WORKQUEUE_DOWN = -5, }; #define CPU_ONLINE 0x0002 /* CPU (unsigned)v is up */ #define CPU_UP_PREPARE 0x0003 /* CPU (unsigned)v coming up */ #define CPU_UP_CANCELED 0x0004 /* CPU (unsigned)v NOT coming up */ #define CPU_DOWN_PREPARE 0x0005 /* CPU (unsigned)v going down */ #define CPU_DOWN_FAILED 0x0006 /* CPU (unsigned)v NOT going down */ #define CPU_DEAD 0x0007 /* CPU (unsigned)v dead */ #define CPU_DYING 0x0008 /* CPU (unsigned)v not running any task, * not handling interrupts, soon dead. * Called on the dying cpu, interrupts * are already disabled. Must not * sleep, must not fail */ #define CPU_POST_DEAD 0x0009 /* CPU (unsigned)v dead, cpu_hotplug * lock is dropped */ #define CPU_STARTING 0x000A /* CPU (unsigned)v soon running. * Called on the new cpu, just before * enabling interrupts. Must not sleep, * must not fail */ #define CPU_DYING_IDLE 0x000B /* CPU (unsigned)v dying, reached * idle loop. */ #define CPU_BROKEN 0x000C /* CPU (unsigned)v did not die properly, * perhaps due to preemption. */ /* Used for CPU hotplug events occurring while tasks are frozen due to a suspend * operation in progress */ #define CPU_TASKS_FROZEN 0x0010 #define CPU_ONLINE_FROZEN (CPU_ONLINE | CPU_TASKS_FROZEN) #define CPU_UP_PREPARE_FROZEN (CPU_UP_PREPARE | CPU_TASKS_FROZEN) #define CPU_UP_CANCELED_FROZEN (CPU_UP_CANCELED | CPU_TASKS_FROZEN) #define CPU_DOWN_PREPARE_FROZEN (CPU_DOWN_PREPARE | CPU_TASKS_FROZEN) #define CPU_DOWN_FAILED_FROZEN (CPU_DOWN_FAILED | CPU_TASKS_FROZEN) #define CPU_DEAD_FROZEN (CPU_DEAD | CPU_TASKS_FROZEN) #define CPU_DYING_FROZEN (CPU_DYING | CPU_TASKS_FROZEN) #define CPU_STARTING_FROZEN (CPU_STARTING | CPU_TASKS_FROZEN) #ifdef CONFIG_SMP /* Need to know about CPUs going up/down? */ #if defined(CONFIG_HOTPLUG_CPU) || !defined(MODULE) #define cpu_notifier(fn, pri) { \ static struct notifier_block fn##_nb = \ { .notifier_call = fn, .priority = pri }; \ register_cpu_notifier(&fn##_nb); \ } #define __cpu_notifier(fn, pri) { \ static struct notifier_block fn##_nb = \ { .notifier_call = fn, .priority = pri }; \ __register_cpu_notifier(&fn##_nb); \ } #else /* #if defined(CONFIG_HOTPLUG_CPU) || !defined(MODULE) */ #define cpu_notifier(fn, pri) do { (void)(fn); } while (0) #define __cpu_notifier(fn, pri) do { (void)(fn); } while (0) #endif /* #else #if defined(CONFIG_HOTPLUG_CPU) || !defined(MODULE) */ #ifdef CONFIG_HOTPLUG_CPU extern int register_cpu_notifier(struct notifier_block *nb); extern int __register_cpu_notifier(struct notifier_block *nb); extern void unregister_cpu_notifier(struct notifier_block *nb); extern void __unregister_cpu_notifier(struct notifier_block *nb); #else #ifndef MODULE extern int register_cpu_notifier(struct notifier_block *nb); extern int __register_cpu_notifier(struct notifier_block *nb); #else static inline int register_cpu_notifier(struct notifier_block *nb) { return 0; } static inline int __register_cpu_notifier(struct notifier_block *nb) { return 0; } #endif static inline void unregister_cpu_notifier(struct notifier_block *nb) { } static inline void __unregister_cpu_notifier(struct notifier_block *nb) { } #endif void smpboot_thread_init(void); int cpu_up(unsigned int cpu); void notify_cpu_starting(unsigned int cpu); extern void cpu_maps_update_begin(void); extern void cpu_maps_update_done(void); #define cpu_notifier_register_begin cpu_maps_update_begin #define cpu_notifier_register_done cpu_maps_update_done #else /* CONFIG_SMP */ #define cpu_notifier(fn, pri) do { (void)(fn); } while (0) #define __cpu_notifier(fn, pri) do { (void)(fn); } while (0) static inline int register_cpu_notifier(struct notifier_block *nb) { return 0; } static inline int __register_cpu_notifier(struct notifier_block *nb) { return 0; } static inline void unregister_cpu_notifier(struct notifier_block *nb) { } static inline void __unregister_cpu_notifier(struct notifier_block *nb) { } static inline void cpu_maps_update_begin(void) { } static inline void cpu_maps_update_done(void) { } static inline void cpu_notifier_register_begin(void) { } static inline void cpu_notifier_register_done(void) { } static inline void smpboot_thread_init(void) { } #endif /* CONFIG_SMP */ extern struct bus_type cpu_subsys; #ifdef CONFIG_HOTPLUG_CPU /* Stop CPUs going up and down. */ extern void cpu_hotplug_begin(void); extern void cpu_hotplug_done(void); extern void get_online_cpus(void); extern bool try_get_online_cpus(void); extern void put_online_cpus(void); extern void cpu_hotplug_disable(void); extern void cpu_hotplug_enable(void); #define hotcpu_notifier(fn, pri) cpu_notifier(fn, pri) #define __hotcpu_notifier(fn, pri) __cpu_notifier(fn, pri) #define register_hotcpu_notifier(nb) register_cpu_notifier(nb) #define __register_hotcpu_notifier(nb) __register_cpu_notifier(nb) #define unregister_hotcpu_notifier(nb) unregister_cpu_notifier(nb) #define __unregister_hotcpu_notifier(nb) __unregister_cpu_notifier(nb) void clear_tasks_mm_cpumask(int cpu); int cpu_down(unsigned int cpu); #else /* CONFIG_HOTPLUG_CPU */ static inline void cpu_hotplug_begin(void) {} static inline void cpu_hotplug_done(void) {} #define get_online_cpus() do { } while (0) #define try_get_online_cpus() true #define put_online_cpus() do { } while (0) #define cpu_hotplug_disable() do { } while (0) #define cpu_hotplug_enable() do { } while (0) #define hotcpu_notifier(fn, pri) do { (void)(fn); } while (0) #define __hotcpu_notifier(fn, pri) do { (void)(fn); } while (0) /* These aren't inline functions due to a GCC bug. */ #define register_hotcpu_notifier(nb) ({ (void)(nb); 0; }) #define __register_hotcpu_notifier(nb) ({ (void)(nb); 0; }) #define unregister_hotcpu_notifier(nb) ({ (void)(nb); }) #define __unregister_hotcpu_notifier(nb) ({ (void)(nb); }) #endif /* CONFIG_HOTPLUG_CPU */ #ifdef CONFIG_PM_SLEEP_SMP extern int disable_nonboot_cpus(void); extern void enable_nonboot_cpus(void); #else /* !CONFIG_PM_SLEEP_SMP */ static inline int disable_nonboot_cpus(void) { return 0; } static inline void enable_nonboot_cpus(void) {} #endif /* !CONFIG_PM_SLEEP_SMP */ enum cpuhp_state { CPUHP_OFFLINE, CPUHP_ONLINE, }; void cpu_startup_entry(enum cpuhp_state state); void cpu_idle_poll_ctrl(bool enable); void arch_cpu_idle(void); void arch_cpu_idle_prepare(void); void arch_cpu_idle_enter(void); void arch_cpu_idle_exit(void); void arch_cpu_idle_dead(void); DECLARE_PER_CPU(bool, cpu_dead_idle); int cpu_report_state(int cpu); int cpu_check_up_prepare(int cpu); void cpu_set_state_online(int cpu); #ifdef CONFIG_HOTPLUG_CPU bool cpu_wait_death(unsigned int cpu, int seconds); bool cpu_report_death(void); #endif /* #ifdef CONFIG_HOTPLUG_CPU */ #endif /* _LINUX_CPU_H_ */