/* * kref.h - library routines for handling generic reference counted objects * * Copyright (C) 2004 Greg Kroah-Hartman * Copyright (C) 2004 IBM Corp. * * based on kobject.h which was: * Copyright (C) 2002-2003 Patrick Mochel * Copyright (C) 2002-2003 Open Source Development Labs * * This file is released under the GPLv2. * */ #ifndef _KREF_H_ #define _KREF_H_ #include #include #include #include #include struct kref { atomic_t refcount; }; /** * kref_init - initialize object. * @kref: object in question. */ static inline void kref_init(struct kref *kref) { atomic_set(&kref->refcount, 1); } /** * kref_get - increment refcount for object. * @kref: object. */ static inline void kref_get(struct kref *kref) { /* If refcount was 0 before incrementing then we have a race * condition when this kref is freeing by some other thread right now. * In this case one should use kref_get_unless_zero() */ WARN_ON_ONCE(atomic_inc_return(&kref->refcount) < 2); } /** * kref_sub - subtract a number of refcounts for object. * @kref: object. * @count: Number of recounts to subtract. * @release: pointer to the function that will clean up the object when the * last reference to the object is released. * This pointer is required, and it is not acceptable to pass kfree * in as this function. If the caller does pass kfree to this * function, you will be publicly mocked mercilessly by the kref * maintainer, and anyone else who happens to notice it. You have * been warned. * * Subtract @count from the refcount, and if 0, call release(). * Return 1 if the object was removed, otherwise return 0. Beware, if this * function returns 0, you still can not count on the kref from remaining in * memory. Only use the return value if you want to see if the kref is now * gone, not present. */ static inline int kref_sub(struct kref *kref, unsigned int count, void (*release)(struct kref *kref)) { WARN_ON(release == NULL); if (atomic_sub_and_test((int) count, &kref->refcount)) { release(kref); return 1; } return 0; } /** * kref_put - decrement refcount for object. * @kref: object. * @release: pointer to the function that will clean up the object when the * last reference to the object is released. * This pointer is required, and it is not acceptable to pass kfree * in as this function. If the caller does pass kfree to this * function, you will be publicly mocked mercilessly by the kref * maintainer, and anyone else who happens to notice it. You have * been warned. * * Decrement the refcount, and if 0, call release(). * Return 1 if the object was removed, otherwise return 0. Beware, if this * function returns 0, you still can not count on the kref from remaining in * memory. Only use the return value if you want to see if the kref is now * gone, not present. */ static inline int kref_put(struct kref *kref, void (*release)(struct kref *kref)) { return kref_sub(kref, 1, release); } /** * kref_put_spinlock_irqsave - decrement refcount for object. * @kref: object. * @release: pointer to the function that will clean up the object when the * last reference to the object is released. * This pointer is required, and it is not acceptable to pass kfree * in as this function. * @lock: lock to take in release case * * Behaves identical to kref_put with one exception. If the reference count * drops to zero, the lock will be taken atomically wrt dropping the reference * count. The release function has to call spin_unlock() without _irqrestore. */ static inline int kref_put_spinlock_irqsave(struct kref *kref, void (*release)(struct kref *kref), spinlock_t *lock) { unsigned long flags; WARN_ON(release == NULL); if (atomic_add_unless(&kref->refcount, -1, 1)) return 0; spin_lock_irqsave(lock, flags); if (atomic_dec_and_test(&kref->refcount)) { release(kref); local_irq_restore(flags); return 1; } spin_unlock_irqrestore(lock, flags); return 0; } static inline int kref_put_mutex(struct kref *kref, void (*release)(struct kref *kref), struct mutex *lock) { WARN_ON(release == NULL); if (unlikely(!atomic_add_unless(&kref->refcount, -1, 1))) { mutex_lock(lock); if (unlikely(!atomic_dec_and_test(&kref->refcount))) { mutex_unlock(lock); return 0; } release(kref); return 1; } return 0; } /** * kref_get_unless_zero - Increment refcount for object unless it is zero. * @kref: object. * * Return non-zero if the increment succeeded. Otherwise return 0. * * This function is intended to simplify locking around refcounting for * objects that can be looked up from a lookup structure, and which are * removed from that lookup structure in the object destructor. * Operations on such objects require at least a read lock around * lookup + kref_get, and a write lock around kref_put + remove from lookup * structure. Furthermore, RCU implementations become extremely tricky. * With a lookup followed by a kref_get_unless_zero *with return value check* * locking in the kref_put path can be deferred to the actual removal from * the lookup structure and RCU lookups become trivial. */ static inline int __must_check kref_get_unless_zero(struct kref *kref) { return atomic_add_unless(&kref->refcount, 1, 0); } #endif /* _KREF_H_ */