/* nubus.h: various definitions and prototypes for NuBus drivers to use. Originally written by Alan Cox. Hacked to death by C. Scott Ananian and David Huggins-Daines. Some of the constants in here are from the corresponding NetBSD/OpenBSD header file, by Allen Briggs. We figured out the rest of them on our own. */ #ifndef LINUX_NUBUS_H #define LINUX_NUBUS_H #include #include struct nubus_board { struct nubus_board* next; struct nubus_dev* first_dev; /* Only 9-E actually exist, though 0-8 are also theoretically possible, and 0 is a special case which represents the motherboard and onboard peripherals (Ethernet, video) */ int slot; /* For slot 0, this is bogus. */ char name[64]; /* Format block */ unsigned char* fblock; /* Root directory (does *not* always equal fblock + doffset!) */ unsigned char* directory; unsigned long slot_addr; /* Offset to root directory (sometimes) */ unsigned long doffset; /* Length over which to compute the crc */ unsigned long rom_length; /* Completely useless most of the time */ unsigned long crc; unsigned char rev; unsigned char format; unsigned char lanes; }; struct nubus_dev { /* Next link in device list */ struct nubus_dev* next; /* Directory entry in /proc/bus/nubus */ struct proc_dir_entry* procdir; /* The functional resource ID of this device */ unsigned char resid; /* These are mostly here for convenience; we could always read them from the ROMs if we wanted to */ unsigned short category; unsigned short type; unsigned short dr_sw; unsigned short dr_hw; /* This is the device's name rather than the board's. Sometimes they are different. Usually the board name is more correct. */ char name[64]; /* MacOS driver (I kid you not) */ unsigned char* driver; /* Actually this is an offset */ unsigned long iobase; unsigned long iosize; unsigned char flags, hwdevid; /* Functional directory */ unsigned char* directory; /* Much of our info comes from here */ struct nubus_board* board; }; /* This is all NuBus devices (used to find devices later on) */ extern struct nubus_dev* nubus_devices; /* This is all NuBus cards */ extern struct nubus_board* nubus_boards; /* Generic NuBus interface functions, modelled after the PCI interface */ void nubus_scan_bus(void); #ifdef CONFIG_PROC_FS extern void nubus_proc_init(void); #else static inline void nubus_proc_init(void) {} #endif int get_nubus_list(char *buf); int nubus_proc_attach_device(struct nubus_dev *dev); /* If we need more precision we can add some more of these */ struct nubus_dev* nubus_find_device(unsigned short category, unsigned short type, unsigned short dr_hw, unsigned short dr_sw, const struct nubus_dev* from); struct nubus_dev* nubus_find_type(unsigned short category, unsigned short type, const struct nubus_dev* from); /* Might have more than one device in a slot, you know... */ struct nubus_dev* nubus_find_slot(unsigned int slot, const struct nubus_dev* from); /* These are somewhat more NuBus-specific. They all return 0 for success and -1 for failure, as you'd expect. */ /* The root directory which contains the board and functional directories */ int nubus_get_root_dir(const struct nubus_board* board, struct nubus_dir* dir); /* The board directory */ int nubus_get_board_dir(const struct nubus_board* board, struct nubus_dir* dir); /* The functional directory */ int nubus_get_func_dir(const struct nubus_dev* dev, struct nubus_dir* dir); /* These work on any directory gotten via the above */ int nubus_readdir(struct nubus_dir* dir, struct nubus_dirent* ent); int nubus_find_rsrc(struct nubus_dir* dir, unsigned char rsrc_type, struct nubus_dirent* ent); int nubus_rewinddir(struct nubus_dir* dir); /* Things to do with directory entries */ int nubus_get_subdir(const struct nubus_dirent* ent, struct nubus_dir* dir); void nubus_get_rsrc_mem(void* dest, const struct nubus_dirent *dirent, int len); void nubus_get_rsrc_str(void* dest, const struct nubus_dirent *dirent, int maxlen); #endif /* LINUX_NUBUS_H */