/* * pm_domain.h - Definitions and headers related to device power domains. * * Copyright (C) 2011 Rafael J. Wysocki , Renesas Electronics Corp. * * This file is released under the GPLv2. */ #ifndef _LINUX_PM_DOMAIN_H #define _LINUX_PM_DOMAIN_H #include #include #include #include #include #include #include /* Defines used for the flags field in the struct generic_pm_domain */ #define GENPD_FLAG_PM_CLK (1U << 0) /* PM domain uses PM clk */ enum gpd_status { GPD_STATE_ACTIVE = 0, /* PM domain is active */ GPD_STATE_WAIT_MASTER, /* PM domain's master is being waited for */ GPD_STATE_BUSY, /* Something is happening to the PM domain */ GPD_STATE_REPEAT, /* Power off in progress, to be repeated */ GPD_STATE_POWER_OFF, /* PM domain is off */ }; struct dev_power_governor { bool (*power_down_ok)(struct dev_pm_domain *domain); bool (*stop_ok)(struct device *dev); }; struct gpd_dev_ops { int (*start)(struct device *dev); int (*stop)(struct device *dev); int (*save_state)(struct device *dev); int (*restore_state)(struct device *dev); bool (*active_wakeup)(struct device *dev); }; struct gpd_cpuidle_data { unsigned int saved_exit_latency; struct cpuidle_state *idle_state; }; struct generic_pm_domain { struct dev_pm_domain domain; /* PM domain operations */ struct list_head gpd_list_node; /* Node in the global PM domains list */ struct list_head master_links; /* Links with PM domain as a master */ struct list_head slave_links; /* Links with PM domain as a slave */ struct list_head dev_list; /* List of devices */ struct mutex lock; struct dev_power_governor *gov; struct work_struct power_off_work; const char *name; unsigned int in_progress; /* Number of devices being suspended now */ atomic_t sd_count; /* Number of subdomains with power "on" */ enum gpd_status status; /* Current state of the domain */ wait_queue_head_t status_wait_queue; struct task_struct *poweroff_task; /* Powering off task */ unsigned int resume_count; /* Number of devices being resumed */ unsigned int device_count; /* Number of devices */ unsigned int suspended_count; /* System suspend device counter */ unsigned int prepared_count; /* Suspend counter of prepared devices */ bool suspend_power_off; /* Power status before system suspend */ int (*power_off)(struct generic_pm_domain *domain); s64 power_off_latency_ns; int (*power_on)(struct generic_pm_domain *domain); s64 power_on_latency_ns; struct gpd_dev_ops dev_ops; s64 max_off_time_ns; /* Maximum allowed "suspended" time. */ bool max_off_time_changed; bool cached_power_down_ok; struct gpd_cpuidle_data *cpuidle_data; int (*attach_dev)(struct generic_pm_domain *domain, struct device *dev); void (*detach_dev)(struct generic_pm_domain *domain, struct device *dev); unsigned int flags; /* Bit field of configs for genpd */ }; static inline struct generic_pm_domain *pd_to_genpd(struct dev_pm_domain *pd) { return container_of(pd, struct generic_pm_domain, domain); } struct gpd_link { struct generic_pm_domain *master; struct list_head master_node; struct generic_pm_domain *slave; struct list_head slave_node; }; struct gpd_timing_data { s64 stop_latency_ns; s64 start_latency_ns; s64 save_state_latency_ns; s64 restore_state_latency_ns; s64 effective_constraint_ns; bool constraint_changed; bool cached_stop_ok; }; struct pm_domain_data { struct list_head list_node; struct device *dev; }; struct generic_pm_domain_data { struct pm_domain_data base; struct gpd_timing_data td; struct notifier_block nb; int need_restore; }; #ifdef CONFIG_PM_GENERIC_DOMAINS static inline struct generic_pm_domain_data *to_gpd_data(struct pm_domain_data *pdd) { return container_of(pdd, struct generic_pm_domain_data, base); } static inline struct generic_pm_domain_data *dev_gpd_data(struct device *dev) { return to_gpd_data(dev->power.subsys_data->domain_data); } extern struct generic_pm_domain *pm_genpd_lookup_dev(struct device *dev); extern int __pm_genpd_add_device(struct generic_pm_domain *genpd, struct device *dev, struct gpd_timing_data *td); extern int __pm_genpd_name_add_device(const char *domain_name, struct device *dev, struct gpd_timing_data *td); extern int pm_genpd_remove_device(struct generic_pm_domain *genpd, struct device *dev); extern int pm_genpd_add_subdomain(struct generic_pm_domain *genpd, struct generic_pm_domain *new_subdomain); extern int pm_genpd_add_subdomain_names(const char *master_name, const char *subdomain_name); extern int pm_genpd_remove_subdomain(struct generic_pm_domain *genpd, struct generic_pm_domain *target); extern int pm_genpd_attach_cpuidle(struct generic_pm_domain *genpd, int state); extern int pm_genpd_name_attach_cpuidle(const char *name, int state); extern int pm_genpd_detach_cpuidle(struct generic_pm_domain *genpd); extern int pm_genpd_name_detach_cpuidle(const char *name); extern void pm_genpd_init(struct generic_pm_domain *genpd, struct dev_power_governor *gov, bool is_off); extern int pm_genpd_poweron(struct generic_pm_domain *genpd); extern int pm_genpd_name_poweron(const char *domain_name); extern void pm_genpd_poweroff_unused(void); extern struct dev_power_governor simple_qos_governor; extern struct dev_power_governor pm_domain_always_on_gov; #else static inline struct generic_pm_domain_data *dev_gpd_data(struct device *dev) { return ERR_PTR(-ENOSYS); } static inline struct generic_pm_domain *pm_genpd_lookup_dev(struct device *dev) { return NULL; } static inline int __pm_genpd_add_device(struct generic_pm_domain *genpd, struct device *dev, struct gpd_timing_data *td) { return -ENOSYS; } static inline int __pm_genpd_name_add_device(const char *domain_name, struct device *dev, struct gpd_timing_data *td) { return -ENOSYS; } static inline int pm_genpd_remove_device(struct generic_pm_domain *genpd, struct device *dev) { return -ENOSYS; } static inline int pm_genpd_add_subdomain(struct generic_pm_domain *genpd, struct generic_pm_domain *new_sd) { return -ENOSYS; } static inline int pm_genpd_add_subdomain_names(const char *master_name, const char *subdomain_name) { return -ENOSYS; } static inline int pm_genpd_remove_subdomain(struct generic_pm_domain *genpd, struct generic_pm_domain *target) { return -ENOSYS; } static inline int pm_genpd_attach_cpuidle(struct generic_pm_domain *genpd, int st) { return -ENOSYS; } static inline int pm_genpd_name_attach_cpuidle(const char *name, int state) { return -ENOSYS; } static inline int pm_genpd_detach_cpuidle(struct generic_pm_domain *genpd) { return -ENOSYS; } static inline int pm_genpd_name_detach_cpuidle(const char *name) { return -ENOSYS; } static inline void pm_genpd_init(struct generic_pm_domain *genpd, struct dev_power_governor *gov, bool is_off) { } static inline int pm_genpd_poweron(struct generic_pm_domain *genpd) { return -ENOSYS; } static inline int pm_genpd_name_poweron(const char *domain_name) { return -ENOSYS; } static inline void pm_genpd_poweroff_unused(void) {} #define simple_qos_governor NULL #define pm_domain_always_on_gov NULL #endif static inline int pm_genpd_add_device(struct generic_pm_domain *genpd, struct device *dev) { return __pm_genpd_add_device(genpd, dev, NULL); } static inline int pm_genpd_name_add_device(const char *domain_name, struct device *dev) { return __pm_genpd_name_add_device(domain_name, dev, NULL); } #ifdef CONFIG_PM_GENERIC_DOMAINS_SLEEP extern void pm_genpd_syscore_poweroff(struct device *dev); extern void pm_genpd_syscore_poweron(struct device *dev); #else static inline void pm_genpd_syscore_poweroff(struct device *dev) {} static inline void pm_genpd_syscore_poweron(struct device *dev) {} #endif /* OF PM domain providers */ struct of_device_id; struct genpd_onecell_data { struct generic_pm_domain **domains; unsigned int num_domains; }; typedef struct generic_pm_domain *(*genpd_xlate_t)(struct of_phandle_args *args, void *data); #ifdef CONFIG_PM_GENERIC_DOMAINS_OF int __of_genpd_add_provider(struct device_node *np, genpd_xlate_t xlate, void *data); void of_genpd_del_provider(struct device_node *np); struct generic_pm_domain *of_genpd_get_from_provider( struct of_phandle_args *genpdspec); struct generic_pm_domain *__of_genpd_xlate_simple( struct of_phandle_args *genpdspec, void *data); struct generic_pm_domain *__of_genpd_xlate_onecell( struct of_phandle_args *genpdspec, void *data); int genpd_dev_pm_attach(struct device *dev); #else /* !CONFIG_PM_GENERIC_DOMAINS_OF */ static inline int __of_genpd_add_provider(struct device_node *np, genpd_xlate_t xlate, void *data) { return 0; } static inline void of_genpd_del_provider(struct device_node *np) {} static inline struct generic_pm_domain *of_genpd_get_from_provider( struct of_phandle_args *genpdspec) { return NULL; } #define __of_genpd_xlate_simple NULL #define __of_genpd_xlate_onecell NULL static inline int genpd_dev_pm_attach(struct device *dev) { return -ENODEV; } #endif /* CONFIG_PM_GENERIC_DOMAINS_OF */ static inline int of_genpd_add_provider_simple(struct device_node *np, struct generic_pm_domain *genpd) { return __of_genpd_add_provider(np, __of_genpd_xlate_simple, genpd); } static inline int of_genpd_add_provider_onecell(struct device_node *np, struct genpd_onecell_data *data) { return __of_genpd_add_provider(np, __of_genpd_xlate_onecell, data); } #ifdef CONFIG_PM extern int dev_pm_domain_attach(struct device *dev, bool power_on); extern void dev_pm_domain_detach(struct device *dev, bool power_off); #else static inline int dev_pm_domain_attach(struct device *dev, bool power_on) { return -ENODEV; } static inline void dev_pm_domain_detach(struct device *dev, bool power_off) {} #endif #endif /* _LINUX_PM_DOMAIN_H */