#ifndef __LINUX_RTNETLINK_H #define __LINUX_RTNETLINK_H #include #include #include #include extern int rtnetlink_send(struct sk_buff *skb, struct net *net, u32 pid, u32 group, int echo); extern int rtnl_unicast(struct sk_buff *skb, struct net *net, u32 pid); extern void rtnl_notify(struct sk_buff *skb, struct net *net, u32 pid, u32 group, struct nlmsghdr *nlh, gfp_t flags); extern void rtnl_set_sk_err(struct net *net, u32 group, int error); extern int rtnetlink_put_metrics(struct sk_buff *skb, u32 *metrics); extern int rtnl_put_cacheinfo(struct sk_buff *skb, struct dst_entry *dst, u32 id, long expires, u32 error); void rtmsg_ifinfo(int type, struct net_device *dev, unsigned change, gfp_t flags); struct sk_buff *rtmsg_ifinfo_build_skb(int type, struct net_device *dev, unsigned change, gfp_t flags); void rtmsg_ifinfo_send(struct sk_buff *skb, struct net_device *dev, gfp_t flags); /* RTNL is used as a global lock for all changes to network configuration */ extern void rtnl_lock(void); extern void rtnl_unlock(void); extern int rtnl_trylock(void); extern int rtnl_is_locked(void); extern wait_queue_head_t netdev_unregistering_wq; extern struct mutex net_mutex; #ifdef CONFIG_PROVE_LOCKING extern int lockdep_rtnl_is_held(void); #else static inline int lockdep_rtnl_is_held(void) { return 1; } #endif /* #ifdef CONFIG_PROVE_LOCKING */ /** * rcu_dereference_rtnl - rcu_dereference with debug checking * @p: The pointer to read, prior to dereferencing * * Do an rcu_dereference(p), but check caller either holds rcu_read_lock() * or RTNL. Note : Please prefer rtnl_dereference() or rcu_dereference() */ #define rcu_dereference_rtnl(p) \ rcu_dereference_check(p, lockdep_rtnl_is_held()) /** * rcu_dereference_bh_rtnl - rcu_dereference_bh with debug checking * @p: The pointer to read, prior to dereference * * Do an rcu_dereference_bh(p), but check caller either holds rcu_read_lock_bh() * or RTNL. Note : Please prefer rtnl_dereference() or rcu_dereference_bh() */ #define rcu_dereference_bh_rtnl(p) \ rcu_dereference_bh_check(p, lockdep_rtnl_is_held()) /** * rtnl_dereference - fetch RCU pointer when updates are prevented by RTNL * @p: The pointer to read, prior to dereferencing * * Return the value of the specified RCU-protected pointer, but omit * both the smp_read_barrier_depends() and the ACCESS_ONCE(), because * caller holds RTNL. */ #define rtnl_dereference(p) \ rcu_dereference_protected(p, lockdep_rtnl_is_held()) static inline struct netdev_queue *dev_ingress_queue(struct net_device *dev) { return rtnl_dereference(dev->ingress_queue); } struct netdev_queue *dev_ingress_queue_create(struct net_device *dev); #ifdef CONFIG_NET_CLS_ACT void net_inc_ingress_queue(void); void net_dec_ingress_queue(void); #else static inline void net_inc_ingress_queue(void) { } static inline void net_dec_ingress_queue(void) { } #endif extern void rtnetlink_init(void); extern void __rtnl_unlock(void); #define ASSERT_RTNL() do { \ if (unlikely(!rtnl_is_locked())) { \ printk(KERN_ERR "RTNL: assertion failed at %s (%d)\n", \ __FILE__, __LINE__); \ dump_stack(); \ } \ } while(0) extern int ndo_dflt_fdb_dump(struct sk_buff *skb, struct netlink_callback *cb, struct net_device *dev, struct net_device *filter_dev, int idx); extern int ndo_dflt_fdb_add(struct ndmsg *ndm, struct nlattr *tb[], struct net_device *dev, const unsigned char *addr, u16 vid, u16 flags); extern int ndo_dflt_fdb_del(struct ndmsg *ndm, struct nlattr *tb[], struct net_device *dev, const unsigned char *addr, u16 vid); extern int ndo_dflt_bridge_getlink(struct sk_buff *skb, u32 pid, u32 seq, struct net_device *dev, u16 mode, u32 flags, u32 mask, int nlflags); #endif /* __LINUX_RTNETLINK_H */