/* * User level driver support for input subsystem * * Heavily based on evdev.c by Vojtech Pavlik * * This program is free software; you can redistribute it and/or modify * it under the terms of the GNU General Public License as published by * the Free Software Foundation; either version 2 of the License, or * (at your option) any later version. * * This program is distributed in the hope that it will be useful, * but WITHOUT ANY WARRANTY; without even the implied warranty of * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the * GNU General Public License for more details. * * You should have received a copy of the GNU General Public License * along with this program; if not, write to the Free Software * Foundation, Inc., 59 Temple Place, Suite 330, Boston, MA 02111-1307 USA * * Author: Aristeu Sergio Rozanski Filho * * Changes/Revisions: * 0.4 01/09/2014 (Benjamin Tissoires ) * - add UI_GET_SYSNAME ioctl * 0.3 24/05/2006 (Anssi Hannula ) * - update ff support for the changes in kernel interface * - add UINPUT_VERSION * 0.2 16/10/2004 (Micah Dowty ) * - added force feedback support * - added UI_SET_PHYS * 0.1 20/06/2002 * - first public version */ #ifndef __UINPUT_H_ #define __UINPUT_H_ #include #define UINPUT_NAME "uinput" #define UINPUT_BUFFER_SIZE 16 #define UINPUT_NUM_REQUESTS 16 enum uinput_state { UIST_NEW_DEVICE, UIST_SETUP_COMPLETE, UIST_CREATED }; struct uinput_request { unsigned int id; unsigned int code; /* UI_FF_UPLOAD, UI_FF_ERASE */ int retval; struct completion done; union { unsigned int effect_id; struct { struct ff_effect *effect; struct ff_effect *old; } upload; } u; }; struct uinput_device { struct input_dev *dev; struct mutex mutex; enum uinput_state state; wait_queue_head_t waitq; unsigned char ready; unsigned char head; unsigned char tail; struct input_event buff[UINPUT_BUFFER_SIZE]; unsigned int ff_effects_max; struct uinput_request *requests[UINPUT_NUM_REQUESTS]; wait_queue_head_t requests_waitq; spinlock_t requests_lock; }; #endif /* __UINPUT_H_ */