/* * include/linux/writeback.h */ #ifndef WRITEBACK_H #define WRITEBACK_H #include #include #include #include #include DECLARE_PER_CPU(int, dirty_throttle_leaks); /* * The 1/4 region under the global dirty thresh is for smooth dirty throttling: * * (thresh - thresh/DIRTY_FULL_SCOPE, thresh) * * Further beyond, all dirtier tasks will enter a loop waiting (possibly long * time) for the dirty pages to drop, unless written enough pages. * * The global dirty threshold is normally equal to the global dirty limit, * except when the system suddenly allocates a lot of anonymous memory and * knocks down the global dirty threshold quickly, in which case the global * dirty limit will follow down slowly to prevent livelocking all dirtier tasks. */ #define DIRTY_SCOPE 8 #define DIRTY_FULL_SCOPE (DIRTY_SCOPE / 2) struct backing_dev_info; /* * fs/fs-writeback.c */ enum writeback_sync_modes { WB_SYNC_NONE, /* Don't wait on anything */ WB_SYNC_ALL, /* Wait on every mapping */ }; /* * why some writeback work was initiated */ enum wb_reason { WB_REASON_BACKGROUND, WB_REASON_TRY_TO_FREE_PAGES, WB_REASON_SYNC, WB_REASON_PERIODIC, WB_REASON_LAPTOP_TIMER, WB_REASON_FREE_MORE_MEM, WB_REASON_FS_FREE_SPACE, /* * There is no bdi forker thread any more and works are done * by emergency worker, however, this is TPs userland visible * and we'll be exposing exactly the same information, * so it has a mismatch name. */ WB_REASON_FORKER_THREAD, WB_REASON_MAX, }; /* * A control structure which tells the writeback code what to do. These are * always on the stack, and hence need no locking. They are always initialised * in a manner such that unspecified fields are set to zero. */ struct writeback_control { long nr_to_write; /* Write this many pages, and decrement this for each page written */ long pages_skipped; /* Pages which were not written */ /* * For a_ops->writepages(): if start or end are non-zero then this is * a hint that the filesystem need only write out the pages inside that * byterange. The byte at `end' is included in the writeout request. */ loff_t range_start; loff_t range_end; enum writeback_sync_modes sync_mode; unsigned for_kupdate:1; /* A kupdate writeback */ unsigned for_background:1; /* A background writeback */ unsigned tagged_writepages:1; /* tag-and-write to avoid livelock */ unsigned for_reclaim:1; /* Invoked from the page allocator */ unsigned range_cyclic:1; /* range_start is cyclic */ unsigned for_sync:1; /* sync(2) WB_SYNC_ALL writeback */ #ifdef CONFIG_CGROUP_WRITEBACK struct bdi_writeback *wb; /* wb this writeback is issued under */ struct inode *inode; /* inode being written out */ /* foreign inode detection, see wbc_detach_inode() */ int wb_id; /* current wb id */ int wb_lcand_id; /* last foreign candidate wb id */ int wb_tcand_id; /* this foreign candidate wb id */ size_t wb_bytes; /* bytes written by current wb */ size_t wb_lcand_bytes; /* bytes written by last candidate */ size_t wb_tcand_bytes; /* bytes written by this candidate */ #endif }; /* * A wb_domain represents a domain that wb's (bdi_writeback's) belong to * and are measured against each other in. There always is one global * domain, global_wb_domain, that every wb in the system is a member of. * This allows measuring the relative bandwidth of each wb to distribute * dirtyable memory accordingly. */ struct wb_domain { spinlock_t lock; /* * Scale the writeback cache size proportional to the relative * writeout speed. * * We do this by keeping a floating proportion between BDIs, based * on page writeback completions [end_page_writeback()]. Those * devices that write out pages fastest will get the larger share, * while the slower will get a smaller share. * * We use page writeout completions because we are interested in * getting rid of dirty pages. Having them written out is the * primary goal. * * We introduce a concept of time, a period over which we measure * these events, because demand can/will vary over time. The length * of this period itself is measured in page writeback completions. */ struct fprop_global completions; struct timer_list period_timer; /* timer for aging of completions */ unsigned long period_time; /* * The dirtyable memory and dirty threshold could be suddenly * knocked down by a large amount (eg. on the startup of KVM in a * swapless system). This may throw the system into deep dirty * exceeded state and throttle heavy/light dirtiers alike. To * retain good responsiveness, maintain global_dirty_limit for * tracking slowly down to the knocked down dirty threshold. * * Both fields are protected by ->lock. */ unsigned long dirty_limit_tstamp; unsigned long dirty_limit; }; /** * wb_domain_size_changed - memory available to a wb_domain has changed * @dom: wb_domain of interest * * This function should be called when the amount of memory available to * @dom has changed. It resets @dom's dirty limit parameters to prevent * the past values which don't match the current configuration from skewing * dirty throttling. Without this, when memory size of a wb_domain is * greatly reduced, the dirty throttling logic may allow too many pages to * be dirtied leading to consecutive unnecessary OOMs and may get stuck in * that situation. */ static inline void wb_domain_size_changed(struct wb_domain *dom) { spin_lock(&dom->lock); dom->dirty_limit_tstamp = jiffies; dom->dirty_limit = 0; spin_unlock(&dom->lock); } /* * fs/fs-writeback.c */ struct bdi_writeback; void writeback_inodes_sb(struct super_block *, enum wb_reason reason); void writeback_inodes_sb_nr(struct super_block *, unsigned long nr, enum wb_reason reason); bool try_to_writeback_inodes_sb(struct super_block *, enum wb_reason reason); bool try_to_writeback_inodes_sb_nr(struct super_block *, unsigned long nr, enum wb_reason reason); void sync_inodes_sb(struct super_block *); void wakeup_flusher_threads(long nr_pages, enum wb_reason reason); void inode_wait_for_writeback(struct inode *inode); /* writeback.h requires fs.h; it, too, is not included from here. */ static inline void wait_on_inode(struct inode *inode) { might_sleep(); wait_on_bit(&inode->i_state, __I_NEW, TASK_UNINTERRUPTIBLE); } #ifdef CONFIG_CGROUP_WRITEBACK #include #include void __inode_attach_wb(struct inode *inode, struct page *page); void wbc_attach_and_unlock_inode(struct writeback_control *wbc, struct inode *inode) __releases(&inode->i_lock); void wbc_detach_inode(struct writeback_control *wbc); void wbc_account_io(struct writeback_control *wbc, struct page *page, size_t bytes); /** * inode_attach_wb - associate an inode with its wb * @inode: inode of interest * @page: page being dirtied (may be NULL) * * If @inode doesn't have its wb, associate it with the wb matching the * memcg of @page or, if @page is NULL, %current. May be called w/ or w/o * @inode->i_lock. */ static inline void inode_attach_wb(struct inode *inode, struct page *page) { if (!inode->i_wb) __inode_attach_wb(inode, page); } /** * inode_detach_wb - disassociate an inode from its wb * @inode: inode of interest * * @inode is being freed. Detach from its wb. */ static inline void inode_detach_wb(struct inode *inode) { if (inode->i_wb) { wb_put(inode->i_wb); inode->i_wb = NULL; } } /** * wbc_attach_fdatawrite_inode - associate wbc and inode for fdatawrite * @wbc: writeback_control of interest * @inode: target inode * * This function is to be used by __filemap_fdatawrite_range(), which is an * alternative entry point into writeback code, and first ensures @inode is * associated with a bdi_writeback and attaches it to @wbc. */ static inline void wbc_attach_fdatawrite_inode(struct writeback_control *wbc, struct inode *inode) { spin_lock(&inode->i_lock); inode_attach_wb(inode, NULL); wbc_attach_and_unlock_inode(wbc, inode); } /** * wbc_init_bio - writeback specific initializtion of bio * @wbc: writeback_control for the writeback in progress * @bio: bio to be initialized * * @bio is a part of the writeback in progress controlled by @wbc. Perform * writeback specific initialization. This is used to apply the cgroup * writeback context. */ static inline void wbc_init_bio(struct writeback_control *wbc, struct bio *bio) { /* * pageout() path doesn't attach @wbc to the inode being written * out. This is intentional as we don't want the function to block * behind a slow cgroup. Ultimately, we want pageout() to kick off * regular writeback instead of writing things out itself. */ if (wbc->wb) bio_associate_blkcg(bio, wbc->wb->blkcg_css); } #else /* CONFIG_CGROUP_WRITEBACK */ static inline void inode_attach_wb(struct inode *inode, struct page *page) { } static inline void inode_detach_wb(struct inode *inode) { } static inline void wbc_attach_and_unlock_inode(struct writeback_control *wbc, struct inode *inode) __releases(&inode->i_lock) { spin_unlock(&inode->i_lock); } static inline void wbc_attach_fdatawrite_inode(struct writeback_control *wbc, struct inode *inode) { } static inline void wbc_detach_inode(struct writeback_control *wbc) { } static inline void wbc_init_bio(struct writeback_control *wbc, struct bio *bio) { } static inline void wbc_account_io(struct writeback_control *wbc, struct page *page, size_t bytes) { } #endif /* CONFIG_CGROUP_WRITEBACK */ /* * mm/page-writeback.c */ #ifdef CONFIG_BLOCK void laptop_io_completion(struct backing_dev_info *info); void laptop_sync_completion(void); void laptop_mode_sync(struct work_struct *work); void laptop_mode_timer_fn(unsigned long data); #else static inline void laptop_sync_completion(void) { } #endif void throttle_vm_writeout(gfp_t gfp_mask); bool zone_dirty_ok(struct zone *zone); int wb_domain_init(struct wb_domain *dom, gfp_t gfp); #ifdef CONFIG_CGROUP_WRITEBACK void wb_domain_exit(struct wb_domain *dom); #endif extern struct wb_domain global_wb_domain; /* These are exported to sysctl. */ extern int dirty_background_ratio; extern unsigned long dirty_background_bytes; extern int vm_dirty_ratio; extern unsigned long vm_dirty_bytes; extern unsigned int dirty_writeback_interval; extern unsigned int dirty_expire_interval; extern unsigned int dirtytime_expire_interval; extern int vm_highmem_is_dirtyable; extern int block_dump; extern int laptop_mode; extern int dirty_background_ratio_handler(struct ctl_table *table, int write, void __user *buffer, size_t *lenp, loff_t *ppos); extern int dirty_background_bytes_handler(struct ctl_table *table, int write, void __user *buffer, size_t *lenp, loff_t *ppos); extern int dirty_ratio_handler(struct ctl_table *table, int write, void __user *buffer, size_t *lenp, loff_t *ppos); extern int dirty_bytes_handler(struct ctl_table *table, int write, void __user *buffer, size_t *lenp, loff_t *ppos); int dirtytime_interval_handler(struct ctl_table *table, int write, void __user *buffer, size_t *lenp, loff_t *ppos); struct ctl_table; int dirty_writeback_centisecs_handler(struct ctl_table *, int, void __user *, size_t *, loff_t *); void global_dirty_limits(unsigned long *pbackground, unsigned long *pdirty); unsigned long wb_calc_thresh(struct bdi_writeback *wb, unsigned long thresh); void wb_update_bandwidth(struct bdi_writeback *wb, unsigned long start_time); void page_writeback_init(void); void balance_dirty_pages_ratelimited(struct address_space *mapping); bool wb_over_bg_thresh(struct bdi_writeback *wb); typedef int (*writepage_t)(struct page *page, struct writeback_control *wbc, void *data); int generic_writepages(struct address_space *mapping, struct writeback_control *wbc); void tag_pages_for_writeback(struct address_space *mapping, pgoff_t start, pgoff_t end); int write_cache_pages(struct address_space *mapping, struct writeback_control *wbc, writepage_t writepage, void *data); int do_writepages(struct address_space *mapping, struct writeback_control *wbc); void writeback_set_ratelimit(void); void tag_pages_for_writeback(struct address_space *mapping, pgoff_t start, pgoff_t end); void account_page_redirty(struct page *page); #endif /* WRITEBACK_H */