aboutsummaryrefslogtreecommitdiffstats
blob: 2f2c6cdd73c0c24ab29dcd3f68034f99f17c3125 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
317
318
319
320
321
322
323
324
325
326
327
328
329
330
331
332
333
334
335
336
337
338
339
340
341
342
343
344
345
346
347
348
349
350
351
352
353
354
355
356
357
358
359
360
361
362
363
364
365
366
367
368
369
370
371
372
373
374
375
376
377
378
379
380
381
382
383
384
385
386
387
388
389
390
391
392
393
394
395
396
397
398
399
400
401
402
403
404
405
406
407
408
409
410
411
412
413
414
415
416
417
418
419
420
421
422
423
424
425
426
427
428
429
430
431
432
433
434
435
436
437
438
439
440
441
442
443
444
445
446
447
448
449
450
451
452
453
454
455
456
457
458
459
460
461
462
463
464
465
466
467
468
469
470
471
472
473
474
475
476
477
478
479
480
481
482
483
484
485
486
487
488
489
490
491
492
493
494
495
496
497
498
499
500
501
502
503
504
505
506
507
508
509
510
511
512
513
514
515
516
517
518
519
520
521
522
523
524
525
526
527
528
529
530
531
532
533
534
535
536
537
538
539
540
541
542
543
544
545
546
547
548
549
550
551
552
553
554
555
556
557
558
559
560
561
562
563
564
565
566
567
568
569
570
571
572
573
574
		   ========================================
		   GENERIC ASSOCIATIVE ARRAY IMPLEMENTATION
		   ========================================

Contents:

 - Overview.

 - The public API.
   - Edit script.
   - Operations table.
   - Manipulation functions.
   - Access functions.
   - Index key form.

 - Internal workings.
   - Basic internal tree layout.
   - Shortcuts.
   - Splitting and collapsing nodes.
   - Non-recursive iteration.
   - Simultaneous alteration and iteration.


========
OVERVIEW
========

This associative array implementation is an object container with the following
properties:

 (1) Objects are opaque pointers.  The implementation does not care where they
     point (if anywhere) or what they point to (if anything).

     [!] NOTE: Pointers to objects _must_ be zero in the least significant bit.

 (2) Objects do not need to contain linkage blocks for use by the array.  This
     permits an object to be located in multiple arrays simultaneously.
     Rather, the array is made up of metadata blocks that point to objects.

 (3) Objects require index keys to locate them within the array.

 (4) Index keys must be unique.  Inserting an object with the same key as one
     already in the array will replace the old object.

 (5) Index keys can be of any length and can be of different lengths.

 (6) Index keys should encode the length early on, before any variation due to
     length is seen.

 (7) Index keys can include a hash to scatter objects throughout the array.

 (8) The array can iterated over.  The objects will not necessarily come out in
     key order.

 (9) The array can be iterated over whilst it is being modified, provided the
     RCU readlock is being held by the iterator.  Note, however, under these
     circumstances, some objects may be seen more than once.  If this is a
     problem, the iterator should lock against modification.  Objects will not
     be missed, however, unless deleted.

(10) Objects in the array can be looked up by means of their index key.

(11) Objects can be looked up whilst the array is being modified, provided the
     RCU readlock is being held by the thread doing the look up.

The implementation uses a tree of 16-pointer nodes internally that are indexed
on each level by nibbles from the index key in the same manner as in a radix
tree.  To improve memory efficiency, shortcuts can be emplaced to skip over
what would otherwise be a series of single-occupancy nodes.  Further, nodes
pack leaf object pointers into spare space in the node rather than making an
extra branch until as such time an object needs to be added to a full node.


==============
THE PUBLIC API
==============

The public API can be found in <linux/assoc_array.h>.  The associative array is
rooted on the following structure:

	struct assoc_array {
		...
	};

The code is selected by enabling CONFIG_ASSOCIATIVE_ARRAY.


EDIT SCRIPT
-----------

The insertion and deletion functions produce an 'edit script' that can later be
applied to effect the changes without risking ENOMEM.  This retains the
preallocated metadata blocks that will be installed in the internal tree and
keeps track of the metadata blocks that will be removed from the tree when the
script is applied.

This is also used to keep track of dead blocks and dead objects after the
script has been applied so that they can be freed later.  The freeing is done
after an RCU grace period has passed - thus allowing access functions to
proceed under the RCU read lock.

The script appears as outside of the API as a pointer of the type:

	struct assoc_array_edit;

There are two functions for dealing with the script:

 (1) Apply an edit script.

	void assoc_array_apply_edit(struct assoc_array_edit *edit);

     This will perform the edit functions, interpolating various write barriers
     to permit accesses under the RCU read lock to continue.  The edit script
     will then be passed to call_rcu() to free it and any dead stuff it points
     to.

 (2) Cancel an edit script.

	void assoc_array_cancel_edit(struct assoc_array_edit *edit);

     This frees the edit script and all preallocated memory immediately.  If
     this was for insertion, the new object is _not_ released by this function,
     but must rather be released by the caller.

These functions are guaranteed not to fail.


OPERATIONS TABLE
----------------

Various functions take a table of operations:

	struct assoc_array_ops {
		...
	};

This points to a number of methods, all of which need to be provided:

 (1) Get a chunk of index key from caller data:

	unsigned long (*get_key_chunk)(const void *index_key, int level);

     This should return a chunk of caller-supplied index key starting at the
     *bit* position given by the level argument.  The level argument will be a
     multiple of ASSOC_ARRAY_KEY_CHUNK_SIZE and the function should return
     ASSOC_ARRAY_KEY_CHUNK_SIZE bits.  No error is possible.


 (2) Get a chunk of an object's index key.

	unsigned long (*get_object_key_chunk)(const void *object, int level);

     As the previous function, but gets its data from an object in the array
     rather than from a caller-supplied index key.


 (3) See if this is the object we're looking for.

	bool (*compare_object)(const void *object, const void *index_key);

     Compare the object against an index key and return true if it matches and
     false if it doesn't.


 (4) Diff the index keys of two objects.

	int (*diff_objects)(const void *object, const void *index_key);

     Return the bit position at which the index key of the specified object
     differs from the given index key or -1 if they are the same.


 (5) Free an object.

	void (*free_object)(void *object);

     Free the specified object.  Note that this may be called an RCU grace
     period after assoc_array_apply_edit() was called, so synchronize_rcu() may
     be necessary on module unloading.


MANIPULATION FUNCTIONS
----------------------

There are a number of functions for manipulating an associative array:

 (1) Initialise an associative array.

	void assoc_array_init(struct assoc_array *array);

     This initialises the base structure for an associative array.  It can't
     fail.


 (2) Insert/replace an object in an associative array.

	struct assoc_array_edit *
	assoc_array_insert(struct assoc_array *array,
			   const struct assoc_array_ops *ops,
			   const void *index_key,
			   void *object);

     This inserts the given object into the array.  Note that the least
     significant bit of the pointer must be zero as it's used to type-mark
     pointers internally.

     If an object already exists for that key then it will be replaced with the
     new object and the old one will be freed automatically.

     The index_key argument should hold index key information and is
     passed to the methods in the ops table when they are called.

     This function makes no alteration to the array itself, but rather returns
     an edit script that must be applied.  -ENOMEM is returned in the case of
     an out-of-memory error.

     The caller should lock exclusively against other modifiers of the array.


 (3) Delete an object from an associative array.

	struct assoc_array_edit *
	assoc_array_delete(struct assoc_array *array,
			   const struct assoc_array_ops *ops,
			   const void *index_key);

     This deletes an object that matches the specified data from the array.

     The index_key argument should hold index key information and is
     passed to the methods in the ops table when they are called.

     This function makes no alteration to the array itself, but rather returns
     an edit script that must be applied.  -ENOMEM is returned in the case of
     an out-of-memory error.  NULL will be returned if the specified object is
     not found within the array.

     The caller should lock exclusively against other modifiers of the array.


 (4) Delete all objects from an associative array.

	struct assoc_array_edit *
	assoc_array_clear(struct assoc_array *array,
			  const struct assoc_array_ops *ops);

     This deletes all the objects from an associative array and leaves it
     completely empty.

     This function makes no alteration to the array itself, but rather returns
     an edit script that must be applied.  -ENOMEM is returned in the case of
     an out-of-memory error.

     The caller should lock exclusively against other modifiers of the array.


 (5) Destroy an associative array, deleting all objects.

	void assoc_array_destroy(struct assoc_array *array,
				 const struct assoc_array_ops *ops);

     This destroys the contents of the associative array and leaves it
     completely empty.  It is not permitted for another thread to be traversing
     the array under the RCU read lock at the same time as this function is
     destroying it as no RCU deferral is performed on memory release -
     something that would require memory to be allocated.

     The caller should lock exclusively against other modifiers and accessors
     of the array.


 (6) Garbage collect an associative array.

	int assoc_array_gc(struct assoc_array *array,
			   const struct assoc_array_ops *ops,
			   bool (*iterator)(void *object, void *iterator_data),
			   void *iterator_data);

     This iterates over the objects in an associative array and passes each one
     to iterator().  If iterator() returns true, the object is kept.  If it
     returns false, the object will be freed.  If the iterator() function
     returns true, it must perform any appropriate refcount incrementing on the
     object before returning.

     The internal tree will be packed down if possible as part of the iteration
     to reduce the number of nodes in it.

     The iterator_data is passed directly to iterator() and is otherwise
     ignored by the function.

     The function will return 0 if successful and -ENOMEM if there wasn't
     enough memory.

     It is possible for other threads to iterate over or search the array under
     the RCU read lock whilst this function is in progress.  The caller should
     lock exclusively against other modifiers of the array.


ACCESS FUNCTIONS
----------------

There are two functions for accessing an associative array:

 (1) Iterate over all the objects in an associative array.

	int assoc_array_iterate(const struct assoc_array *array,
				int (*iterator)(const void *object,
						void *iterator_data),
				void *iterator_data);

     This passes each object in the array to the iterator callback function.
     iterator_data is private data for that function.

     This may be used on an array at the same time as the array is being
     modified, provided the RCU read lock is held.  Under such circumstances,
     it is possible for the iteration function to see some objects twice.  If
     this is a problem, then modification should be locked against.  The
     iteration algorithm should not, however, miss any objects.

     The function will return 0 if no objects were in the array or else it will
     return the result of the last iterator function called.  Iteration stops
     immediately if any call to the iteration function results in a non-zero
     return.


 (2) Find an object in an associative array.

	void *assoc_array_find(const struct assoc_array *array,
			       const struct assoc_array_ops *ops,
			       const void *index_key);

     This walks through the array's internal tree directly to the object
     specified by the index key..

     This may be used on an array at the same time as the array is being
     modified, provided the RCU read lock is held.

     The function will return the object if found (and set *_type to the object
     type) or will return NULL if the object was not found.


INDEX KEY FORM
--------------

The index key can be of any form, but since the algorithms aren't told how long
the key is, it is strongly recommended that the index key includes its length
very early on before any variation due to the length would have an effect on
comparisons.

This will cause leaves with different length keys to scatter away from each
other - and those with the same length keys to cluster together.

It is also recommended that the index key begin with a hash of the rest of the
key to maximise scattering throughout keyspace.

The better the scattering, the wider and lower the internal tree will be.

Poor scattering isn't too much of a problem as there are shortcuts and nodes
can contain mixtures of leaves and metadata pointers.

The index key is read in chunks of machine word.  Each chunk is subdivided into
one nibble (4 bits) per level, so on a 32-bit CPU this is good for 8 levels and
on a 64-bit CPU, 16 levels.  Unless the scattering is really poor, it is
unlikely that more than one word of any particular index key will have to be
used.


=================
INTERNAL WORKINGS
=================

The associative array data structure has an internal tree.  This tree is
constructed of two types of metadata blocks: nodes and shortcuts.

A node is an array of slots.  Each slot can contain one of four things:

 (*) A NULL pointer, indicating that the slot is empty.

 (*) A pointer to an object (a leaf).

 (*) A pointer to a node at the next level.

 (*) A pointer to a shortcut.


BASIC INTERNAL TREE LAYOUT
--------------------------

Ignoring shortcuts for the moment, the nodes form a multilevel tree.  The index
key space is strictly subdivided by the nodes in the tree and nodes occur on
fixed levels.  For example:

 Level:	0		1		2		3
	===============	===============	===============	===============
							NODE D
			NODE B		NODE C	+------>+---+
		+------>+---+	+------>+---+	|	| 0 |
	NODE A	|	| 0 |	|	| 0 |	|	+---+
	+---+	|	+---+	|	+---+	|	:   :
	| 0 |	|	:   :	|	:   :	|	+---+
	+---+	|	+---+	|	+---+	|	| f |
	| 1 |---+	| 3 |---+	| 7 |---+	+---+
	+---+		+---+		+---+
	:   :		:   :		| 8 |---+
	+---+		+---+		+---+	|	NODE E
	| e |---+	| f |		:   :   +------>+---+
	+---+	|	+---+		+---+		| 0 |
	| f |	|			| f |		+---+
	+---+	|			+---+		:   :
		|	NODE F				+---+
		+------>+---+				| f |
			| 0 |		NODE G		+---+
			+---+	+------>+---+
			:   :	|	| 0 |
			+---+	|	+---+
			| 6 |---+	:   :
			+---+		+---+
			:   :		| f |
			+---+		+---+
			| f |
			+---+

In the above example, there are 7 nodes (A-G), each with 16 slots (0-f).
Assuming no other meta data nodes in the tree, the key space is divided thusly:

	KEY PREFIX	NODE
	==========	====
	137*		D
	138*		E
	13[0-69-f]*	C
	1[0-24-f]*	B
	e6*		G
	e[0-57-f]*	F
	[02-df]*	A

So, for instance, keys with the following example index keys will be found in
the appropriate nodes:

	INDEX KEY	PREFIX	NODE
	===============	=======	====
	13694892892489	13	C
	13795289025897	137	D
	13889dde88793	138	E
	138bbb89003093	138	E
	1394879524789	12	C
	1458952489	1	B
	9431809de993ba	-	A
	b4542910809cd	-	A
	e5284310def98	e	F
	e68428974237	e6	G
	e7fffcbd443	e	F
	f3842239082	-	A

To save memory, if a node can hold all the leaves in its portion of keyspace,
then the node will have all those leaves in it and will not have any metadata
pointers - even if some of those leaves would like to be in the same slot.

A node can contain a heterogeneous mix of leaves and metadata pointers.
Metadata pointers must be in the slots that match their subdivisions of key
space.  The leaves can be in any slot not occupied by a metadata pointer.  It
is guaranteed that none of the leaves in a node will match a slot occupied by a
metadata pointer.  If the metadata pointer is there, any leaf whose key matches
the metadata key prefix must be in the subtree that the metadata pointer points
to.

In the above example list of index keys, node A will contain:

	SLOT	CONTENT		INDEX KEY (PREFIX)
	====	===============	==================
	1	PTR TO NODE B	1*
	any	LEAF		9431809de993ba
	any	LEAF		b4542910809cd
	e	PTR TO NODE F	e*
	any	LEAF		f3842239082

and node B:

	3	PTR TO NODE C	13*
	any	LEAF		1458952489


SHORTCUTS
---------

Shortcuts are metadata records that jump over a piece of keyspace.  A shortcut
is a replacement for a series of single-occupancy nodes ascending through the
levels.  Shortcuts exist to save memory and to speed up traversal.

It is possible for the root of the tree to be a shortcut - say, for example,
the tree contains at least 17 nodes all with key prefix '1111'.  The insertion
algorithm will insert a shortcut to skip over the '1111' keyspace in a single
bound and get to the fourth level where these actually become different.


SPLITTING AND COLLAPSING NODES
------------------------------

Each node has a maximum capacity of 16 leaves and metadata pointers.  If the
insertion algorithm finds that it is trying to insert a 17th object into a
node, that node will be split such that at least two leaves that have a common
key segment at that level end up in a separate node rooted on that slot for
that common key segment.

If the leaves in a full node and the leaf that is being inserted are
sufficiently similar, then a shortcut will be inserted into the tree.

When the number of objects in the subtree rooted at a node falls to 16 or
fewer, then the subtree will be collapsed down to a single node - and this will
ripple towards the root if possible.


NON-RECURSIVE ITERATION
-----------------------

Each node and shortcut contains a back pointer to its parent and the number of
slot in that parent that points to it.  None-recursive iteration uses these to
proceed rootwards through the tree, going to the parent node, slot N + 1 to
make sure progress is made without the need for a stack.

The backpointers, however, make simultaneous alteration and iteration tricky.


SIMULTANEOUS ALTERATION AND ITERATION
-------------------------------------

There are a number of cases to consider:

 (1) Simple insert/replace.  This involves simply replacing a NULL or old
     matching leaf pointer with the pointer to the new leaf after a barrier.
     The metadata blocks don't change otherwise.  An old leaf won't be freed
     until after the RCU grace period.

 (2) Simple delete.  This involves just clearing an old matching leaf.  The
     metadata blocks don't change otherwise.  The old leaf won't be freed until
     after the RCU grace period.

 (3) Insertion replacing part of a subtree that we haven't yet entered.  This
     may involve replacement of part of that subtree - but that won't affect
     the iteration as we won't have reached the pointer to it yet and the
     ancestry blocks are not replaced (the layout of those does not change).

 (4) Insertion replacing nodes that we're actively processing.  This isn't a
     problem as we've passed the anchoring pointer and won't switch onto the
     new layout until we follow the back pointers - at which point we've
     already examined the leaves in the replaced node (we iterate over all the
     leaves in a node before following any of its metadata pointers).

     We might, however, re-see some leaves that have been split out into a new
     branch that's in a slot further along than we were at.

 (5) Insertion replacing nodes that we're processing a dependent branch of.
     This won't affect us until we follow the back pointers.  Similar to (4).

 (6) Deletion collapsing a branch under us.  This doesn't affect us because the
     back pointers will get us back to the parent of the new node before we
     could see the new node.  The entire collapsed subtree is thrown away
     unchanged - and will still be rooted on the same slot, so we shouldn't
     process it a second time as we'll go back to slot + 1.

Note:

 (*) Under some circumstances, we need to simultaneously change the parent
     pointer and the parent slot pointer on a node (say, for example, we
     inserted another node before it and moved it up a level).  We cannot do
     this without locking against a read - so we have to replace that node too.

     However, when we're changing a shortcut into a node this isn't a problem
     as shortcuts only have one slot and so the parent slot number isn't used
     when traversing backwards over one.  This means that it's okay to change
     the slot number first - provided suitable barriers are used to make sure
     the parent slot number is read after the back pointer.

Obsolete blocks and leaves are freed up after an RCU grace period has passed,
so as long as anyone doing walking or iteration holds the RCU read lock, the
old superstructure should not go away on them.