1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
|
# SPDX-License-Identifier: GPL-2.0
%YAML 1.2
---
$id: http://devicetree.org/schemas/net/ethernet-controller.yaml#
$schema: http://devicetree.org/meta-schemas/core.yaml#
title: Ethernet Controller Generic Binding
maintainers:
- David S. Miller <davem@davemloft.net>
properties:
$nodename:
pattern: "^ethernet(@.*)?$"
local-mac-address:
description:
Specifies the MAC address that was assigned to the network device.
$ref: /schemas/types.yaml#definitions/uint8-array
items:
- minItems: 6
maxItems: 6
mac-address:
description:
Specifies the MAC address that was last used by the boot
program; should be used in cases where the MAC address assigned
to the device by the boot program is different from the
local-mac-address property.
$ref: /schemas/types.yaml#definitions/uint8-array
items:
- minItems: 6
maxItems: 6
max-frame-size:
$ref: /schemas/types.yaml#definitions/uint32
description:
Maximum transfer unit (IEEE defined MTU), rather than the
maximum frame size (there\'s contradiction in the Devicetree
Specification).
max-speed:
$ref: /schemas/types.yaml#definitions/uint32
description:
Specifies maximum speed in Mbit/s supported by the device.
nvmem-cells:
maxItems: 1
description:
Reference to an nvmem node for the MAC address
nvmem-cell-names:
const: mac-address
phy-connection-type:
description:
Specifies interface type between the Ethernet device and a physical
layer (PHY) device.
enum:
# There is not a standard bus between the MAC and the PHY,
# something proprietary is being used to embed the PHY in the
# MAC.
- internal
- mii
- gmii
- sgmii
- qsgmii
- tbi
- rev-mii
- rmii
- rev-rmii
# RX and TX delays are added by the MAC when required
- rgmii
# RGMII with internal RX and TX delays provided by the PHY,
# the MAC should not add the RX or TX delays in this case
- rgmii-id
# RGMII with internal RX delay provided by the PHY, the MAC
# should not add an RX delay in this case
- rgmii-rxid
# RGMII with internal TX delay provided by the PHY, the MAC
# should not add an TX delay in this case
- rgmii-txid
- rtbi
- smii
- xgmii
- trgmii
- 1000base-x
- 2500base-x
- rxaui
- xaui
# 10GBASE-KR, XFI, SFI
- 10gbase-kr
- usxgmii
phy-mode:
$ref: "#/properties/phy-connection-type"
phy-handle:
$ref: /schemas/types.yaml#definitions/phandle
description:
Specifies a reference to a node representing a PHY device.
phy:
$ref: "#/properties/phy-handle"
deprecated: true
phy-device:
$ref: "#/properties/phy-handle"
deprecated: true
rx-fifo-depth:
$ref: /schemas/types.yaml#definitions/uint32
description:
The size of the controller\'s receive fifo in bytes. This is used
for components that can have configurable receive fifo sizes,
and is useful for determining certain configuration settings
such as flow control thresholds.
rx-internal-delay-ps:
$ref: /schemas/types.yaml#/definitions/uint32
description: |
RGMII Receive Clock Delay defined in pico seconds.
This is used for controllers that have configurable RX internal delays.
If this property is present then the MAC applies the RX delay.
sfp:
$ref: /schemas/types.yaml#definitions/phandle
description:
Specifies a reference to a node representing a SFP cage.
tx-fifo-depth:
$ref: /schemas/types.yaml#definitions/uint32
description:
The size of the controller\'s transmit fifo in bytes. This
is used for components that can have configurable fifo sizes.
tx-internal-delay-ps:
$ref: /schemas/types.yaml#/definitions/uint32
description: |
RGMII Transmit Clock Delay defined in pico seconds.
This is used for controllers that have configurable TX internal delays.
If this property is present then the MAC applies the TX delay.
managed:
description:
Specifies the PHY management type. If auto is set and fixed-link
is not specified, it uses MDIO for management.
$ref: /schemas/types.yaml#definitions/string
default: auto
enum:
- auto
- in-band-status
fixed-link:
allOf:
- if:
type: array
then:
deprecated: true
minItems: 1
maxItems: 1
items:
items:
- minimum: 0
maximum: 31
description:
Emulated PHY ID, choose any but unique to the all
specified fixed-links
- enum: [0, 1]
description:
Duplex configuration. 0 for half duplex or 1 for
full duplex
- enum: [10, 100, 1000]
description:
Link speed in Mbits/sec.
- enum: [0, 1]
description:
Pause configuration. 0 for no pause, 1 for pause
- enum: [0, 1]
description:
Asymmetric pause configuration. 0 for no asymmetric
pause, 1 for asymmetric pause
- if:
type: object
then:
properties:
speed:
description:
Link speed.
$ref: /schemas/types.yaml#definitions/uint32
enum: [10, 100, 1000]
full-duplex:
$ref: /schemas/types.yaml#definitions/flag
description:
Indicates that full-duplex is used. When absent, half
duplex is assumed.
pause:
$ref: /schemas/types.yaml#definitions/flag
description:
Indicates that pause should be enabled.
asym-pause:
$ref: /schemas/types.yaml#definitions/flag
description:
Indicates that asym_pause should be enabled.
link-gpios:
maxItems: 1
description:
GPIO to determine if the link is up
required:
- speed
additionalProperties: true
...
|