aboutsummaryrefslogtreecommitdiffstats
blob: d9b62741a2259bd2c10dec78658fbcba0ca6232f (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
# SPDX-License-Identifier: GPL-2.0
%YAML 1.2
---
$id: http://devicetree.org/schemas/net/ethernet-phy.yaml#
$schema: http://devicetree.org/meta-schemas/core.yaml#

title: Ethernet PHY Common Properties

maintainers:
  - Andrew Lunn <andrew@lunn.ch>
  - Florian Fainelli <f.fainelli@gmail.com>
  - Heiner Kallweit <hkallweit1@gmail.com>

# The dt-schema tools will generate a select statement first by using
# the compatible, and second by using the node name if any. In our
# case, the node name is the one we want to match on, while the
# compatible is optional.
select:
  properties:
    $nodename:
      pattern: "^ethernet-phy(@[a-f0-9]+)?$"

  required:
    - $nodename

properties:
  $nodename:
    pattern: "^ethernet-phy(@[a-f0-9]+)?$"

  compatible:
    oneOf:
      - const: ethernet-phy-ieee802.3-c22
        description: PHYs that implement IEEE802.3 clause 22
      - const: ethernet-phy-ieee802.3-c45
        description: PHYs that implement IEEE802.3 clause 45
      - pattern: "^ethernet-phy-id[a-f0-9]{4}\\.[a-f0-9]{4}$"
        description:
          If the PHY reports an incorrect ID (or none at all) then the
          compatible list may contain an entry with the correct PHY ID
          in the above form.
          The first group of digits is the 16 bit Phy Identifier 1
          register, this is the chip vendor OUI bits 3:18. The
          second group of digits is the Phy Identifier 2 register,
          this is the chip vendor OUI bits 19:24, followed by 10
          bits of a vendor specific ID.
      - items:
          - pattern: "^ethernet-phy-id[a-f0-9]{4}\\.[a-f0-9]{4}$"
          - const: ethernet-phy-ieee802.3-c22
      - items:
          - pattern: "^ethernet-phy-id[a-f0-9]{4}\\.[a-f0-9]{4}$"
          - const: ethernet-phy-ieee802.3-c45

  reg:
    minimum: 0
    maximum: 31
    description:
      The ID number for the PHY.

  interrupts:
    maxItems: 1

  max-speed:
    enum:
      - 10
      - 100
      - 1000
      - 2500
      - 5000
      - 10000
      - 20000
      - 25000
      - 40000
      - 50000
      - 56000
      - 100000
      - 200000
    description:
      Maximum PHY supported speed in Mbits / seconds.

  phy-10base-t1l-2.4vpp:
    description: |
      tristate, request/disable 2.4 Vpp operating mode. The values are:
      0: Disable 2.4 Vpp operating mode.
      1: Request 2.4 Vpp operating mode from link partner.
      Absence of this property will leave configuration to default values.
    $ref: /schemas/types.yaml#/definitions/uint32
    enum: [0, 1]

  broken-turn-around:
    $ref: /schemas/types.yaml#/definitions/flag
    description:
      If set, indicates the PHY device does not correctly release
      the turn around line low at end of the control phase of the
      MDIO transaction.

  brr-mode:
    $ref: /schemas/types.yaml#/definitions/flag
    description:
      If set, indicates the network cable interface is an alternative one as
      defined in the BroadR-Reach link mode specification under 1BR-100 and
      1BR-10 names. The PHY must be configured to operate in BroadR-Reach mode
      by software.

  clocks:
    maxItems: 1
    description:
      External clock connected to the PHY. If not specified it is assumed
      that the PHY uses a fixed crystal or an internal oscillator.

  enet-phy-lane-swap:
    $ref: /schemas/types.yaml#/definitions/flag
    description:
      If set, indicates the PHY will swap the TX/RX lanes to
      compensate for the board being designed with the lanes
      swapped.

  enet-phy-lane-no-swap:
    $ref: /schemas/types.yaml#/definitions/flag
    description:
      If set, indicates that PHY will disable swap of the
      TX/RX lanes. This property allows the PHY to work correctly after
      e.g. wrong bootstrap configuration caused by issues in PCB
      layout design.

  eee-broken-100tx:
    $ref: /schemas/types.yaml#/definitions/flag
    description:
      Mark the corresponding energy efficient ethernet mode as
      broken and request the ethernet to stop advertising it.

  eee-broken-1000t:
    $ref: /schemas/types.yaml#/definitions/flag
    description:
      Mark the corresponding energy efficient ethernet mode as
      broken and request the ethernet to stop advertising it.

  eee-broken-10gt:
    $ref: /schemas/types.yaml#/definitions/flag
    description:
      Mark the corresponding energy efficient ethernet mode as
      broken and request the ethernet to stop advertising it.

  eee-broken-1000kx:
    $ref: /schemas/types.yaml#/definitions/flag
    description:
      Mark the corresponding energy efficient ethernet mode as
      broken and request the ethernet to stop advertising it.

  eee-broken-10gkx4:
    $ref: /schemas/types.yaml#/definitions/flag
    description:
      Mark the corresponding energy efficient ethernet mode as
      broken and request the ethernet to stop advertising it.

  eee-broken-10gkr:
    $ref: /schemas/types.yaml#/definitions/flag
    description:
      Mark the corresponding energy efficient ethernet mode as
      broken and request the ethernet to stop advertising it.

  pses:
    $ref: /schemas/types.yaml#/definitions/phandle-array
    maxItems: 1
    description:
      Specifies a reference to a node representing a Power Sourcing Equipment.

  phy-is-integrated:
    $ref: /schemas/types.yaml#/definitions/flag
    description:
      If set, indicates that the PHY is integrated into the same
      physical package as the Ethernet MAC. If needed, muxers
      should be configured to ensure the integrated PHY is
      used. The absence of this property indicates the muxers
      should be configured so that the external PHY is used.

  resets:
    maxItems: 1

  reset-names:
    const: phy

  reset-gpios:
    maxItems: 1
    description:
      The GPIO phandle and specifier for the PHY reset signal.

  reset-assert-us:
    description:
      Delay after the reset was asserted in microseconds. If this
      property is missing the delay will be skipped.

  reset-deassert-us:
    description:
      Delay after the reset was deasserted in microseconds. If
      this property is missing the delay will be skipped.

  sfp:
    $ref: /schemas/types.yaml#/definitions/phandle
    description:
      Specifies a reference to a node representing a SFP cage.

  rx-internal-delay-ps:
    description: |
      RGMII Receive PHY Clock Delay defined in pico seconds.  This is used for
      PHY's that have configurable RX internal delays.  If this property is
      present then the PHY applies the RX delay.

  tx-internal-delay-ps:
    description: |
      RGMII Transmit PHY Clock Delay defined in pico seconds.  This is used for
      PHY's that have configurable TX internal delays. If this property is
      present then the PHY applies the TX delay.

  leds:
    type: object

    properties:
      '#address-cells':
        const: 1

      '#size-cells':
        const: 0

    patternProperties:
      '^led@[a-f0-9]+$':
        $ref: /schemas/leds/common.yaml#

        properties:
          reg:
            maxItems: 1
            description:
              This define the LED index in the PHY or the MAC. It's really
              driver dependent and required for ports that define multiple
              LED for the same port.

        required:
          - reg

        unevaluatedProperties: false

    additionalProperties: false

required:
  - reg

additionalProperties: true

examples:
  - |
    #include <dt-bindings/leds/common.h>

    ethernet {
        #address-cells = <1>;
        #size-cells = <0>;

        ethernet-phy@0 {
            compatible = "ethernet-phy-id0141.0e90", "ethernet-phy-ieee802.3-c45";
            interrupt-parent = <&PIC>;
            interrupts = <35 1>;
            reg = <0>;

            resets = <&rst 8>;
            reset-names = "phy";
            reset-gpios = <&gpio1 4 1>;
            reset-assert-us = <1000>;
            reset-deassert-us = <2000>;

            leds {
                #address-cells = <1>;
                #size-cells = <0>;

                led@0 {
                    reg = <0>;
                    color = <LED_COLOR_ID_WHITE>;
                    function = LED_FUNCTION_LAN;
                    default-state = "keep";
                };
            };
        };
    };