aboutsummaryrefslogtreecommitdiffstats
blob: c7d49b8855593b2a75e263363a9360e905f50773 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
Email clients info for Linux
======================================================================

Git
----------------------------------------------------------------------
These days most developers use `git send-email` instead of regular
email clients.  The man page for this is quite good.  On the receiving
end, maintainers use `git am` to apply the patches.

If you are new to git then send your first patch to yourself.  Save it
as raw text including all the headers.  Run `git am raw_email.txt` and
then review the changelog with `git log`.  When that works then send
the patch to the appropriate mailing list(s).

General Preferences
----------------------------------------------------------------------
Patches for the Linux kernel are submitted via email, preferably as
inline text in the body of the email.  Some maintainers accept
attachments, but then the attachments should have content-type
"text/plain".  However, attachments are generally frowned upon because
it makes quoting portions of the patch more difficult in the patch
review process.

Email clients that are used for Linux kernel patches should send the
patch text untouched.  For example, they should not modify or delete tabs
or spaces, even at the beginning or end of lines.

Don't send patches with "format=flowed".  This can cause unexpected
and unwanted line breaks.

Don't let your email client do automatic word wrapping for you.
This can also corrupt your patch.

Email clients should not modify the character set encoding of the text.
Emailed patches should be in ASCII or UTF-8 encoding only.
If you configure your email client to send emails with UTF-8 encoding,
you avoid some possible charset problems.

Email clients should generate and maintain References: or In-Reply-To:
headers so that mail threading is not broken.

Copy-and-paste (or cut-and-paste) usually does not work for patches
because tabs are converted to spaces.  Using xclipboard, xclip, and/or
xcutsel may work, but it's best to test this for yourself or just avoid
copy-and-paste.

Don't use PGP/GPG signatures in mail that contains patches.
This breaks many scripts that read and apply the patches.
(This should be fixable.)

It's a good idea to send a patch to yourself, save the received message,
and successfully apply it with 'patch' before sending patches to Linux
mailing lists.


Some email client (MUA) hints
----------------------------------------------------------------------
Here are some specific MUA configuration hints for editing and sending
patches for the Linux kernel.  These are not meant to be complete
software package configuration summaries.

Legend:
TUI = text-based user interface
GUI = graphical user interface

~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
Alpine (TUI)

Config options:
In the "Sending Preferences" section:

- "Do Not Send Flowed Text" must be enabled
- "Strip Whitespace Before Sending" must be disabled

When composing the message, the cursor should be placed where the patch
should appear, and then pressing CTRL-R let you specify the patch file
to insert into the message.

~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
Claws Mail (GUI)

Works. Some people use this successfully for patches.

To insert a patch use Message->Insert File (CTRL+i) or an external editor.

If the inserted patch has to be edited in the Claws composition window
"Auto wrapping" in Configuration->Preferences->Compose->Wrapping should be
disabled.

~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
Evolution (GUI)

Some people use this successfully for patches.

When composing mail select: Preformat
  from Format->Heading->Preformatted (Ctrl-7)
  or the toolbar

Then use:
  Insert->Text File... (Alt-n x)
to insert the patch.

You can also "diff -Nru old.c new.c | xclip", select Preformat, then
paste with the middle button.

~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
Kmail (GUI)

Some people use Kmail successfully for patches.

The default setting of not composing in HTML is appropriate; do not
enable it.

When composing an email, under options, uncheck "word wrap". The only
disadvantage is any text you type in the email will not be word-wrapped
so you will have to manually word wrap text before the patch. The easiest
way around this is to compose your email with word wrap enabled, then save
it as a draft. Once you pull it up again from your drafts it is now hard
word-wrapped and you can uncheck "word wrap" without losing the existing
wrapping.

At the bottom of your email, put the commonly-used patch delimiter before
inserting your patch:  three hyphens (---).

Then from the "Message" menu item, select insert file and choose your patch.
As an added bonus you can customise the message creation toolbar menu
and put the "insert file" icon there.

Make the composer window wide enough so that no lines wrap. As of
KMail 1.13.5 (KDE 4.5.4), KMail will apply word wrapping when sending
the email if the lines wrap in the composer window. Having word wrapping
disabled in the Options menu isn't enough. Thus, if your patch has very
long lines, you must make the composer window very wide before sending
the email. See: https://bugs.kde.org/show_bug.cgi?id=174034

You can safely GPG sign attachments, but inlined text is preferred for
patches so do not GPG sign them.  Signing patches that have been inserted
as inlined text will make them tricky to extract from their 7-bit encoding.

If you absolutely must send patches as attachments instead of inlining
them as text, right click on the attachment and select properties, and
highlight "Suggest automatic display" to make the attachment inlined to
make it more viewable.

When saving patches that are sent as inlined text, select the email that
contains the patch from the message list pane, right click and select
"save as".  You can use the whole email unmodified as a patch if it was
properly composed.  There is no option currently to save the email when you
are actually viewing it in its own window -- there has been a request filed
at kmail's bugzilla and hopefully this will be addressed.  Emails are saved
as read-write for user only so you will have to chmod them to make them
group and world readable if you copy them elsewhere.

~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
Lotus Notes (GUI)

Run away from it.

~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
Mutt (TUI)

Plenty of Linux developers use mutt, so it must work pretty well.

Mutt doesn't come with an editor, so whatever editor you use should be
used in a way that there are no automatic linebreaks.  Most editors have
an "insert file" option that inserts the contents of a file unaltered.

To use 'vim' with mutt:
  set editor="vi"

  If using xclip, type the command
  :set paste
  before middle button or shift-insert or use
  :r filename

if you want to include the patch inline.
(a)ttach works fine without "set paste".

Config options:
It should work with default settings.
However, it's a good idea to set the "send_charset" to:
  set send_charset="us-ascii:utf-8"

~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
Pine (TUI)

Pine has had some whitespace truncation issues in the past, but these
should all be fixed now.

Use alpine (pine's successor) if you can.

Config options:
- quell-flowed-text is needed for recent versions
- the "no-strip-whitespace-before-send" option is needed


~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
Sylpheed (GUI)

- Works well for inlining text (or using attachments).
- Allows use of an external editor.
- Is slow on large folders.
- Won't do TLS SMTP auth over a non-SSL connection.
- Has a helpful ruler bar in the compose window.
- Adding addresses to address book doesn't understand the display name
  properly.

~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
Thunderbird (GUI)

Thunderbird is an Outlook clone that likes to mangle text, but there are ways
to coerce it into behaving.

- Allow use of an external editor:
  The easiest thing to do with Thunderbird and patches is to use an
  "external editor" extension and then just use your favorite $EDITOR
  for reading/merging patches into the body text.  To do this, download
  and install the extension, then add a button for it using
  View->Toolbars->Customize... and finally just click on it when in the
  Compose dialog.

  Please note that "external editor" requires that your editor must not
  fork, or in other words, the editor must not return before closing. 
  You may have to pass additional flags or change the settings of your
  editor. Most notably if you are using gvim then you must pass the -f
  option to gvim by putting "/usr/bin/gvim -f" (if the binary is in
  /usr/bin) to the text editor field in "external editor" settings. If you
  are using some other editor then please read its manual to find out how
  to do this.

To beat some sense out of the internal editor, do this:

- Edit your Thunderbird config settings so that it won't use format=flowed.
  Go to "edit->preferences->advanced->config editor" to bring up the
  thunderbird's registry editor.

- Set "mailnews.send_plaintext_flowed" to "false"

- Set "mailnews.wraplength" from "72" to "0"

- "View" > "Message Body As" > "Plain Text"

- "View" > "Character Encoding" > "Unicode (UTF-8)"

~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
TkRat (GUI)

Works.  Use "Insert file..." or external editor.

~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
Gmail (Web GUI)

Does not work for sending patches.

Gmail web client converts tabs to spaces automatically.

At the same time it wraps lines every 78 chars with CRLF style line breaks
although tab2space problem can be solved with external editor.

Another problem is that Gmail will base64-encode any message that has a
non-ASCII character. That includes things like European names.

                                ###