aboutsummaryrefslogtreecommitdiffstats
blob: e69274de8d0c9c1754cc40b8d99d78a724e63e50 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
317
318
319
320
321
322
323
324
325
326
327
328
329
330
331
332
333
334
335
336
337
338
339
340
341
342
343
344
345
346
347
348
349
350
351
352
353
354
355
356
357
358
359
360
361
362
363
364
365
366
367
368
369
370
371
372
373
374
375
376
377
378
379
380
381
382
383
384
385
386
387
388
389
390
391
392
393
394
395
396
397
398
399
400
401
402
403
404
405
406
407
408
409
410
411
412
413
414
415
416
417
418
419
420
421
422
423
424
425
426
427
428
429
430
431
432
433
434
435
436
437
438
439
440
441
442
443
444
445
446
447
448
449
450
451
452
453
454
455
456
457
458
459
460
461
462
463
464
465
466
467
468
469
470
471
472
473
474
475
476
477
478
479
480
481
482
483
484
485
Changes since 2.5.0:

---
[recommended]

New helpers: sb_bread(), sb_getblk(), sb_find_get_block(), set_bh(),
	sb_set_blocksize() and sb_min_blocksize().

Use them.

(sb_find_get_block() replaces 2.4's get_hash_table())

---
[recommended]

New methods: ->alloc_inode() and ->destroy_inode().

Remove inode->u.foo_inode_i
Declare
	struct foo_inode_info {
		/* fs-private stuff */
		struct inode vfs_inode;
	};
	static inline struct foo_inode_info *FOO_I(struct inode *inode)
	{
		return list_entry(inode, struct foo_inode_info, vfs_inode);
	}

Use FOO_I(inode) instead of &inode->u.foo_inode_i;

Add foo_alloc_inode() and foo_destroy_inode() - the former should allocate
foo_inode_info and return the address of ->vfs_inode, the latter should free
FOO_I(inode) (see in-tree filesystems for examples).

Make them ->alloc_inode and ->destroy_inode in your super_operations.

Keep in mind that now you need explicit initialization of private data
typically between calling iget_locked() and unlocking the inode.

At some point that will become mandatory.

---
[mandatory]

Change of file_system_type method (->read_super to ->get_sb)

->read_super() is no more.  Ditto for DECLARE_FSTYPE and DECLARE_FSTYPE_DEV.

Turn your foo_read_super() into a function that would return 0 in case of
success and negative number in case of error (-EINVAL unless you have more
informative error value to report).  Call it foo_fill_super().  Now declare

int foo_get_sb(struct file_system_type *fs_type,
	int flags, const char *dev_name, void *data, struct vfsmount *mnt)
{
	return get_sb_bdev(fs_type, flags, dev_name, data, foo_fill_super,
			   mnt);
}

(or similar with s/bdev/nodev/ or s/bdev/single/, depending on the kind of
filesystem).

Replace DECLARE_FSTYPE... with explicit initializer and have ->get_sb set as
foo_get_sb.

---
[mandatory]

Locking change: ->s_vfs_rename_sem is taken only by cross-directory renames.
Most likely there is no need to change anything, but if you relied on
global exclusion between renames for some internal purpose - you need to
change your internal locking.  Otherwise exclusion warranties remain the
same (i.e. parents and victim are locked, etc.).

---
[informational]

Now we have the exclusion between ->lookup() and directory removal (by
->rmdir() and ->rename()).  If you used to need that exclusion and do
it by internal locking (most of filesystems couldn't care less) - you
can relax your locking.

---
[mandatory]

->lookup(), ->truncate(), ->create(), ->unlink(), ->mknod(), ->mkdir(),
->rmdir(), ->link(), ->lseek(), ->symlink(), ->rename()
and ->readdir() are called without BKL now.  Grab it on entry, drop upon return
- that will guarantee the same locking you used to have.  If your method or its
parts do not need BKL - better yet, now you can shift lock_kernel() and
unlock_kernel() so that they would protect exactly what needs to be
protected.

---
[mandatory]

BKL is also moved from around sb operations. BKL should have been shifted into
individual fs sb_op functions.  If you don't need it, remove it.

---
[informational]

check for ->link() target not being a directory is done by callers.  Feel
free to drop it...

---
[informational]

->link() callers hold ->i_mutex on the object we are linking to.  Some of your
problems might be over...

---
[mandatory]

new file_system_type method - kill_sb(superblock).  If you are converting
an existing filesystem, set it according to ->fs_flags:
	FS_REQUIRES_DEV		-	kill_block_super
	FS_LITTER		-	kill_litter_super
	neither			-	kill_anon_super
FS_LITTER is gone - just remove it from fs_flags.

---
[mandatory]

	FS_SINGLE is gone (actually, that had happened back when ->get_sb()
went in - and hadn't been documented ;-/).  Just remove it from fs_flags
(and see ->get_sb() entry for other actions).

---
[mandatory]

->setattr() is called without BKL now.  Caller _always_ holds ->i_mutex, so
watch for ->i_mutex-grabbing code that might be used by your ->setattr().
Callers of notify_change() need ->i_mutex now.

---
[recommended]

New super_block field "struct export_operations *s_export_op" for
explicit support for exporting, e.g. via NFS.  The structure is fully
documented at its declaration in include/linux/fs.h, and in
Documentation/filesystems/nfs/Exporting.

Briefly it allows for the definition of decode_fh and encode_fh operations
to encode and decode filehandles, and allows the filesystem to use
a standard helper function for decode_fh, and provide file-system specific
support for this helper, particularly get_parent.

It is planned that this will be required for exporting once the code
settles down a bit.

[mandatory]

s_export_op is now required for exporting a filesystem.
isofs, ext2, ext3, resierfs, fat
can be used as examples of very different filesystems.

---
[mandatory]

iget4() and the read_inode2 callback have been superseded by iget5_locked()
which has the following prototype,

    struct inode *iget5_locked(struct super_block *sb, unsigned long ino,
				int (*test)(struct inode *, void *),
				int (*set)(struct inode *, void *),
				void *data);

'test' is an additional function that can be used when the inode
number is not sufficient to identify the actual file object. 'set'
should be a non-blocking function that initializes those parts of a
newly created inode to allow the test function to succeed. 'data' is
passed as an opaque value to both test and set functions.

When the inode has been created by iget5_locked(), it will be returned with the
I_NEW flag set and will still be locked.  The filesystem then needs to finalize
the initialization. Once the inode is initialized it must be unlocked by
calling unlock_new_inode().

The filesystem is responsible for setting (and possibly testing) i_ino
when appropriate. There is also a simpler iget_locked function that
just takes the superblock and inode number as arguments and does the
test and set for you.

e.g.
	inode = iget_locked(sb, ino);
	if (inode->i_state & I_NEW) {
		err = read_inode_from_disk(inode);
		if (err < 0) {
			iget_failed(inode);
			return err;
		}
		unlock_new_inode(inode);
	}

Note that if the process of setting up a new inode fails, then iget_failed()
should be called on the inode to render it dead, and an appropriate error
should be passed back to the caller.

---
[recommended]

->getattr() finally getting used.  See instances in nfs, minix, etc.

---
[mandatory]

->revalidate() is gone.  If your filesystem had it - provide ->getattr()
and let it call whatever you had as ->revlidate() + (for symlinks that
had ->revalidate()) add calls in ->follow_link()/->readlink().

---
[mandatory]

->d_parent changes are not protected by BKL anymore.  Read access is safe
if at least one of the following is true:
	* filesystem has no cross-directory rename()
	* we know that parent had been locked (e.g. we are looking at
->d_parent of ->lookup() argument).
	* we are called from ->rename().
	* the child's ->d_lock is held
Audit your code and add locking if needed.  Notice that any place that is
not protected by the conditions above is risky even in the old tree - you
had been relying on BKL and that's prone to screwups.  Old tree had quite
a few holes of that kind - unprotected access to ->d_parent leading to
anything from oops to silent memory corruption.

---
[mandatory]

	FS_NOMOUNT is gone.  If you use it - just set MS_NOUSER in flags
(see rootfs for one kind of solution and bdev/socket/pipe for another).

---
[recommended]

	Use bdev_read_only(bdev) instead of is_read_only(kdev).  The latter
is still alive, but only because of the mess in drivers/s390/block/dasd.c.
As soon as it gets fixed is_read_only() will die.

---
[mandatory]

->permission() is called without BKL now. Grab it on entry, drop upon
return - that will guarantee the same locking you used to have.  If
your method or its parts do not need BKL - better yet, now you can
shift lock_kernel() and unlock_kernel() so that they would protect
exactly what needs to be protected.

---
[mandatory]

->statfs() is now called without BKL held.  BKL should have been
shifted into individual fs sb_op functions where it's not clear that
it's safe to remove it.  If you don't need it, remove it.

---
[mandatory]

	is_read_only() is gone; use bdev_read_only() instead.

---
[mandatory]

	destroy_buffers() is gone; use invalidate_bdev().

---
[mandatory]

	fsync_dev() is gone; use fsync_bdev().  NOTE: lvm breakage is
deliberate; as soon as struct block_device * is propagated in a reasonable
way by that code fixing will become trivial; until then nothing can be
done.

[mandatory]

	block truncatation on error exit from ->write_begin, and ->direct_IO
moved from generic methods (block_write_begin, cont_write_begin,
nobh_write_begin, blockdev_direct_IO*) to callers.  Take a look at
ext2_write_failed and callers for an example.

[mandatory]

	->truncate is gone.  The whole truncate sequence needs to be
implemented in ->setattr, which is now mandatory for filesystems
implementing on-disk size changes.  Start with a copy of the old inode_setattr
and vmtruncate, and the reorder the vmtruncate + foofs_vmtruncate sequence to
be in order of zeroing blocks using block_truncate_page or similar helpers,
size update and on finally on-disk truncation which should not fail.
inode_change_ok now includes the size checks for ATTR_SIZE and must be called
in the beginning of ->setattr unconditionally.

[mandatory]

	->clear_inode() and ->delete_inode() are gone; ->evict_inode() should
be used instead.  It gets called whenever the inode is evicted, whether it has
remaining links or not.  Caller does *not* evict the pagecache or inode-associated
metadata buffers; the method has to use truncate_inode_pages_final() to get rid
of those. Caller makes sure async writeback cannot be running for the inode while
(or after) ->evict_inode() is called.

	->drop_inode() returns int now; it's called on final iput() with
inode->i_lock held and it returns true if filesystems wants the inode to be
dropped.  As before, generic_drop_inode() is still the default and it's been
updated appropriately.  generic_delete_inode() is also alive and it consists
simply of return 1.  Note that all actual eviction work is done by caller after
->drop_inode() returns.

	As before, clear_inode() must be called exactly once on each call of
->evict_inode() (as it used to be for each call of ->delete_inode()).  Unlike
before, if you are using inode-associated metadata buffers (i.e.
mark_buffer_dirty_inode()), it's your responsibility to call
invalidate_inode_buffers() before clear_inode().

	NOTE: checking i_nlink in the beginning of ->write_inode() and bailing out
if it's zero is not *and* *never* *had* *been* enough.  Final unlink() and iput()
may happen while the inode is in the middle of ->write_inode(); e.g. if you blindly
free the on-disk inode, you may end up doing that while ->write_inode() is writing
to it.

---
[mandatory]

	.d_delete() now only advises the dcache as to whether or not to cache
unreferenced dentries, and is now only called when the dentry refcount goes to
0. Even on 0 refcount transition, it must be able to tolerate being called 0,
1, or more times (eg. constant, idempotent).

---
[mandatory]

	.d_compare() calling convention and locking rules are significantly
changed. Read updated documentation in Documentation/filesystems/vfs.txt (and
look at examples of other filesystems) for guidance.

---
[mandatory]

	.d_hash() calling convention and locking rules are significantly
changed. Read updated documentation in Documentation/filesystems/vfs.txt (and
look at examples of other filesystems) for guidance.

---
[mandatory]
	dcache_lock is gone, replaced by fine grained locks. See fs/dcache.c
for details of what locks to replace dcache_lock with in order to protect
particular things. Most of the time, a filesystem only needs ->d_lock, which
protects *all* the dcache state of a given dentry.

--
[mandatory]

	Filesystems must RCU-free their inodes, if they can have been accessed
via rcu-walk path walk (basically, if the file can have had a path name in the
vfs namespace).

	Even though i_dentry and i_rcu share storage in a union, we will
initialize the former in inode_init_always(), so just leave it alone in
the callback.  It used to be necessary to clean it there, but not anymore
(starting at 3.2).

--
[recommended]
	vfs now tries to do path walking in "rcu-walk mode", which avoids
atomic operations and scalability hazards on dentries and inodes (see
Documentation/filesystems/path-lookup.txt). d_hash and d_compare changes
(above) are examples of the changes required to support this. For more complex
filesystem callbacks, the vfs drops out of rcu-walk mode before the fs call, so
no changes are required to the filesystem. However, this is costly and loses
the benefits of rcu-walk mode. We will begin to add filesystem callbacks that
are rcu-walk aware, shown below. Filesystems should take advantage of this
where possible.

--
[mandatory]
	d_revalidate is a callback that is made on every path element (if
the filesystem provides it), which requires dropping out of rcu-walk mode. This
may now be called in rcu-walk mode (nd->flags & LOOKUP_RCU). -ECHILD should be
returned if the filesystem cannot handle rcu-walk. See
Documentation/filesystems/vfs.txt for more details.

	permission and check_acl are inode permission checks that are called
on many or all directory inodes on the way down a path walk (to check for
exec permission). These must now be rcu-walk aware (flags & IPERM_FLAG_RCU).
See Documentation/filesystems/vfs.txt for more details.
 
--
[mandatory]
	In ->fallocate() you must check the mode option passed in.  If your
filesystem does not support hole punching (deallocating space in the middle of a
file) you must return -EOPNOTSUPP if FALLOC_FL_PUNCH_HOLE is set in mode.
Currently you can only have FALLOC_FL_PUNCH_HOLE with FALLOC_FL_KEEP_SIZE set,
so the i_size should not change when hole punching, even when puching the end of
a file off.

--
[mandatory]
	->get_sb() is gone.  Switch to use of ->mount().  Typically it's just
a matter of switching from calling get_sb_... to mount_... and changing the
function type.  If you were doing it manually, just switch from setting ->mnt_root
to some pointer to returning that pointer.  On errors return ERR_PTR(...).

--
[mandatory]
	->permission() and generic_permission()have lost flags
argument; instead of passing IPERM_FLAG_RCU we add MAY_NOT_BLOCK into mask.
	generic_permission() has also lost the check_acl argument; ACL checking
has been taken to VFS and filesystems need to provide a non-NULL ->i_op->get_acl
to read an ACL from disk.

--
[mandatory]
	If you implement your own ->llseek() you must handle SEEK_HOLE and
SEEK_DATA.  You can hanle this by returning -EINVAL, but it would be nicer to
support it in some way.  The generic handler assumes that the entire file is
data and there is a virtual hole at the end of the file.  So if the provided
offset is less than i_size and SEEK_DATA is specified, return the same offset.
If the above is true for the offset and you are given SEEK_HOLE, return the end
of the file.  If the offset is i_size or greater return -ENXIO in either case.

[mandatory]
	If you have your own ->fsync() you must make sure to call
filemap_write_and_wait_range() so that all dirty pages are synced out properly.
You must also keep in mind that ->fsync() is not called with i_mutex held
anymore, so if you require i_mutex locking you must make sure to take it and
release it yourself.

--
[mandatory]
	d_alloc_root() is gone, along with a lot of bugs caused by code
misusing it.  Replacement: d_make_root(inode).  The difference is,
d_make_root() drops the reference to inode if dentry allocation fails.  

--
[mandatory]
	The witch is dead!  Well, 2/3 of it, anyway.  ->d_revalidate() and
->lookup() do *not* take struct nameidata anymore; just the flags.
--
[mandatory]
	->create() doesn't take struct nameidata *; unlike the previous
two, it gets "is it an O_EXCL or equivalent?" boolean argument.  Note that
local filesystems can ignore tha argument - they are guaranteed that the
object doesn't exist.  It's remote/distributed ones that might care...
--
[mandatory]
	FS_REVAL_DOT is gone; if you used to have it, add ->d_weak_revalidate()
in your dentry operations instead.
--
[mandatory]
	vfs_readdir() is gone; switch to iterate_dir() instead
--
[mandatory]
	->readdir() is gone now; switch to ->iterate()
[mandatory]
	vfs_follow_link has been removed.  Filesystems must use nd_set_link
	from ->follow_link for normal symlinks, or nd_jump_link for magic
	/proc/<pid> style links.
--
[mandatory]
	iget5_locked()/ilookup5()/ilookup5_nowait() test() callback used to be
	called with both ->i_lock and inode_hash_lock held; the former is *not*
	taken anymore, so verify that your callbacks do not rely on it (none
	of the in-tree instances did).  inode_hash_lock is still held,
	of course, so they are still serialized wrt removal from inode hash,
	as well as wrt set() callback of iget5_locked().
--
[mandatory]
	d_materialise_unique() is gone; d_splice_alias() does everything you
	need now.  Remember that they have opposite orders of arguments ;-/
--
[mandatory]
	f_dentry is gone; use f_path.dentry, or, better yet, see if you can avoid
	it entirely.
--
[mandatory]
	never call ->read() and ->write() directly; use __vfs_{read,write} or
	wrappers; instead of checking for ->write or ->read being NULL, look for
	FMODE_CAN_{WRITE,READ} in file->f_mode.
--
[mandatory]
	do _not_ use new_sync_{read,write} for ->read/->write; leave it NULL
	instead.
--
[mandatory]
	->aio_read/->aio_write are gone.  Use ->read_iter/->write_iter.