aboutsummaryrefslogtreecommitdiffstats
blob: 418020584ccc171b8ff079e496e73383f0f55c29 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
317
318
319
320
321
322
323
324
325
326
327
328
329
330
331
332
333
334
335
336
337
338
339
340
341
342
343
344
345
346
347
348
349
350
351
352
353
354
355
356
357
358
359
360
361
362
363
364
365
366
367
368
369
370
371
372
373
374
375
376
377
378
379
380
381
382
383
384
385
386
387
388
389
390
391
392
393
394
395
396
397
398
399
400
401
402
403
404
               Java(tm) Binary Kernel Support for Linux v1.03
               ----------------------------------------------

Linux beats them ALL! While all other OS's are TALKING about direct
support of Java Binaries in the OS, Linux is doing it!

You can execute Java applications and Java Applets just like any
other program after you have done the following:

1) You MUST FIRST install the Java Developers Kit for Linux.
   The Java on Linux HOWTO gives the details on getting and
   installing this. This HOWTO can be found at:

	ftp://sunsite.unc.edu/pub/Linux/docs/HOWTO/Java-HOWTO

   You should also set up a reasonable CLASSPATH environment
   variable to use Java applications that make use of any
   nonstandard classes (not included in the same directory
   as the application itself).

2) You have to compile BINFMT_MISC either as a module or into
   the kernel (CONFIG_BINFMT_MISC) and set it up properly.
   If you choose to compile it as a module, you will have
   to insert it manually with modprobe/insmod, as kmod
   cannot easily be supported with binfmt_misc. 
   Read the file 'binfmt_misc.txt' in this directory to know
   more about the configuration process.

3) Add the following configuration items to binfmt_misc
   (you should really have read binfmt_misc.txt now):
   support for Java applications:
     ':Java:M::\xca\xfe\xba\xbe::/usr/local/bin/javawrapper:'
   support for executable Jar files:
     ':ExecutableJAR:E::jar::/usr/local/bin/jarwrapper:'
   support for Java Applets:
     ':Applet:E::html::/usr/bin/appletviewer:'
   or the following, if you want to be more selective:
     ':Applet:M::<!--applet::/usr/bin/appletviewer:'

   Of course you have to fix the path names. The path/file names given in this
   document match the Debian 2.1 system. (i.e. jdk installed in /usr,
   custom wrappers from this document in /usr/local)

   Note, that for the more selective applet support you have to modify
   existing html-files to contain <!--applet--> in the first line
   ('<' has to be the first character!) to let this work!

   For the compiled Java programs you need a wrapper script like the
   following (this is because Java is broken in case of the filename
   handling), again fix the path names, both in the script and in the
   above given configuration string.

   You, too, need the little program after the script. Compile like
   gcc -O2 -o javaclassname javaclassname.c
   and stick it to /usr/local/bin.

   Both the javawrapper shellscript and the javaclassname program
   were supplied by Colin J. Watson <cjw44@cam.ac.uk>.

====================== Cut here ===================
#!/bin/bash
# /usr/local/bin/javawrapper - the wrapper for binfmt_misc/java

if [ -z "$1" ]; then
	exec 1>&2
	echo Usage: $0 class-file
	exit 1
fi

CLASS=$1
FQCLASS=`/usr/local/bin/javaclassname $1`
FQCLASSN=`echo $FQCLASS | sed -e 's/^.*\.\([^.]*\)$/\1/'`
FQCLASSP=`echo $FQCLASS | sed -e 's-\.-/-g' -e 's-^[^/]*$--' -e 's-/[^/]*$--'`

# for example:
# CLASS=Test.class
# FQCLASS=foo.bar.Test
# FQCLASSN=Test
# FQCLASSP=foo/bar

unset CLASSBASE

declare -i LINKLEVEL=0

while :; do
	if [ "`basename $CLASS .class`" == "$FQCLASSN" ]; then
		# See if this directory works straight off
		cd -L `dirname $CLASS`
		CLASSDIR=$PWD
		cd $OLDPWD
		if echo $CLASSDIR | grep -q "$FQCLASSP$"; then
			CLASSBASE=`echo $CLASSDIR | sed -e "s.$FQCLASSP$.."`
			break;
		fi
		# Try dereferencing the directory name
		cd -P `dirname $CLASS`
		CLASSDIR=$PWD
		cd $OLDPWD
		if echo $CLASSDIR | grep -q "$FQCLASSP$"; then
			CLASSBASE=`echo $CLASSDIR | sed -e "s.$FQCLASSP$.."`
			break;
		fi
		# If no other possible filename exists
		if [ ! -L $CLASS ]; then
			exec 1>&2
			echo $0:
			echo "  $CLASS should be in a" \
			     "directory tree called $FQCLASSP"
			exit 1
		fi
	fi
	if [ ! -L $CLASS ]; then break; fi
	# Go down one more level of symbolic links
	let LINKLEVEL+=1
	if [ $LINKLEVEL -gt 5 ]; then
		exec 1>&2
		echo $0:
		echo "  Too many symbolic links encountered"
		exit 1
	fi
	CLASS=`ls --color=no -l $CLASS | sed -e 's/^.* \([^ ]*\)$/\1/'`
done

if [ -z "$CLASSBASE" ]; then
	if [ -z "$FQCLASSP" ]; then
		GOODNAME=$FQCLASSN.class
	else
		GOODNAME=$FQCLASSP/$FQCLASSN.class
	fi
	exec 1>&2
	echo $0:
	echo "  $FQCLASS should be in a file called $GOODNAME"
	exit 1
fi

if ! echo $CLASSPATH | grep -q "^\(.*:\)*$CLASSBASE\(:.*\)*"; then
	# class is not in CLASSPATH, so prepend dir of class to CLASSPATH
	if [ -z "${CLASSPATH}" ] ; then
		export CLASSPATH=$CLASSBASE
	else
		export CLASSPATH=$CLASSBASE:$CLASSPATH
	fi
fi

shift
/usr/bin/java $FQCLASS "$@"
====================== Cut here ===================


====================== Cut here ===================
/* javaclassname.c
 *
 * Extracts the class name from a Java class file; intended for use in a Java
 * wrapper of the type supported by the binfmt_misc option in the Linux kernel.
 *
 * Copyright (C) 1999 Colin J. Watson <cjw44@cam.ac.uk>.
 *
 * This program is free software; you can redistribute it and/or modify
 * it under the terms of the GNU General Public License as published by
 * the Free Software Foundation; either version 2 of the License, or
 * (at your option) any later version.
 *
 * This program is distributed in the hope that it will be useful,
 * but WITHOUT ANY WARRANTY; without even the implied warranty of
 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
 * GNU General Public License for more details.
 *
 * You should have received a copy of the GNU General Public License
 * along with this program; if not, write to the Free Software
 * Foundation, Inc., 59 Temple Place, Suite 330, Boston, MA  02111-1307  USA
 */

#include <stdlib.h>
#include <stdio.h>
#include <stdarg.h>
#include <sys/types.h>

/* From Sun's Java VM Specification, as tag entries in the constant pool. */

#define CP_UTF8 1
#define CP_INTEGER 3
#define CP_FLOAT 4
#define CP_LONG 5
#define CP_DOUBLE 6
#define CP_CLASS 7
#define CP_STRING 8
#define CP_FIELDREF 9
#define CP_METHODREF 10
#define CP_INTERFACEMETHODREF 11
#define CP_NAMEANDTYPE 12
#define CP_METHODHANDLE 15
#define CP_METHODTYPE 16
#define CP_INVOKEDYNAMIC 18

/* Define some commonly used error messages */

#define seek_error() error("%s: Cannot seek\n", program)
#define corrupt_error() error("%s: Class file corrupt\n", program)
#define eof_error() error("%s: Unexpected end of file\n", program)
#define utf8_error() error("%s: Only ASCII 1-255 supported\n", program);

char *program;

long *pool;

u_int8_t read_8(FILE *classfile);
u_int16_t read_16(FILE *classfile);
void skip_constant(FILE *classfile, u_int16_t *cur);
void error(const char *format, ...);
int main(int argc, char **argv);

/* Reads in an unsigned 8-bit integer. */
u_int8_t read_8(FILE *classfile)
{
	int b = fgetc(classfile);
	if(b == EOF)
		eof_error();
	return (u_int8_t)b;
}

/* Reads in an unsigned 16-bit integer. */
u_int16_t read_16(FILE *classfile)
{
	int b1, b2;
	b1 = fgetc(classfile);
	if(b1 == EOF)
		eof_error();
	b2 = fgetc(classfile);
	if(b2 == EOF)
		eof_error();
	return (u_int16_t)((b1 << 8) | b2);
}

/* Reads in a value from the constant pool. */
void skip_constant(FILE *classfile, u_int16_t *cur)
{
	u_int16_t len;
	int seekerr = 1;
	pool[*cur] = ftell(classfile);
	switch(read_8(classfile))
	{
	case CP_UTF8:
		len = read_16(classfile);
		seekerr = fseek(classfile, len, SEEK_CUR);
		break;
	case CP_CLASS:
	case CP_STRING:
	case CP_METHODTYPE:
		seekerr = fseek(classfile, 2, SEEK_CUR);
		break;
	case CP_METHODHANDLE:
		seekerr = fseek(classfile, 3, SEEK_CUR);
		break;
	case CP_INTEGER:
	case CP_FLOAT:
	case CP_FIELDREF:
	case CP_METHODREF:
	case CP_INTERFACEMETHODREF:
	case CP_NAMEANDTYPE:
	case CP_INVOKEDYNAMIC:
		seekerr = fseek(classfile, 4, SEEK_CUR);
		break;
	case CP_LONG:
	case CP_DOUBLE:
		seekerr = fseek(classfile, 8, SEEK_CUR);
		++(*cur);
		break;
	default:
		corrupt_error();
	}
	if(seekerr)
		seek_error();
}

void error(const char *format, ...)
{
	va_list ap;
	va_start(ap, format);
	vfprintf(stderr, format, ap);
	va_end(ap);
	exit(1);
}

int main(int argc, char **argv)
{
	FILE *classfile;
	u_int16_t cp_count, i, this_class, classinfo_ptr;
	u_int8_t length;

	program = argv[0];

	if(!argv[1])
		error("%s: Missing input file\n", program);
	classfile = fopen(argv[1], "rb");
	if(!classfile)
		error("%s: Error opening %s\n", program, argv[1]);

	if(fseek(classfile, 8, SEEK_SET))  /* skip magic and version numbers */
		seek_error();
	cp_count = read_16(classfile);
	pool = calloc(cp_count, sizeof(long));
	if(!pool)
		error("%s: Out of memory for constant pool\n", program);

	for(i = 1; i < cp_count; ++i)
		skip_constant(classfile, &i);
	if(fseek(classfile, 2, SEEK_CUR))	/* skip access flags */
		seek_error();

	this_class = read_16(classfile);
	if(this_class < 1 || this_class >= cp_count)
		corrupt_error();
	if(!pool[this_class] || pool[this_class] == -1)
		corrupt_error();
	if(fseek(classfile, pool[this_class] + 1, SEEK_SET))
		seek_error();

	classinfo_ptr = read_16(classfile);
	if(classinfo_ptr < 1 || classinfo_ptr >= cp_count)
		corrupt_error();
	if(!pool[classinfo_ptr] || pool[classinfo_ptr] == -1)
		corrupt_error();
	if(fseek(classfile, pool[classinfo_ptr] + 1, SEEK_SET))
		seek_error();

	length = read_16(classfile);
	for(i = 0; i < length; ++i)
	{
		u_int8_t x = read_8(classfile);
		if((x & 0x80) || !x)
		{
			if((x & 0xE0) == 0xC0)
			{
				u_int8_t y = read_8(classfile);
				if((y & 0xC0) == 0x80)
				{
					int c = ((x & 0x1f) << 6) + (y & 0x3f);
					if(c) putchar(c);
					else utf8_error();
				}
				else utf8_error();
			}
			else utf8_error();
		}
		else if(x == '/') putchar('.');
		else putchar(x);
	}
	putchar('\n');
	free(pool);
	fclose(classfile);
	return 0;
}
====================== Cut here ===================


====================== Cut here ===================
#!/bin/bash
# /usr/local/java/bin/jarwrapper - the wrapper for binfmt_misc/jar

java -jar $1
====================== Cut here ===================


Now simply chmod +x the .class, .jar and/or .html files you want to execute.
To add a Java program to your path best put a symbolic link to the main
.class file into /usr/bin (or another place you like) omitting the .class
extension. The directory containing the original .class file will be
added to your CLASSPATH during execution.


To test your new setup, enter in the following simple Java app, and name
it "HelloWorld.java":

	class HelloWorld {
		public static void main(String args[]) {
			System.out.println("Hello World!");
		}
	}

Now compile the application with:
	javac HelloWorld.java

Set the executable permissions of the binary file, with:
	chmod 755 HelloWorld.class

And then execute it:
	./HelloWorld.class


To execute Java Jar files, simple chmod the *.jar files to include
the execution bit, then just do
       ./Application.jar


To execute Java Applets, simple chmod the *.html files to include
the execution bit, then just do
	./Applet.html


originally by Brian A. Lantz, brian@lantz.com
heavily edited for binfmt_misc by Richard Günther
new scripts by Colin J. Watson <cjw44@cam.ac.uk>
added executable Jar file support by Kurt Huwig <kurt@iku-netz.de>