aboutsummaryrefslogtreecommitdiffstats
blob: 0e307c94809a02586d59c13ca8c56985b632cfaf (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
Linux Magic System Request Key Hacks
Documentation for sysrq.c

*  What is the magic SysRq key?
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
It is a 'magical' key combo you can hit which the kernel will respond to
regardless of whatever else it is doing, unless it is completely locked up.

*  How do I enable the magic SysRq key?
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
You need to say "yes" to 'Magic SysRq key (CONFIG_MAGIC_SYSRQ)' when
configuring the kernel. When running a kernel with SysRq compiled in,
/proc/sys/kernel/sysrq controls the functions allowed to be invoked via
the SysRq key. The default value in this file is set by the
CONFIG_MAGIC_SYSRQ_DEFAULT_ENABLE config symbol, which itself defaults
to 1. Here is the list of possible values in /proc/sys/kernel/sysrq:
   0 - disable sysrq completely
   1 - enable all functions of sysrq
  >1 - bitmask of allowed sysrq functions (see below for detailed function
       description):
          2 =   0x2 - enable control of console logging level
          4 =   0x4 - enable control of keyboard (SAK, unraw)
          8 =   0x8 - enable debugging dumps of processes etc.
         16 =  0x10 - enable sync command
         32 =  0x20 - enable remount read-only
         64 =  0x40 - enable signalling of processes (term, kill, oom-kill)
        128 =  0x80 - allow reboot/poweroff
        256 = 0x100 - allow nicing of all RT tasks

You can set the value in the file by the following command:
    echo "number" >/proc/sys/kernel/sysrq

The number may be written here either as decimal or as hexadecimal
with the 0x prefix. CONFIG_MAGIC_SYSRQ_DEFAULT_ENABLE must always be
written in hexadecimal.

Note that the value of /proc/sys/kernel/sysrq influences only the invocation
via a keyboard. Invocation of any operation via /proc/sysrq-trigger is always
allowed (by a user with admin privileges).

*  How do I use the magic SysRq key?
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
On x86   - You press the key combo 'ALT-SysRq-<command key>'. Note - Some
           keyboards may not have a key labeled 'SysRq'. The 'SysRq' key is
           also known as the 'Print Screen' key. Also some keyboards cannot
	   handle so many keys being pressed at the same time, so you might
	   have better luck with "press Alt", "press SysRq", "release SysRq",
	   "press <command key>", release everything.

On SPARC - You press 'ALT-STOP-<command key>', I believe.

On the serial console (PC style standard serial ports only) -
           You send a BREAK, then within 5 seconds a command key. Sending
           BREAK twice is interpreted as a normal BREAK.

On PowerPC - Press 'ALT - Print Screen (or F13) - <command key>,  
             Print Screen (or F13) - <command key> may suffice.

On other - If you know of the key combos for other architectures, please
           let me know so I can add them to this section.

On all -  write a character to /proc/sysrq-trigger.  e.g.:

		echo t > /proc/sysrq-trigger

*  What are the 'command' keys?
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
'b'     - Will immediately reboot the system without syncing or unmounting
          your disks.

'c'	- Will perform a system crash by a NULL pointer dereference.
          A crashdump will be taken if configured.

'd'	- Shows all locks that are held.

'e'     - Send a SIGTERM to all processes, except for init.

'f'	- Will call oom_kill to kill a memory hog process.

'g'	- Used by kgdb (kernel debugger)

'h'     - Will display help (actually any other key than those listed
          here will display help. but 'h' is easy to remember :-)

'i'     - Send a SIGKILL to all processes, except for init.

'j'     - Forcibly "Just thaw it" - filesystems frozen by the FIFREEZE ioctl.

'k'     - Secure Access Key (SAK) Kills all programs on the current virtual
          console. NOTE: See important comments below in SAK section.

'l'     - Shows a stack backtrace for all active CPUs.

'm'     - Will dump current memory info to your console.

'n'	- Used to make RT tasks nice-able

'o'     - Will shut your system off (if configured and supported).

'p'     - Will dump the current registers and flags to your console.

'q'     - Will dump per CPU lists of all armed hrtimers (but NOT regular
          timer_list timers) and detailed information about all
          clockevent devices.

'r'     - Turns off keyboard raw mode and sets it to XLATE.

's'     - Will attempt to sync all mounted filesystems.

't'     - Will dump a list of current tasks and their information to your
          console.

'u'     - Will attempt to remount all mounted filesystems read-only.

'v'	- Forcefully restores framebuffer console
'v'	- Causes ETM buffer dump [ARM-specific]

'w'	- Dumps tasks that are in uninterruptable (blocked) state.

'x'	- Used by xmon interface on ppc/powerpc platforms.
          Show global PMU Registers on sparc64.

'y'	- Show global CPU Registers [SPARC-64 specific]

'z'	- Dump the ftrace buffer

'0'-'9' - Sets the console log level, controlling which kernel messages
          will be printed to your console. ('0', for example would make
          it so that only emergency messages like PANICs or OOPSes would
          make it to your console.)

*  Okay, so what can I use them for?
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
Well, unraw(r) is very handy when your X server or a svgalib program crashes.

sak(k) (Secure Access Key) is useful when you want to be sure there is no
trojan program running at console which could grab your password
when you would try to login. It will kill all programs on given console,
thus letting you make sure that the login prompt you see is actually
the one from init, not some trojan program.
IMPORTANT: In its true form it is not a true SAK like the one in a :IMPORTANT
IMPORTANT: c2 compliant system, and it should not be mistaken as   :IMPORTANT
IMPORTANT: such.                                                   :IMPORTANT
       It seems others find it useful as (System Attention Key) which is
useful when you want to exit a program that will not let you switch consoles.
(For example, X or a svgalib program.)

reboot(b) is good when you're unable to shut down. But you should also
sync(s) and umount(u) first.

crash(c) can be used to manually trigger a crashdump when the system is hung.
Note that this just triggers a crash if there is no dump mechanism available.

sync(s) is great when your system is locked up, it allows you to sync your
disks and will certainly lessen the chance of data loss and fscking. Note
that the sync hasn't taken place until you see the "OK" and "Done" appear
on the screen. (If the kernel is really in strife, you may not ever get the
OK or Done message...)

umount(u) is basically useful in the same ways as sync(s). I generally sync(s),
umount(u), then reboot(b) when my system locks. It's saved me many a fsck.
Again, the unmount (remount read-only) hasn't taken place until you see the
"OK" and "Done" message appear on the screen.

The loglevels '0'-'9' are useful when your console is being flooded with
kernel messages you do not want to see. Selecting '0' will prevent all but
the most urgent kernel messages from reaching your console. (They will
still be logged if syslogd/klogd are alive, though.)

term(e) and kill(i) are useful if you have some sort of runaway process you
are unable to kill any other way, especially if it's spawning other
processes.

"just thaw it(j)" is useful if your system becomes unresponsive due to a frozen
(probably root) filesystem via the FIFREEZE ioctl.

*  Sometimes SysRq seems to get 'stuck' after using it, what can I do?
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
That happens to me, also. I've found that tapping shift, alt, and control
on both sides of the keyboard, and hitting an invalid sysrq sequence again
will fix the problem. (i.e., something like alt-sysrq-z). Switching to another
virtual console (ALT+Fn) and then back again should also help.

*  I hit SysRq, but nothing seems to happen, what's wrong?
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
There are some keyboards that produce a different keycode for SysRq than the
pre-defined value of 99 (see KEY_SYSRQ in include/linux/input.h), or which
don't have a SysRq key at all. In these cases, run 'showkey -s' to find an
appropriate scancode sequence, and use 'setkeycodes <sequence> 99' to map
this sequence to the usual SysRq code (e.g., 'setkeycodes e05b 99'). It's
probably best to put this command in a boot script. Oh, and by the way, you
exit 'showkey' by not typing anything for ten seconds.

*  I want to add SysRQ key events to a module, how does it work?
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
In order to register a basic function with the table, you must first include
the header 'include/linux/sysrq.h', this will define everything else you need.
Next, you must create a sysrq_key_op struct, and populate it with A) the key
handler function you will use, B) a help_msg string, that will print when SysRQ
prints help, and C) an action_msg string, that will print right before your
handler is called. Your handler must conform to the prototype in 'sysrq.h'.

After the sysrq_key_op is created, you can call the kernel function
register_sysrq_key(int key, struct sysrq_key_op *op_p); this will
register the operation pointed to by 'op_p' at table key 'key',
if that slot in the table is blank. At module unload time, you must call
the function unregister_sysrq_key(int key, struct sysrq_key_op *op_p), which
will remove the key op pointed to by 'op_p' from the key 'key', if and only if
it is currently registered in that slot. This is in case the slot has been
overwritten since you registered it.

The Magic SysRQ system works by registering key operations against a key op
lookup table, which is defined in 'drivers/char/sysrq.c'. This key table has
a number of operations registered into it at compile time, but is mutable,
and 2 functions are exported for interface to it:
	register_sysrq_key and unregister_sysrq_key.
Of course, never ever leave an invalid pointer in the table. I.e., when
your module that called register_sysrq_key() exits, it must call
unregister_sysrq_key() to clean up the sysrq key table entry that it used.
Null pointers in the table are always safe. :)

If for some reason you feel the need to call the handle_sysrq function from
within a function called by handle_sysrq, you must be aware that you are in
a lock (you are also in an interrupt handler, which means don't sleep!), so
you must call __handle_sysrq_nolock instead.

*  When I hit a SysRq key combination only the header appears on the console?
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
Sysrq output is subject to the same console loglevel control as all
other console output.  This means that if the kernel was booted 'quiet'
as is common on distro kernels the output may not appear on the actual
console, even though it will appear in the dmesg buffer, and be accessible
via the dmesg command and to the consumers of /proc/kmsg.  As a specific
exception the header line from the sysrq command is passed to all console
consumers as if the current loglevel was maximum.  If only the header
is emitted it is almost certain that the kernel loglevel is too low.
Should you require the output on the console channel then you will need
to temporarily up the console loglevel using alt-sysrq-8 or:

    echo 8 > /proc/sysrq-trigger

Remember to return the loglevel to normal after triggering the sysrq
command you are interested in.

*  I have more questions, who can I ask?
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
Just ask them on the linux-kernel mailing list:
	linux-kernel@vger.kernel.org

*  Credits
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
Written by Mydraal <vulpyne@vulpyne.net>
Updated by Adam Sulmicki <adam@cfar.umd.edu>
Updated by Jeremy M. Dolan <jmd@turbogeek.org> 2001/01/28 10:15:59
Added to by Crutcher Dunnavant <crutcher+kernel@datastacks.com>