aboutsummaryrefslogtreecommitdiffstats
path: root/fs/attr.c
blob: ee697ddc6c2edc1018a4d1d75c903cfdb4dde4b9 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
/*
 *  linux/fs/attr.c
 *
 *  Copyright (C) 1991, 1992  Linus Torvalds
 *  changes by Thomas Schoebel-Theuer
 */

#include <linux/export.h>
#include <linux/time.h>
#include <linux/mm.h>
#include <linux/string.h>
#include <linux/capability.h>
#include <linux/fsnotify.h>
#include <linux/fcntl.h>
#include <linux/security.h>
#include <linux/evm.h>
#include <linux/ima.h>

/**
 * setattr_prepare - check if attribute changes to a dentry are allowed
 * @dentry:	dentry to check
 * @attr:	attributes to change
 *
 * Check if we are allowed to change the attributes contained in @attr
 * in the given dentry.  This includes the normal unix access permission
 * checks, as well as checks for rlimits and others. The function also clears
 * SGID bit from mode if user is not allowed to set it. Also file capabilities
 * and IMA extended attributes are cleared if ATTR_KILL_PRIV is set.
 *
 * Should be called as the first thing in ->setattr implementations,
 * possibly after taking additional locks.
 */
int setattr_prepare(struct dentry *dentry, struct iattr *attr)
{
	struct inode *inode = d_inode(dentry);
	unsigned int ia_valid = attr->ia_valid;

	/*
	 * First check size constraints.  These can't be overriden using
	 * ATTR_FORCE.
	 */
	if (ia_valid & ATTR_SIZE) {
		int error = inode_newsize_ok(inode, attr->ia_size);
		if (error)
			return error;
	}

	/* If force is set do it anyway. */
	if (ia_valid & ATTR_FORCE)
		goto kill_priv;

	/* Make sure a caller can chown. */
	if ((ia_valid & ATTR_UID) &&
	    (!uid_eq(current_fsuid(), inode->i_uid) ||
	     !uid_eq(attr->ia_uid, inode->i_uid)) &&
	    !capable_wrt_inode_uidgid(inode, CAP_CHOWN))
		return -EPERM;

	/* Make sure caller can chgrp. */
	if ((ia_valid & ATTR_GID) &&
	    (!uid_eq(current_fsuid(), inode->i_uid) ||
	    (!in_group_p(attr->ia_gid) && !gid_eq(attr->ia_gid, inode->i_gid))) &&
	    !capable_wrt_inode_uidgid(inode, CAP_CHOWN))
		return -EPERM;

	/* Make sure a caller can chmod. */
	if (ia_valid & ATTR_MODE) {
		if (!inode_owner_or_capable(inode))
			return -EPERM;
		/* Also check the setgid bit! */
		if (!in_group_p((ia_valid & ATTR_GID) ? attr->ia_gid :
				inode->i_gid) &&
		    !capable_wrt_inode_uidgid(inode, CAP_FSETID))
			attr->ia_mode &= ~S_ISGID;
	}

	/* Check for setting the inode time. */
	if (ia_valid & (ATTR_MTIME_SET | ATTR_ATIME_SET | ATTR_TIMES_SET)) {
		if (!inode_owner_or_capable(inode))
			return -EPERM;
	}

kill_priv:
	/* User has permission for the change */
	if (ia_valid & ATTR_KILL_PRIV) {
		int error;

		error = security_inode_killpriv(dentry);
		if (error)
			return error;
	}

	return 0;
}
EXPORT_SYMBOL(setattr_prepare);

/**
 * inode_newsize_ok - may this inode be truncated to a given size
 * @inode:	the inode to be truncated
 * @offset:	the new size to assign to the inode
 * @Returns:	0 on success, -ve errno on failure
 *
 * inode_newsize_ok must be called with i_mutex held.
 *
 * inode_newsize_ok will check filesystem limits and ulimits to check that the
 * new inode size is within limits. inode_newsize_ok will also send SIGXFSZ
 * when necessary. Caller must not proceed with inode size change if failure is
 * returned. @inode must be a file (not directory), with appropriate
 * permissions to allow truncate (inode_newsize_ok does NOT check these
 * conditions).
 */
int inode_newsize_ok(const struct inode *inode, loff_t offset)
{
	if (inode->i_size < offset) {
		unsigned long limit;

		limit = rlimit(RLIMIT_FSIZE);
		if (limit != RLIM_INFINITY && offset > limit)
			goto out_sig;
		if (offset > inode->i_sb->s_maxbytes)
			goto out_big;
	} else {
		/*
		 * truncation of in-use swapfiles is disallowed - it would
		 * cause subsequent swapout to scribble on the now-freed
		 * blocks.
		 */
		if (IS_SWAPFILE(inode))
			return -ETXTBSY;
	}

	return 0;
out_sig:
	send_sig(SIGXFSZ, current, 0);
out_big:
	return -EFBIG;
}
EXPORT_SYMBOL(inode_newsize_ok);

/**
 * setattr_copy - copy simple metadata updates into the generic inode
 * @inode:	the inode to be updated
 * @attr:	the new attributes
 *
 * setattr_copy must be called with i_mutex held.
 *
 * setattr_copy updates the inode's metadata with that specified
 * in attr. Noticeably missing is inode size update, which is more complex
 * as it requires pagecache updates.
 *
 * The inode is not marked as dirty after this operation. The rationale is
 * that for "simple" filesystems, the struct inode is the inode storage.
 * The caller is free to mark the inode dirty afterwards if needed.
 */
void setattr_copy(struct inode *inode, const struct iattr *attr)
{
	unsigned int ia_valid = attr->ia_valid;

	if (ia_valid & ATTR_UID)
		inode->i_uid = attr->ia_uid;
	if (ia_valid & ATTR_GID)
		inode->i_gid = attr->ia_gid;
	if (ia_valid & ATTR_ATIME)
		inode->i_atime = timespec_trunc(attr->ia_atime,
						inode->i_sb->s_time_gran);
	if (ia_valid & ATTR_MTIME)
		inode->i_mtime = timespec_trunc(attr->ia_mtime,
						inode->i_sb->s_time_gran);
	if (ia_valid & ATTR_CTIME)
		inode->i_ctime = timespec_trunc(attr->ia_ctime,
						inode->i_sb->s_time_gran);
	if (ia_valid & ATTR_MODE) {
		umode_t mode = attr->ia_mode;

		if (!in_group_p(inode->i_gid) &&
		    !capable_wrt_inode_uidgid(inode, CAP_FSETID))
			mode &= ~S_ISGID;
		inode->i_mode = mode;
	}
}
EXPORT_SYMBOL(setattr_copy);

/**
 * notify_change - modify attributes of a filesytem object
 * @dentry:	object affected
 * @iattr:	new attributes
 * @delegated_inode: returns inode, if the inode is delegated
 *
 * The caller must hold the i_mutex on the affected object.
 *
 * If notify_change discovers a delegation in need of breaking,
 * it will return -EWOULDBLOCK and return a reference to the inode in
 * delegated_inode.  The caller should then break the delegation and
 * retry.  Because breaking a delegation may take a long time, the
 * caller should drop the i_mutex before doing so.
 *
 * Alternatively, a caller may pass NULL for delegated_inode.  This may
 * be appropriate for callers that expect the underlying filesystem not
 * to be NFS exported.  Also, passing NULL is fine for callers holding
 * the file open for write, as there can be no conflicting delegation in
 * that case.
 */
int notify_change(struct dentry * dentry, struct iattr * attr, struct inode **delegated_inode)
{
	struct inode *inode = dentry->d_inode;
	umode_t mode = inode->i_mode;
	int error;
	struct timespec now;
	unsigned int ia_valid = attr->ia_valid;

	WARN_ON_ONCE(!mutex_is_locked(&inode->i_mutex));

	if (ia_valid & (ATTR_MODE | ATTR_UID | ATTR_GID | ATTR_TIMES_SET)) {
		if (IS_IMMUTABLE(inode) || IS_APPEND(inode))
			return -EPERM;
	}

	if ((ia_valid & ATTR_MODE)) {
		umode_t amode = attr->ia_mode;
		/* Flag setting protected by i_mutex */
		if (is_sxid(amode))
			inode->i_flags &= ~S_NOSEC;
	}

	now = current_fs_time(inode->i_sb);

	attr->ia_ctime = now;
	if (!(ia_valid & ATTR_ATIME_SET))
		attr->ia_atime = now;
	if (!(ia_valid & ATTR_MTIME_SET))
		attr->ia_mtime = now;
	if (ia_valid & ATTR_KILL_PRIV) {
		error = security_inode_need_killpriv(dentry);
		if (error < 0)
			return error;
		if (error == 0)
			ia_valid = attr->ia_valid &= ~ATTR_KILL_PRIV;
	}

	/*
	 * We now pass ATTR_KILL_S*ID to the lower level setattr function so
	 * that the function has the ability to reinterpret a mode change
	 * that's due to these bits. This adds an implicit restriction that
	 * no function will ever call notify_change with both ATTR_MODE and
	 * ATTR_KILL_S*ID set.
	 */
	if ((ia_valid & (ATTR_KILL_SUID|ATTR_KILL_SGID)) &&
	    (ia_valid & ATTR_MODE))
		BUG();

	if (ia_valid & ATTR_KILL_SUID) {
		if (mode & S_ISUID) {
			ia_valid = attr->ia_valid |= ATTR_MODE;
			attr->ia_mode = (inode->i_mode & ~S_ISUID);
		}
	}
	if (ia_valid & ATTR_KILL_SGID) {
		if ((mode & (S_ISGID | S_IXGRP)) == (S_ISGID | S_IXGRP)) {
			if (!(ia_valid & ATTR_MODE)) {
				ia_valid = attr->ia_valid |= ATTR_MODE;
				attr->ia_mode = inode->i_mode;
			}
			attr->ia_mode &= ~S_ISGID;
		}
	}
	if (!(attr->ia_valid & ~(ATTR_KILL_SUID | ATTR_KILL_SGID)))
		return 0;

	error = security_inode_setattr(dentry, attr);
	if (error)
		return error;
	error = try_break_deleg(inode, delegated_inode);
	if (error)
		return error;

	if (inode->i_op->setattr)
		error = inode->i_op->setattr(dentry, attr);
	else
		error = simple_setattr(dentry, attr);

	if (!error) {
		fsnotify_change(dentry, ia_valid);
		ima_inode_post_setattr(dentry);
		evm_inode_post_setattr(dentry, ia_valid);
	}

	return error;
}
EXPORT_SYMBOL(notify_change);