aboutsummaryrefslogtreecommitdiffstats
blob: 8b6c083e68a7338c4b5eee9938cc73f40c7faa19 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
317
318
319
320
321
322
323
324
325
326
327
328
329
330
331
332
333
334
335
336
337
338
339
340
341
342
343
344
345
346
347
348
349
350
351
352
353
354
355
356
357
358
359
360
361
362
363
364
365
366
367
368
369
370
371
372
373
374
375
376
377
378
379
380
381
382
383
384
385
386
387
388
389
390
391
392
393
394
395
396
397
398
399
400
/* Credentials management - see Documentation/security/credentials.txt
 *
 * Copyright (C) 2008 Red Hat, Inc. All Rights Reserved.
 * Written by David Howells (dhowells@redhat.com)
 *
 * This program is free software; you can redistribute it and/or
 * modify it under the terms of the GNU General Public Licence
 * as published by the Free Software Foundation; either version
 * 2 of the Licence, or (at your option) any later version.
 */

#ifndef _LINUX_CRED_H
#define _LINUX_CRED_H

#include <linux/capability.h>
#include <linux/init.h>
#include <linux/key.h>
#include <linux/selinux.h>
#include <linux/atomic.h>
#include <linux/uidgid.h>

struct user_struct;
struct cred;
struct inode;

/*
 * COW Supplementary groups list
 */
#define NGROUPS_SMALL		32
#define NGROUPS_PER_BLOCK	((unsigned int)(PAGE_SIZE / sizeof(kgid_t)))

struct group_info {
	atomic_t	usage;
	int		ngroups;
	int		nblocks;
	kgid_t		small_block[NGROUPS_SMALL];
	kgid_t		*blocks[0];
};

/**
 * get_group_info - Get a reference to a group info structure
 * @group_info: The group info to reference
 *
 * This gets a reference to a set of supplementary groups.
 *
 * If the caller is accessing a task's credentials, they must hold the RCU read
 * lock when reading.
 */
static inline struct group_info *get_group_info(struct group_info *gi)
{
	atomic_inc(&gi->usage);
	return gi;
}

/**
 * put_group_info - Release a reference to a group info structure
 * @group_info: The group info to release
 */
#define put_group_info(group_info)			\
do {							\
	if (atomic_dec_and_test(&(group_info)->usage))	\
		groups_free(group_info);		\
} while (0)

extern struct group_info init_groups;
#ifdef CONFIG_MULTIUSER
extern struct group_info *groups_alloc(int);
extern void groups_free(struct group_info *);

extern int in_group_p(kgid_t);
extern int in_egroup_p(kgid_t);
#else
static inline void groups_free(struct group_info *group_info)
{
}

static inline int in_group_p(kgid_t grp)
{
        return 1;
}
static inline int in_egroup_p(kgid_t grp)
{
        return 1;
}
#endif
extern int set_current_groups(struct group_info *);
extern void set_groups(struct cred *, struct group_info *);
extern int groups_search(const struct group_info *, kgid_t);
extern bool may_setgroups(void);

/* access the groups "array" with this macro */
#define GROUP_AT(gi, i) \
	((gi)->blocks[(i) / NGROUPS_PER_BLOCK][(i) % NGROUPS_PER_BLOCK])

/*
 * The security context of a task
 *
 * The parts of the context break down into two categories:
 *
 *  (1) The objective context of a task.  These parts are used when some other
 *	task is attempting to affect this one.
 *
 *  (2) The subjective context.  These details are used when the task is acting
 *	upon another object, be that a file, a task, a key or whatever.
 *
 * Note that some members of this structure belong to both categories - the
 * LSM security pointer for instance.
 *
 * A task has two security pointers.  task->real_cred points to the objective
 * context that defines that task's actual details.  The objective part of this
 * context is used whenever that task is acted upon.
 *
 * task->cred points to the subjective context that defines the details of how
 * that task is going to act upon another object.  This may be overridden
 * temporarily to point to another security context, but normally points to the
 * same context as task->real_cred.
 */
struct cred {
	atomic_t	usage;
#ifdef CONFIG_DEBUG_CREDENTIALS
	atomic_t	subscribers;	/* number of processes subscribed */
	void		*put_addr;
	unsigned	magic;
#define CRED_MAGIC	0x43736564
#define CRED_MAGIC_DEAD	0x44656144
#endif
	kuid_t		uid;		/* real UID of the task */
	kgid_t		gid;		/* real GID of the task */
	kuid_t		suid;		/* saved UID of the task */
	kgid_t		sgid;		/* saved GID of the task */
	kuid_t		euid;		/* effective UID of the task */
	kgid_t		egid;		/* effective GID of the task */
	kuid_t		fsuid;		/* UID for VFS ops */
	kgid_t		fsgid;		/* GID for VFS ops */
	unsigned	securebits;	/* SUID-less security management */
	kernel_cap_t	cap_inheritable; /* caps our children can inherit */
	kernel_cap_t	cap_permitted;	/* caps we're permitted */
	kernel_cap_t	cap_effective;	/* caps we can actually use */
	kernel_cap_t	cap_bset;	/* capability bounding set */
#ifdef CONFIG_KEYS
	unsigned char	jit_keyring;	/* default keyring to attach requested
					 * keys to */
	struct key __rcu *session_keyring; /* keyring inherited over fork */
	struct key	*process_keyring; /* keyring private to this process */
	struct key	*thread_keyring; /* keyring private to this thread */
	struct key	*request_key_auth; /* assumed request_key authority */
#endif
#ifdef CONFIG_SECURITY
	void		*security;	/* subjective LSM security */
#endif
	struct user_struct *user;	/* real user ID subscription */
	struct user_namespace *user_ns; /* user_ns the caps and keyrings are relative to. */
	struct group_info *group_info;	/* supplementary groups for euid/fsgid */
	struct rcu_head	rcu;		/* RCU deletion hook */
};

extern void __put_cred(struct cred *);
extern void exit_creds(struct task_struct *);
extern int copy_creds(struct task_struct *, unsigned long);
extern const struct cred *get_task_cred(struct task_struct *);
extern struct cred *cred_alloc_blank(void);
extern struct cred *prepare_creds(void);
extern struct cred *prepare_exec_creds(void);
extern int commit_creds(struct cred *);
extern void abort_creds(struct cred *);
extern const struct cred *override_creds(const struct cred *);
extern void revert_creds(const struct cred *);
extern struct cred *prepare_kernel_cred(struct task_struct *);
extern int change_create_files_as(struct cred *, struct inode *);
extern int set_security_override(struct cred *, u32);
extern int set_security_override_from_ctx(struct cred *, const char *);
extern int set_create_files_as(struct cred *, struct inode *);
extern void __init cred_init(void);

/*
 * check for validity of credentials
 */
#ifdef CONFIG_DEBUG_CREDENTIALS
extern void __invalid_creds(const struct cred *, const char *, unsigned);
extern void __validate_process_creds(struct task_struct *,
				     const char *, unsigned);

extern bool creds_are_invalid(const struct cred *cred);

static inline void __validate_creds(const struct cred *cred,
				    const char *file, unsigned line)
{
	if (unlikely(creds_are_invalid(cred)))
		__invalid_creds(cred, file, line);
}

#define validate_creds(cred)				\
do {							\
	__validate_creds((cred), __FILE__, __LINE__);	\
} while(0)

#define validate_process_creds()				\
do {								\
	__validate_process_creds(current, __FILE__, __LINE__);	\
} while(0)

extern void validate_creds_for_do_exit(struct task_struct *);
#else
static inline void validate_creds(const struct cred *cred)
{
}
static inline void validate_creds_for_do_exit(struct task_struct *tsk)
{
}
static inline void validate_process_creds(void)
{
}
#endif

/**
 * get_new_cred - Get a reference on a new set of credentials
 * @cred: The new credentials to reference
 *
 * Get a reference on the specified set of new credentials.  The caller must
 * release the reference.
 */
static inline struct cred *get_new_cred(struct cred *cred)
{
	atomic_inc(&cred->usage);
	return cred;
}

/**
 * get_cred - Get a reference on a set of credentials
 * @cred: The credentials to reference
 *
 * Get a reference on the specified set of credentials.  The caller must
 * release the reference.
 *
 * This is used to deal with a committed set of credentials.  Although the
 * pointer is const, this will temporarily discard the const and increment the
 * usage count.  The purpose of this is to attempt to catch at compile time the
 * accidental alteration of a set of credentials that should be considered
 * immutable.
 */
static inline const struct cred *get_cred(const struct cred *cred)
{
	struct cred *nonconst_cred = (struct cred *) cred;
	validate_creds(cred);
	return get_new_cred(nonconst_cred);
}

/**
 * put_cred - Release a reference to a set of credentials
 * @cred: The credentials to release
 *
 * Release a reference to a set of credentials, deleting them when the last ref
 * is released.
 *
 * This takes a const pointer to a set of credentials because the credentials
 * on task_struct are attached by const pointers to prevent accidental
 * alteration of otherwise immutable credential sets.
 */
static inline void put_cred(const struct cred *_cred)
{
	struct cred *cred = (struct cred *) _cred;

	validate_creds(cred);
	if (atomic_dec_and_test(&(cred)->usage))
		__put_cred(cred);
}

/**
 * current_cred - Access the current task's subjective credentials
 *
 * Access the subjective credentials of the current task.  RCU-safe,
 * since nobody else can modify it.
 */
#define current_cred() \
	rcu_dereference_protected(current->cred, 1)

/**
 * current_real_cred - Access the current task's objective credentials
 *
 * Access the objective credentials of the current task.  RCU-safe,
 * since nobody else can modify it.
 */
#define current_real_cred() \
	rcu_dereference_protected(current->real_cred, 1)

/**
 * __task_cred - Access a task's objective credentials
 * @task: The task to query
 *
 * Access the objective credentials of a task.  The caller must hold the RCU
 * readlock.
 *
 * The result of this function should not be passed directly to get_cred();
 * rather get_task_cred() should be used instead.
 */
#define __task_cred(task)	\
	rcu_dereference((task)->real_cred)

/**
 * get_current_cred - Get the current task's subjective credentials
 *
 * Get the subjective credentials of the current task, pinning them so that
 * they can't go away.  Accessing the current task's credentials directly is
 * not permitted.
 */
#define get_current_cred()				\
	(get_cred(current_cred()))

/**
 * get_current_user - Get the current task's user_struct
 *
 * Get the user record of the current task, pinning it so that it can't go
 * away.
 */
#define get_current_user()				\
({							\
	struct user_struct *__u;			\
	const struct cred *__cred;			\
	__cred = current_cred();			\
	__u = get_uid(__cred->user);			\
	__u;						\
})

/**
 * get_current_groups - Get the current task's supplementary group list
 *
 * Get the supplementary group list of the current task, pinning it so that it
 * can't go away.
 */
#define get_current_groups()				\
({							\
	struct group_info *__groups;			\
	const struct cred *__cred;			\
	__cred = current_cred();			\
	__groups = get_group_info(__cred->group_info);	\
	__groups;					\
})

#define task_cred_xxx(task, xxx)			\
({							\
	__typeof__(((struct cred *)NULL)->xxx) ___val;	\
	rcu_read_lock();				\
	___val = __task_cred((task))->xxx;		\
	rcu_read_unlock();				\
	___val;						\
})

#define task_uid(task)		(task_cred_xxx((task), uid))
#define task_euid(task)		(task_cred_xxx((task), euid))

#define current_cred_xxx(xxx)			\
({						\
	current_cred()->xxx;			\
})

#define current_uid()		(current_cred_xxx(uid))
#define current_gid()		(current_cred_xxx(gid))
#define current_euid()		(current_cred_xxx(euid))
#define current_egid()		(current_cred_xxx(egid))
#define current_suid()		(current_cred_xxx(suid))
#define current_sgid()		(current_cred_xxx(sgid))
#define current_fsuid() 	(current_cred_xxx(fsuid))
#define current_fsgid() 	(current_cred_xxx(fsgid))
#define current_cap()		(current_cred_xxx(cap_effective))
#define current_user()		(current_cred_xxx(user))
#define current_security()	(current_cred_xxx(security))

extern struct user_namespace init_user_ns;
#ifdef CONFIG_USER_NS
#define current_user_ns()	(current_cred_xxx(user_ns))
#else
#define current_user_ns()	(&init_user_ns)
#endif


#define current_uid_gid(_uid, _gid)		\
do {						\
	const struct cred *__cred;		\
	__cred = current_cred();		\
	*(_uid) = __cred->uid;			\
	*(_gid) = __cred->gid;			\
} while(0)

#define current_euid_egid(_euid, _egid)		\
do {						\
	const struct cred *__cred;		\
	__cred = current_cred();		\
	*(_euid) = __cred->euid;		\
	*(_egid) = __cred->egid;		\
} while(0)

#define current_fsuid_fsgid(_fsuid, _fsgid)	\
do {						\
	const struct cred *__cred;		\
	__cred = current_cred();		\
	*(_fsuid) = __cred->fsuid;		\
	*(_fsgid) = __cred->fsgid;		\
} while(0)

#endif /* _LINUX_CRED_H */