aboutsummaryrefslogtreecommitdiffstats
blob: 5e386444194b00302d07cbb744aca813716ee64d (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
317
318
319
320
321
322
323
324
325
326
327
328
329
330
331
332
333
334
335
336
337
338
339
340
341
342
343
344
345
346
347
348
349
350
351
352
353
354
355
356
357
358
359
360
361
362
363
364
365
366
367
368
369
370
371
372
373
374
375
376
377
378
379
380
381
382
383
384
385
386
387
388
389
390
391
392
393
#ifndef _LINUX_INIT_H
#define _LINUX_INIT_H

#include <linux/compiler.h>
#include <linux/types.h>

/* These macros are used to mark some functions or 
 * initialized data (doesn't apply to uninitialized data)
 * as `initialization' functions. The kernel can take this
 * as hint that the function is used only during the initialization
 * phase and free up used memory resources after
 *
 * Usage:
 * For functions:
 * 
 * You should add __init immediately before the function name, like:
 *
 * static void __init initme(int x, int y)
 * {
 *    extern int z; z = x * y;
 * }
 *
 * If the function has a prototype somewhere, you can also add
 * __init between closing brace of the prototype and semicolon:
 *
 * extern int initialize_foobar_device(int, int, int) __init;
 *
 * For initialized data:
 * You should insert __initdata or __initconst between the variable name
 * and equal sign followed by value, e.g.:
 *
 * static int init_variable __initdata = 0;
 * static const char linux_logo[] __initconst = { 0x32, 0x36, ... };
 *
 * Don't forget to initialize data not at file scope, i.e. within a function,
 * as gcc otherwise puts the data into the bss section and not into the init
 * section.
 */

/* These are for everybody (although not all archs will actually
   discard it in modules) */
#define __init		__section(.init.text) __cold notrace
#define __initdata	__section(.init.data)
#define __initconst	__constsection(.init.rodata)
#define __exitdata	__section(.exit.data)
#define __exit_call	__used __section(.exitcall.exit)

/*
 * Some architecture have tool chains which do not handle rodata attributes
 * correctly. For those disable special sections for const, so that other
 * architectures can annotate correctly.
 */
#ifdef CONFIG_BROKEN_RODATA
#define __constsection(x)
#else
#define __constsection(x) __section(x)
#endif

/*
 * modpost check for section mismatches during the kernel build.
 * A section mismatch happens when there are references from a
 * code or data section to an init section (both code or data).
 * The init sections are (for most archs) discarded by the kernel
 * when early init has completed so all such references are potential bugs.
 * For exit sections the same issue exists.
 *
 * The following markers are used for the cases where the reference to
 * the *init / *exit section (code or data) is valid and will teach
 * modpost not to issue a warning.  Intended semantics is that a code or
 * data tagged __ref* can reference code or data from init section without
 * producing a warning (of course, no warning does not mean code is
 * correct, so optimally document why the __ref is needed and why it's OK).
 *
 * The markers follow same syntax rules as __init / __initdata.
 */
#define __ref            __section(.ref.text) noinline
#define __refdata        __section(.ref.data)
#define __refconst       __constsection(.ref.rodata)

/* compatibility defines */
#define __init_refok     __ref
#define __initdata_refok __refdata
#define __exit_refok     __ref


#ifdef MODULE
#define __exitused
#else
#define __exitused  __used
#endif

#define __exit          __section(.exit.text) __exitused __cold notrace

/* temporary, until all users are removed */
#define __cpuinit
#define __cpuinitdata
#define __cpuinitconst
#define __cpuexit
#define __cpuexitdata
#define __cpuexitconst

/* Used for MEMORY_HOTPLUG */
#define __meminit        __section(.meminit.text) __cold notrace
#define __meminitdata    __section(.meminit.data)
#define __meminitconst   __constsection(.meminit.rodata)
#define __memexit        __section(.memexit.text) __exitused __cold notrace
#define __memexitdata    __section(.memexit.data)
#define __memexitconst   __constsection(.memexit.rodata)

/* For assembly routines */
#define __HEAD		.section	".head.text","ax"
#define __INIT		.section	".init.text","ax"
#define __FINIT		.previous

#define __INITDATA	.section	".init.data","aw",%progbits
#define __INITRODATA	.section	".init.rodata","a",%progbits
#define __FINITDATA	.previous

/* temporary, until all users are removed */
#define __CPUINIT

#define __MEMINIT        .section	".meminit.text", "ax"
#define __MEMINITDATA    .section	".meminit.data", "aw"
#define __MEMINITRODATA  .section	".meminit.rodata", "a"

/* silence warnings when references are OK */
#define __REF            .section       ".ref.text", "ax"
#define __REFDATA        .section       ".ref.data", "aw"
#define __REFCONST       .section       ".ref.rodata", "a"

#ifndef __ASSEMBLY__
/*
 * Used for initialization calls..
 */
typedef int (*initcall_t)(void);
typedef void (*exitcall_t)(void);

extern initcall_t __con_initcall_start[], __con_initcall_end[];
extern initcall_t __security_initcall_start[], __security_initcall_end[];

/* Used for contructor calls. */
typedef void (*ctor_fn_t)(void);

/* Defined in init/main.c */
extern int do_one_initcall(initcall_t fn);
extern char __initdata boot_command_line[];
extern char *saved_command_line;
extern unsigned int reset_devices;

/* used by init/main.c */
void setup_arch(char **);
void prepare_namespace(void);
void __init load_default_modules(void);
int __init init_rootfs(void);

#ifdef CONFIG_DEBUG_RODATA
void mark_rodata_ro(void);
#endif

extern void (*late_time_init)(void);

extern bool initcall_debug;

#endif
  
#ifndef MODULE

#ifndef __ASSEMBLY__

#ifdef CONFIG_LTO
/* Work around a LTO gcc problem: when there is no reference to a variable
 * in a module it will be moved to the end of the program. This causes
 * reordering of initcalls which the kernel does not like.
 * Add a dummy reference function to avoid this. The function is
 * deleted by the linker.
 */
#define LTO_REFERENCE_INITCALL(x) \
	; /* yes this is needed */			\
	static __used __exit void *reference_##x(void)	\
	{						\
		return &x;				\
	}
#else
#define LTO_REFERENCE_INITCALL(x)
#endif

/* initcalls are now grouped by functionality into separate 
 * subsections. Ordering inside the subsections is determined
 * by link order. 
 * For backwards compatibility, initcall() puts the call in 
 * the device init subsection.
 *
 * The `id' arg to __define_initcall() is needed so that multiple initcalls
 * can point at the same handler without causing duplicate-symbol build errors.
 */

#define __define_initcall(fn, id) \
	static initcall_t __initcall_##fn##id __used \
	__attribute__((__section__(".initcall" #id ".init"))) = fn; \
	LTO_REFERENCE_INITCALL(__initcall_##fn##id)

/*
 * Early initcalls run before initializing SMP.
 *
 * Only for built-in code, not modules.
 */
#define early_initcall(fn)		__define_initcall(fn, early)

/*
 * A "pure" initcall has no dependencies on anything else, and purely
 * initializes variables that couldn't be statically initialized.
 *
 * This only exists for built-in code, not for modules.
 * Keep main.c:initcall_level_names[] in sync.
 */
#define pure_initcall(fn)		__define_initcall(fn, 0)

#define core_initcall(fn)		__define_initcall(fn, 1)
#define core_initcall_sync(fn)		__define_initcall(fn, 1s)
#define postcore_initcall(fn)		__define_initcall(fn, 2)
#define postcore_initcall_sync(fn)	__define_initcall(fn, 2s)
#define arch_initcall(fn)		__define_initcall(fn, 3)
#define arch_initcall_sync(fn)		__define_initcall(fn, 3s)
#define subsys_initcall(fn)		__define_initcall(fn, 4)
#define subsys_initcall_sync(fn)	__define_initcall(fn, 4s)
#define fs_initcall(fn)			__define_initcall(fn, 5)
#define fs_initcall_sync(fn)		__define_initcall(fn, 5s)
#define rootfs_initcall(fn)		__define_initcall(fn, rootfs)
#define device_initcall(fn)		__define_initcall(fn, 6)
#define device_initcall_sync(fn)	__define_initcall(fn, 6s)
#define late_initcall(fn)		__define_initcall(fn, 7)
#define late_initcall_sync(fn)		__define_initcall(fn, 7s)

#define __initcall(fn) device_initcall(fn)

#define __exitcall(fn) \
	static exitcall_t __exitcall_##fn __exit_call = fn

#define console_initcall(fn) \
	static initcall_t __initcall_##fn \
	__used __section(.con_initcall.init) = fn

#define security_initcall(fn) \
	static initcall_t __initcall_##fn \
	__used __section(.security_initcall.init) = fn

struct obs_kernel_param {
	const char *str;
	int (*setup_func)(char *);
	int early;
};

/*
 * Only for really core code.  See moduleparam.h for the normal way.
 *
 * Force the alignment so the compiler doesn't space elements of the
 * obs_kernel_param "array" too far apart in .init.setup.
 */
#define __setup_param(str, unique_id, fn, early)			\
	static const char __setup_str_##unique_id[] __initconst		\
		__aligned(1) = str; 					\
	static struct obs_kernel_param __setup_##unique_id		\
		__used __section(.init.setup)				\
		__attribute__((aligned((sizeof(long)))))		\
		= { __setup_str_##unique_id, fn, early }

#define __setup(str, fn)						\
	__setup_param(str, fn, fn, 0)

/*
 * NOTE: fn is as per module_param, not __setup!
 * Emits warning if fn returns non-zero.
 */
#define early_param(str, fn)						\
	__setup_param(str, fn, fn, 1)

#define early_param_on_off(str_on, str_off, var, config)		\
									\
	int var = IS_ENABLED(config);					\
									\
	static int __init parse_##var##_on(char *arg)			\
	{								\
		var = 1;						\
		return 0;						\
	}								\
	__setup_param(str_on, parse_##var##_on, parse_##var##_on, 1);	\
									\
	static int __init parse_##var##_off(char *arg)			\
	{								\
		var = 0;						\
		return 0;						\
	}								\
	__setup_param(str_off, parse_##var##_off, parse_##var##_off, 1)

/* Relies on boot_command_line being set */
void __init parse_early_param(void);
void __init parse_early_options(char *cmdline);
#endif /* __ASSEMBLY__ */

/**
 * module_init() - driver initialization entry point
 * @x: function to be run at kernel boot time or module insertion
 * 
 * module_init() will either be called during do_initcalls() (if
 * builtin) or at module insertion time (if a module).  There can only
 * be one per module.
 */
#define module_init(x)	__initcall(x);

/**
 * module_exit() - driver exit entry point
 * @x: function to be run when driver is removed
 * 
 * module_exit() will wrap the driver clean-up code
 * with cleanup_module() when used with rmmod when
 * the driver is a module.  If the driver is statically
 * compiled into the kernel, module_exit() has no effect.
 * There can only be one per module.
 */
#define module_exit(x)	__exitcall(x);

#else /* MODULE */

/*
 * In most cases loadable modules do not need custom
 * initcall levels. There are still some valid cases where
 * a driver may be needed early if built in, and does not
 * matter when built as a loadable module. Like bus
 * snooping debug drivers.
 */
#define early_initcall(fn)		module_init(fn)
#define core_initcall(fn)		module_init(fn)
#define core_initcall_sync(fn)		module_init(fn)
#define postcore_initcall(fn)		module_init(fn)
#define postcore_initcall_sync(fn)	module_init(fn)
#define arch_initcall(fn)		module_init(fn)
#define subsys_initcall(fn)		module_init(fn)
#define subsys_initcall_sync(fn)	module_init(fn)
#define fs_initcall(fn)			module_init(fn)
#define fs_initcall_sync(fn)		module_init(fn)
#define rootfs_initcall(fn)		module_init(fn)
#define device_initcall(fn)		module_init(fn)
#define device_initcall_sync(fn)	module_init(fn)
#define late_initcall(fn)		module_init(fn)
#define late_initcall_sync(fn)		module_init(fn)

#define console_initcall(fn)		module_init(fn)
#define security_initcall(fn)		module_init(fn)

/* Each module must use one module_init(). */
#define module_init(initfn)					\
	static inline initcall_t __inittest(void)		\
	{ return initfn; }					\
	int init_module(void) __attribute__((alias(#initfn)));

/* This is only required if you want to be unloadable. */
#define module_exit(exitfn)					\
	static inline exitcall_t __exittest(void)		\
	{ return exitfn; }					\
	void cleanup_module(void) __attribute__((alias(#exitfn)));

#define __setup_param(str, unique_id, fn)	/* nothing */
#define __setup(str, func) 			/* nothing */
#endif

/* Data marked not to be saved by software suspend */
#define __nosavedata __section(.data..nosave)

/* This means "can be init if no module support, otherwise module load
   may call it." */
#ifdef CONFIG_MODULES
#define __init_or_module
#define __initdata_or_module
#define __initconst_or_module
#define __INIT_OR_MODULE	.text
#define __INITDATA_OR_MODULE	.data
#define __INITRODATA_OR_MODULE	.section ".rodata","a",%progbits
#else
#define __init_or_module __init
#define __initdata_or_module __initdata
#define __initconst_or_module __initconst
#define __INIT_OR_MODULE __INIT
#define __INITDATA_OR_MODULE __INITDATA
#define __INITRODATA_OR_MODULE __INITRODATA
#endif /*CONFIG_MODULES*/

#ifdef MODULE
#define __exit_p(x) x
#else
#define __exit_p(x) NULL
#endif

#endif /* _LINUX_INIT_H */