aboutsummaryrefslogtreecommitdiffstats
blob: 5d87f810a3b747d028c47dc9c70264c6eccd6cc0 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
#ifndef _PPP_CHANNEL_H_
#define _PPP_CHANNEL_H_
/*
 * Definitions for the interface between the generic PPP code
 * and a PPP channel.
 *
 * A PPP channel provides a way for the generic PPP code to send
 * and receive packets over some sort of communications medium.
 * Packets are stored in sk_buffs and have the 2-byte PPP protocol
 * number at the start, but not the address and control bytes.
 *
 * Copyright 1999 Paul Mackerras.
 *
 *  This program is free software; you can redistribute it and/or
 *  modify it under the terms of the GNU General Public License
 *  as published by the Free Software Foundation; either version
 *  2 of the License, or (at your option) any later version.
 *
 * ==FILEVERSION 20000322==
 */

#include <linux/list.h>
#include <linux/skbuff.h>
#include <linux/poll.h>
#include <net/net_namespace.h>

struct ppp_channel;

struct ppp_channel_ops {
	/* Send a packet (or multilink fragment) on this channel.
	   Returns 1 if it was accepted, 0 if not. */
	int	(*start_xmit)(struct ppp_channel *, struct sk_buff *);
	/* Handle an ioctl call that has come in via /dev/ppp. */
	int	(*ioctl)(struct ppp_channel *, unsigned int, unsigned long);
};

struct ppp_channel {
	void		*private;	/* channel private data */
	const struct ppp_channel_ops *ops; /* operations for this channel */
	int		mtu;		/* max transmit packet size */
	int		hdrlen;		/* amount of headroom channel needs */
	void		*ppp;		/* opaque to channel */
	int		speed;		/* transfer rate (bytes/second) */
	/* the following is not used at present */
	int		latency;	/* overhead time in milliseconds */
};

#ifdef __KERNEL__
/* Called by the channel when it can send some more data. */
extern void ppp_output_wakeup(struct ppp_channel *);

/* Called by the channel to process a received PPP packet.
   The packet should have just the 2-byte PPP protocol header. */
extern void ppp_input(struct ppp_channel *, struct sk_buff *);

/* Called by the channel when an input error occurs, indicating
   that we may have missed a packet. */
extern void ppp_input_error(struct ppp_channel *, int code);

/* Attach a channel to a given PPP unit in specified net. */
extern int ppp_register_net_channel(struct net *, struct ppp_channel *);

/* Attach a channel to a given PPP unit. */
extern int ppp_register_channel(struct ppp_channel *);

/* Detach a channel from its PPP unit (e.g. on hangup). */
extern void ppp_unregister_channel(struct ppp_channel *);

/* Get the channel number for a channel */
extern int ppp_channel_index(struct ppp_channel *);

/* Get the unit number associated with a channel, or -1 if none */
extern int ppp_unit_number(struct ppp_channel *);

/* Get the device name associated with a channel, or NULL if none */
extern char *ppp_dev_name(struct ppp_channel *);

/*
 * SMP locking notes:
 * The channel code must ensure that when it calls ppp_unregister_channel,
 * nothing is executing in any of the procedures above, for that
 * channel.  The generic layer will ensure that nothing is executing
 * in the start_xmit and ioctl routines for the channel by the time
 * that ppp_unregister_channel returns.
 */

#endif /* __KERNEL__ */
#endif