1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
|
/*
* Texas Instruments System Control Interface Protocol
*
* Copyright (C) 2015 Texas Instruments Incorporated - http://www.ti.com/
* Nishanth Menon
*
* This program is free software; you can redistribute it and/or modify
* it under the terms of the GNU General Public License version 2 as
* published by the Free Software Foundation.
*
* This program is distributed "as is" WITHOUT ANY WARRANTY of any
* kind, whether express or implied; without even the implied warranty
* of MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
* GNU General Public License for more details.
*/
#ifndef __TISCI_PROTOCOL_H
#define __TISCI_PROTOCOL_H
/**
* struct ti_sci_version_info - version information structure
* @abi_major: Major ABI version. Change here implies risk of backward
* compatibility break.
* @abi_minor: Minor ABI version. Change here implies new feature addition,
* or compatible change in ABI.
* @firmware_revision: Firmware revision (not usually used).
* @firmware_description: Firmware description (not usually used).
*/
struct ti_sci_version_info {
u8 abi_major;
u8 abi_minor;
u16 firmware_revision;
char firmware_description[32];
};
struct ti_sci_handle;
/**
* struct ti_sci_dev_ops - Device control operations
* @get_device: Command to request for device managed by TISCI
* Returns 0 for successful exclusive request, else returns
* corresponding error message.
* @idle_device: Command to idle a device managed by TISCI
* Returns 0 for successful exclusive request, else returns
* corresponding error message.
* @put_device: Command to release a device managed by TISCI
* Returns 0 for successful release, else returns corresponding
* error message.
* @is_valid: Check if the device ID is a valid ID.
* Returns 0 if the ID is valid, else returns corresponding error.
* @get_context_loss_count: Command to retrieve context loss counter - this
* increments every time the device looses context. Overflow
* is possible.
* - count: pointer to u32 which will retrieve counter
* Returns 0 for successful information request and count has
* proper data, else returns corresponding error message.
* @is_idle: Reports back about device idle state
* - req_state: Returns requested idle state
* Returns 0 for successful information request and req_state and
* current_state has proper data, else returns corresponding error
* message.
* @is_stop: Reports back about device stop state
* - req_state: Returns requested stop state
* - current_state: Returns current stop state
* Returns 0 for successful information request and req_state and
* current_state has proper data, else returns corresponding error
* message.
* @is_on: Reports back about device ON(or active) state
* - req_state: Returns requested ON state
* - current_state: Returns current ON state
* Returns 0 for successful information request and req_state and
* current_state has proper data, else returns corresponding error
* message.
* @is_transitioning: Reports back if the device is in the middle of transition
* of state.
* -current_state: Returns 'true' if currently transitioning.
* @set_device_resets: Command to configure resets for device managed by TISCI.
* -reset_state: Device specific reset bit field
* Returns 0 for successful request, else returns
* corresponding error message.
* @get_device_resets: Command to read state of resets for device managed
* by TISCI.
* -reset_state: pointer to u32 which will retrieve resets
* Returns 0 for successful request, else returns
* corresponding error message.
*
* NOTE: for all these functions, the following parameters are generic in
* nature:
* -handle: Pointer to TISCI handle as retrieved by *ti_sci_get_handle
* -id: Device Identifier
*
* Request for the device - NOTE: the client MUST maintain integrity of
* usage count by balancing get_device with put_device. No refcounting is
* managed by driver for that purpose.
*/
struct ti_sci_dev_ops {
int (*get_device)(const struct ti_sci_handle *handle, u32 id);
int (*idle_device)(const struct ti_sci_handle *handle, u32 id);
int (*put_device)(const struct ti_sci_handle *handle, u32 id);
int (*is_valid)(const struct ti_sci_handle *handle, u32 id);
int (*get_context_loss_count)(const struct ti_sci_handle *handle,
u32 id, u32 *count);
int (*is_idle)(const struct ti_sci_handle *handle, u32 id,
bool *requested_state);
int (*is_stop)(const struct ti_sci_handle *handle, u32 id,
bool *req_state, bool *current_state);
int (*is_on)(const struct ti_sci_handle *handle, u32 id,
bool *req_state, bool *current_state);
int (*is_transitioning)(const struct ti_sci_handle *handle, u32 id,
bool *current_state);
int (*set_device_resets)(const struct ti_sci_handle *handle, u32 id,
u32 reset_state);
int (*get_device_resets)(const struct ti_sci_handle *handle, u32 id,
u32 *reset_state);
};
/**
* struct ti_sci_clk_ops - Clock control operations
* @get_clock: Request for activation of clock and manage by processor
* - needs_ssc: 'true' if Spread Spectrum clock is desired.
* - can_change_freq: 'true' if frequency change is desired.
* - enable_input_term: 'true' if input termination is desired.
* @idle_clock: Request for Idling a clock managed by processor
* @put_clock: Release the clock to be auto managed by TISCI
* @is_auto: Is the clock being auto managed
* - req_state: state indicating if the clock is auto managed
* @is_on: Is the clock ON
* - req_state: if the clock is requested to be forced ON
* - current_state: if the clock is currently ON
* @is_off: Is the clock OFF
* - req_state: if the clock is requested to be forced OFF
* - current_state: if the clock is currently Gated
* @set_parent: Set the clock source of a specific device clock
* - parent_id: Parent clock identifier to set.
* @get_parent: Get the current clock source of a specific device clock
* - parent_id: Parent clock identifier which is the parent.
* @get_num_parents: Get the number of parents of the current clock source
* - num_parents: returns the number of parent clocks.
* @get_best_match_freq: Find a best matching frequency for a frequency
* range.
* - match_freq: Best matching frequency in Hz.
* @set_freq: Set the Clock frequency
* @get_freq: Get the Clock frequency
* - current_freq: Frequency in Hz that the clock is at.
*
* NOTE: for all these functions, the following parameters are generic in
* nature:
* -handle: Pointer to TISCI handle as retrieved by *ti_sci_get_handle
* -did: Device identifier this request is for
* -cid: Clock identifier for the device for this request.
* Each device has it's own set of clock inputs. This indexes
* which clock input to modify.
* -min_freq: The minimum allowable frequency in Hz. This is the minimum
* allowable programmed frequency and does not account for clock
* tolerances and jitter.
* -target_freq: The target clock frequency in Hz. A frequency will be
* processed as close to this target frequency as possible.
* -max_freq: The maximum allowable frequency in Hz. This is the maximum
* allowable programmed frequency and does not account for clock
* tolerances and jitter.
*
* Request for the clock - NOTE: the client MUST maintain integrity of
* usage count by balancing get_clock with put_clock. No refcounting is
* managed by driver for that purpose.
*/
struct ti_sci_clk_ops {
int (*get_clock)(const struct ti_sci_handle *handle, u32 did, u8 cid,
bool needs_ssc, bool can_change_freq,
bool enable_input_term);
int (*idle_clock)(const struct ti_sci_handle *handle, u32 did, u8 cid);
int (*put_clock)(const struct ti_sci_handle *handle, u32 did, u8 cid);
int (*is_auto)(const struct ti_sci_handle *handle, u32 did, u8 cid,
bool *req_state);
int (*is_on)(const struct ti_sci_handle *handle, u32 did, u8 cid,
bool *req_state, bool *current_state);
int (*is_off)(const struct ti_sci_handle *handle, u32 did, u8 cid,
bool *req_state, bool *current_state);
int (*set_parent)(const struct ti_sci_handle *handle, u32 did, u8 cid,
u8 parent_id);
int (*get_parent)(const struct ti_sci_handle *handle, u32 did, u8 cid,
u8 *parent_id);
int (*get_num_parents)(const struct ti_sci_handle *handle, u32 did,
u8 cid, u8 *num_parents);
int (*get_best_match_freq)(const struct ti_sci_handle *handle, u32 did,
u8 cid, u64 min_freq, u64 target_freq,
u64 max_freq, u64 *match_freq);
int (*set_freq)(const struct ti_sci_handle *handle, u32 did, u8 cid,
u64 min_freq, u64 target_freq, u64 max_freq);
int (*get_freq)(const struct ti_sci_handle *handle, u32 did, u8 cid,
u64 *current_freq);
};
/**
* struct ti_sci_ops - Function support for TI SCI
* @dev_ops: Device specific operations
* @clk_ops: Clock specific operations
*/
struct ti_sci_ops {
struct ti_sci_dev_ops dev_ops;
struct ti_sci_clk_ops clk_ops;
};
/**
* struct ti_sci_handle - Handle returned to TI SCI clients for usage.
* @version: structure containing version information
* @ops: operations that are made available to TI SCI clients
*/
struct ti_sci_handle {
struct ti_sci_version_info version;
struct ti_sci_ops ops;
};
#if IS_ENABLED(CONFIG_TI_SCI_PROTOCOL)
const struct ti_sci_handle *ti_sci_get_handle(struct device *dev);
int ti_sci_put_handle(const struct ti_sci_handle *handle);
const struct ti_sci_handle *devm_ti_sci_get_handle(struct device *dev);
#else /* CONFIG_TI_SCI_PROTOCOL */
static inline const struct ti_sci_handle *ti_sci_get_handle(struct device *dev)
{
return ERR_PTR(-EINVAL);
}
static inline int ti_sci_put_handle(const struct ti_sci_handle *handle)
{
return -EINVAL;
}
static inline
const struct ti_sci_handle *devm_ti_sci_get_handle(struct device *dev)
{
return ERR_PTR(-EINVAL);
}
#endif /* CONFIG_TI_SCI_PROTOCOL */
#endif /* __TISCI_PROTOCOL_H */
|