aboutsummaryrefslogtreecommitdiffstats
blob: eb60e8d83e71e408553916417f4ce0411c11b1b5 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
The most frequent cause of problems when porting U-Boot to new
hardware, or when using a sloppy port on some board, is memory errors.
In most cases these are not caused by failing hardware, but by
incorrect initialization of the memory controller.  So it appears to
be a good idea to always test if the memory is working correctly,
before looking for any other potential causes of any problems.

U-Boot implements 3 different approaches to perform memory tests:

1. The get_ram_size() function (see "common/memsize.c").

   This function is supposed to be used in each and every U-Boot port
   determine the presence and actual size of each of the potential
   memory banks on this piece of hardware.  The code is supposed to be
   very fast, so running it for each reboot does not hurt.  It is a
   little known and generally underrated fact that this code will also
   catch 99% of hardware related (i. e. reliably reproducible) memory
   errors.  It is strongly recommended to always use this function, in
   each and every port of U-Boot.

2. The "mtest" command.

   This is probably the best known memory test utility in U-Boot.
   Unfortunately, it is also the most problematic, and the most
   useless one.

   There are a number of serious problems with this command:

   - It is terribly slow.  Running "mtest" on the whole system RAM
     takes a _long_ time before there is any significance in the fact
     that no errors have been found so far.

   - It is difficult to configure, and to use.  And any errors here
     will reliably crash or hang your system.  "mtest" is dumb and has
     no knowledge about memory ranges that may be in use for other
     purposes, like exception code, U-Boot code and data, stack,
     malloc arena, video buffer, log buffer, etc.  If you let it, it
     will happily "test" all such areas, which of course will cause
     some problems.

   - It is not easy to configure and use, and a large number of
     systems are seriously misconfigured.  The original idea was to
     test basically the whole system RAM, with only exempting the
     areas used by U-Boot itself - on most systems these are the areas
     used for the exception vectors (usually at the very lower end of
     system memory) and for U-Boot (code, data, etc. - see above;
     these are usually at the very upper end of system memory).  But
     experience has shown that a very large number of ports use
     pretty much bogus settings of CONFIG_SYS_MEMTEST_START and
     CONFIG_SYS_MEMTEST_END; this results in useless tests (because
     the ranges is too small and/or badly located) or in critical
     failures (system crashes).

   Because of these issues, the "mtest" command is considered depre-
   cated.  It should not be enabled in most normal ports of U-Boot,
   especially not in production.  If you really need a memory test,
   then see 1. and 3. above resp. below.

3. The most thorough memory test facility is available as part of the
   POST (Power-On Self Test) sub-system, see "post/drivers/memory.c".

   If you really need to perform memory tests (for example, because
   it is mandatory part of your requirement specification), then
   enable this test which is generic and should work on all archi-
   tectures.

WARNING:

It should pointed out that _all_ these memory tests have one
fundamental, unfixable design flaw:  they are based on the assumption
that memory errors can be found by writing to and reading from memory.
Unfortunately, this is only true for the relatively harmless, usually
static errors like shorts between data or address lines, unconnected
pins, etc.  All the really nasty errors which will first turn your
hair gray, only to make you tear it out later, are dynamical errors,
which usually happen not with simple read or write cycles on the bus,
but when performing back-to-back data transfers in burst mode.  Such
accesses usually happen only for certain DMA operations, or for heavy
cache use (instruction fetching, cache flushing).  So far I am not
aware of any freely available code that implements a generic, and
efficient, memory test like that.  The best known test case to stress
a system like that is to boot Linux with root file system mounted over
NFS, and then build some larger software package natively (say,
compile a Linux kernel on the system) - this will cause enough context
switches, network traffic (and thus DMA transfers from the network
controller), varying RAM use, etc. to trigger any weak spots in this
area.

Note: An attempt was made once to implement such a test to catch
memory problems on a specific board.  The code is pretty much board
specific (for example, it includes setting specific GPIO signals to
provide triggers for an attached logic analyzer), but you can get an
idea how it works: see "examples/standalone/test_burst*".

Note 2: Ironically enough, the "test_burst" did not catch any RAM
errors, not a single one ever.  The problems this code was supposed
to catch did not happen when accessing the RAM, but when reading from
NOR flash.