aboutsummaryrefslogtreecommitdiffstats
diff options
context:
space:
mode:
Diffstat (limited to 'docs/source/using_api.rst')
-rw-r--r--docs/source/using_api.rst6
1 files changed, 5 insertions, 1 deletions
diff --git a/docs/source/using_api.rst b/docs/source/using_api.rst
index d56bd52..f744690 100644
--- a/docs/source/using_api.rst
+++ b/docs/source/using_api.rst
@@ -326,7 +326,7 @@ Subgraph config file
326 326
327Subgraph config file are named as "subgraph<number>.cfg", while <number> 327Subgraph config file are named as "subgraph<number>.cfg", while <number>
328is the subgraph index in the original graph/network. The environment 328is the subgraph index in the original graph/network. The environment
329variable `TIDL_SUBGRAPH_DIR` speicifies the directory where subgraph config 329variable `TIDL_SUBGRAPH_DIR` specifies the directory where subgraph config
330files reside. If not specified, the current directory is assumed. 330files reside. If not specified, the current directory is assumed.
331 331
332Subgraph config file requires extra parameters to describe data conversion 332Subgraph config file requires extra parameters to describe data conversion
@@ -337,3 +337,7 @@ set of required parameters.
337Subgraph runtime API 337Subgraph runtime API
338==================== 338====================
339Please see `tidl_api/inc/subgraph_runtime.h` for details. 339Please see `tidl_api/inc/subgraph_runtime.h` for details.
340
341The envrionment variable `TIDL_SUBGRAPH_NUM_EVES` specifies the number of
342EVEs used for inferencing. If not specified, all available EVEs will be
343initialized and used.