aboutsummaryrefslogtreecommitdiffstats
blob: dc1035be9442a76b567bb994be12c1e6ace5e632 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
317
318
319
320
321
322
323
324
325
326
327
328
329
330
331
332
333
334
335
336
337
338
339
340
341
342
343
344
345
346
347
348
349
350
351
352
353
354
355
356
357
358
359
360
361
362
363
364
365
366
367
368
369
370
371
372
/******************************************************************************
 * Copyright (c) 2018, Texas Instruments Incorporated - http://www.ti.com/
 *   All rights reserved.
 *
 *   Redistribution and use in source and binary forms, with or without
 *   modification, are permitted provided that the following conditions are met:
 *       * Redistributions of source code must retain the above copyright
 *         notice, this list of conditions and the following disclaimer.
 *       * Redistributions in binary form must reproduce the above copyright
 *         notice, this list of conditions and the following disclaimer in the
 *         documentation and/or other materials provided with the distribution.
 *       * Neither the name of Texas Instruments Incorporated nor the
 *         names of its contributors may be used to endorse or promote products
 *         derived from this software without specific prior written permission.
 *
 *   THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
 *   AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
 *   IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE
 *   ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR CONTRIBUTORS BE
 *   LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR
 *   CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF
 *   SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS
 *   INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN
 *   CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE)
 *   ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF
 *   THE POSSIBILITY OF SUCH DAMAGE.
 *****************************************************************************/
#include <signal.h>
#include <iostream>
#include <iomanip>
#include <fstream>
#include <cassert>
#include <string>
#include <functional>
#include <algorithm>
#include <time.h>
#include <unistd.h>

#include <queue>
#include <vector>
#include <chrono>

#include "executor.h"
#include "execution_object.h"
#include "execution_object_pipeline.h"
#include "configuration.h"
#include "../common/object_classes.h"
#include "imgutil.h"
#include "../common/video_utils.h"

#include "opencv2/core.hpp"
#include "opencv2/imgproc.hpp"
#include "opencv2/highgui.hpp"
#include "opencv2/videoio.hpp"

using namespace std;
using namespace tidl;
using namespace cv;

#define NUM_VIDEO_FRAMES  300
#define DEFAULT_CONFIG    "j11_v2"
#define NUM_DEFAULT_INPUTS  1
#define DEFAULT_OBJECT_CLASSES_LIST_FILE "imagenet_objects.json"
#define DEFAULT_OUTPUT_PROB_THRESHOLD  5
const char *default_inputs[NUM_DEFAULT_INPUTS] =
{
    "../test/testvecs/input/objects/cat-pet-animal-domestic-104827.jpeg"
};
std::unique_ptr<ObjectClasses> object_classes;


Executor* CreateExecutor(DeviceType dt, uint32_t num, const Configuration& c);
bool RunConfiguration(cmdline_opts_t& opts);
bool ReadFrame(ExecutionObjectPipeline& eop,
               uint32_t frame_idx, const Configuration& c,
               const cmdline_opts_t& opts, VideoCapture &cap);
bool WriteFrameOutput(const ExecutionObjectPipeline &eop,
                      const cmdline_opts_t& opts);
void DisplayHelp();


int main(int argc, char *argv[])
{
    // Catch ctrl-c to ensure a clean exit
    signal(SIGABRT, exit);
    signal(SIGTERM, exit);

    // If there are no devices capable of offloading TIDL on the SoC, exit
    uint32_t num_eves = Executor::GetNumDevices(DeviceType::EVE);
    uint32_t num_dsps = Executor::GetNumDevices(DeviceType::DSP);
    if (num_eves == 0 && num_dsps == 0)
    {
        cout << "TI DL not supported on this SoC." << endl;
        return EXIT_SUCCESS;
    }

    // Process arguments
    cmdline_opts_t opts;
    opts.config = DEFAULT_CONFIG;
    opts.object_classes_list_file = DEFAULT_OBJECT_CLASSES_LIST_FILE;
    opts.output_prob_threshold = DEFAULT_OUTPUT_PROB_THRESHOLD;
    if (num_eves != 0) { opts.num_eves = 1;  opts.num_dsps = 0; }
    else               { opts.num_eves = 0;  opts.num_dsps = 1; }
    if (! ProcessArgs(argc, argv, opts))
    {
        DisplayHelp();
        exit(EXIT_SUCCESS);
    }
    assert(opts.num_dsps != 0 || opts.num_eves != 0);
    if (opts.num_frames == 0)
        opts.num_frames = (opts.is_camera_input || opts.is_video_input) ?
                          NUM_VIDEO_FRAMES : 1;
    if (opts.input_file.empty())
        cout << "Input: " << default_inputs[0] << endl;
    else
        cout << "Input: " << opts.input_file << endl;

    // Get object classes list
    object_classes = std::unique_ptr<ObjectClasses>(
                             new ObjectClasses(opts.object_classes_list_file));
    if (object_classes->GetNumClasses() == 0)
    {
        cout << "No object classes defined for this config." << endl;
        return EXIT_FAILURE;
    }

    // Run network
    bool status = RunConfiguration(opts);
    if (!status)
    {
        cout << "imagenet FAILED" << endl;
        return EXIT_FAILURE;
    }

    cout << "imagenet PASSED" << endl;
    return EXIT_SUCCESS;
}

bool RunConfiguration(cmdline_opts_t& opts)
{
    // Read the TI DL configuration file
    Configuration c;
    string config_file = "../test/testvecs/config/infer/tidl_config_"
                              + opts.config + ".txt";
    bool status = c.ReadFromFile(config_file);
    if (!status)
    {
        cerr << "Error in configuration file: " << config_file << endl;
        return false;
    }
    c.enableApiTrace = opts.verbose;

    // setup camera/video input/output
    VideoCapture cap;
    if (! SetVideoInputOutput(cap, opts, "ImageNet"))  return false;

    try
    {
        // Create Executors with the approriate core type, number of cores
        // and configuration specified
        Executor* e_eve = CreateExecutor(DeviceType::EVE, opts.num_eves, c);
        Executor* e_dsp = CreateExecutor(DeviceType::DSP, opts.num_dsps, c);

        // Get ExecutionObjects from Executors
        vector<ExecutionObject*> eos;
        for (uint32_t i = 0; i < opts.num_eves; i++) eos.push_back((*e_eve)[i]);
        for (uint32_t i = 0; i < opts.num_dsps; i++) eos.push_back((*e_dsp)[i]);
        uint32_t num_eos = eos.size();

        // Use duplicate EOPs to do double buffering on frame input/output
        //    because each EOP has its own set of input/output buffers,
        //    so that host ReadFrame() can be overlapped with device processing
        // Use one EO as an example, with different buffer_factor,
        //    we have different execution behavior:
        // If buffer_factor is set to 1 -> single buffering
        //    we create one EOP: eop0 (eo0)
        //    pipeline execution of multiple frames over time is as follows:
        //    --------------------- time ------------------->
        //    eop0: [RF][eo0.....][WF]
        //    eop0:                   [RF][eo0.....][WF]
        //    eop0:                                     [RF][eo0.....][WF]
        // If buffer_factor is set to 2 -> double buffering
        //    we create two EOPs: eop0 (eo0), eop1(eo0)
        //    pipeline execution of multiple frames over time is as follows:
        //    --------------------- time ------------------->
        //    eop0: [RF][eo0.....][WF]
        //    eop1:     [RF]      [eo0.....][WF]
        //    eop0:                   [RF]  [eo0.....][WF]
        //    eop1:                             [RF]  [eo0.....][WF]
        vector<ExecutionObjectPipeline *> eops;
        uint32_t buffer_factor = 2;  // set to 1 for single buffering
        for (uint32_t j = 0; j < buffer_factor; j++)
            for (uint32_t i = 0; i < num_eos; i++)
                eops.push_back(new ExecutionObjectPipeline({eos[i]}));
        uint32_t num_eops = eops.size();

        // Allocate input and output buffers for each EOP
        AllocateMemory(eops);

        chrono::time_point<chrono::steady_clock> tloop0, tloop1;
        tloop0 = chrono::steady_clock::now();

        // Process frames with available eops in a pipelined manner
        // additional num_eos iterations to flush the pipeline (epilogue)
        for (uint32_t frame_idx = 0;
             frame_idx < opts.num_frames + num_eops; frame_idx++)
        {
            ExecutionObjectPipeline* eop = eops[frame_idx % num_eops];

            // Wait for previous frame on the same eop to finish processing
            if (eop->ProcessFrameWait())
            {
                WriteFrameOutput(*eop, opts);
            }

            // Read a frame and start processing it with current eop
            if (ReadFrame(*eop, frame_idx, c, opts, cap))
                eop->ProcessFrameStartAsync();
        }

        tloop1 = chrono::steady_clock::now();
        chrono::duration<float> elapsed = tloop1 - tloop0;
        cout << "Loop total time (including read/write/opencv/print/etc): "
                  << setw(6) << setprecision(4)
                  << (elapsed.count() * 1000) << "ms" << endl;

        FreeMemory(eops);
        for (auto eop : eops)  delete eop;
        delete e_eve;
        delete e_dsp;
    }
    catch (tidl::Exception &e)
    {
        cerr << e.what() << endl;
        status = false;
    }

    return status;
}

// Create an Executor with the specified type and number of EOs
Executor* CreateExecutor(DeviceType dt, uint32_t num, const Configuration& c)
{
    if (num == 0) return nullptr;

    DeviceIds ids;
    for (uint32_t i = 0; i < num; i++)
        ids.insert(static_cast<DeviceId>(i));

    return new Executor(dt, ids, c);
}

bool ReadFrame(ExecutionObjectPipeline &eop,
               uint32_t frame_idx, const Configuration& c,
               const cmdline_opts_t& opts, VideoCapture &cap)
{
    if (frame_idx >= opts.num_frames)
        return false;

    eop.SetFrameIndex(frame_idx);

    char*  frame_buffer = eop.GetInputBufferPtr();
    assert (frame_buffer != nullptr);

    Mat image;
    if (! opts.is_camera_input && ! opts.is_video_input)
    {
        if (opts.input_file.empty())
            image = cv::imread(default_inputs[frame_idx % NUM_DEFAULT_INPUTS],
                               CV_LOAD_IMAGE_COLOR);
        else
            image = cv::imread(opts.input_file, CV_LOAD_IMAGE_COLOR);
        if (image.empty())
        {
            cerr << "Unable to read input image" << endl;
            return false;
        }
    }
    else
    {
        Mat v_image;
        if (! cap.grab())  return false;
        if (! cap.retrieve(v_image)) return false;
        int orig_width  = v_image.cols;
        int orig_height = v_image.rows;
        // Crop camera/video input to center 256x256 input
        if (orig_width > 256 && orig_height > 256)
        {
            image = Mat(v_image, Rect((orig_width-256)/2, (orig_height-256)/2,
                                       256, 256));
        }
        else
            image = v_image;
        cv::imshow("ImageNet", image);
        waitKey(2);
    }

    // TI DL image preprocessing, into frame_buffer
    return imgutil::PreprocessImage(image, frame_buffer, c);
}

// Display top 5 classified imagenet classes with probabilities 5% or higher
bool WriteFrameOutput(const ExecutionObjectPipeline &eop,
                      const cmdline_opts_t& opts)
{
    const int k = 5;
    unsigned char *out = (unsigned char *) eop.GetOutputBufferPtr();
    int out_size = eop.GetOutputBufferSizeInBytes();

    // sort and get k largest values and corresponding indices
    typedef pair<unsigned char, int> val_index;
    auto cmp = [](val_index &left, val_index &right)
                         { return left.first > right.first; };
    priority_queue<val_index, vector<val_index>, decltype(cmp)> queue(cmp);
    // initialize priority queue with smallest value on top
    for (int i = 0; i < k; i++)
        queue.push(val_index(out[i], i));

    // for rest output, if larger than current min, pop min, push new val
    for (int i = k; i < out_size; i++)
    {
        if (out[i] > queue.top().first)
        {
          queue.pop();
          queue.push(val_index(out[i], i));
        }
    }

    // output top k values in reverse order: largest val first
    vector<val_index> sorted;
    while (! queue.empty())
    {
      sorted.push_back(queue.top());
      queue.pop();
    }

    unsigned int min_prob_255 = opts.output_prob_threshold * 255;
    for (int i = k - 1; i >= 0; i--)
    {
        if (sorted[i].first * 100 < min_prob_255)  break;
        cout << k-i << ": "
             << object_classes->At(sorted[i].second).label
             << ",   prob = " << setprecision(4)
             << ((sorted[i].first * 100) / 255.0f) << "%" << endl;
    }

    return true;
}

void DisplayHelp()
{
    cout <<
    "Usage: imagenet\n"
    "  Will run imagenet network to predict top 5 object"
    " classes for the input.\n  Use -c to run a"
    "  different imagenet network. Default is j11_v2.\n"
    "Optional arguments:\n"
    " -c <config>          Valid configs: j11_bn, j11_prelu, j11_v2\n"
    " -d <number>          Number of dsp cores to use\n"
    " -e <number>          Number of eve cores to use\n"
    " -i <image>           Path to the image file as input\n"
    " -i camera<number>    Use camera as input\n"
    "                      video input port: /dev/video<number>\n"
    " -i <name>.{mp4,mov,avi}  Use video file as input\n"
    " -l <objects_list>    Path to the object classes list file\n"
    " -f <number>          Number of frames to process\n"
    " -p <number>          Output probablity threshold in percentage\n"
    "                      Default is 5 percent or higher.\n"
    " -v                   Verbose output during execution\n"
    " -h                   Help\n";
}