1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
|
/******************************************************************************
* Copyright (c) 2017-2018 Texas Instruments Incorporated - http://www.ti.com/
* All rights reserved.
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions are met:
* * Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
* * Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the distribution.
* * Neither the name of Texas Instruments Incorporated nor the
* names of its contributors may be used to endorse or promote products
* derived from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
* AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
* IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE
* ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR CONTRIBUTORS BE
* LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR
* CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF
* SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS
* INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN
* CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE)
* ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF
* THE POSSIBILITY OF SUCH DAMAGE.
*****************************************************************************/
//
// This example illustrates using a single EO to process a frame. To increase
// throughput, multiple EOs are used.
// For details, refer http://downloads.ti.com/mctools/esd/docs/tidl-api/
//
#include <signal.h>
#include <iostream>
#include <fstream>
#include <cassert>
#include <string>
#include "executor.h"
#include "execution_object.h"
#include "configuration.h"
#include "utils.h"
using namespace tidl;
using std::string;
using std::unique_ptr;
using std::vector;
bool Run(const string& config_file, int num_eve,int num_dsp,
const char* ref_output);
Executor* CreateExecutor(DeviceType dt, int num, const Configuration& c);
void CollectEOs(const Executor *e, vector<ExecutionObject *>& EOs);
int main(int argc, char *argv[])
{
// Catch ctrl-c to ensure a clean exit
signal(SIGABRT, exit);
signal(SIGTERM, exit);
// If there are no devices capable of offloading TIDL on the SoC, exit
uint32_t num_eve = Executor::GetNumDevices(DeviceType::EVE);
uint32_t num_dsp = Executor::GetNumDevices(DeviceType::DSP);
if (num_eve == 0 && num_dsp == 0)
{
std::cout << "TI DL not supported on this SoC." << std::endl;
return EXIT_SUCCESS;
}
string config_file ="../test/testvecs/config/infer/tidl_config_j11_v2.txt";
string ref_file ="../test/testvecs/reference/j11_v2_ref.bin";
unique_ptr<const char> reference_output(ReadReferenceOutput(ref_file));
// Enable time stamp generation. The timestamp file is post processed
// by execution_graph.py to generate graphical view of frame execution.
// Refer to the User's Guide for details.
EnableTimeStamps("1eo.log");
bool status = Run(config_file, num_eve, num_dsp, reference_output.get());
if (!status)
{
std::cout << "FAILED" << std::endl;
return EXIT_FAILURE;
}
std::cout << "PASSED" << std::endl;
return EXIT_SUCCESS;
}
bool Run(const string& config_file, int num_eve, int num_dsp,
const char* ref_output)
{
Configuration c;
if (!c.ReadFromFile(config_file))
return false;
// Heap sizes for this network determined using Configuration::showHeapStats
c.PARAM_HEAP_SIZE = (3 << 20); // 3MB
c.NETWORK_HEAP_SIZE = (20 << 20); // 20MB
c.numFrames = 16;
// Open input file for reading
std::ifstream input_data_file(c.inData, std::ios::binary);
bool status = true;
try
{
// Create Executors - use all the DSP and EVE cores available
unique_ptr<Executor> e_dsp(CreateExecutor(DeviceType::DSP, num_dsp, c));
unique_ptr<Executor> e_eve(CreateExecutor(DeviceType::EVE, num_eve, c));
// Accumulate all the EOs from across the Executors
vector<ExecutionObject *> EOs;
CollectEOs(e_eve.get(), EOs);
CollectEOs(e_dsp.get(), EOs);
AllocateMemory(EOs);
// Process frames with EOs in a pipelined manner
// additional num_eos iterations to flush the pipeline (epilogue)
int num_eos = EOs.size();
for (int frame_idx = 0; frame_idx < c.numFrames + num_eos; frame_idx++)
{
ExecutionObject* eo = EOs[frame_idx % num_eos];
// Wait for previous frame on the same eo to finish processing
if (eo->ProcessFrameWait())
{
ReportTime(eo);
if (frame_idx < num_eos && !CheckFrame(eo, ref_output))
status = false;
}
// Read a frame and start processing it with current eo
if (ReadFrame(eo, frame_idx, c, input_data_file))
eo->ProcessFrameStartAsync();
}
FreeMemory(EOs);
}
catch (tidl::Exception &e)
{
std::cerr << e.what() << std::endl;
status = false;
}
input_data_file.close();
return status;
}
// Create an Executor with the specified type and number of EOs
Executor* CreateExecutor(DeviceType dt, int num, const Configuration& c)
{
if (num == 0) return nullptr;
DeviceIds ids;
for (int i = 0; i < num; i++)
ids.insert(static_cast<DeviceId>(i));
return new Executor(dt, ids, c);
}
// Accumulate EOs from an Executor into a vector of EOs
void CollectEOs(const Executor *e, vector<ExecutionObject *>& EOs)
{
if (!e) return;
for (unsigned int i = 0; i < e->GetNumExecutionObjects(); i++)
EOs.push_back((*e)[i]);
}
|