summaryrefslogtreecommitdiffstats
blob: eaa61bd2d40708f7352a49b7c00eae62a7f4bbc9 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
317
318
319
320
321
322
323
324
325
326
327
328
329
330
331
332
333
334
335
336
337
338
339
340
341
342
343
344
345
346
347
348
349
350
351
352
353
354
355
356
357
358
359
360
361
362
363
364
365
366
367
368
369
370
371
372
373
374
375
376
377
378
379
380
381
382
383
384
385
386
387
388
389
390
391
392
393
394
395
396
397
398
399
400
401
402
403
404
405
406
407
408
409
410
411
412
413
414
415
416
417
418
419
420
421
422
423
424
425
426
427
428
429
430
431
432
433
434
435
436
437
438
439
440
441
442
443
444
445
446
447
448
449
450
451
452
453
454
455
456
457
458
459
460
461
462
463
464
465
466
467
468
469
470
471
472
473
474
475
476
477
478
479
480
481
482
483
484
485
486
487
488
489
490
491
492
493
494
495
496
497
498
499
500
501
502
503
504
505
506
507
508
509
510
511
512
513
514
515
516
517
518
519
520
521
522
523
524
525
526
527
528
529
530
531
532
533
534
535
536
537
538
539
540
541
542
543
544
545
546
547
548
549
550
551
552
553
554
555
556
557
558
559
560
561
562
563
564
565
566
567
568
569
570
571
572
573
574
575
576
577
578
579
580
581
582
583
584
585
586
587
/******************************************************************************
 * Copyright (c) 2018, Texas Instruments Incorporated - http://www.ti.com/
 *   All rights reserved.
 *
 *   Redistribution and use in source and binary forms, with or without
 *   modification, are permitted provided that the following conditions are met:
 *       * Redistributions of source code must retain the above copyright
 *         notice, this list of conditions and the following disclaimer.
 *       * Redistributions in binary form must reproduce the above copyright
 *         notice, this list of conditions and the following disclaimer in the
 *         documentation and/or other materials provided with the distribution.
 *       * Neither the name of Texas Instruments Incorporated nor the
 *         names of its contributors may be used to endorse or promote products
 *         derived from this software without specific prior written permission.
 *
 *   THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
 *   AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
 *   IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE
 *   ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR CONTRIBUTORS BE
 *   LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR
 *   CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF
 *   SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS
 *   INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN
 *   CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE)
 *   ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF
 *   THE POSSIBILITY OF SUCH DAMAGE.
 *****************************************************************************/
#include <signal.h>
#include <iostream>
#include <iomanip>
#include <fstream>
#include <cassert>
#include <string>
#include <functional>
#include <algorithm>
#include <time.h>
#include <unistd.h>

#include <queue>
#include <vector>
#include <cstdio>
#include <string>
#include <chrono>

#include "executor.h"
#include "execution_object.h"
#include "execution_object_pipeline.h"
#include "configuration.h"
#include "../common/object_classes.h"
#include "../common/utils.h"
#include "../common/video_utils.h"

using namespace std;
using namespace tidl;
using namespace cv;


#define NUM_VIDEO_FRAMES  100
#define DEFAULT_CONFIG    "jdetnet_voc"
#define DEFAULT_INPUT     "../test/testvecs/input/horse_768x320.y"
#define DEFAULT_INPUT_FRAMES (1)
#define DEFAULT_OBJECT_CLASSES_LIST_FILE "./jdetnet_voc_objects.json"
#define DEFAULT_OUTPUT_PROB_THRESHOLD  25

/* Enable this macro to record individual output files and */
/* resized, cropped network input files                    */
//#define DEBUG_FILES

std::unique_ptr<ObjectClasses> object_classes;
uint32_t orig_width;
uint32_t orig_height;
uint32_t num_frames_file;

bool RunConfiguration(const cmdline_opts_t& opts);
Executor* CreateExecutor(DeviceType dt, uint32_t num, const Configuration& c,
                         int layers_group_id);
bool ReadFrame(ExecutionObjectPipeline& eop, uint32_t frame_idx,
               const Configuration& c, const cmdline_opts_t& opts,
               VideoCapture &cap, ifstream &ifs);
bool WriteFrameOutput(const ExecutionObjectPipeline& eop,
                      const Configuration& c, const cmdline_opts_t& opts,
                      float confidence_value);
static void DisplayHelp();

/***************************************************************/
/* Slider to control detection confidence level                */
/***************************************************************/
static void on_trackbar( int slider_id, void *inst )
{
  //This function is invoked on every slider move.
  //No action required, since prob_slider is automatically updated.
  //But, for any additional operation on slider move, this is the place to insert code.
}


int main(int argc, char *argv[])
{
    // Catch ctrl-c to ensure a clean exit
    signal(SIGABRT, exit);
    signal(SIGTERM, exit);

    // If there are no devices capable of offloading TIDL on the SoC, exit
    uint32_t num_eves = Executor::GetNumDevices(DeviceType::EVE);
    uint32_t num_dsps = Executor::GetNumDevices(DeviceType::DSP);
    if (num_eves == 0 && num_dsps == 0)
    {
        cout << "ssd_multibox requires EVE or DSP for execution." << endl;
        return EXIT_SUCCESS;
    }

    // Process arguments
    cmdline_opts_t opts;
    opts.config = DEFAULT_CONFIG;
    opts.object_classes_list_file = DEFAULT_OBJECT_CLASSES_LIST_FILE;
    opts.num_eves = num_eves > 0 ? 1 : 0;
    opts.num_dsps = num_dsps > 0 ? 1 : 0;
    opts.input_file = DEFAULT_INPUT;
    opts.output_prob_threshold = DEFAULT_OUTPUT_PROB_THRESHOLD;
    if (! ProcessArgs(argc, argv, opts))
    {
        DisplayHelp();
        exit(EXIT_SUCCESS);
    }
    assert(opts.num_dsps != 0 || opts.num_eves != 0);
    if (opts.num_frames == 0)
        opts.num_frames = (opts.is_camera_input || opts.is_video_input) ?
                          NUM_VIDEO_FRAMES :
                          ((opts.input_file == DEFAULT_INPUT) ?
                           DEFAULT_INPUT_FRAMES : 1);
    cout << "Input: " << opts.input_file << endl;

    // Get object classes list
    object_classes = std::unique_ptr<ObjectClasses>(
                             new ObjectClasses(opts.object_classes_list_file));
    if (object_classes->GetNumClasses() == 0)
    {
        cout << "No object classes defined for this config." << endl;
        return EXIT_FAILURE;
    }

    // Run network
    bool status = RunConfiguration(opts);
    if (!status)
    {
        cout << "ssd_multibox FAILED" << endl;
        return EXIT_FAILURE;
    }

    cout << "ssd_multibox PASSED" << endl;
    return EXIT_SUCCESS;
}

bool RunConfiguration(const cmdline_opts_t& opts)
{
    int prob_slider     = opts.output_prob_threshold;
    // Read the TI DL configuration file
    Configuration c;
    std::string config_file = "../test/testvecs/config/infer/tidl_config_"
                              + opts.config + ".txt";
    bool status = c.ReadFromFile(config_file);
    if (!status)
    {
        cerr << "Error in configuration file: " << config_file << endl;
        return false;
    }
    c.enableApiTrace = opts.verbose;
    if (opts.num_eves == 0 || opts.num_dsps == 0)
        c.runFullNet = true;
    // DSP only execution requires larger NETWORK HEAP size
    if (opts.num_eves == 0)
        c.NETWORK_HEAP_SIZE = 75000000;

    // setup camera/video input
    VideoCapture cap;
    if (! SetVideoInputOutput(cap, opts, "SSD_Multibox"))  return false;

    if (opts.is_camera_input || opts.is_video_input)
    {
        std::string TrackbarName("Confidence(%):");
        createTrackbar( TrackbarName.c_str(), "SSD_Multibox",
                        &prob_slider, 100, on_trackbar );
        std::cout << TrackbarName << std::endl;
    }

    // setup preprocessed input
    ifstream ifs;
    if (opts.is_preprocessed_input)
    {
        ifs.open(opts.input_file, ios::binary | ios::ate);
        if (! ifs.good())
        {
            cerr << "Cannot open " << opts.input_file << endl;
            return false;
        }
        num_frames_file = ((int) ifs.tellg()) /
                          (c.inWidth * c.inHeight * c.inNumChannels);
    }

    try
    {
        // Create Executors with the approriate core type, number of cores
        // and configuration specified
        // EVE will run layersGroupId 1 in the network, while
        // DSP will run layersGroupId 2 in the network
        Executor* e_eve = CreateExecutor(DeviceType::EVE, opts.num_eves, c, 1);
        Executor* e_dsp = CreateExecutor(DeviceType::DSP, opts.num_dsps, c, 2);
        vector<ExecutionObjectPipeline *> eops;

        if (e_eve != nullptr && e_dsp != nullptr)
        {
            // Construct ExecutionObjectPipeline that utilizes multiple
            // ExecutionObjects to process a single frame, each ExecutionObject
            // processes one layerGroup of the network
            //
            // Pipeline depth can enable more optimized pipeline execution:
            // Given one EVE and one DSP as an example, with different
            //     pipeline_depth, we have different execution behavior:
            // If pipeline_depth is set to 1,
            //    we create one EOP: eop0 (eve0, dsp0)
            //    pipeline execution of multiple frames over time is as follows:
            //    --------------------- time ------------------->
            //    eop0: [eve0...][dsp0]
            //    eop0:                [eve0...][dsp0]
            //    eop0:                               [eve0...][dsp0]
            //    eop0:                                              [eve0...][dsp0]
            // If pipeline_depth is set to 2,
            //    we create two EOPs: eop0 (eve0, dsp0), eop1(eve0, dsp0)
            //    pipeline execution of multiple frames over time is as follows:
            //    --------------------- time ------------------->
            //    eop0: [eve0...][dsp0]
            //    eop1:          [eve0...][dsp0]
            //    eop0:                   [eve0...][dsp0]
            //    eop1:                            [eve0...][dsp0]
            // Additional benefit of setting pipeline_depth to 2 is that
            //    it can also overlap host ReadFrame() with device processing:
            //    --------------------- time ------------------->
            //    eop0: [RF][eve0...][dsp0]
            //    eop1:     [RF]     [eve0...][dsp0]
            //    eop0:                    [RF][eve0...][dsp0]
            //    eop1:                             [RF][eve0...][dsp0]
            uint32_t pipeline_depth = 2;  // 2 EOs in EOP -> depth 2
            for (uint32_t j = 0; j < pipeline_depth; j++)
                for (uint32_t i = 0; i < max(opts.num_eves, opts.num_dsps); i++)
                    eops.push_back(new ExecutionObjectPipeline(
                      {(*e_eve)[i%opts.num_eves], (*e_dsp)[i%opts.num_dsps]}));
        }
        else
        {
            // Construct ExecutionObjectPipeline that utilizes a
            // ExecutionObject to process a single frame, each ExecutionObject
            // processes the full network
            //
            // Use duplicate EOPs to do double buffering on frame input/output
            //    because each EOP has its own set of input/output buffers,
            //    so that host ReadFrame() can overlap device processing
            // Use one EO as an example, with different buffer_factor,
            //    we have different execution behavior:
            // If buffer_factor is set to 1 -> single buffering
            //    we create one EOP: eop0 (eo0)
            //    pipeline execution of multiple frames over time is as follows:
            //    --------------------- time ------------------->
            //    eop0: [RF][eo0.....][WF]
            //    eop0:                   [RF][eo0.....][WF]
            //    eop0:                                     [RF][eo0.....][WF]
            // If buffer_factor is set to 2 -> double buffering
            //    we create two EOPs: eop0 (eo0), eop1(eo0)
            //    pipeline execution of multiple frames over time is as follows:
            //    --------------------- time ------------------->
            //    eop0: [RF][eo0.....][WF]
            //    eop1:     [RF]      [eo0.....][WF]
            //    eop0:                   [RF]  [eo0.....][WF]
            //    eop1:                             [RF]  [eo0.....][WF]
            uint32_t buffer_factor = 2;  // set to 1 for single buffering
            for (uint32_t j = 0; j < buffer_factor; j++)
            {
                for (uint32_t i = 0; i < opts.num_eves; i++)
                    eops.push_back(new ExecutionObjectPipeline({(*e_eve)[i]}));
                for (uint32_t i = 0; i < opts.num_dsps; i++)
                    eops.push_back(new ExecutionObjectPipeline({(*e_dsp)[i]}));
            }
        }
        uint32_t num_eops = eops.size();

        // Allocate input/output memory for each EOP
        AllocateMemory(eops);

        chrono::time_point<chrono::steady_clock> tloop0, tloop1;
        tloop0 = chrono::steady_clock::now();

        // Process frames with available eops in a pipelined manner
        // additional num_eops iterations to flush pipeline (epilogue)
        for (uint32_t frame_idx = 0;
             frame_idx < opts.num_frames + num_eops; frame_idx++)
        {
            ExecutionObjectPipeline* eop = eops[frame_idx % num_eops];

            // Wait for previous frame on the same eop to finish processing
            if (eop->ProcessFrameWait())
                WriteFrameOutput(*eop, c, opts, (float)prob_slider);

            // Read a frame and start processing it with current eo
            if (ReadFrame(*eop, frame_idx, c, opts, cap, ifs))
                eop->ProcessFrameStartAsync();
        }

        tloop1 = chrono::steady_clock::now();
        chrono::duration<float> elapsed = tloop1 - tloop0;
        cout << "Loop total time (including read/write/opencv/print/etc): "
                  << setw(6) << setprecision(4)
                  << (elapsed.count() * 1000) << "ms" << endl;

        FreeMemory(eops);
        for (auto eop : eops)  delete eop;
        delete e_eve;
        delete e_dsp;
    }
    catch (tidl::Exception &e)
    {
        cerr << e.what() << endl;
        status = false;
    }

    return status;
}

// Create an Executor with the specified type and number of EOs
Executor* CreateExecutor(DeviceType dt, uint32_t num, const Configuration& c,
                         int layers_group_id)
{
    if (num == 0) return nullptr;

    DeviceIds ids;
    for (uint32_t i = 0; i < num; i++)
        ids.insert(static_cast<DeviceId>(i));

    Executor* e = new Executor(dt, ids, c, layers_group_id);
    assert(e != nullptr);
    return e;
}

bool ReadFrame(ExecutionObjectPipeline& eop, uint32_t frame_idx,
               const Configuration& c, const cmdline_opts_t& opts,
               VideoCapture &cap, ifstream &ifs)
{
    if ((uint32_t)frame_idx >= opts.num_frames)
        return false;

    eop.SetFrameIndex(frame_idx);

    char*  frame_buffer = eop.GetInputBufferPtr();
    assert (frame_buffer != nullptr);
    int channel_size = c.inWidth * c.inHeight;
    int frame_size   = channel_size * c.inNumChannels;

    Mat image;
    if (!opts.is_camera_input && !opts.is_video_input)
    {
        if (opts.is_preprocessed_input)
        {
            orig_width  = c.inWidth;
            orig_height = c.inHeight;
            ifs.seekg((frame_idx % num_frames_file) * frame_size);
            ifs.read(frame_buffer, frame_size);
            return ifs.good();
        }
        else
        {
            image = cv::imread(opts.input_file, CV_LOAD_IMAGE_COLOR);
            if (image.empty())
            {
                cerr << "Unable to read from: " << opts.input_file << endl;
                return false;
            }
        }
    }
    else
    {
        if(opts.is_camera_input)
        {
           if (! cap.grab()) return false;
           if (! cap.retrieve(image)) return false;
        }
        else
        { // Video clip
           if (cap.grab())
           {
             if (! cap.retrieve(image)) return false;
           } else {
             //Rewind!
             std::cout << "Video clip rewinded!" << std::endl;
             cap.set(CAP_PROP_POS_FRAMES, 0);
             if (! cap.grab()) return false;
             if (! cap.retrieve(image)) return false;
           }
        }
    }

    // Scale to network input size:
    Mat s_image, bgr_frames[3];
    orig_width  = image.cols;
    orig_height = image.rows;
    if (!opts.is_camera_input && !opts.is_video_input)
    {
        cv::resize(image, s_image, Size(c.inWidth, c.inHeight),
                   0, 0, cv::INTER_AREA);
    }
    else
    {
        // Preserve aspect ratio, by doing central cropping
        // Choose vertical or horizontal central cropping
        // based on dimension reduction
        if(orig_width > orig_height)
        {
            float change_width  = (float)c.inWidth / (float)orig_width;
            float change_height = (float)c.inHeight / (float)orig_height;
            if(change_width < change_height)
            {
                // E.g. for 1920x1080->512x512, we first crop central part
                // roi(420, 0, 1080, 1080), then resize to (512x512)
                int offset_x = (int)round(0.5 * ((float)orig_width -
                  ((float)orig_height * (float)c.inWidth / (float)c.inHeight)));
                cv::resize(image(Rect(offset_x, 0, orig_width - 2 * offset_x,
                                      orig_height)), s_image,
                           Size(c.inWidth, c.inHeight), 0, 0, cv::INTER_AREA);
            } else {
                // E.g. for 1920x1080->768x320, we first crop central part
                // roi(0, 140, 1920, 800), then resize to (768x320)
                int offset_y = (int)round(0.5 * ((float)orig_height -
                  ((float)orig_width * (float)c.inHeight / (float)c.inWidth)));
                cv::resize(image(Rect(0, offset_y, orig_width,
                                      orig_height - 2 * offset_y)), s_image,
                           Size(c.inWidth, c.inHeight), 0, 0, cv::INTER_AREA);
            }
        } else {
          // E.g. for 540x960->512x512, we first crop central part
          //      roi(0, 210, 540, 540), then resize to (512x512)
          // E.g. for 540x960->768x320, we first crop central part
          //      roi(0, 367, 540, 225), then resize to (768x320)
          int offset_y = (int)round(0.5 * ((float)orig_height -
              ((float)orig_width * (float)c.inHeight / (float)c.inWidth)));
          cv::resize(image(Rect(0, offset_y, orig_width, orig_height -
                                2 * offset_y)), s_image,
                     Size(c.inWidth, c.inHeight), 0, 0, cv::INTER_AREA);
        }
    }

    #ifdef DEBUG_FILES
    {
        // Image files can be converted into video using, example script
        // (on desktop Ubuntu, with ffmpeg installed):
        // ffmpeg -i netin_%04d.png -vf "scale=(iw*sar)*max(768/(iw*sar)\,320/ih):ih*max(768/(iw*sar)\,320/ih), crop=768:320" -b:v 4000k out.mp4
        // Update width 768, height 320, if necessary
        char netin_name[80];
        sprintf(netin_name, "netin_%04d.png", frame_idx);
        cv::imwrite(netin_name, s_image);
        std::cout << "Video input, width:" << orig_width << " height:"
                  << orig_height << " Network width:" << c.inWidth
                  << " height:" << c.inHeight << std::endl;
    }
    #endif

    cv::split(s_image, bgr_frames);
    memcpy(frame_buffer,                bgr_frames[0].ptr(), channel_size);
    memcpy(frame_buffer+1*channel_size, bgr_frames[1].ptr(), channel_size);
    memcpy(frame_buffer+2*channel_size, bgr_frames[2].ptr(), channel_size);
    return true;
}

// Create frame with boxes drawn around classified objects
bool WriteFrameOutput(const ExecutionObjectPipeline& eop,
                      const Configuration& c, const cmdline_opts_t& opts,
                      float confidence_value)
{
    // Asseembly original frame
    int width  = c.inWidth;
    int height = c.inHeight;
    int channel_size = width * height;
    Mat frame, bgr[3];

    unsigned char *in = (unsigned char *) eop.GetInputBufferPtr();
    bgr[0] = Mat(height, width, CV_8UC(1), in);
    bgr[1] = Mat(height, width, CV_8UC(1), in + channel_size);
    bgr[2] = Mat(height, width, CV_8UC(1), in + channel_size*2);
    cv::merge(bgr, 3, frame);

    int frame_index = eop.GetFrameIndex();
    char outfile_name[64];
    if (opts.is_preprocessed_input)
    {
        snprintf(outfile_name, 64, "frame_%d.png", frame_index);
        cv::imwrite(outfile_name, frame);
        printf("Saving frame %d to: %s\n", frame_index, outfile_name);
    }

    // Draw boxes around classified objects
    float *out = (float *) eop.GetOutputBufferPtr();
    int num_floats = eop.GetOutputBufferSizeInBytes() / sizeof(float);
    for (int i = 0; i < num_floats / 7; i++)
    {
        int index = (int)    out[i * 7 + 0];
        if (index < 0)  break;

        float score =        out[i * 7 + 2];
        if (score * 100 < confidence_value)  continue;

        int   label = (int)  out[i * 7 + 1];
        int   xmin  = (int) (out[i * 7 + 3] * width);
        int   ymin  = (int) (out[i * 7 + 4] * height);
        int   xmax  = (int) (out[i * 7 + 5] * width);
        int   ymax  = (int) (out[i * 7 + 6] * height);

        const ObjectClass& object_class = object_classes->At(label);

        if(opts.verbose) {
            printf("%2d: (%d, %d) -> (%d, %d): %s, score=%f\n",
               i, xmin, ymin, xmax, ymax, object_class.label.c_str(), score);
        }

        if (xmin < 0)       xmin = 0;
        if (ymin < 0)       ymin = 0;
        if (xmax > width)   xmax = width;
        if (ymax > height)  ymax = height;
        cv::rectangle(frame, Point(xmin, ymin), Point(xmax, ymax),
                      Scalar(object_class.color.blue,
                             object_class.color.green,
                             object_class.color.red), 2);
    }

    if (opts.is_camera_input || opts.is_video_input)
    {
        cv::imshow("SSD_Multibox", frame);
#ifdef DEBUG_FILES
        // Image files can be converted into video using, example script
        // (on desktop Ubuntu, with ffmpeg installed):
        // ffmpeg -i multibox_%04d.png -vf "scale=(iw*sar)*max(768/(iw*sar)\,320/ih):ih*max(768/(iw*sar)\,320/ih), crop=768:320" -b:v 4000k out.mp4
        // Update width 768, height 320, if necessary
        snprintf(outfile_name, 64, "multibox_%04d.png", frame_index);
        cv::imwrite(outfile_name, r_frame);
#endif
        waitKey(1);
    }
    else
    {
        // Resize to output width/height, keep aspect ratio
        Mat r_frame;
        uint32_t output_width = opts.output_width;
        if (output_width == 0)  output_width = orig_width;
        uint32_t output_height = (output_width*1.0f) / orig_width * orig_height;
        cv::resize(frame, r_frame, Size(output_width, output_height));

        snprintf(outfile_name, 64, "multibox_%d.png", frame_index);
        cv::imwrite(outfile_name, frame);
        printf("Saving frame %d with SSD multiboxes to: %s\n",
               frame_index, outfile_name);
    }

    return true;
}

void DisplayHelp()
{
    std::cout <<
    "Usage: ssd_multibox\n"
    "  Will run partitioned ssd_multibox network to perform "
    "multi-objects detection\n"
    "  and classification.  First part of network "
    "(layersGroupId 1) runs on EVE,\n"
    "  second part (layersGroupId 2) runs on DSP.\n"
    "  Use -c to run a different segmentation network.  Default is jdetnet_voc.\n"
    "Optional arguments:\n"
    " -c <config>          Valid configs: jdetnet_voc, jdetnet \n"
    " -d <number>          Number of dsp cores to use\n"
    " -e <number>          Number of eve cores to use\n"
    " -i <image>           Path to the image file as input\n"
    "                      Default are 9 frames in testvecs\n"
    " -i camera<number>    Use camera as input\n"
    "                      video input port: /dev/video<number>\n"
    " -i <name>.{mp4,mov,avi}  Use video file as input\n"
    " -l <objects_list>    Path to the object classes list file\n"
    " -f <number>          Number of frames to process\n"
    " -w <number>          Output image/video width\n"
    " -p <number>          Output probability threshold in percentage\n"
    "                      Default is 25 percent or higher\n"
    " -v                   Verbose output during execution\n"
    " -h                   Help\n";
}