summaryrefslogtreecommitdiffstats
Commit message (Expand)AuthorAgeFilesLines
* Preparation for [#1443] saving Netbeans development environmentHEADmasterlnetsch2017-10-0457-812/+3017
* Preparation for [#1443]lnetsch2017-10-031-0/+13
* Part of [#1471], update perl libraries usedlnetsch2017-10-031-2/+2
* [#1470] included index for _SILlnetsch2017-10-031-0/+1
* [#1469] Add handling of HTK varFloors macrolnetsch2017-10-031-1/+24
* [#1468] Add arbitrary mixture tying and mean macro sharinglnetsch2017-10-031-18/+558
* [#1461] modify loop to process mean adaptation so index_mean and nbr_cpy are ...lnetsch2014-03-131-3/+5
* [#1455] Add comment on parameter to run continuously.lnetsch2013-10-161-1/+2
* [#1454] Merge changes from C55 branch revision 143 to add a debug function to...lnetsch2013-10-154-0/+120
* [#1451] Merge changes from C55 branch to expand frames search engine can hand...lnetsch2013-10-144-70/+96
* [#1455] Add capability to run continuous live-mode testing in TestTIesrSIlnetsch2013-06-197-6/+30
* [#1455] Add capability to run continuous live-mode testing in TestTIesrSIlnetsch2013-06-192-75/+100
* [#1450] Clarify documentation.lnetsch2013-04-161-4/+4
* [#1450] Track beam and time cell usage. Trigger compression when time cell bu...lnetsch2013-04-123-76/+175
* [#1449] Added capability in TIesrDT to make phones beginning with _ as specia...lnetsch2013-04-012-0/+1
* [#1449] add capability in TIesrDT to handle special HMMs with names beginning...lnetsch2013-01-182-5/+10
* [#1407] add shell script to indicate how to run TestTIesrSD.lnetsch2012-07-051-0/+23
* [#1271] Merge changes and improvements from C55 branch to trunk.lnetsch2012-07-052-16/+16
* [#1271] Merge changes and improvements from C55 branch to trunk. Includes fea...lnetsch2012-07-0335-533/+677
* [#1440] Modify character handling so that hmm indices will never be negative.lnetsch2012-04-121-4/+4
* [#1437] Add stereo data collection in TIesrFA interface and implement in TIes...lnetsch2012-02-014-13/+58
* [#1344] add draft document about TIesr parameters. Fix some TIesr documentation.lnetsch2012-01-065-4/+845
* [#1434] Add Netbeans configurations to build TestTIesrSI for ARM using cross-...lnetsch2012-01-069-1/+299
* [#1434] Add Netbeans configurations to build TIesrSI API for ARM using cross-...lnetsch2012-01-0610-1/+373
* [#1434] Add Netbeans configurations to build TestTIesrFA for ARM using cross-...lnetsch2012-01-069-1/+299
* [#1434] Add Netbeans configurations to build TIesrFA_ALSA API for ARM using c...lnetsch2012-01-0610-1/+290
* [#1434] Add Netbeans configurations to build TIesrEngineSI API for ARM using ...lnetsch2012-01-0610-1/+304
* [#1434] Add Netbeans configurations to build TIesrEngineCore API for ARM usin...lnetsch2012-01-0610-1/+280
* [#1434] Add Netbeans configurations to build TestTIesrFlex for ARM using cros...lnetsch2012-01-069-1/+297
* [#1434] Add Netbeans configurations to build TIesrFlex API for ARM using cros...lnetsch2012-01-0610-1/+319
* [#1434] Add Netbeans configurations to build TestTIesrDict for ARM using cros...lnetsch2012-01-069-1/+293
* [#1434] Add Netbeans configurations to build TIesrDict API for ARM using cros...lnetsch2012-01-0610-1/+310
* [#1434] Add Netbeans configurations to build TestTIesrDT for ARM using cross-...lnetsch2012-01-069-1/+289
* [#1434] Add Netbeans configurations to build TIesrDT for ARM using cross-comp...lnetsch2012-01-0610-1/+280
* [#1429] fixed htk_model_compare bug that did not check correctly if any trail...lnetsch2011-12-011-1/+1
* [#1427] Test specifically for sil or sp phone nameslnetsch2011-11-281-1/+1
* [#1417] Add newline in error message.lnetsch2011-11-111-1/+1
* [#1417] Add maximum limit to number of allowable phones. This limits the numb...lnetsch2011-11-112-1/+10
* [#1407] Initial commit of the TIesr speaker-dependent set of APIs, and suppor...lnetsch2011-08-25116-5/+14775
* [#1407] For some configurations of TIesr hmm2phone.bin is not needed, so tool...lnetsch2011-07-051-6/+8
* [#1358] - Prepare documentation additions and release notes for Beta_1.4 releaseBeta_1.4lnetsch2011-05-172-22/+1681
* [#1354] Add documentation comments to TRAN_DUR_BIAS macrolnetsch2011-05-171-1/+5
* [#1355] Add default SAMPLE_RATE for windows version of TestTIesrSI. Set check...lnetsch2011-05-162-1/+2
* [#1354] Merge r75 changes from cm_mods branch to trunk to implement a penalty...lnetsch2011-05-132-61/+115
* [#1350] Set defaults for scaling in the event of an all-zero input vector, or...lnetsch2011-05-132-33/+34
* [#1341] Fix loc_accum normalization to use frame_cnt[0].lnetsch2011-05-111-2/+3
* [#1348] Merge changes that fix FFT normalization from cm_mods branch to trunk.lnetsch2011-04-215-3/+11
* [#1347] added relative reference to versioning file in TIesrSIso, TIesrEngine...lnetsch2011-04-153-2/+3
* [#1345] Update default configuration for TestTIesrDT Netbeans projectlnetsch2011-04-141-1/+1
* [#1326] Allow priors for MFCC vectors of any size. User should define constan...lnetsch2011-04-124-35/+79