#
# For a description of the syntax of this configuration file,
# see the file Documentation/kbuild/kconfig-language.txt in the
# Linux kernel source tree.
#
mainmenu "U-Boot $UBOOTVERSION Configuration"
config UBOOTVERSION
string
option env="UBOOTVERSION"
# Allow defaults in arch-specific code to override any given here
source "arch/Kconfig"
menu "General setup"
config LOCALVERSION
string "Local version - append to U-Boot release"
help
Append an extra string to the end of your U-Boot version.
This will show up in your boot log, for example.
The string you set here will be appended after the contents of
any files with a filename matching localversion* in your
object and source tree, in that order. Your total string can
be a maximum of 64 characters.
config LOCALVERSION_AUTO
bool "Automatically append version information to the version string"
default y
help
This will try to automatically determine if the current tree is a
release tree by looking for Git tags that belong to the current
top of tree revision.
A string of the format -gxxxxxxxx will be added to the localversion
if a Git-based tree is found. The string generated by this will be
appended after any matching localversion* files, and after the value
set in CONFIG_LOCALVERSION.
(The actual string used here is the first eight characters produced
by running the command:
$ git rev-parse --verify HEAD
which is done within the script "scripts/setlocalversion".)
config CC_OPTIMIZE_FOR_SIZE
bool "Optimize for size"
default y
help
Enabling this option will pass "-Os" instead of "-O2" to gcc
resulting in a smaller U-Boot image.
This option is enabled by default for U-Boot.
config SYS_MALLOC_F
bool "Enable malloc() pool before relocation"
default y if DM
help
Before relocation, memory is very limited on many platforms. Still,
we can provide a small malloc() pool if needed. Driver model in
particular needs this to operate, so that it can allocate the
initial serial device and any others that are needed.
config SYS_MALLOC_F_LEN
hex "Size of malloc() pool before relocation"
depends on SYS_MALLOC_F
default 0x400
help
Before relocation, memory is very limited on many platforms. Still,
we can provide a small malloc() pool if needed. Driver model in
particular needs this to operate, so that it can allocate the
initial serial device and any others that are needed.
menuconfig EXPERT
bool "Configure standard U-Boot features (expert users)"
default y
help
This option allows certain base U-Boot options and settings
to be disabled or tweaked. This is for specialized
environments which can tolerate a "non-standard" U-Boot.
Use this only if you really know what you are doing.
if EXPERT
config SYS_MALLOC_CLEAR_ON_INIT
bool "Init with zeros the memory reserved for malloc (slow)"
default y
help
This setting is enabled by default. The reserved malloc
memory is initialized with zeros, so first malloc calls
will return the pointer to the zeroed memory. But this
slows the boot time.
It is recommended to disable it, when CONFIG_SYS_MALLOC_LEN
value, has more than few MiB, e.g. when uses bzip2 or bmp logo.
Then the boot time can be significantly reduced.
Warning:
When disabling this, please check if malloc calls, maybe
should be replaced by calloc - if one expects zeroed memory.
endif
endmenu # General setup
menu "Boot images"
config SUPPORT_SPL
bool
config SUPPORT_TPL
bool
config SPL
bool
depends on SUPPORT_SPL
prompt "Enable SPL"
help
If you want to build SPL as well as the normal image, say Y.
config SPL_SYS_MALLOC_SIMPLE
bool
depends on SPL
prompt "Only use malloc_simple functions in the SPL"
help
Say Y here to only use the *_simple malloc functions from
malloc_simple.c, rather then using the versions from dlmalloc.c;
this will make the SPL binary smaller at the cost of more heap
usage as the *_simple malloc functions do not re-use free-ed mem.
config SPL_STACK_R
depends on SPL
bool "Enable SDRAM location for SPL stack"
help
SPL starts off execution in SRAM and thus typically has only a small
stack available. Since SPL sets up DRAM while in its board_init_f()
function, it is possible for the stack to move there before
board_init_r() is reached. This option enables a special SDRAM
location for the SPL stack. U-Boot SPL switches to this after
board_init_f() completes, and before board_init_r() starts.
config SPL_STACK_R_ADDR
depends on SPL_STACK_R
hex "SDRAM location for SPL stack"
help
Specify the address in SDRAM for the SPL stack. This will be set up
before board_init_r() is called.
config SPL_STACK_R_MALLOC_SIMPLE_LEN
depends on SPL_STACK_R && SPL_SYS_MALLOC_SIMPLE
hex "Size of malloc_simple heap after switching to DRAM SPL stack"
default 0x100000
help
Specify the amount of the stack to use as memory pool for
malloc_simple after switching the stack to DRAM. This may be set
to give board_init_r() a larger heap then the initial heap in
SRAM which is limited to SYS_MALLOC_F_LEN bytes.
config SPL_SEPARATE_BSS
depends on SPL
bool "BSS section is in a different memory region from text"
help
Some platforms need a large BSS region in SPL and can provide this
because RAM is already set up. In this case BSS can be moved to RAM.
This option should then be enabled so that the correct device tree
location is used. Normally we put the device tree at the end of BSS
but with this option enabled, it goes at _image_binary_end.
config TPL
bool
depends on SPL && SUPPORT_TPL
prompt "Enable TPL"
help
If you want to build TPL as well as the normal image and SPL, say Y.
config FIT
bool "Support Flattened Image Tree"
help
This option allows to boot the new uImage structrure,
Flattened Image Tree. FIT is formally a FDT, which can include
images of various types (kernel, FDT blob, ramdisk, etc.)
in a single blob. To boot this new uImage structure,
pass the address of the blob to the "bootm" command.
FIT is very flexible, supporting compression, multiple images,
multiple configurations, verification through hashing and also
verified boot (secure boot using RSA). This option enables that
feature.
config FIT_VERBOSE
bool "Display verbose messages on FIT boot"
depends on FIT
config FIT_SIGNATURE
bool "Enable signature verification of FIT uImages"
depends on FIT
depends on DM
select RSA
help
This option enables signature verification of FIT uImages,
using a hash signed and verified using RSA. If
CONFIG_SHA_PROG_HW_ACCEL is defined, i.e support for progressive
hashing is available using hardware, then then RSA library will use
it. See doc/uImage.FIT/signature.txt for more details.
WARNING: When relying on signed FIT images with a required signature
check the legacy image format is disabled by default, so that
unsigned images cannot be loaded. If a board needs the legacy image
format support in this case, enable it using
CONFIG_IMAGE_FORMAT_LEGACY.
config FIT_BEST_MATCH
bool "Select the best match for the kernel device tree"
depends on FIT
help
When no configuration is explicitly selected, default to the
one whose fdt's compatibility field best matches that of
U-Boot itself. A match is considered "best" if it matches the
most specific compatibility entry of U-Boot's fdt's root node.
The order of entries in the configuration's fdt is ignored.
config FIT_VERBOSE
bool "Show verbose messages when FIT images fails"
depends on FIT
help
Generally a system will have valid FIT images so debug messages
are a waste of code space. If you are debugging your images then
you can enable this option to get more verbose information about
failures.
config OF_BOARD_SETUP
bool "Set up board-specific details in device tree before boot"
depends on OF_LIBFDT
help
This causes U-Boot to call ft_board_setup() before booting into
the Operating System. This function can set up various
board-specific information in the device tree for use by the OS.
The device tree is then passed to the OS.
config OF_SYSTEM_SETUP
bool "Set up system-specific details in device tree before boot"
depends on OF_LIBFDT
help
This causes U-Boot to call ft_system_setup() before booting into
the Operating System. This function can set up various
system-specific information in the device tree for use by the OS.
The device tree is then passed to the OS.
config OF_STDOUT_VIA_ALIAS
bool "Update the device-tree stdout alias from U-Boot"
depends on OF_LIBFDT
help
This uses U-Boot's serial alias from the aliases node to update
the device tree passed to the OS. The "linux,stdout-path" property
in the chosen node is set to point to the correct serial node.
This option currently references CONFIG_CONS_INDEX, which is
incorrect when used with device tree as this option does not
exist / should not be used.
config SYS_EXTRA_OPTIONS
string "Extra Options (DEPRECATED)"
help
The old configuration infrastructure (= mkconfig + boards.cfg)
provided the extra options field. If you have something like
"HAS_BAR,BAZ=64", the optional options
#define CONFIG_HAS
#define CONFIG_BAZ 64
will be defined in include/config.h.
This option was prepared for the smooth migration from the old
configuration to Kconfig. Since this option will be removed sometime,
new boards should not use this option.
config SYS_TEXT_BASE
depends on SPARC || ARC || X86 || ARCH_UNIPHIER || ARCH_ZYNQMP || \
(M68K && !TARGET_ASTRO_MCF5373L) || MICROBLAZE
depends on !EFI_APP
hex "Text Base"
help
TODO: Move CONFIG_SYS_TEXT_BASE for all the architecture
config SPL_LOAD_FIT
bool "Enable SPL loading U-Boot as a FIT"
depends on FIT
help
Normally with the SPL framework a legacy image is generated as part
of the build. This contains U-Boot along with information as to
where it should be loaded. This option instead enables generation
of a FIT (Flat Image Tree) which provides more flexibility. In
particular it can handle selecting from multiple device tree
and passing the correct one to U-Boot.
config SYS_CLK_FREQ
depends on ARC || ARCH_SUNXI
int "CPU clock frequency"
help
TODO: Move CONFIG_SYS_CLK_FREQ for all the architecture
endmenu # Boot images
source "common/Kconfig"
source "cmd/Kconfig"
source "dts/Kconfig"
source "net/Kconfig"
source "drivers/Kconfig"
source "fs/Kconfig"
source "lib/Kconfig"
source "test/Kconfig"