diff options
author | Laszlo Ersek | 2016-03-03 17:53:12 -0600 |
---|---|---|
committer | Laszlo Ersek | 2016-03-10 14:28:29 -0600 |
commit | 7523788faa51e1a94e87ddb984ceacf8dc8a49bb (patch) | |
tree | f9b62be3eeaa23a4594ade74e9b8a771aeaf813c | |
parent | 7b8fe63561b43f0ae47673a32d27e4967149b556 (diff) | |
download | ti-edk2-7523788faa51e1a94e87ddb984ceacf8dc8a49bb.tar.gz ti-edk2-7523788faa51e1a94e87ddb984ceacf8dc8a49bb.tar.xz ti-edk2-7523788faa51e1a94e87ddb984ceacf8dc8a49bb.zip |
OvmfPkg: add DxePciLibI440FxQ35
This library is a trivial unification of the following two PciLib
instances (and the result is easily diffable against each):
- MdePkg/Library/BasePciLibCf8
- MdePkg/Library/BasePciLibPciExpress
The PCI config access method is determined in the constructor function,
from the dynamic PCD "PcdOvmfHostBridgePciDevId" that is set by
PlatformPei.
The library instance is usable in DXE phase or later modules: the PciLib
instances being unified have no firmware phase / client module type
restrictions, and here the only PCD access is made in the constructor
function. That is, even before a given client executable's entry point is
invoked.
The library instance depends on PlatformPei both for setting the PCD
mentioned above, and also for enabling MMCONFIG on Q35. PEI and earlier
phase modules are not expected to need extended config access even on Q35.
Cc: Gabriel Somlo <somlo@cmu.edu>
Cc: Gerd Hoffmann <kraxel@redhat.com>
Cc: Jordan Justen <jordan.l.justen@intel.com>
Cc: Marcel Apfelbaum <marcel@redhat.com>
Cc: Michał Zegan <webczat_200@poczta.onet.pl>
Contributed-under: TianoCore Contribution Agreement 1.0
Signed-off-by: Laszlo Ersek <lersek@redhat.com>
Reviewed-by: Jordan Justen <jordan.l.justen@intel.com>
Tested-by: Gabriel Somlo <somlo@cmu.edu>
Tested-by: Michał Zegan <webczat_200@poczta.onet.pl>
-rw-r--r-- | OvmfPkg/Library/DxePciLibI440FxQ35/DxePciLibI440FxQ35.inf | 47 | ||||
-rw-r--r-- | OvmfPkg/Library/DxePciLibI440FxQ35/PciLib.c | 1229 |
2 files changed, 1276 insertions, 0 deletions
diff --git a/OvmfPkg/Library/DxePciLibI440FxQ35/DxePciLibI440FxQ35.inf b/OvmfPkg/Library/DxePciLibI440FxQ35/DxePciLibI440FxQ35.inf new file mode 100644 index 000000000..2bd10cc23 --- /dev/null +++ b/OvmfPkg/Library/DxePciLibI440FxQ35/DxePciLibI440FxQ35.inf | |||
@@ -0,0 +1,47 @@ | |||
1 | ## @file | ||
2 | # An instance of the PCI Library that is based on both the PCI CF8 Library and | ||
3 | # the PCI Express Library. | ||
4 | # | ||
5 | # This PciLib instance caches the OVMF platform type (I440FX vs. Q35) in | ||
6 | # its entry point function, then delegates function calls to one of the | ||
7 | # PciCf8Lib or PciExpressLib "backends" as appropriate. | ||
8 | # | ||
9 | # Copyright (C) 2016, Red Hat, Inc. | ||
10 | # | ||
11 | # Copyright (c) 2007 - 2014, Intel Corporation. All rights reserved.<BR> | ||
12 | # | ||
13 | # This program and the accompanying materials are licensed and made available | ||
14 | # under the terms and conditions of the BSD License which accompanies this | ||
15 | # distribution. The full text of the license may be found at | ||
16 | # http://opensource.org/licenses/bsd-license.php. | ||
17 | # | ||
18 | # THE PROGRAM IS DISTRIBUTED UNDER THE BSD LICENSE ON AN "AS IS" BASIS, | ||
19 | # WITHOUT WARRANTIES OR REPRESENTATIONS OF ANY KIND, EITHER EXPRESS OR | ||
20 | # IMPLIED. | ||
21 | ## | ||
22 | |||
23 | [Defines] | ||
24 | INF_VERSION = 0x00010005 | ||
25 | BASE_NAME = DxePciLibI440FxQ35 | ||
26 | FILE_GUID = 5360bff6-3911-4495-ae3c-b02ff004b585 | ||
27 | MODULE_TYPE = BASE | ||
28 | VERSION_STRING = 1.0 | ||
29 | LIBRARY_CLASS = PciLib|DXE_DRIVER DXE_RUNTIME_DRIVER SMM_CORE DXE_SMM_DRIVER UEFI_DRIVER UEFI_APPLICATION | ||
30 | CONSTRUCTOR = InitializeConfigAccessMethod | ||
31 | |||
32 | # VALID_ARCHITECTURES = IA32 X64 | ||
33 | |||
34 | [Sources] | ||
35 | PciLib.c | ||
36 | |||
37 | [Packages] | ||
38 | MdePkg/MdePkg.dec | ||
39 | OvmfPkg/OvmfPkg.dec | ||
40 | |||
41 | [LibraryClasses] | ||
42 | PcdLib | ||
43 | PciCf8Lib | ||
44 | PciExpressLib | ||
45 | |||
46 | [Pcd] | ||
47 | gUefiOvmfPkgTokenSpaceGuid.PcdOvmfHostBridgePciDevId | ||
diff --git a/OvmfPkg/Library/DxePciLibI440FxQ35/PciLib.c b/OvmfPkg/Library/DxePciLibI440FxQ35/PciLib.c new file mode 100644 index 000000000..6c1a27297 --- /dev/null +++ b/OvmfPkg/Library/DxePciLibI440FxQ35/PciLib.c | |||
@@ -0,0 +1,1229 @@ | |||
1 | /** @file | ||
2 | PCI Library functions that use | ||
3 | (a) I/O ports 0xCF8 and 0xCFC to perform PCI Configuration cycles, layering | ||
4 | on top of one PCI CF8 Library instance; or | ||
5 | (b) PCI Library functions that use the 256 MB PCI Express MMIO window to | ||
6 | perform PCI Configuration cycles, layering on PCI Express Library. | ||
7 | |||
8 | The decision is made in the entry point function, based on the OVMF platform | ||
9 | type, and then adhered to during the lifetime of the client module. | ||
10 | |||
11 | Copyright (C) 2016, Red Hat, Inc. | ||
12 | |||
13 | Copyright (c) 2006 - 2012, Intel Corporation. All rights reserved.<BR> | ||
14 | This program and the accompanying materials | ||
15 | are licensed and made available under the terms and conditions of the BSD License | ||
16 | which accompanies this distribution. The full text of the license may be found at | ||
17 | http://opensource.org/licenses/bsd-license.php. | ||
18 | |||
19 | THE PROGRAM IS DISTRIBUTED UNDER THE BSD LICENSE ON AN "AS IS" BASIS, | ||
20 | WITHOUT WARRANTIES OR REPRESENTATIONS OF ANY KIND, EITHER EXPRESS OR IMPLIED. | ||
21 | |||
22 | **/ | ||
23 | |||
24 | |||
25 | #include <Base.h> | ||
26 | |||
27 | #include <IndustryStandard/Q35MchIch9.h> | ||
28 | |||
29 | #include <Library/PciLib.h> | ||
30 | #include <Library/PciCf8Lib.h> | ||
31 | #include <Library/PciExpressLib.h> | ||
32 | #include <Library/PcdLib.h> | ||
33 | |||
34 | STATIC BOOLEAN mRunningOnQ35; | ||
35 | |||
36 | RETURN_STATUS | ||
37 | EFIAPI | ||
38 | InitializeConfigAccessMethod ( | ||
39 | VOID | ||
40 | ) | ||
41 | { | ||
42 | mRunningOnQ35 = (PcdGet16 (PcdOvmfHostBridgePciDevId) == | ||
43 | INTEL_Q35_MCH_DEVICE_ID); | ||
44 | return RETURN_SUCCESS; | ||
45 | } | ||
46 | |||
47 | /** | ||
48 | Registers a PCI device so PCI configuration registers may be accessed after | ||
49 | SetVirtualAddressMap(). | ||
50 | |||
51 | Registers the PCI device specified by Address so all the PCI configuration registers | ||
52 | associated with that PCI device may be accessed after SetVirtualAddressMap() is called. | ||
53 | |||
54 | If Address > 0x0FFFFFFF, then ASSERT(). | ||
55 | |||
56 | @param Address The address that encodes the PCI Bus, Device, Function and | ||
57 | Register. | ||
58 | |||
59 | @retval RETURN_SUCCESS The PCI device was registered for runtime access. | ||
60 | @retval RETURN_UNSUPPORTED An attempt was made to call this function | ||
61 | after ExitBootServices(). | ||
62 | @retval RETURN_UNSUPPORTED The resources required to access the PCI device | ||
63 | at runtime could not be mapped. | ||
64 | @retval RETURN_OUT_OF_RESOURCES There are not enough resources available to | ||
65 | complete the registration. | ||
66 | |||
67 | **/ | ||
68 | RETURN_STATUS | ||
69 | EFIAPI | ||
70 | PciRegisterForRuntimeAccess ( | ||
71 | IN UINTN Address | ||
72 | ) | ||
73 | { | ||
74 | return mRunningOnQ35 ? | ||
75 | PciExpressRegisterForRuntimeAccess (Address) : | ||
76 | PciCf8RegisterForRuntimeAccess (Address); | ||
77 | } | ||
78 | |||
79 | /** | ||
80 | Reads an 8-bit PCI configuration register. | ||
81 | |||
82 | Reads and returns the 8-bit PCI configuration register specified by Address. | ||
83 | This function must guarantee that all PCI read and write operations are | ||
84 | serialized. | ||
85 | |||
86 | If Address > 0x0FFFFFFF, then ASSERT(). | ||
87 | |||
88 | @param Address The address that encodes the PCI Bus, Device, Function and | ||
89 | Register. | ||
90 | |||
91 | @return The read value from the PCI configuration register. | ||
92 | |||
93 | **/ | ||
94 | UINT8 | ||
95 | EFIAPI | ||
96 | PciRead8 ( | ||
97 | IN UINTN Address | ||
98 | ) | ||
99 | { | ||
100 | return mRunningOnQ35 ? | ||
101 | PciExpressRead8 (Address) : | ||
102 | PciCf8Read8 (Address); | ||
103 | } | ||
104 | |||
105 | /** | ||
106 | Writes an 8-bit PCI configuration register. | ||
107 | |||
108 | Writes the 8-bit PCI configuration register specified by Address with the | ||
109 | value specified by Value. Value is returned. This function must guarantee | ||
110 | that all PCI read and write operations are serialized. | ||
111 | |||
112 | If Address > 0x0FFFFFFF, then ASSERT(). | ||
113 | |||
114 | @param Address The address that encodes the PCI Bus, Device, Function and | ||
115 | Register. | ||
116 | @param Value The value to write. | ||
117 | |||
118 | @return The value written to the PCI configuration register. | ||
119 | |||
120 | **/ | ||
121 | UINT8 | ||
122 | EFIAPI | ||
123 | PciWrite8 ( | ||
124 | IN UINTN Address, | ||
125 | IN UINT8 Value | ||
126 | ) | ||
127 | { | ||
128 | return mRunningOnQ35 ? | ||
129 | PciExpressWrite8 (Address, Value) : | ||
130 | PciCf8Write8 (Address, Value); | ||
131 | } | ||
132 | |||
133 | /** | ||
134 | Performs a bitwise OR of an 8-bit PCI configuration register with | ||
135 | an 8-bit value. | ||
136 | |||
137 | Reads the 8-bit PCI configuration register specified by Address, performs a | ||
138 | bitwise OR between the read result and the value specified by | ||
139 | OrData, and writes the result to the 8-bit PCI configuration register | ||
140 | specified by Address. The value written to the PCI configuration register is | ||
141 | returned. This function must guarantee that all PCI read and write operations | ||
142 | are serialized. | ||
143 | |||
144 | If Address > 0x0FFFFFFF, then ASSERT(). | ||
145 | |||
146 | @param Address The address that encodes the PCI Bus, Device, Function and | ||
147 | Register. | ||
148 | @param OrData The value to OR with the PCI configuration register. | ||
149 | |||
150 | @return The value written back to the PCI configuration register. | ||
151 | |||
152 | **/ | ||
153 | UINT8 | ||
154 | EFIAPI | ||
155 | PciOr8 ( | ||
156 | IN UINTN Address, | ||
157 | IN UINT8 OrData | ||
158 | ) | ||
159 | { | ||
160 | return mRunningOnQ35 ? | ||
161 | PciExpressOr8 (Address, OrData) : | ||
162 | PciCf8Or8 (Address, OrData); | ||
163 | } | ||
164 | |||
165 | /** | ||
166 | Performs a bitwise AND of an 8-bit PCI configuration register with an 8-bit | ||
167 | value. | ||
168 | |||
169 | Reads the 8-bit PCI configuration register specified by Address, performs a | ||
170 | bitwise AND between the read result and the value specified by AndData, and | ||
171 | writes the result to the 8-bit PCI configuration register specified by | ||
172 | Address. The value written to the PCI configuration register is returned. | ||
173 | This function must guarantee that all PCI read and write operations are | ||
174 | serialized. | ||
175 | |||
176 | If Address > 0x0FFFFFFF, then ASSERT(). | ||
177 | |||
178 | @param Address The address that encodes the PCI Bus, Device, Function and | ||
179 | Register. | ||
180 | @param AndData The value to AND with the PCI configuration register. | ||
181 | |||
182 | @return The value written back to the PCI configuration register. | ||
183 | |||
184 | **/ | ||
185 | UINT8 | ||
186 | EFIAPI | ||
187 | PciAnd8 ( | ||
188 | IN UINTN Address, | ||
189 | IN UINT8 AndData | ||
190 | ) | ||
191 | { | ||
192 | return mRunningOnQ35 ? | ||
193 | PciExpressAnd8 (Address, AndData) : | ||
194 | PciCf8And8 (Address, AndData); | ||
195 | } | ||
196 | |||
197 | /** | ||
198 | Performs a bitwise AND of an 8-bit PCI configuration register with an 8-bit | ||
199 | value, followed a bitwise OR with another 8-bit value. | ||
200 | |||
201 | Reads the 8-bit PCI configuration register specified by Address, performs a | ||
202 | bitwise AND between the read result and the value specified by AndData, | ||
203 | performs a bitwise OR between the result of the AND operation and | ||
204 | the value specified by OrData, and writes the result to the 8-bit PCI | ||
205 | configuration register specified by Address. The value written to the PCI | ||
206 | configuration register is returned. This function must guarantee that all PCI | ||
207 | read and write operations are serialized. | ||
208 | |||
209 | If Address > 0x0FFFFFFF, then ASSERT(). | ||
210 | |||
211 | @param Address The address that encodes the PCI Bus, Device, Function and | ||
212 | Register. | ||
213 | @param AndData The value to AND with the PCI configuration register. | ||
214 | @param OrData The value to OR with the result of the AND operation. | ||
215 | |||
216 | @return The value written back to the PCI configuration register. | ||
217 | |||
218 | **/ | ||
219 | UINT8 | ||
220 | EFIAPI | ||
221 | PciAndThenOr8 ( | ||
222 | IN UINTN Address, | ||
223 | IN UINT8 AndData, | ||
224 | IN UINT8 OrData | ||
225 | ) | ||
226 | { | ||
227 | return mRunningOnQ35 ? | ||
228 | PciExpressAndThenOr8 (Address, AndData, OrData) : | ||
229 | PciCf8AndThenOr8 (Address, AndData, OrData); | ||
230 | } | ||
231 | |||
232 | /** | ||
233 | Reads a bit field of a PCI configuration register. | ||
234 | |||
235 | Reads the bit field in an 8-bit PCI configuration register. The bit field is | ||
236 | specified by the StartBit and the EndBit. The value of the bit field is | ||
237 | returned. | ||
238 | |||
239 | If Address > 0x0FFFFFFF, then ASSERT(). | ||
240 | If StartBit is greater than 7, then ASSERT(). | ||
241 | If EndBit is greater than 7, then ASSERT(). | ||
242 | If EndBit is less than StartBit, then ASSERT(). | ||
243 | |||
244 | @param Address The PCI configuration register to read. | ||
245 | @param StartBit The ordinal of the least significant bit in the bit field. | ||
246 | Range 0..7. | ||
247 | @param EndBit The ordinal of the most significant bit in the bit field. | ||
248 | Range 0..7. | ||
249 | |||
250 | @return The value of the bit field read from the PCI configuration register. | ||
251 | |||
252 | **/ | ||
253 | UINT8 | ||
254 | EFIAPI | ||
255 | PciBitFieldRead8 ( | ||
256 | IN UINTN Address, | ||
257 | IN UINTN StartBit, | ||
258 | IN UINTN EndBit | ||
259 | ) | ||
260 | { | ||
261 | return mRunningOnQ35 ? | ||
262 | PciExpressBitFieldRead8 (Address, StartBit, EndBit) : | ||
263 | PciCf8BitFieldRead8 (Address, StartBit, EndBit); | ||
264 | } | ||
265 | |||
266 | /** | ||
267 | Writes a bit field to a PCI configuration register. | ||
268 | |||
269 | Writes Value to the bit field of the PCI configuration register. The bit | ||
270 | field is specified by the StartBit and the EndBit. All other bits in the | ||
271 | destination PCI configuration register are preserved. The new value of the | ||
272 | 8-bit register is returned. | ||
273 | |||
274 | If Address > 0x0FFFFFFF, then ASSERT(). | ||
275 | If StartBit is greater than 7, then ASSERT(). | ||
276 | If EndBit is greater than 7, then ASSERT(). | ||
277 | If EndBit is less than StartBit, then ASSERT(). | ||
278 | If Value is larger than the bitmask value range specified by StartBit and EndBit, then ASSERT(). | ||
279 | |||
280 | @param Address The PCI configuration register to write. | ||
281 | @param StartBit The ordinal of the least significant bit in the bit field. | ||
282 | Range 0..7. | ||
283 | @param EndBit The ordinal of the most significant bit in the bit field. | ||
284 | Range 0..7. | ||
285 | @param Value The new value of the bit field. | ||
286 | |||
287 | @return The value written back to the PCI configuration register. | ||
288 | |||
289 | **/ | ||
290 | UINT8 | ||
291 | EFIAPI | ||
292 | PciBitFieldWrite8 ( | ||
293 | IN UINTN Address, | ||
294 | IN UINTN StartBit, | ||
295 | IN UINTN EndBit, | ||
296 | IN UINT8 Value | ||
297 | ) | ||
298 | { | ||
299 | return mRunningOnQ35 ? | ||
300 | PciExpressBitFieldWrite8 (Address, StartBit, EndBit, Value) : | ||
301 | PciCf8BitFieldWrite8 (Address, StartBit, EndBit, Value); | ||
302 | } | ||
303 | |||
304 | /** | ||
305 | Reads a bit field in an 8-bit PCI configuration, performs a bitwise OR, and | ||
306 | writes the result back to the bit field in the 8-bit port. | ||
307 | |||
308 | Reads the 8-bit PCI configuration register specified by Address, performs a | ||
309 | bitwise OR between the read result and the value specified by | ||
310 | OrData, and writes the result to the 8-bit PCI configuration register | ||
311 | specified by Address. The value written to the PCI configuration register is | ||
312 | returned. This function must guarantee that all PCI read and write operations | ||
313 | are serialized. Extra left bits in OrData are stripped. | ||
314 | |||
315 | If Address > 0x0FFFFFFF, then ASSERT(). | ||
316 | If StartBit is greater than 7, then ASSERT(). | ||
317 | If EndBit is greater than 7, then ASSERT(). | ||
318 | If EndBit is less than StartBit, then ASSERT(). | ||
319 | If OrData is larger than the bitmask value range specified by StartBit and EndBit, then ASSERT(). | ||
320 | |||
321 | @param Address The PCI configuration register to write. | ||
322 | @param StartBit The ordinal of the least significant bit in the bit field. | ||
323 | Range 0..7. | ||
324 | @param EndBit The ordinal of the most significant bit in the bit field. | ||
325 | Range 0..7. | ||
326 | @param OrData The value to OR with the PCI configuration register. | ||
327 | |||
328 | @return The value written back to the PCI configuration register. | ||
329 | |||
330 | **/ | ||
331 | UINT8 | ||
332 | EFIAPI | ||
333 | PciBitFieldOr8 ( | ||
334 | IN UINTN Address, | ||
335 | IN UINTN StartBit, | ||
336 | IN UINTN EndBit, | ||
337 | IN UINT8 OrData | ||
338 | ) | ||
339 | { | ||
340 | return mRunningOnQ35 ? | ||
341 | PciExpressBitFieldOr8 (Address, StartBit, EndBit, OrData) : | ||
342 | PciCf8BitFieldOr8 (Address, StartBit, EndBit, OrData); | ||
343 | } | ||
344 | |||
345 | /** | ||
346 | Reads a bit field in an 8-bit PCI configuration register, performs a bitwise | ||
347 | AND, and writes the result back to the bit field in the 8-bit register. | ||
348 | |||
349 | Reads the 8-bit PCI configuration register specified by Address, performs a | ||
350 | bitwise AND between the read result and the value specified by AndData, and | ||
351 | writes the result to the 8-bit PCI configuration register specified by | ||
352 | Address. The value written to the PCI configuration register is returned. | ||
353 | This function must guarantee that all PCI read and write operations are | ||
354 | serialized. Extra left bits in AndData are stripped. | ||
355 | |||
356 | If Address > 0x0FFFFFFF, then ASSERT(). | ||
357 | If StartBit is greater than 7, then ASSERT(). | ||
358 | If EndBit is greater than 7, then ASSERT(). | ||
359 | If EndBit is less than StartBit, then ASSERT(). | ||
360 | If AndData is larger than the bitmask value range specified by StartBit and EndBit, then ASSERT(). | ||
361 | |||
362 | @param Address The PCI configuration register to write. | ||
363 | @param StartBit The ordinal of the least significant bit in the bit field. | ||
364 | Range 0..7. | ||
365 | @param EndBit The ordinal of the most significant bit in the bit field. | ||
366 | Range 0..7. | ||
367 | @param AndData The value to AND with the PCI configuration register. | ||
368 | |||
369 | @return The value written back to the PCI configuration register. | ||
370 | |||
371 | **/ | ||
372 | UINT8 | ||
373 | EFIAPI | ||
374 | PciBitFieldAnd8 ( | ||
375 | IN UINTN Address, | ||
376 | IN UINTN StartBit, | ||
377 | IN UINTN EndBit, | ||
378 | IN UINT8 AndData | ||
379 | ) | ||
380 | { | ||
381 | return mRunningOnQ35 ? | ||
382 | PciExpressBitFieldAnd8 (Address, StartBit, EndBit, AndData) : | ||
383 | PciCf8BitFieldAnd8 (Address, StartBit, EndBit, AndData); | ||
384 | } | ||
385 | |||
386 | /** | ||
387 | Reads a bit field in an 8-bit port, performs a bitwise AND followed by a | ||
388 | bitwise OR, and writes the result back to the bit field in the | ||
389 | 8-bit port. | ||
390 | |||
391 | Reads the 8-bit PCI configuration register specified by Address, performs a | ||
392 | bitwise AND followed by a bitwise OR between the read result and | ||
393 | the value specified by AndData, and writes the result to the 8-bit PCI | ||
394 | configuration register specified by Address. The value written to the PCI | ||
395 | configuration register is returned. This function must guarantee that all PCI | ||
396 | read and write operations are serialized. Extra left bits in both AndData and | ||
397 | OrData are stripped. | ||
398 | |||
399 | If Address > 0x0FFFFFFF, then ASSERT(). | ||
400 | If StartBit is greater than 7, then ASSERT(). | ||
401 | If EndBit is greater than 7, then ASSERT(). | ||
402 | If EndBit is less than StartBit, then ASSERT(). | ||
403 | If AndData is larger than the bitmask value range specified by StartBit and EndBit, then ASSERT(). | ||
404 | If OrData is larger than the bitmask value range specified by StartBit and EndBit, then ASSERT(). | ||
405 | |||
406 | @param Address The PCI configuration register to write. | ||
407 | @param StartBit The ordinal of the least significant bit in the bit field. | ||
408 | Range 0..7. | ||
409 | @param EndBit The ordinal of the most significant bit in the bit field. | ||
410 | Range 0..7. | ||
411 | @param AndData The value to AND with the PCI configuration register. | ||
412 | @param OrData The value to OR with the result of the AND operation. | ||
413 | |||
414 | @return The value written back to the PCI configuration register. | ||
415 | |||
416 | **/ | ||
417 | UINT8 | ||
418 | EFIAPI | ||
419 | PciBitFieldAndThenOr8 ( | ||
420 | IN UINTN Address, | ||
421 | IN UINTN StartBit, | ||
422 | IN UINTN EndBit, | ||
423 | IN UINT8 AndData, | ||
424 | IN UINT8 OrData | ||
425 | ) | ||
426 | { | ||
427 | return mRunningOnQ35 ? | ||
428 | PciExpressBitFieldAndThenOr8 (Address, StartBit, EndBit, AndData, OrData) : | ||
429 | PciCf8BitFieldAndThenOr8 (Address, StartBit, EndBit, AndData, OrData); | ||
430 | } | ||
431 | |||
432 | /** | ||
433 | Reads a 16-bit PCI configuration register. | ||
434 | |||
435 | Reads and returns the 16-bit PCI configuration register specified by Address. | ||
436 | This function must guarantee that all PCI read and write operations are | ||
437 | serialized. | ||
438 | |||
439 | If Address > 0x0FFFFFFF, then ASSERT(). | ||
440 | If Address is not aligned on a 16-bit boundary, then ASSERT(). | ||
441 | |||
442 | @param Address The address that encodes the PCI Bus, Device, Function and | ||
443 | Register. | ||
444 | |||
445 | @return The read value from the PCI configuration register. | ||
446 | |||
447 | **/ | ||
448 | UINT16 | ||
449 | EFIAPI | ||
450 | PciRead16 ( | ||
451 | IN UINTN Address | ||
452 | ) | ||
453 | { | ||
454 | return mRunningOnQ35 ? | ||
455 | PciExpressRead16 (Address) : | ||
456 | PciCf8Read16 (Address); | ||
457 | } | ||
458 | |||
459 | /** | ||
460 | Writes a 16-bit PCI configuration register. | ||
461 | |||
462 | Writes the 16-bit PCI configuration register specified by Address with the | ||
463 | value specified by Value. Value is returned. This function must guarantee | ||
464 | that all PCI read and write operations are serialized. | ||
465 | |||
466 | If Address > 0x0FFFFFFF, then ASSERT(). | ||
467 | If Address is not aligned on a 16-bit boundary, then ASSERT(). | ||
468 | |||
469 | @param Address The address that encodes the PCI Bus, Device, Function and | ||
470 | Register. | ||
471 | @param Value The value to write. | ||
472 | |||
473 | @return The value written to the PCI configuration register. | ||
474 | |||
475 | **/ | ||
476 | UINT16 | ||
477 | EFIAPI | ||
478 | PciWrite16 ( | ||
479 | IN UINTN Address, | ||
480 | IN UINT16 Value | ||
481 | ) | ||
482 | { | ||
483 | return mRunningOnQ35 ? | ||
484 | PciExpressWrite16 (Address, Value) : | ||
485 | PciCf8Write16 (Address, Value); | ||
486 | } | ||
487 | |||
488 | /** | ||
489 | Performs a bitwise OR of a 16-bit PCI configuration register with | ||
490 | a 16-bit value. | ||
491 | |||
492 | Reads the 16-bit PCI configuration register specified by Address, performs a | ||
493 | bitwise OR between the read result and the value specified by | ||
494 | OrData, and writes the result to the 16-bit PCI configuration register | ||
495 | specified by Address. The value written to the PCI configuration register is | ||
496 | returned. This function must guarantee that all PCI read and write operations | ||
497 | are serialized. | ||
498 | |||
499 | If Address > 0x0FFFFFFF, then ASSERT(). | ||
500 | If Address is not aligned on a 16-bit boundary, then ASSERT(). | ||
501 | |||
502 | @param Address The address that encodes the PCI Bus, Device, Function and | ||
503 | Register. | ||
504 | @param OrData The value to OR with the PCI configuration register. | ||
505 | |||
506 | @return The value written back to the PCI configuration register. | ||
507 | |||
508 | **/ | ||
509 | UINT16 | ||
510 | EFIAPI | ||
511 | PciOr16 ( | ||
512 | IN UINTN Address, | ||
513 | IN UINT16 OrData | ||
514 | ) | ||
515 | { | ||
516 | return mRunningOnQ35 ? | ||
517 | PciExpressOr16 (Address, OrData) : | ||
518 | PciCf8Or16 (Address, OrData); | ||
519 | } | ||
520 | |||
521 | /** | ||
522 | Performs a bitwise AND of a 16-bit PCI configuration register with a 16-bit | ||
523 | value. | ||
524 | |||
525 | Reads the 16-bit PCI configuration register specified by Address, performs a | ||
526 | bitwise AND between the read result and the value specified by AndData, and | ||
527 | writes the result to the 16-bit PCI configuration register specified by | ||
528 | Address. The value written to the PCI configuration register is returned. | ||
529 | This function must guarantee that all PCI read and write operations are | ||
530 | serialized. | ||
531 | |||
532 | If Address > 0x0FFFFFFF, then ASSERT(). | ||
533 | If Address is not aligned on a 16-bit boundary, then ASSERT(). | ||
534 | |||
535 | @param Address The address that encodes the PCI Bus, Device, Function and | ||
536 | Register. | ||
537 | @param AndData The value to AND with the PCI configuration register. | ||
538 | |||
539 | @return The value written back to the PCI configuration register. | ||
540 | |||
541 | **/ | ||
542 | UINT16 | ||
543 | EFIAPI | ||
544 | PciAnd16 ( | ||
545 | IN UINTN Address, | ||
546 | IN UINT16 AndData | ||
547 | ) | ||
548 | { | ||
549 | return mRunningOnQ35 ? | ||
550 | PciExpressAnd16 (Address, AndData) : | ||
551 | PciCf8And16 (Address, AndData); | ||
552 | } | ||
553 | |||
554 | /** | ||
555 | Performs a bitwise AND of a 16-bit PCI configuration register with a 16-bit | ||
556 | value, followed a bitwise OR with another 16-bit value. | ||
557 | |||
558 | Reads the 16-bit PCI configuration register specified by Address, performs a | ||
559 | bitwise AND between the read result and the value specified by AndData, | ||
560 | performs a bitwise OR between the result of the AND operation and | ||
561 | the value specified by OrData, and writes the result to the 16-bit PCI | ||
562 | configuration register specified by Address. The value written to the PCI | ||
563 | configuration register is returned. This function must guarantee that all PCI | ||
564 | read and write operations are serialized. | ||
565 | |||
566 | If Address > 0x0FFFFFFF, then ASSERT(). | ||
567 | If Address is not aligned on a 16-bit boundary, then ASSERT(). | ||
568 | |||
569 | @param Address The address that encodes the PCI Bus, Device, Function and | ||
570 | Register. | ||
571 | @param AndData The value to AND with the PCI configuration register. | ||
572 | @param OrData The value to OR with the result of the AND operation. | ||
573 | |||
574 | @return The value written back to the PCI configuration register. | ||
575 | |||
576 | **/ | ||
577 | UINT16 | ||
578 | EFIAPI | ||
579 | PciAndThenOr16 ( | ||
580 | IN UINTN Address, | ||
581 | IN UINT16 AndData, | ||
582 | IN UINT16 OrData | ||
583 | ) | ||
584 | { | ||
585 | return mRunningOnQ35 ? | ||
586 | PciExpressAndThenOr16 (Address, AndData, OrData) : | ||
587 | PciCf8AndThenOr16 (Address, AndData, OrData); | ||
588 | } | ||
589 | |||
590 | /** | ||
591 | Reads a bit field of a PCI configuration register. | ||
592 | |||
593 | Reads the bit field in a 16-bit PCI configuration register. The bit field is | ||
594 | specified by the StartBit and the EndBit. The value of the bit field is | ||
595 | returned. | ||
596 | |||
597 | If Address > 0x0FFFFFFF, then ASSERT(). | ||
598 | If Address is not aligned on a 16-bit boundary, then ASSERT(). | ||
599 | If StartBit is greater than 15, then ASSERT(). | ||
600 | If EndBit is greater than 15, then ASSERT(). | ||
601 | If EndBit is less than StartBit, then ASSERT(). | ||
602 | |||
603 | @param Address The PCI configuration register to read. | ||
604 | @param StartBit The ordinal of the least significant bit in the bit field. | ||
605 | Range 0..15. | ||
606 | @param EndBit The ordinal of the most significant bit in the bit field. | ||
607 | Range 0..15. | ||
608 | |||
609 | @return The value of the bit field read from the PCI configuration register. | ||
610 | |||
611 | **/ | ||
612 | UINT16 | ||
613 | EFIAPI | ||
614 | PciBitFieldRead16 ( | ||
615 | IN UINTN Address, | ||
616 | IN UINTN StartBit, | ||
617 | IN UINTN EndBit | ||
618 | ) | ||
619 | { | ||
620 | return mRunningOnQ35 ? | ||
621 | PciExpressBitFieldRead16 (Address, StartBit, EndBit) : | ||
622 | PciCf8BitFieldRead16 (Address, StartBit, EndBit); | ||
623 | } | ||
624 | |||
625 | /** | ||
626 | Writes a bit field to a PCI configuration register. | ||
627 | |||
628 | Writes Value to the bit field of the PCI configuration register. The bit | ||
629 | field is specified by the StartBit and the EndBit. All other bits in the | ||
630 | destination PCI configuration register are preserved. The new value of the | ||
631 | 16-bit register is returned. | ||
632 | |||
633 | If Address > 0x0FFFFFFF, then ASSERT(). | ||
634 | If Address is not aligned on a 16-bit boundary, then ASSERT(). | ||
635 | If StartBit is greater than 15, then ASSERT(). | ||
636 | If EndBit is greater than 15, then ASSERT(). | ||
637 | If EndBit is less than StartBit, then ASSERT(). | ||
638 | If Value is larger than the bitmask value range specified by StartBit and EndBit, then ASSERT(). | ||
639 | |||
640 | @param Address The PCI configuration register to write. | ||
641 | @param StartBit The ordinal of the least significant bit in the bit field. | ||
642 | Range 0..15. | ||
643 | @param EndBit The ordinal of the most significant bit in the bit field. | ||
644 | Range 0..15. | ||
645 | @param Value The new value of the bit field. | ||
646 | |||
647 | @return The value written back to the PCI configuration register. | ||
648 | |||
649 | **/ | ||
650 | UINT16 | ||
651 | EFIAPI | ||
652 | PciBitFieldWrite16 ( | ||
653 | IN UINTN Address, | ||
654 | IN UINTN StartBit, | ||
655 | IN UINTN EndBit, | ||
656 | IN UINT16 Value | ||
657 | ) | ||
658 | { | ||
659 | return mRunningOnQ35 ? | ||
660 | PciExpressBitFieldWrite16 (Address, StartBit, EndBit, Value) : | ||
661 | PciCf8BitFieldWrite16 (Address, StartBit, EndBit, Value); | ||
662 | } | ||
663 | |||
664 | /** | ||
665 | Reads a bit field in a 16-bit PCI configuration, performs a bitwise OR, and | ||
666 | writes the result back to the bit field in the 16-bit port. | ||
667 | |||
668 | Reads the 16-bit PCI configuration register specified by Address, performs a | ||
669 | bitwise OR between the read result and the value specified by | ||
670 | OrData, and writes the result to the 16-bit PCI configuration register | ||
671 | specified by Address. The value written to the PCI configuration register is | ||
672 | returned. This function must guarantee that all PCI read and write operations | ||
673 | are serialized. Extra left bits in OrData are stripped. | ||
674 | |||
675 | If Address > 0x0FFFFFFF, then ASSERT(). | ||
676 | If Address is not aligned on a 16-bit boundary, then ASSERT(). | ||
677 | If StartBit is greater than 15, then ASSERT(). | ||
678 | If EndBit is greater than 15, then ASSERT(). | ||
679 | If EndBit is less than StartBit, then ASSERT(). | ||
680 | If OrData is larger than the bitmask value range specified by StartBit and EndBit, then ASSERT(). | ||
681 | |||
682 | @param Address The PCI configuration register to write. | ||
683 | @param StartBit The ordinal of the least significant bit in the bit field. | ||
684 | Range 0..15. | ||
685 | @param EndBit The ordinal of the most significant bit in the bit field. | ||
686 | Range 0..15. | ||
687 | @param OrData The value to OR with the PCI configuration register. | ||
688 | |||
689 | @return The value written back to the PCI configuration register. | ||
690 | |||
691 | **/ | ||
692 | UINT16 | ||
693 | EFIAPI | ||
694 | PciBitFieldOr16 ( | ||
695 | IN UINTN Address, | ||
696 | IN UINTN StartBit, | ||
697 | IN UINTN EndBit, | ||
698 | IN UINT16 OrData | ||
699 | ) | ||
700 | { | ||
701 | return mRunningOnQ35 ? | ||
702 | PciExpressBitFieldOr16 (Address, StartBit, EndBit, OrData) : | ||
703 | PciCf8BitFieldOr16 (Address, StartBit, EndBit, OrData); | ||
704 | } | ||
705 | |||
706 | /** | ||
707 | Reads a bit field in a 16-bit PCI configuration register, performs a bitwise | ||
708 | AND, and writes the result back to the bit field in the 16-bit register. | ||
709 | |||
710 | Reads the 16-bit PCI configuration register specified by Address, performs a | ||
711 | bitwise AND between the read result and the value specified by AndData, and | ||
712 | writes the result to the 16-bit PCI configuration register specified by | ||
713 | Address. The value written to the PCI configuration register is returned. | ||
714 | This function must guarantee that all PCI read and write operations are | ||
715 | serialized. Extra left bits in AndData are stripped. | ||
716 | |||
717 | If Address > 0x0FFFFFFF, then ASSERT(). | ||
718 | If Address is not aligned on a 16-bit boundary, then ASSERT(). | ||
719 | If StartBit is greater than 15, then ASSERT(). | ||
720 | If EndBit is greater than 15, then ASSERT(). | ||
721 | If EndBit is less than StartBit, then ASSERT(). | ||
722 | If AndData is larger than the bitmask value range specified by StartBit and EndBit, then ASSERT(). | ||
723 | |||
724 | @param Address The PCI configuration register to write. | ||
725 | @param StartBit The ordinal of the least significant bit in the bit field. | ||
726 | Range 0..15. | ||
727 | @param EndBit The ordinal of the most significant bit in the bit field. | ||
728 | Range 0..15. | ||
729 | @param AndData The value to AND with the PCI configuration register. | ||
730 | |||
731 | @return The value written back to the PCI configuration register. | ||
732 | |||
733 | **/ | ||
734 | UINT16 | ||
735 | EFIAPI | ||
736 | PciBitFieldAnd16 ( | ||
737 | IN UINTN Address, | ||
738 | IN UINTN StartBit, | ||
739 | IN UINTN EndBit, | ||
740 | IN UINT16 AndData | ||
741 | ) | ||
742 | { | ||
743 | return mRunningOnQ35 ? | ||
744 | PciExpressBitFieldAnd16 (Address, StartBit, EndBit, AndData) : | ||
745 | PciCf8BitFieldAnd16 (Address, StartBit, EndBit, AndData); | ||
746 | } | ||
747 | |||
748 | /** | ||
749 | Reads a bit field in a 16-bit port, performs a bitwise AND followed by a | ||
750 | bitwise OR, and writes the result back to the bit field in the | ||
751 | 16-bit port. | ||
752 | |||
753 | Reads the 16-bit PCI configuration register specified by Address, performs a | ||
754 | bitwise AND followed by a bitwise OR between the read result and | ||
755 | the value specified by AndData, and writes the result to the 16-bit PCI | ||
756 | configuration register specified by Address. The value written to the PCI | ||
757 | configuration register is returned. This function must guarantee that all PCI | ||
758 | read and write operations are serialized. Extra left bits in both AndData and | ||
759 | OrData are stripped. | ||
760 | |||
761 | If Address > 0x0FFFFFFF, then ASSERT(). | ||
762 | If Address is not aligned on a 16-bit boundary, then ASSERT(). | ||
763 | If StartBit is greater than 15, then ASSERT(). | ||
764 | If EndBit is greater than 15, then ASSERT(). | ||
765 | If EndBit is less than StartBit, then ASSERT(). | ||
766 | If AndData is larger than the bitmask value range specified by StartBit and EndBit, then ASSERT(). | ||
767 | If OrData is larger than the bitmask value range specified by StartBit and EndBit, then ASSERT(). | ||
768 | |||
769 | @param Address The PCI configuration register to write. | ||
770 | @param StartBit The ordinal of the least significant bit in the bit field. | ||
771 | Range 0..15. | ||
772 | @param EndBit The ordinal of the most significant bit in the bit field. | ||
773 | Range 0..15. | ||
774 | @param AndData The value to AND with the PCI configuration register. | ||
775 | @param OrData The value to OR with the result of the AND operation. | ||
776 | |||
777 | @return The value written back to the PCI configuration register. | ||
778 | |||
779 | **/ | ||
780 | UINT16 | ||
781 | EFIAPI | ||
782 | PciBitFieldAndThenOr16 ( | ||
783 | IN UINTN Address, | ||
784 | IN UINTN StartBit, | ||
785 | IN UINTN EndBit, | ||
786 | IN UINT16 AndData, | ||
787 | IN UINT16 OrData | ||
788 | ) | ||
789 | { | ||
790 | return mRunningOnQ35 ? | ||
791 | PciExpressBitFieldAndThenOr16 (Address, StartBit, EndBit, AndData, OrData) : | ||
792 | PciCf8BitFieldAndThenOr16 (Address, StartBit, EndBit, AndData, OrData); | ||
793 | } | ||
794 | |||
795 | /** | ||
796 | Reads a 32-bit PCI configuration register. | ||
797 | |||
798 | Reads and returns the 32-bit PCI configuration register specified by Address. | ||
799 | This function must guarantee that all PCI read and write operations are | ||
800 | serialized. | ||
801 | |||
802 | If Address > 0x0FFFFFFF, then ASSERT(). | ||
803 | If Address is not aligned on a 32-bit boundary, then ASSERT(). | ||
804 | |||
805 | @param Address The address that encodes the PCI Bus, Device, Function and | ||
806 | Register. | ||
807 | |||
808 | @return The read value from the PCI configuration register. | ||
809 | |||
810 | **/ | ||
811 | UINT32 | ||
812 | EFIAPI | ||
813 | PciRead32 ( | ||
814 | IN UINTN Address | ||
815 | ) | ||
816 | { | ||
817 | return mRunningOnQ35 ? | ||
818 | PciExpressRead32 (Address) : | ||
819 | PciCf8Read32 (Address); | ||
820 | } | ||
821 | |||
822 | /** | ||
823 | Writes a 32-bit PCI configuration register. | ||
824 | |||
825 | Writes the 32-bit PCI configuration register specified by Address with the | ||
826 | value specified by Value. Value is returned. This function must guarantee | ||
827 | that all PCI read and write operations are serialized. | ||
828 | |||
829 | If Address > 0x0FFFFFFF, then ASSERT(). | ||
830 | If Address is not aligned on a 32-bit boundary, then ASSERT(). | ||
831 | |||
832 | @param Address The address that encodes the PCI Bus, Device, Function and | ||
833 | Register. | ||
834 | @param Value The value to write. | ||
835 | |||
836 | @return The value written to the PCI configuration register. | ||
837 | |||
838 | **/ | ||
839 | UINT32 | ||
840 | EFIAPI | ||
841 | PciWrite32 ( | ||
842 | IN UINTN Address, | ||
843 | IN UINT32 Value | ||
844 | ) | ||
845 | { | ||
846 | return mRunningOnQ35 ? | ||
847 | PciExpressWrite32 (Address, Value) : | ||
848 | PciCf8Write32 (Address, Value); | ||
849 | } | ||
850 | |||
851 | /** | ||
852 | Performs a bitwise OR of a 32-bit PCI configuration register with | ||
853 | a 32-bit value. | ||
854 | |||
855 | Reads the 32-bit PCI configuration register specified by Address, performs a | ||
856 | bitwise OR between the read result and the value specified by | ||
857 | OrData, and writes the result to the 32-bit PCI configuration register | ||
858 | specified by Address. The value written to the PCI configuration register is | ||
859 | returned. This function must guarantee that all PCI read and write operations | ||
860 | are serialized. | ||
861 | |||
862 | If Address > 0x0FFFFFFF, then ASSERT(). | ||
863 | If Address is not aligned on a 32-bit boundary, then ASSERT(). | ||
864 | |||
865 | @param Address The address that encodes the PCI Bus, Device, Function and | ||
866 | Register. | ||
867 | @param OrData The value to OR with the PCI configuration register. | ||
868 | |||
869 | @return The value written back to the PCI configuration register. | ||
870 | |||
871 | **/ | ||
872 | UINT32 | ||
873 | EFIAPI | ||
874 | PciOr32 ( | ||
875 | IN UINTN Address, | ||
876 | IN UINT32 OrData | ||
877 | ) | ||
878 | { | ||
879 | return mRunningOnQ35 ? | ||
880 | PciExpressOr32 (Address, OrData) : | ||
881 | PciCf8Or32 (Address, OrData); | ||
882 | } | ||
883 | |||
884 | /** | ||
885 | Performs a bitwise AND of a 32-bit PCI configuration register with a 32-bit | ||
886 | value. | ||
887 | |||
888 | Reads the 32-bit PCI configuration register specified by Address, performs a | ||
889 | bitwise AND between the read result and the value specified by AndData, and | ||
890 | writes the result to the 32-bit PCI configuration register specified by | ||
891 | Address. The value written to the PCI configuration register is returned. | ||
892 | This function must guarantee that all PCI read and write operations are | ||
893 | serialized. | ||
894 | |||
895 | If Address > 0x0FFFFFFF, then ASSERT(). | ||
896 | If Address is not aligned on a 32-bit boundary, then ASSERT(). | ||
897 | |||
898 | @param Address The address that encodes the PCI Bus, Device, Function and | ||
899 | Register. | ||
900 | @param AndData The value to AND with the PCI configuration register. | ||
901 | |||
902 | @return The value written back to the PCI configuration register. | ||
903 | |||
904 | **/ | ||
905 | UINT32 | ||
906 | EFIAPI | ||
907 | PciAnd32 ( | ||
908 | IN UINTN Address, | ||
909 | IN UINT32 AndData | ||
910 | ) | ||
911 | { | ||
912 | return mRunningOnQ35 ? | ||
913 | PciExpressAnd32 (Address, AndData) : | ||
914 | PciCf8And32 (Address, AndData); | ||
915 | } | ||
916 | |||
917 | /** | ||
918 | Performs a bitwise AND of a 32-bit PCI configuration register with a 32-bit | ||
919 | value, followed a bitwise OR with another 32-bit value. | ||
920 | |||
921 | Reads the 32-bit PCI configuration register specified by Address, performs a | ||
922 | bitwise AND between the read result and the value specified by AndData, | ||
923 | performs a bitwise OR between the result of the AND operation and | ||
924 | the value specified by OrData, and writes the result to the 32-bit PCI | ||
925 | configuration register specified by Address. The value written to the PCI | ||
926 | configuration register is returned. This function must guarantee that all PCI | ||
927 | read and write operations are serialized. | ||
928 | |||
929 | If Address > 0x0FFFFFFF, then ASSERT(). | ||
930 | If Address is not aligned on a 32-bit boundary, then ASSERT(). | ||
931 | |||
932 | @param Address The address that encodes the PCI Bus, Device, Function and | ||
933 | Register. | ||
934 | @param AndData The value to AND with the PCI configuration register. | ||
935 | @param OrData The value to OR with the result of the AND operation. | ||
936 | |||
937 | @return The value written back to the PCI configuration register. | ||
938 | |||
939 | **/ | ||
940 | UINT32 | ||
941 | EFIAPI | ||
942 | PciAndThenOr32 ( | ||
943 | IN UINTN Address, | ||
944 | IN UINT32 AndData, | ||
945 | IN UINT32 OrData | ||
946 | ) | ||
947 | { | ||
948 | return mRunningOnQ35 ? | ||
949 | PciExpressAndThenOr32 (Address, AndData, OrData) : | ||
950 | PciCf8AndThenOr32 (Address, AndData, OrData); | ||
951 | } | ||
952 | |||
953 | /** | ||
954 | Reads a bit field of a PCI configuration register. | ||
955 | |||
956 | Reads the bit field in a 32-bit PCI configuration register. The bit field is | ||
957 | specified by the StartBit and the EndBit. The value of the bit field is | ||
958 | returned. | ||
959 | |||
960 | If Address > 0x0FFFFFFF, then ASSERT(). | ||
961 | If Address is not aligned on a 32-bit boundary, then ASSERT(). | ||
962 | If StartBit is greater than 31, then ASSERT(). | ||
963 | If EndBit is greater than 31, then ASSERT(). | ||
964 | If EndBit is less than StartBit, then ASSERT(). | ||
965 | |||
966 | @param Address The PCI configuration register to read. | ||
967 | @param StartBit The ordinal of the least significant bit in the bit field. | ||
968 | Range 0..31. | ||
969 | @param EndBit The ordinal of the most significant bit in the bit field. | ||
970 | Range 0..31. | ||
971 | |||
972 | @return The value of the bit field read from the PCI configuration register. | ||
973 | |||
974 | **/ | ||
975 | UINT32 | ||
976 | EFIAPI | ||
977 | PciBitFieldRead32 ( | ||
978 | IN UINTN Address, | ||
979 | IN UINTN StartBit, | ||
980 | IN UINTN EndBit | ||
981 | ) | ||
982 | { | ||
983 | return mRunningOnQ35 ? | ||
984 | PciExpressBitFieldRead32 (Address, StartBit, EndBit) : | ||
985 | PciCf8BitFieldRead32 (Address, StartBit, EndBit); | ||
986 | } | ||
987 | |||
988 | /** | ||
989 | Writes a bit field to a PCI configuration register. | ||
990 | |||
991 | Writes Value to the bit field of the PCI configuration register. The bit | ||
992 | field is specified by the StartBit and the EndBit. All other bits in the | ||
993 | destination PCI configuration register are preserved. The new value of the | ||
994 | 32-bit register is returned. | ||
995 | |||
996 | If Address > 0x0FFFFFFF, then ASSERT(). | ||
997 | If Address is not aligned on a 32-bit boundary, then ASSERT(). | ||
998 | If StartBit is greater than 31, then ASSERT(). | ||
999 | If EndBit is greater than 31, then ASSERT(). | ||
1000 | If EndBit is less than StartBit, then ASSERT(). | ||
1001 | If Value is larger than the bitmask value range specified by StartBit and EndBit, then ASSERT(). | ||
1002 | |||
1003 | @param Address The PCI configuration register to write. | ||
1004 | @param StartBit The ordinal of the least significant bit in the bit field. | ||
1005 | Range 0..31. | ||
1006 | @param EndBit The ordinal of the most significant bit in the bit field. | ||
1007 | Range 0..31. | ||
1008 | @param Value The new value of the bit field. | ||
1009 | |||
1010 | @return The value written back to the PCI configuration register. | ||
1011 | |||
1012 | **/ | ||
1013 | UINT32 | ||
1014 | EFIAPI | ||
1015 | PciBitFieldWrite32 ( | ||
1016 | IN UINTN Address, | ||
1017 | IN UINTN StartBit, | ||
1018 | IN UINTN EndBit, | ||
1019 | IN UINT32 Value | ||
1020 | ) | ||
1021 | { | ||
1022 | return mRunningOnQ35 ? | ||
1023 | PciExpressBitFieldWrite32 (Address, StartBit, EndBit, Value) : | ||
1024 | PciCf8BitFieldWrite32 (Address, StartBit, EndBit, Value); | ||
1025 | } | ||
1026 | |||
1027 | /** | ||
1028 | Reads a bit field in a 32-bit PCI configuration, performs a bitwise OR, and | ||
1029 | writes the result back to the bit field in the 32-bit port. | ||
1030 | |||
1031 | Reads the 32-bit PCI configuration register specified by Address, performs a | ||
1032 | bitwise OR between the read result and the value specified by | ||
1033 | OrData, and writes the result to the 32-bit PCI configuration register | ||
1034 | specified by Address. The value written to the PCI configuration register is | ||
1035 | returned. This function must guarantee that all PCI read and write operations | ||
1036 | are serialized. Extra left bits in OrData are stripped. | ||
1037 | |||
1038 | If Address > 0x0FFFFFFF, then ASSERT(). | ||
1039 | If Address is not aligned on a 32-bit boundary, then ASSERT(). | ||
1040 | If StartBit is greater than 31, then ASSERT(). | ||
1041 | If EndBit is greater than 31, then ASSERT(). | ||
1042 | If EndBit is less than StartBit, then ASSERT(). | ||
1043 | If OrData is larger than the bitmask value range specified by StartBit and EndBit, then ASSERT(). | ||
1044 | |||
1045 | @param Address The PCI configuration register to write. | ||
1046 | @param StartBit The ordinal of the least significant bit in the bit field. | ||
1047 | Range 0..31. | ||
1048 | @param EndBit The ordinal of the most significant bit in the bit field. | ||
1049 | Range 0..31. | ||
1050 | @param OrData The value to OR with the PCI configuration register. | ||
1051 | |||
1052 | @return The value written back to the PCI configuration register. | ||
1053 | |||
1054 | **/ | ||
1055 | UINT32 | ||
1056 | EFIAPI | ||
1057 | PciBitFieldOr32 ( | ||
1058 | IN UINTN Address, | ||
1059 | IN UINTN StartBit, | ||
1060 | IN UINTN EndBit, | ||
1061 | IN UINT32 OrData | ||
1062 | ) | ||
1063 | { | ||
1064 | return mRunningOnQ35 ? | ||
1065 | PciExpressBitFieldOr32 (Address, StartBit, EndBit, OrData) : | ||
1066 | PciCf8BitFieldOr32 (Address, StartBit, EndBit, OrData); | ||
1067 | } | ||
1068 | |||
1069 | /** | ||
1070 | Reads a bit field in a 32-bit PCI configuration register, performs a bitwise | ||
1071 | AND, and writes the result back to the bit field in the 32-bit register. | ||
1072 | |||
1073 | Reads the 32-bit PCI configuration register specified by Address, performs a | ||
1074 | bitwise AND between the read result and the value specified by AndData, and | ||
1075 | writes the result to the 32-bit PCI configuration register specified by | ||
1076 | Address. The value written to the PCI configuration register is returned. | ||
1077 | This function must guarantee that all PCI read and write operations are | ||
1078 | serialized. Extra left bits in AndData are stripped. | ||
1079 | |||
1080 | If Address > 0x0FFFFFFF, then ASSERT(). | ||
1081 | If Address is not aligned on a 32-bit boundary, then ASSERT(). | ||
1082 | If StartBit is greater than 31, then ASSERT(). | ||
1083 | If EndBit is greater than 31, then ASSERT(). | ||
1084 | If EndBit is less than StartBit, then ASSERT(). | ||
1085 | If AndData is larger than the bitmask value range specified by StartBit and EndBit, then ASSERT(). | ||
1086 | |||
1087 | @param Address The PCI configuration register to write. | ||
1088 | @param StartBit The ordinal of the least significant bit in the bit field. | ||
1089 | Range 0..31. | ||
1090 | @param EndBit The ordinal of the most significant bit in the bit field. | ||
1091 | Range 0..31. | ||
1092 | @param AndData The value to AND with the PCI configuration register. | ||
1093 | |||
1094 | @return The value written back to the PCI configuration register. | ||
1095 | |||
1096 | **/ | ||
1097 | UINT32 | ||
1098 | EFIAPI | ||
1099 | PciBitFieldAnd32 ( | ||
1100 | IN UINTN Address, | ||
1101 | IN UINTN StartBit, | ||
1102 | IN UINTN EndBit, | ||
1103 | IN UINT32 AndData | ||
1104 | ) | ||
1105 | { | ||
1106 | return mRunningOnQ35 ? | ||
1107 | PciExpressBitFieldAnd32 (Address, StartBit, EndBit, AndData) : | ||
1108 | PciCf8BitFieldAnd32 (Address, StartBit, EndBit, AndData); | ||
1109 | } | ||
1110 | |||
1111 | /** | ||
1112 | Reads a bit field in a 32-bit port, performs a bitwise AND followed by a | ||
1113 | bitwise OR, and writes the result back to the bit field in the | ||
1114 | 32-bit port. | ||
1115 | |||
1116 | Reads the 32-bit PCI configuration register specified by Address, performs a | ||
1117 | bitwise AND followed by a bitwise OR between the read result and | ||
1118 | the value specified by AndData, and writes the result to the 32-bit PCI | ||
1119 | configuration register specified by Address. The value written to the PCI | ||
1120 | configuration register is returned. This function must guarantee that all PCI | ||
1121 | read and write operations are serialized. Extra left bits in both AndData and | ||
1122 | OrData are stripped. | ||
1123 | |||
1124 | If Address > 0x0FFFFFFF, then ASSERT(). | ||
1125 | If Address is not aligned on a 32-bit boundary, then ASSERT(). | ||
1126 | If StartBit is greater than 31, then ASSERT(). | ||
1127 | If EndBit is greater than 31, then ASSERT(). | ||
1128 | If EndBit is less than StartBit, then ASSERT(). | ||
1129 | If AndData is larger than the bitmask value range specified by StartBit and EndBit, then ASSERT(). | ||
1130 | If OrData is larger than the bitmask value range specified by StartBit and EndBit, then ASSERT(). | ||
1131 | |||
1132 | @param Address The PCI configuration register to write. | ||
1133 | @param StartBit The ordinal of the least significant bit in the bit field. | ||
1134 | Range 0..31. | ||
1135 | @param EndBit The ordinal of the most significant bit in the bit field. | ||
1136 | Range 0..31. | ||
1137 | @param AndData The value to AND with the PCI configuration register. | ||
1138 | @param OrData The value to OR with the result of the AND operation. | ||
1139 | |||
1140 | @return The value written back to the PCI configuration register. | ||
1141 | |||
1142 | **/ | ||
1143 | UINT32 | ||
1144 | EFIAPI | ||
1145 | PciBitFieldAndThenOr32 ( | ||
1146 | IN UINTN Address, | ||
1147 | IN UINTN StartBit, | ||
1148 | IN UINTN EndBit, | ||
1149 | IN UINT32 AndData, | ||
1150 | IN UINT32 OrData | ||
1151 | ) | ||
1152 | { | ||
1153 | return mRunningOnQ35 ? | ||
1154 | PciExpressBitFieldAndThenOr32 (Address, StartBit, EndBit, AndData, OrData) : | ||
1155 | PciCf8BitFieldAndThenOr32 (Address, StartBit, EndBit, AndData, OrData); | ||
1156 | } | ||
1157 | |||
1158 | /** | ||
1159 | Reads a range of PCI configuration registers into a caller supplied buffer. | ||
1160 | |||
1161 | Reads the range of PCI configuration registers specified by StartAddress and | ||
1162 | Size into the buffer specified by Buffer. This function only allows the PCI | ||
1163 | configuration registers from a single PCI function to be read. Size is | ||
1164 | returned. When possible 32-bit PCI configuration read cycles are used to read | ||
1165 | from StartAdress to StartAddress + Size. Due to alignment restrictions, 8-bit | ||
1166 | and 16-bit PCI configuration read cycles may be used at the beginning and the | ||
1167 | end of the range. | ||
1168 | |||
1169 | If StartAddress > 0x0FFFFFFF, then ASSERT(). | ||
1170 | If ((StartAddress & 0xFFF) + Size) > 0x1000, then ASSERT(). | ||
1171 | If Size > 0 and Buffer is NULL, then ASSERT(). | ||
1172 | |||
1173 | @param StartAddress The starting address that encodes the PCI Bus, Device, | ||
1174 | Function and Register. | ||
1175 | @param Size The size in bytes of the transfer. | ||
1176 | @param Buffer The pointer to a buffer receiving the data read. | ||
1177 | |||
1178 | @return Size | ||
1179 | |||
1180 | **/ | ||
1181 | UINTN | ||
1182 | EFIAPI | ||
1183 | PciReadBuffer ( | ||
1184 | IN UINTN StartAddress, | ||
1185 | IN UINTN Size, | ||
1186 | OUT VOID *Buffer | ||
1187 | ) | ||
1188 | { | ||
1189 | return mRunningOnQ35 ? | ||
1190 | PciExpressReadBuffer (StartAddress, Size, Buffer) : | ||
1191 | PciCf8ReadBuffer (StartAddress, Size, Buffer); | ||
1192 | } | ||
1193 | |||
1194 | /** | ||
1195 | Copies the data in a caller supplied buffer to a specified range of PCI | ||
1196 | configuration space. | ||
1197 | |||
1198 | Writes the range of PCI configuration registers specified by StartAddress and | ||
1199 | Size from the buffer specified by Buffer. This function only allows the PCI | ||
1200 | configuration registers from a single PCI function to be written. Size is | ||
1201 | returned. When possible 32-bit PCI configuration write cycles are used to | ||
1202 | write from StartAdress to StartAddress + Size. Due to alignment restrictions, | ||
1203 | 8-bit and 16-bit PCI configuration write cycles may be used at the beginning | ||
1204 | and the end of the range. | ||
1205 | |||
1206 | If StartAddress > 0x0FFFFFFF, then ASSERT(). | ||
1207 | If ((StartAddress & 0xFFF) + Size) > 0x1000, then ASSERT(). | ||
1208 | If Size > 0 and Buffer is NULL, then ASSERT(). | ||
1209 | |||
1210 | @param StartAddress The starting address that encodes the PCI Bus, Device, | ||
1211 | Function and Register. | ||
1212 | @param Size The size in bytes of the transfer. | ||
1213 | @param Buffer The pointer to a buffer containing the data to write. | ||
1214 | |||
1215 | @return Size written to StartAddress. | ||
1216 | |||
1217 | **/ | ||
1218 | UINTN | ||
1219 | EFIAPI | ||
1220 | PciWriteBuffer ( | ||
1221 | IN UINTN StartAddress, | ||
1222 | IN UINTN Size, | ||
1223 | IN VOID *Buffer | ||
1224 | ) | ||
1225 | { | ||
1226 | return mRunningOnQ35 ? | ||
1227 | PciExpressWriteBuffer (StartAddress, Size, Buffer) : | ||
1228 | PciCf8WriteBuffer (StartAddress, Size, Buffer); | ||
1229 | } | ||