# List the minimum kernel version required for each # of the listed Kconfig symbols # platform_get_device_id() ATH9K_AHB 2.6.30 BT 2.6.27 BT_RFCOMM_TTY 2.6.33 BT_HIDP 2.6.28 BT_WILINK 2.6.39 MAC80211_HWSIM 2.6.31 ATH6KL 2.6.27 WIL6210 2.6.31 ATH10K 2.6.30 ATL1C 3.5 ATL1E 2.6.26 ALX 2.6.31 LIBERTAS 2.6.27 LIBERTAS_THINFIRM 2.6.27 LIBERTAS_SDIO 2.6.32 ZD1211RW 2.6.29 USB_NET_RNDIS_WLAN 2.6.29 CARL9170 2.6.29 WL1251_SPI 2.6.37 WL1251_SDIO 2.6.37 WLCORE_SDIO 2.6.38 CW1200_WLAN_SDIO 2.6.32 CW1200_WLAN_SPI 2.6.35 BRCMFMAC 2.6.29 WL_TI 2.6.30 WLCORE 2.6.30 # requires irq_modify_status() which was only exported in 3.0 WL1251 3.0 MWIFIEX 2.6.27 # Regulator # Because of -EPROBE_DEFER see commit d1c3414c and note that # we can't backport the core regulator as its part of the core # vmlinux. REGULATOR 3.4 # requires some work REGULATOR_88PM800 3.12 REGULATOR_88PM8607 3.10 REGULATOR_AAT2870 3.6 REGULATOR_AD5398 3.5 REGULATOR_ARIZONA 3.8 REGULATOR_AS3711 3.12 REGULATOR_DA903X 3.12 REGULATOR_DA9052 3.9 REGULATOR_DA9055 3.8 REGULATOR_DA9210 3.5 REGULATOR_FAN53555 3.5 REGULATOR_FIXED_VOLTAGE 3.6 REGULATOR_GPIO 3.6 REGULATOR_ISL6271A 3.5 REGULATOR_LP3971 3.6 REGULATOR_LP3972 3.6 REGULATOR_LP872X 3.6 REGULATOR_LP8755 3.6 REGULATOR_MAX1586 3.6 REGULATOR_MAX77686 3.7 REGULATOR_MAX77693 3.11 REGULATOR_MAX8649 3.10 REGULATOR_MAX8660 3.5 REGULATOR_MAX8925 3.5 REGULATOR_MAX8952 3.6 REGULATOR_MAX8973 3.6 REGULATOR_MAX8997 3.8 REGULATOR_MAX8998 3.11 REGULATOR_MC13783 3.6 REGULATOR_MC13892 3.6 REGULATOR_MC13XXX_CORE 3.6 REGULATOR_PALMAS 3.12 REGULATOR_PCAP 3.6 REGULATOR_PCF50633 3.8 REGULATOR_PFUZE100 3.6 REGULATOR_RC5T583 3.6 REGULATOR_S2MPS11 3.12 REGULATOR_S5M8767 3.9 REGULATOR_TPS51632 3.8 REGULATOR_TPS6105X 3.6 REGULATOR_TPS62360 3.6 REGULATOR_TPS62360 3.6 REGULATOR_TPS65023 3.9 REGULATOR_TPS6507X 3.6 REGULATOR_TPS65090 3.9 REGULATOR_TPS65217 3.12 REGULATOR_TPS6524X 3.6 REGULATOR_TPS6586X 3.9 REGULATOR_TPS65910 3.6 REGULATOR_TPS65912 3.12 REGULATOR_TWL4030 3.11 REGULATOR_WM831X 3.12 REGULATOR_WM8350 3.12 REGULATOR_WM8400 3.12 REGULATOR_WM8994 3.8 # Media MEDIA_SUPPORT 3.2 # There's something wrong with backporting this/dma-buf to 3.2, # so disable it for now until Luis figures it out MEDIA_SUPPORT 3.3 # Some media drivers however depend on module deferral mechanism # Lets not enable those unless that's available. VIDEO_S3C_CAMIF 3.4 VIDEO_SAMSUNG_S5P_FIMC 3.4 IR_GPIO_CIR 3.4 # Some media drivers depend on the CONFIG_REGULATOR which # we only support on >= 3.4 give that reguatory itself depends # on -EPROBE_DEFER. SOC_CAMERA 3.4 SOC_CAMERA_IMX074 3.4 SOC_CAMERA_MT9M001 3.4 SOC_CAMERA_MT9M111 3.4 SOC_CAMERA_MT9T031 3.4 SOC_CAMERA_MT9T112 3.4 SOC_CAMERA_MT9V022 3.4 SOC_CAMERA_OV2640 3.4 SOC_CAMERA_OV5642 3.4 SOC_CAMERA_OV6650 3.4 SOC_CAMERA_OV772X 3.4 SOC_CAMERA_OV9640 3.4 SOC_CAMERA_OV9740 3.4 SOC_CAMERA_RJ54N1 3.4 SOC_CAMERA_TW9910 3.4 # There are some odd comile errors here I don't want # to bother with right now VIDEO_MEM2MEM_DEINTERLACE DISABLE # 49920bc6 and 1003cab8 and while it seems there is a # one to one map DMA_FROM_DEVICE to DMA_DEV_TO_MEM # I can't verify this fully yet. VIDEO_TIMBERDALE 3.4 # Can't figure this out yet either DVB_DDBRIDGE DISABLE # These require I2C_CLIENT_SCCB which can't be backported # since the core I2C code has to know about it VIDEO_OV7640 3.6 VIDEO_EM28XX 3.6 # someone has to backport "firewire: introduce fw_driver.probe and .remove methods" DVB_FIREDTV 3.11 # I give up on these guys for now RADIO_MAXIRADIO DISABLE RADIO_SHARK DISABLE VIDEO_IVTV DISABLE VIDEO_MEYE DISABLE DVB_NGENE DISABLE DVB_USB_PCTV452E DISABLE USB_GSPCA DISABLE VIDEO_MXB DISABLE VIDEO_RENESAS_VSP1 3.6 # struct gpio_chip only got the required members in 2.6.28 BCMA_DRIVER_GPIO 2.6.28 SSB_DRIVER_GPIO 2.6.28 # shash was only added in 2.6.29 BT 2.6.29 # GPIOF_OUT_INIT_HIGH definitions were only moved # out of #ifdef in kernel 3.0. These are required # by some users of BCMA_DRIVER_GPIO. We'd better # just backport the definitions, but right now # this is easier. BCMA_DRIVER_GPIO 3.0 BCMA_DRIVER_MIPS 3.3 SSB_DRIVER_MIPS 3.3 # rfkill-regulator uses a kernel header file # (rfkill-regulator.h) that we don't backport # right now, so make it depend on 3.0 RFKILL_REGULATOR 3.0 # drivers/regulator/ab3100.c and drivers/mfd/ab3100-core.c # both depend on include/linux/mfd/ab3100.h and we should # only backport REGULATOR_AB3100 if the mfd driver is # backported as well. REGULATOR_AB3100 3.9 # This is a fun one ... the implementation of this # uses subdir-ccflags-$(CONFIG_BRCMDBG) which was # only introduced in kernel 2.6.30. BRCMDBG 2.6.30 # HID_QUIRK_NO_INIT_REPORTS was only introduced in # kernel 2.6.33, so depend on that. We could instead # backport it, but I can't test that and this is a # lot easier right now. BT_HIDP 2.6.33 # NFC core needs PF_NFC defined in socket.h which was # only introduced in kernel 3.1 NFC 3.1 INTEL_IPS 3.2 NFC_MEI_PHY 3.10 IEEE802154_MRF24J40 3.5 IEEE802154 2.6.38