blob: 5d0115c9ca6f2b91ee43cff419a6612abc5801f4 (
plain) (
tree)
|
|
wpa_supplicant and hostapd
--------------------------
Copyright (c) 2002-2019, Jouni Malinen <j@w1.fi> and contributors
All Rights Reserved.
See the README file for the current license terms.
This software was previously distributed under BSD/GPL v2 dual license
terms that allowed either of those license alternatives to be
selected. As of February 11, 2012, the project has chosen to use only
the BSD license option for future distribution. As such, the GPL v2
license option is no longer used. It should be noted that the BSD
license option (the one with advertisement clause removed) is compatible
with GPL and as such, does not prevent use of this software in projects
that use GPL.
Some of the files may still include pointers to GPL version 2 license
terms. However, such copyright and license notifications are maintained
only for attribution purposes and any distribution of this software
after February 11, 2012 is no longer under the GPL v2 option.
|