am43-open-source/am43-linux-kernel.git
8 years agoMerge branch 'merge' of git://git.kernel.org/pub/scm/linux/kernel/git/benh/powerpc master
Linus Torvalds [Wed, 6 Mar 2013 02:56:22 +0000 (18:56 -0800)]
Merge branch 'merge' of git://git./linux/kernel/git/benh/powerpc

Pull powerpc fixes from Ben Herrenschmidt:
 "Here are a few powerpc bits & fixes for rc1.  A couple of str*cpy
  fixes, some fixes in handling the FSCR register on Power8 (controls
  the enabling of processor features), a 32-bit build fix and a couple
  more nits."

* 'merge' of git://git.kernel.org/pub/scm/linux/kernel/git/benh/powerpc:
  powerpc: Set DSCR bit in FSCR setup
  powerpc: Add DSCR FSCR register bit definition
  powerpc: Fix setting FSCR for HV=0 and on secondary CPUs
  powerpc: Wireup the kcmp syscall to sys_ni
  powerpc: Remove unused BITOP_LE_SWIZZLE macro
  powerpc: Avoid link stack corruption in MMU on syscall entry path
  drivers/tty/hvc: Use strlcpy instead of strncpy
  powerpc/pseries/hvcserver: Fix strncpy buffer limit in location code
  powerpc: Fix compile of sha1-powerpc-asm.S on 32-bit

8 years agoMerge tag 'fixes-for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/rusty...
Linus Torvalds [Wed, 6 Mar 2013 02:54:28 +0000 (18:54 -0800)]
Merge tag 'fixes-for-linus' of git://git./linux/kernel/git/rusty/linux

Pull virtio hwrng fix from Rusty Russell:
 "Nasty side-effect of vmalloc'ing modules: their static vars cannot be
  put into scatterlists.  Jens has a check queued for this, so it
  shouldn't happen again.

  We could fix this in virtio_rng, but it's actually far easier to just
  do it in the core"

* tag 'fixes-for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/rusty/linux:
  hw_random: make buffer usable in scatterlist.

8 years agoMerge git://git.kernel.org/pub/scm/linux/kernel/git/davem/net
Linus Torvalds [Wed, 6 Mar 2013 02:42:29 +0000 (18:42 -0800)]
Merge git://git./linux/kernel/git/davem/net

Pull networking fixes from David Miller:
 "A moderately sized pile of fixes, some specifically for merge window
  introduced regressions although others are for longer standing items
  and have been queued up for -stable.

  I'm kind of tired of all the RDS protocol bugs over the years, to be
  honest, it's way out of proportion to the number of people who
  actually use it.

   1) Fix missing range initialization in netfilter IPSET, from Jozsef
      Kadlecsik.

   2) ieee80211_local->tim_lock needs to use BH disabling, from Johannes
      Berg.

   3) Fix DMA syncing in SFC driver, from Ben Hutchings.

   4) Fix regression in BOND device MAC address setting, from Jiri
      Pirko.

   5) Missing usb_free_urb in ISDN Hisax driver, from Marina Makienko.

   6) Fix UDP checksumming in bnx2x driver for 57710 and 57711 chips,
      fix from Dmitry Kravkov.

   7) Missing cfgspace_lock initialization in BCMA driver.

   8) Validate parameter size for SCTP assoc stats getsockopt(), from
      Guenter Roeck.

   9) Fix SCTP association hangs, from Lee A Roberts.

  10) Fix jumbo frame handling in r8169, from Francois Romieu.

  11) Fix phy_device memory leak, from Petr Malat.

  12) Omit trailing FCS from frames received in BGMAC driver, from Hauke
      Mehrtens.

  13) Missing socket refcount release in L2TP, from Guillaume Nault.

  14) sctp_endpoint_init should respect passed in gfp_t, rather than use
      GFP_KERNEL unconditionally.  From Dan Carpenter.

  15) Add AISX AX88179 USB driver, from Freddy Xin.

  16) Remove MAINTAINERS entries for drivers deleted during the merge
      window, from Cesar Eduardo Barros.

  17) RDS protocol can try to allocate huge amounts of memory, check
      that the user's request length makes sense, from Cong Wang.

  18) SCTP should use the provided KMALLOC_MAX_SIZE instead of it's own,
      bogus, definition.  From Cong Wang.

  19) Fix deadlocks in FEC driver by moving TX reclaim into NAPI poll,
      from Frank Li.  Also, fix a build error introduced in the merge
      window.

  20) Fix bogus purging of default routes in ipv6, from Lorenzo Colitti.

  21) Don't double count RTT measurements when we leave the TCP receive
      fast path, from Neal Cardwell."

* git://git.kernel.org/pub/scm/linux/kernel/git/davem/net: (61 commits)
  tcp: fix double-counted receiver RTT when leaving receiver fast path
  CAIF: fix sparse warning for caif_usb
  rds: simplify a warning message
  net: fec: fix build error in no MXC platform
  net: ipv6: Don't purge default router if accept_ra=2
  net: fec: put tx to napi poll function to fix dead lock
  sctp: use KMALLOC_MAX_SIZE instead of its own MAX_KMALLOC_SIZE
  rds: limit the size allocated by rds_message_alloc()
  MAINTAINERS: remove eexpress
  MAINTAINERS: remove drivers/net/wan/cycx*
  MAINTAINERS: remove 3c505
  caif_dev: fix sparse warnings for caif_flow_cb
  ax88179_178a: ASIX AX88179_178A USB 3.0/2.0 to gigabit ethernet adapter driver
  sctp: use the passed in gfp flags instead GFP_KERNEL
  ipv[4|6]: correct dropwatch false positive in local_deliver_finish
  l2tp: Restore socket refcount when sendmsg succeeds
  net/phy: micrel: Disable asymmetric pause for KSZ9021
  bgmac: omit the fcs
  phy: Fix phy_device_free memory leak
  bnx2x: Fix KR2 work-around condition
  ...

8 years agoMerge branch 'irq-urgent-for-linus' of git://git.kernel.org/pub/scm/linux/kernel...
Linus Torvalds [Wed, 6 Mar 2013 02:10:04 +0000 (18:10 -0800)]
Merge branch 'irq-urgent-for-linus' of git://git./linux/kernel/git/tip/tip

Pull irq fixes and cleanups from Thomas Gleixner:
 "Commit e5ab012c3271 ("nohz: Make tick_nohz_irq_exit() irq safe") is
  the first commit in the series and the minimal necessary bugfix, which
  needs to go back into stable.

  The remanining commits enforce irq disabling in irq_exit(), sanitize
  the hardirq/softirq preempt count transition and remove a bunch of no
  longer necessary conditionals."

I personally love getting rid of the very subtle and confusing
IRQ_EXIT_OFFSET thing.  Even apart from the whole "more lines removed
than added" thing.

* 'irq-urgent-for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/tip/tip:
  irq: Don't re-enable interrupts at the end of irq_exit
  irq: Remove IRQ_EXIT_OFFSET workaround
  Revert "nohz: Make tick_nohz_irq_exit() irq safe"
  irq: Sanitize invoke_softirq
  irq: Ensure irq_exit() code runs with interrupts disabled
  nohz: Make tick_nohz_irq_exit() irq safe

8 years agoMerge branch 'core-urgent-for-linus' of git://git.kernel.org/pub/scm/linux/kernel...
Linus Torvalds [Wed, 6 Mar 2013 02:07:12 +0000 (18:07 -0800)]
Merge branch 'core-urgent-for-linus' of git://git./linux/kernel/git/tip/tip

Pull smpboot bugfix from Thomas Gleixner:
 "A single bugfix for a regression introduced with the conversion of the
  stop machine threads to the generic smpboot thread management
  facility"

* 'core-urgent-for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/tip/tip:
  stop_machine: Mark per cpu stopper enabled early

8 years agoMerge tag 'gpio-for-linus' of git://git.secretlab.ca/git/linux
Linus Torvalds [Wed, 6 Mar 2013 01:25:59 +0000 (17:25 -0800)]
Merge tag 'gpio-for-linus' of git://git.secretlab.ca/git/linux

Pull second round of GPIO changes from Grant Likely:
 "This branch contains a few bug fixes that I missed the first time
  around and updates to the gpio_desc series included in the first pull
  request.  This tag has been retagged to drop the 2 head commits
  because the one of them caused a build failure."

* tag 'gpio-for-linus' of git://git.secretlab.ca/git/linux:
  gpio/gpio-ich: fix ichx_gpio_check_available() return what callers expect
  gpiolib: move comment to right function
  gpiolib: use const parameters when possible
  gpiolib: check descriptors validity before use

8 years agoMerge tag 'md-3.9' of git://neil.brown.name/md
Linus Torvalds [Wed, 6 Mar 2013 01:22:08 +0000 (17:22 -0800)]
Merge tag 'md-3.9' of git://neil.brown.name/md

Pull md updates from NeilBrown:
 "Mostly little bugfixes.

  Only "feature" is a new RAID10 layout which slightly improves the
  number of sets of devices that can concurrently fail, without data
  loss."

* tag 'md-3.9' of git://neil.brown.name/md:
  md: expedite metadata update when switching  read-auto -> active
  md: remove CONFIG_MULTICORE_RAID456
  md/raid1,raid10: fix deadlock with freeze_array()
  md/raid0: improve error message when converting RAID4-with-spares to RAID0
  md: raid0: fix error return from create_stripe_zones.
  md: fix two bugs when attempting to resize RAID0 array.
  DM RAID: Add support for MD's RAID10 "far" and "offset" algorithms
  MD RAID10: Improve redundancy for 'far' and 'offset' algorithms (part 2)
  MD RAID10: Improve redundancy for 'far' and 'offset' algorithms (part 1)
  MD RAID10: Minor non-functional code changes
  md: raid1,10: Handle REQ_WRITE_SAME flag in write bios
  md: protect against crash upon fsync on ro array

8 years agopowerpc: Set DSCR bit in FSCR setup
Michael Neuling [Mon, 4 Mar 2013 19:45:52 +0000 (19:45 +0000)]
powerpc: Set DSCR bit in FSCR setup

We support DSCR (Data Stream Control Register) so we should make sure we set it
in the FSCR (Facility Status & Control Register) incase some firmwares don't
set it.  If we don't set this, we'll take a facility unavailable exception when
using the DSCR.

Signed-off-by: Michael Neuling <mikey@neuling.org>
Signed-off-by: Benjamin Herrenschmidt <benh@kernel.crashing.org>
8 years agopowerpc: Add DSCR FSCR register bit definition
Michael Neuling [Mon, 4 Mar 2013 19:45:51 +0000 (19:45 +0000)]
powerpc: Add DSCR FSCR register bit definition

This sets the DSCR (Data Stream Control Register) in the FSCR (Facility Status
& Control Register).

Also harmonise TAR (Target Address Register) FSCR bit definition too.

Signed-off-by: Michael Neuling <mikey@neuling.org>
Signed-off-by: Benjamin Herrenschmidt <benh@kernel.crashing.org>
8 years agopowerpc: Fix setting FSCR for HV=0 and on secondary CPUs
Michael Neuling [Mon, 4 Mar 2013 19:45:50 +0000 (19:45 +0000)]
powerpc: Fix setting FSCR for HV=0 and on secondary CPUs

Currently we only set the FSCR (Facility Status and Control Register) when HV=1
but this feature is available when HV=0 also.  This patch sets FSCR when HV=0.

Also, we currently only set the FSCR on the master CPU.  This patch also sets
the FSCR on secondary CPUs.

Signed-off-by: Michael Neuling <mikey@neuling.org>
cc: Ian Munsie <imunsie@au1.ibm.com>
Signed-off-by: Benjamin Herrenschmidt <benh@kernel.crashing.org>
8 years agopowerpc: Wireup the kcmp syscall to sys_ni
Tony Breeds [Mon, 4 Mar 2013 15:57:30 +0000 (15:57 +0000)]
powerpc: Wireup the kcmp syscall to sys_ni

Since kmp takes 2 unsigned long args there should be a compat wrapper.
Since one isn't provided I think it's safer just to hook this up to not
implemented.  If we need it later we can do it properly then.

Signed-off-by: Tony Breeds <tony@bakeyournoodle.com>
Signed-off-by: Benjamin Herrenschmidt <benh@kernel.crashing.org>
8 years agopowerpc: Remove unused BITOP_LE_SWIZZLE macro
Akinobu Mita [Sat, 2 Mar 2013 04:06:30 +0000 (04:06 +0000)]
powerpc: Remove unused BITOP_LE_SWIZZLE macro

The BITOP_LE_SWIZZLE macro was used in the little-endian bitops functions
for powerpc.  But these functions were converted to generic bitops and
the BITOP_LE_SWIZZLE is not used anymore.

Signed-off-by: Akinobu Mita <akinobu.mita@gmail.com>
Cc: Benjamin Herrenschmidt <benh@kernel.crashing.org>
Cc: Paul Mackerras <paulus@samba.org>
Cc: linuxppc-dev@lists.ozlabs.org
Signed-off-by: Benjamin Herrenschmidt <benh@kernel.crashing.org>
8 years agopowerpc: Avoid link stack corruption in MMU on syscall entry path
Michael Neuling [Wed, 27 Feb 2013 10:45:52 +0000 (10:45 +0000)]
powerpc: Avoid link stack corruption in MMU on syscall entry path

Currently we use the link register to branch up high in the early MMU on
syscall entry path.  Unfortunately, this trashes the link stack as the
address we are going to is not associated with the earlier mflr.

This patch simply converts us to used the count register (volatile over
syscalls anyway) instead.  This is much better at predicting in this
scenario and doesn't trash link stack causing a bunch of additional
branch mispredicts later.  Benchmarking this on POWER8 saves a bunch of
cycles on Anton's null syscall benchmark here:
   http://ozlabs.org/~anton/junkcode/null_syscall.c

Signed-off-by: Michael Neuling <mikey@neuling.org>
Signed-off-by: Benjamin Herrenschmidt <benh@kernel.crashing.org>
8 years agodrivers/tty/hvc: Use strlcpy instead of strncpy
Chen Gang [Mon, 25 Feb 2013 17:43:25 +0000 (17:43 +0000)]
drivers/tty/hvc: Use strlcpy instead of strncpy

when strlen pi->location_code is larger than HVCS_CLC_LENGTH + 1,
    original implementation can not let hvcsd->p_location_code NUL terminated.
  so need fix it (also can simplify the code)

Signed-off-by: Chen Gang <gang.chen@asianux.com>
Signed-off-by: Benjamin Herrenschmidt <benh@kernel.crashing.org>
8 years agopowerpc/pseries/hvcserver: Fix strncpy buffer limit in location code
Chen Gang [Mon, 25 Feb 2013 16:51:49 +0000 (16:51 +0000)]
powerpc/pseries/hvcserver: Fix strncpy buffer limit in location code

the dest buf len is 80 (HVCS_CLC_LENGTH + 1).
  the src buf len is PAGE_SIZE.
  if src buf string len is more than 80, it will cause issue.

Signed-off-by: Chen Gang <gang.chen@asianux.com>
Signed-off-by: Benjamin Herrenschmidt <benh@kernel.crashing.org>
8 years agopowerpc: Fix compile of sha1-powerpc-asm.S on 32-bit
Tony Breeds [Mon, 25 Feb 2013 16:20:05 +0000 (16:20 +0000)]
powerpc: Fix compile of sha1-powerpc-asm.S on 32-bit

When building with CRYPTO_SHA1_PPC enabled we fail with:

powerpc/crypto/sha1-powerpc-asm.S: Assembler messages:
powerpc/crypto/sha1-powerpc-asm.S:116: Error: can't resolve `0' {*ABS* section} - `STACKFRAMESIZE' {*UND* section}
powerpc/crypto/sha1-powerpc-asm.S:116: Error: expression too complex
powerpc/crypto/sha1-powerpc-asm.S:178: Error: unsupported relocation against STACKFRAMESIZE

Use INT_FRAME_SIZE instead of STACKFRAMESIZE.

Signed-off-by: Tony Breeds <tony@bakeyournoodle.com>
Tested-by: Christian Kujau <lists@nerdbynature.de>
Signed-off-by: Benjamin Herrenschmidt <benh@kernel.crashing.org>
8 years agohw_random: make buffer usable in scatterlist.
Rusty Russell [Mon, 4 Mar 2013 23:37:08 +0000 (10:07 +1030)]
hw_random: make buffer usable in scatterlist.

virtio_rng feeds the randomness buffer handed by the core directly
into the scatterlist, since commit bb347d98079a547e80bd4722dee1de61e4dca0e8.

However, if CONFIG_HW_RANDOM=m, the static buffer isn't a linear address
(at least on most archs).  We could fix this in virtio_rng, but it's actually
far easier to just do it in the core as virtio_rng would have to allocate
a buffer every time (it doesn't know how much the core will want to read).

Reported-by: Aurelien Jarno <aurelien@aurel32.net>
Tested-by: Aurelien Jarno <aurelien@aurel32.net>
Signed-off-by: Rusty Russell <rusty@rustcorp.com.au>
Cc: stable@kernel.org
8 years agotcp: fix double-counted receiver RTT when leaving receiver fast path
Neal Cardwell [Mon, 4 Mar 2013 06:23:05 +0000 (06:23 +0000)]
tcp: fix double-counted receiver RTT when leaving receiver fast path

We should not update ts_recent and call tcp_rcv_rtt_measure_ts() both
before and after going to step5. That wastes CPU and double-counts the
receiver-side RTT sample.

Signed-off-by: Neal Cardwell <ncardwell@google.com>
Acked-by: Eric Dumazet <edumazet@google.com>
Signed-off-by: David S. Miller <davem@davemloft.net>
8 years agoCAIF: fix sparse warning for caif_usb
Silviu-Mihai Popescu [Sun, 3 Mar 2013 21:09:31 +0000 (21:09 +0000)]
CAIF: fix sparse warning for caif_usb

This fixes the following sparse warning:
net/caif/caif_usb.c:84:16: warning: symbol 'cfusbl_create' was not
declared. Should it be static?

Signed-off-by: Silviu-Mihai Popescu <silviupopescu1990@gmail.com>
Signed-off-by: David S. Miller <davem@davemloft.net>
8 years agords: simplify a warning message
Cong Wang [Sun, 3 Mar 2013 20:57:18 +0000 (20:57 +0000)]
rds: simplify a warning message

Cc: David S. Miller <davem@davemloft.net>
Cc: Venkat Venkatsubra <venkat.x.venkatsubra@oracle.com>
Signed-off-by: Cong Wang <amwang@redhat.com>
Signed-off-by: David S. Miller <davem@davemloft.net>
8 years agonet: fec: fix build error in no MXC platform
Frank Li [Sun, 3 Mar 2013 20:52:38 +0000 (20:52 +0000)]
net: fec: fix build error in no MXC platform

build error cause by
Commit ff43da86c69d76a726ffe7d1666148960dc1d108
("NET: FEC: dynamtic check DMA desc buff type")

drivers/net/ethernet/freescale/fec.c: In function ‘fec_enet_get_nextdesc’:
drivers/net/ethernet/freescale/fec.c:215:18: error: invalid use of undefined type ‘struct bufdesc_ex’
drivers/net/ethernet/freescale/fec.c: In function ‘fec_enet_get_prevdesc’:
drivers/net/ethernet/freescale/fec.c:224:18: error: invalid use of undefined type ‘struct bufdesc_ex’
drivers/net/ethernet/freescale/fec.c: In function ‘fec_enet_start_xmit’:
drivers/net/ethernet/freescale/fec.c:286:37: error: arithmetic on pointer to an incomplete type
drivers/net/ethernet/freescale/fec.c:287:13: error: arithmetic on pointer to an incomplete type
drivers/net/ethernet/freescale/fec.c:324:7: error: dereferencing pointer to incomplete type etc....

Signed-off-by: Frank Li <Frank.Li@freescale.com>
Signed-off-by: David S. Miller <davem@davemloft.net>
8 years agonet: ipv6: Don't purge default router if accept_ra=2
Lorenzo Colitti [Sun, 3 Mar 2013 20:46:46 +0000 (20:46 +0000)]
net: ipv6: Don't purge default router if accept_ra=2

Setting net.ipv6.conf.<interface>.accept_ra=2 causes the kernel
to accept RAs even when forwarding is enabled. However, enabling
forwarding purges all default routes on the system, breaking
connectivity until the next RA is received. Fix this by not
purging default routes on interfaces that have accept_ra=2.

Signed-off-by: Lorenzo Colitti <lorenzo@google.com>
Acked-by: YOSHIFUJI Hideaki <yoshfuji@linux-ipv6.org>
Acked-by: Eric Dumazet <edumazet@google.com>
Signed-off-by: David S. Miller <davem@davemloft.net>
8 years agonet: fec: put tx to napi poll function to fix dead lock
Frank Li [Sun, 3 Mar 2013 17:34:25 +0000 (17:34 +0000)]
net: fec: put tx to napi poll function to fix dead lock

up stack ndo_start_xmit already hold lock.
fec_enet_start_xmit needn't spin lock.
stat_xmit just update fep->cur_tx
fec_enet_tx just update fep->dirty_tx

Reserve a empty bdb to check full or empty
cur_tx == dirty_tx    means full
cur_tx == dirty_tx +1 means empty

So needn't is_full variable.

Fix spin lock deadlock

=================================
[ INFO: inconsistent lock state ]
3.8.0-rc5+ #107 Not tainted
---------------------------------
inconsistent {HARDIRQ-ON-W} -> {IN-HARDIRQ-W} usage.
ptp4l/615 [HC1[1]:SC0[0]:HE0:SE1] takes:
 (&(&list->lock)->rlock#3){?.-...}, at: [<8042c3c4>] skb_queue_tail+0x20/0x50
 {HARDIRQ-ON-W} state was registered at:
 [<80067250>] mark_lock+0x154/0x4e8
 [<800676f4>] mark_irqflags+0x110/0x1a4
 [<80069208>] __lock_acquire+0x494/0x9c0
 [<80069ce8>] lock_acquire+0x90/0xa4
 [<80527ad0>] _raw_spin_lock_bh+0x44/0x54
 [<804877e0>] first_packet_length+0x38/0x1f0
 [<804879e4>] udp_poll+0x4c/0x5c
 [<804231f8>] sock_poll+0x24/0x28
 [<800d27f0>] do_poll.isra.10+0x120/0x254
 [<800d36e4>] do_sys_poll+0x15c/0x1e8
 [<800d3828>] sys_poll+0x60/0xc8
 [<8000e780>] ret_fast_syscall+0x0/0x3c

 *** DEADLOCK ***

 1 lock held by ptp4l/615:
  #0:  (&(&fep->hw_lock)->rlock){-.-...}, at: [<80355f9c>] fec_enet_tx+0x24/0x268
  stack backtrace:
  Backtrace:
  [<800121e0>] (dump_backtrace+0x0/0x10c) from [<80516210>] (dump_stack+0x18/0x1c)
  r6:8063b1fc r5:bf38b2f8 r4:bf38b000 r3:bf38b000
  [<805161f8>] (dump_stack+0x0/0x1c) from [<805189d0>] (print_usage_bug.part.34+0x164/0x1a4)
  [<8051886c>] (print_usage_bug.part.34+0x0/0x1a4) from [<80518a88>] (print_usage_bug+0x78/0x88)
  r8:80065664 r7:bf38b2f8 r6:00000002 r5:00000000 r4:bf38b000
  [<80518a10>] (print_usage_bug+0x0/0x88) from [<80518b58>] (mark_lock_irq+0xc0/0x270)
  r7:bf38b000 r6:00000002 r5:bf38b2f8 r4:00000000
  [<80518a98>] (mark_lock_irq+0x0/0x270) from [<80067270>] (mark_lock+0x174/0x4e8)
  [<800670fc>] (mark_lock+0x0/0x4e8) from [<80067744>] (mark_irqflags+0x160/0x1a4)
  [<800675e4>] (mark_irqflags+0x0/0x1a4) from [<80069208>] (__lock_acquire+0x494/0x9c0)
  r5:00000002 r4:bf38b2f8
  [<80068d74>] (__lock_acquire+0x0/0x9c0) from [<80069ce8>] (lock_acquire+0x90/0xa4)
  [<80069c58>] (lock_acquire+0x0/0xa4) from [<805278d8>] (_raw_spin_lock_irqsave+0x4c/0x60)
  [<8052788c>] (_raw_spin_lock_irqsave+0x0/0x60) from [<8042c3c4>] (skb_queue_tail+0x20/0x50)
  r6:bfbb2180 r5:bf1d0190 r4:bf1d0184
  [<8042c3a4>] (skb_queue_tail+0x0/0x50) from [<8042c4cc>] (sock_queue_err_skb+0xd8/0x188)
  r6:00000056 r5:bfbb2180 r4:bf1d0000 r3:00000000
  [<8042c3f4>] (sock_queue_err_skb+0x0/0x188) from [<8042d15c>] (skb_tstamp_tx+0x70/0xa0)
  r6:bf0dddb0 r5:bf1d0000 r4:bfbb2180 r3:00000004
  [<8042d0ec>] (skb_tstamp_tx+0x0/0xa0) from [<803561d0>] (fec_enet_tx+0x258/0x268)
  r6:c089d260 r5:00001c00 r4:bfbd0000
  [<80355f78>] (fec_enet_tx+0x0/0x268) from [<803562cc>] (fec_enet_interrupt+0xec/0xf8)
  [<803561e0>] (fec_enet_interrupt+0x0/0xf8) from [<8007d5b0>] (handle_irq_event_percpu+0x54/0x1a0)
  [<8007d55c>] (handle_irq_event_percpu+0x0/0x1a0) from [<8007d740>] (handle_irq_event+0x44/0x64)
  [<8007d6fc>] (handle_irq_event+0x0/0x64) from [<80080690>] (handle_fasteoi_irq+0xc4/0x15c)
  r6:bf0dc000 r5:bf811290 r4:bf811240 r3:00000000
  [<800805cc>] (handle_fasteoi_irq+0x0/0x15c) from [<8007ceec>] (generic_handle_irq+0x28/0x38)
  r5:807130c8 r4:00000096
  [<8007cec4>] (generic_handle_irq+0x0/0x38) from [<8000f16c>] (handle_IRQ+0x54/0xb4)
  r4:8071d280 r3:00000180
  [<8000f118>] (handle_IRQ+0x0/0xb4) from [<80008544>] (gic_handle_irq+0x30/0x64)
  r8:8000e924 r7:f4000100 r6:bf0ddef8 r5:8071c974 r4:f400010c
  r3:00000000
  [<80008514>] (gic_handle_irq+0x0/0x64) from [<8000e2e4>] (__irq_svc+0x44/0x5c)
  Exception stack(0xbf0ddef8 to 0xbf0ddf40)

Signed-off-by: Frank Li <Frank.Li@freescale.com>
Signed-off-by: David S. Miller <davem@davemloft.net>
8 years agosctp: use KMALLOC_MAX_SIZE instead of its own MAX_KMALLOC_SIZE
Cong Wang [Sun, 3 Mar 2013 16:28:27 +0000 (16:28 +0000)]
sctp: use KMALLOC_MAX_SIZE instead of its own MAX_KMALLOC_SIZE

Don't definite its own MAX_KMALLOC_SIZE, use the one
defined in mm.

Cc: Vlad Yasevich <vyasevich@gmail.com>
Cc: Sridhar Samudrala <sri@us.ibm.com>
Cc: Neil Horman <nhorman@tuxdriver.com>
Cc: David S. Miller <davem@davemloft.net>
Signed-off-by: Cong Wang <amwang@redhat.com>
Acked-by: Neil Horman <nhorman@tuxdriver.com>
Signed-off-by: David S. Miller <davem@davemloft.net>
8 years agords: limit the size allocated by rds_message_alloc()
Cong Wang [Sun, 3 Mar 2013 16:18:11 +0000 (16:18 +0000)]
rds: limit the size allocated by rds_message_alloc()

Dave Jones reported the following bug:

"When fed mangled socket data, rds will trust what userspace gives it,
and tries to allocate enormous amounts of memory larger than what
kmalloc can satisfy."

WARNING: at mm/page_alloc.c:2393 __alloc_pages_nodemask+0xa0d/0xbe0()
Hardware name: GA-MA78GM-S2H
Modules linked in: vmw_vsock_vmci_transport vmw_vmci vsock fuse bnep dlci bridge 8021q garp stp mrp binfmt_misc l2tp_ppp l2tp_core rfcomm s
Pid: 24652, comm: trinity-child2 Not tainted 3.8.0+ #65
Call Trace:
 [<ffffffff81044155>] warn_slowpath_common+0x75/0xa0
 [<ffffffff8104419a>] warn_slowpath_null+0x1a/0x20
 [<ffffffff811444ad>] __alloc_pages_nodemask+0xa0d/0xbe0
 [<ffffffff8100a196>] ? native_sched_clock+0x26/0x90
 [<ffffffff810b2128>] ? trace_hardirqs_off_caller+0x28/0xc0
 [<ffffffff810b21cd>] ? trace_hardirqs_off+0xd/0x10
 [<ffffffff811861f8>] alloc_pages_current+0xb8/0x180
 [<ffffffff8113eaaa>] __get_free_pages+0x2a/0x80
 [<ffffffff811934fe>] kmalloc_order_trace+0x3e/0x1a0
 [<ffffffff81193955>] __kmalloc+0x2f5/0x3a0
 [<ffffffff8104df0c>] ? local_bh_enable_ip+0x7c/0xf0
 [<ffffffffa0401ab3>] rds_message_alloc+0x23/0xb0 [rds]
 [<ffffffffa04043a1>] rds_sendmsg+0x2b1/0x990 [rds]
 [<ffffffff810b21cd>] ? trace_hardirqs_off+0xd/0x10
 [<ffffffff81564620>] sock_sendmsg+0xb0/0xe0
 [<ffffffff810b2052>] ? get_lock_stats+0x22/0x70
 [<ffffffff810b24be>] ? put_lock_stats.isra.23+0xe/0x40
 [<ffffffff81567f30>] sys_sendto+0x130/0x180
 [<ffffffff810b872d>] ? trace_hardirqs_on+0xd/0x10
 [<ffffffff816c547b>] ? _raw_spin_unlock_irq+0x3b/0x60
 [<ffffffff816cd767>] ? sysret_check+0x1b/0x56
 [<ffffffff810b8695>] ? trace_hardirqs_on_caller+0x115/0x1a0
 [<ffffffff81341d8e>] ? trace_hardirqs_on_thunk+0x3a/0x3f
 [<ffffffff816cd742>] system_call_fastpath+0x16/0x1b
---[ end trace eed6ae990d018c8b ]---

Reported-by: Dave Jones <davej@redhat.com>
Cc: Dave Jones <davej@redhat.com>
Cc: David S. Miller <davem@davemloft.net>
Cc: Venkat Venkatsubra <venkat.x.venkatsubra@oracle.com>
Signed-off-by: Cong Wang <amwang@redhat.com>
Acked-by: Venkat Venkatsubra <venkat.x.venkatsubra@oracle.com>
Signed-off-by: David S. Miller <davem@davemloft.net>
8 years agoLinux 3.9-rc1
Linus Torvalds [Sun, 3 Mar 2013 23:11:05 +0000 (15:11 -0800)]
Linux 3.9-rc1

8 years agoMerge tag 'disintegrate-fbdev-20121220' of git://git.infradead.org/users/dhowells...
Linus Torvalds [Sun, 3 Mar 2013 22:24:59 +0000 (14:24 -0800)]
Merge tag 'disintegrate-fbdev-20121220' of git://git.infradead.org/users/dhowells/linux-headers

Pull fbdev UAPI disintegration from David Howells:
 "You'll be glad to here that the end is nigh for the UAPI patches.
  Only the fbdev/framebuffer piece remains now that the SCSI stuff has
  gone in.

  Here are the UAPI disintegration bits for the fbdev drivers.  It
  appears that Florian hasn't had time to deal with my patch, but back
  in December he did say he didn't mind if I pushed it forward."

Yay.  No more uapi movement.  And hopefully no more big header file
cleanups coming up either, it just tends to be very painful.

* tag 'disintegrate-fbdev-20121220' of git://git.infradead.org/users/dhowells/linux-headers:
  UAPI: (Scripted) Disintegrate include/video

8 years agoMerge tag 'stable/for-linus-3.9-rc1-tag' of git://git.kernel.org/pub/scm/linux/kernel...
Linus Torvalds [Sun, 3 Mar 2013 22:22:53 +0000 (14:22 -0800)]
Merge tag 'stable/for-linus-3.9-rc1-tag' of git://git./linux/kernel/git/konrad/xen

Pull Xen bug-fixes from Konrad Rzeszutek Wilk:
 - Update the Xen ACPI memory and CPU hotplug locking mechanism.
 - Fix PAT issues wherein various applications would not start
 - Fix handling of multiple MSI as AHCI now does it.
 - Fix ARM compile failures.

* tag 'stable/for-linus-3.9-rc1-tag' of git://git.kernel.org/pub/scm/linux/kernel/git/konrad/xen:
  xenbus: fix compile failure on ARM with Xen enabled
  xen/pci: We don't do multiple MSI's.
  xen/pat: Disable PAT using pat_enabled value.
  xen/acpi: xen cpu hotplug minor updates
  xen/acpi: xen memory hotplug minor updates

8 years agoMerge branch 'for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/viro/vfs
Linus Torvalds [Sun, 3 Mar 2013 21:23:02 +0000 (13:23 -0800)]
Merge branch 'for-linus' of git://git./linux/kernel/git/viro/vfs

Pull  more VFS bits from Al Viro:
 "Unfortunately, it looks like xattr series will have to wait until the
  next cycle ;-/

  This pile contains 9p cleanups and fixes (races in v9fs_fid_add()
  etc), fixup for nommu breakage in shmem.c, several cleanups and a bit
  more file_inode() work"

* 'for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/viro/vfs:
  constify path_get/path_put and fs_struct.c stuff
  fix nommu breakage in shmem.c
  cache the value of file_inode() in struct file
  9p: if v9fs_fid_lookup() gets to asking server, it'd better have hashed dentry
  9p: make sure ->lookup() adds fid to the right dentry
  9p: untangle ->lookup() a bit
  9p: double iput() in ->lookup() if d_materialise_unique() fails
  9p: v9fs_fid_add() can't fail now
  v9fs: get rid of v9fs_dentry
  9p: turn fid->dlist into hlist
  9p: don't bother with private lock in ->d_fsdata; dentry->d_lock will do just fine
  more file_inode() open-coded instances
  selinux: opened file can't have NULL or negative ->f_path.dentry

(In the meantime, the hlist traversal macros have changed, so this
required a semantic conflict fixup for the newly hlistified fid->dlist)

8 years agoMerge branch 'for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/mason/linux...
Linus Torvalds [Sun, 3 Mar 2013 21:13:20 +0000 (13:13 -0800)]
Merge branch 'for-linus' of git://git./linux/kernel/git/mason/linux-btrfs

Pull btrfs fixup from Chris Mason:
 "Geert and James both sent this one in, sorry guys"

* 'for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/mason/linux-btrfs:
  btrfs/raid56: Add missing #include <linux/vmalloc.h>

8 years agoMerge branch 'for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/s390/linux
Linus Torvalds [Sun, 3 Mar 2013 20:58:43 +0000 (12:58 -0800)]
Merge branch 'for-linus' of git://git./linux/kernel/git/s390/linux

Pull second set of s390 patches from Martin Schwidefsky:
 "The main part of this merge are Heikos uaccess patches.  Together with
  commit 09884964335e ("mm: do not grow the stack vma just because of an
  overrun on preceding vma") the user string access is hopefully fixed
  for good.

  In addition some bug fixes and two cleanup patches."

* 'for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/s390/linux:
  s390/module: fix compile warning
  qdio: remove unused parameters
  s390/uaccess: fix kernel ds access for page table walk
  s390/uaccess: fix strncpy_from_user string length check
  input: disable i8042 PC Keyboard controller for s390
  s390/dis: Fix invalid array size
  s390/uaccess: remove pointless access_ok() checks
  s390/uaccess: fix strncpy_from_user/strnlen_user zero maxlen case
  s390/uaccess: shorten strncpy_from_user/strnlen_user
  s390/dasd: fix unresponsive device after all channel paths were lost
  s390/mm: ignore change bit for vmemmap
  s390/page table dumper: add support for change-recording override bit

8 years agoMerge branch 'fixes-for-3.9-latest' of git://git.kernel.org/pub/scm/linux/kernel...
Linus Torvalds [Sun, 3 Mar 2013 20:57:38 +0000 (12:57 -0800)]
Merge branch 'fixes-for-3.9-latest' of git://git./linux/kernel/git/deller/parisc-linux

Pull second round of PARISC updates from Helge Deller:
 "The most important fix in this branch is the switch of io_setup,
  io_getevents and io_submit syscalls to use the available compat
  syscalls when running 32bit userspace on 64bit kernel.  Other than
  that it's mostly removal of compile warnings."

* 'fixes-for-3.9-latest' of git://git.kernel.org/pub/scm/linux/kernel/git/deller/parisc-linux:
  parisc: fix redefinition of SET_PERSONALITY
  parisc: do not install modules when installing kernel
  parisc: fix compile warnings triggered by atomic_sub(sizeof(),v)
  parisc: check return value of down_interruptible() in hp_sdc_rtc.c
  parisc: avoid unitialized variable warning in pa_memcpy()
  parisc: remove unused variable 'compat_val'
  parisc: switch to compat_functions of io_setup, io_getevents and io_submit
  parisc: select ARCH_WANT_FRAME_POINTERS

8 years agoMerge tag 'metag-v3.9-rc1-v4' of git://git.kernel.org/pub/scm/linux/kernel/git/jhogan...
Linus Torvalds [Sun, 3 Mar 2013 20:06:09 +0000 (12:06 -0800)]
Merge tag 'metag-v3.9-rc1-v4' of git://git./linux/kernel/git/jhogan/metag

Pull new ImgTec Meta architecture from James Hogan:
 "This adds core architecture support for Imagination's Meta processor
  cores, followed by some later miscellaneous arch/metag cleanups and
  fixes which I kept separate to ease review:

   - Support for basic Meta 1 (ATP) and Meta 2 (HTP) core architecture
   - A few fixes all over, particularly for symbol prefixes
   - A few privilege protection fixes
   - Several cleanups (setup.c includes, split out a lot of
     metag_ksyms.c)
   - Fix some missing exports
   - Convert hugetlb to use vm_unmapped_area()
   - Copy device tree to non-init memory
   - Provide dma_get_sgtable()"

* tag 'metag-v3.9-rc1-v4' of git://git.kernel.org/pub/scm/linux/kernel/git/jhogan/metag: (61 commits)
  metag: Provide dma_get_sgtable()
  metag: prom.h: remove declaration of metag_dt_memblock_reserve()
  metag: copy devicetree to non-init memory
  metag: cleanup metag_ksyms.c includes
  metag: move mm/init.c exports out of metag_ksyms.c
  metag: move usercopy.c exports out of metag_ksyms.c
  metag: move setup.c exports out of metag_ksyms.c
  metag: move kick.c exports out of metag_ksyms.c
  metag: move traps.c exports out of metag_ksyms.c
  metag: move irq enable out of irqflags.h on SMP
  genksyms: fix metag symbol prefix on crc symbols
  metag: hugetlb: convert to vm_unmapped_area()
  metag: export clear_page and copy_page
  metag: export metag_code_cache_flush_all
  metag: protect more non-MMU memory regions
  metag: make TXPRIVEXT bits explicit
  metag: kernel/setup.c: sort includes
  perf: Enable building perf tools for Meta
  metag: add boot time LNKGET/LNKSET check
  metag: add __init to metag_cache_probe()
  ...

8 years agoMerge branch 'for-linus' of git://git.linaro.org/people/rmk/linux-arm
Linus Torvalds [Sun, 3 Mar 2013 19:54:39 +0000 (11:54 -0800)]
Merge branch 'for-linus' of git://git.linaro.org/people/rmk/linux-arm

Pull late ARM updates from Russell King:
 "Here is the late set of ARM updates for this merge window; in here is:

   - The ARM parts of the broadcast timer support, core parts merged
     through tglx's tree.  This was left over from the previous merge to
     allow the dependency on tglx's tree to be resolved.

   - A fix to the VFP code which shows up on Raspberry Pi's, as well as
     fixing the fallout from a previous commit in this area.

   - A number of smaller fixes scattered throughout the ARM tree"

* 'for-linus' of git://git.linaro.org/people/rmk/linux-arm:
  ARM: Fix broken commit 0cc41e4a21d43 corrupting kernel messages
  ARM: fix scheduling while atomic warning in alignment handling code
  ARM: VFP: fix emulation of second VFP instruction
  ARM: 7656/1: uImage: Error out on build of multiplatform without LOADADDR
  ARM: 7640/1: memory: tegra_ahb_enable_smmu() depends on TEGRA_IOMMU_SMMU
  ARM: 7654/1: Preserve L_PTE_VALID in pte_modify()
  ARM: 7653/2: do not scale loops_per_jiffy when using a constant delay clock
  ARM: 7651/1: remove unused smp_timer_broadcast #define

8 years agoMerge tag 'char-misc-3.9-rc1' of git://git.kernel.org/pub/scm/linux/kernel/git/gregkh...
Linus Torvalds [Sun, 3 Mar 2013 18:25:47 +0000 (10:25 -0800)]
Merge tag 'char-misc-3.9-rc1' of git://git./linux/kernel/git/gregkh/char-misc

Pull char/misc patch from Greg Kroah-Hartman:
 "Here is one remaining patch for 3.9-rc1.  It is for the hyper-v
  drivers, and had to wait until some other patches went in through the
  x86 tree."

Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* tag 'char-misc-3.9-rc1' of git://git.kernel.org/pub/scm/linux/kernel/git/gregkh/char-misc:
  Drivers: hv: vmbus: Use the new infrastructure for delivering VMBUS interrupts

8 years agoMerge tag 'usb-3.9-rc1' of git://git.kernel.org/pub/scm/linux/kernel/git/gregkh/usb
Linus Torvalds [Sun, 3 Mar 2013 18:24:57 +0000 (10:24 -0800)]
Merge tag 'usb-3.9-rc1' of git://git./linux/kernel/git/gregkh/usb

Pull USB patch revert from Greg Kroah-Hartman:
 "Here is one remaining USB patch for 3.9-rc1, it reverts a 3.8 patch
  that has caused a lot of regressions for some VIA EHCI controllers."

* tag 'usb-3.9-rc1' of git://git.kernel.org/pub/scm/linux/kernel/git/gregkh/usb:
  USB: EHCI: revert "remove ASS/PSS polling timeout"

8 years agoMerge git://www.linux-watchdog.org/linux-watchdog
Linus Torvalds [Sun, 3 Mar 2013 18:23:29 +0000 (10:23 -0800)]
Merge git://www.linux-watchdog.org/linux-watchdog

Pull watchdog updates from Wim Van Sebroeck:
 "This contains:
   - fixes and improvements
   - devicetree bindings
   - conversion to watchdog generic framework of the following drivers:
        - booke_wdt
        - bcm47xx_wdt.c
        - at91sam9_wdt
   - Removal of old STMP3xxx driver
   - Addition of following new drivers:
        - new driver for STMP3xxx and i.MX23/28
        - Retu watchdog driver"

* git://www.linux-watchdog.org/linux-watchdog: (30 commits)
  watchdog: sp805_wdt depends on ARM
  watchdog: davinci_wdt: update to devm_* API
  watchdog: davinci_wdt: use devm managed clk get
  watchdog: at91rm9200: add DT support
  watchdog: add timeout-sec property binding
  watchdog: at91sam9_wdt: Convert to use the watchdog framework
  watchdog: omap_wdt: Add option nowayout
  watchdog: core: dt: add support for the timeout-sec dt property
  watchdog: bcm47xx_wdt.c: add hard timer
  watchdog: bcm47xx_wdt.c: rename wdt_time to timeout
  watchdog: bcm47xx_wdt.c: rename ops methods
  watchdog: bcm47xx_wdt.c: use platform device
  watchdog: bcm47xx_wdt.c: convert to watchdog core api
  watchdog: Convert BookE watchdog driver to watchdog infrastructure
  watchdog: s3c2410_wdt: Use devm_* functions
  watchdog: remove old STMP3xxx driver
  watchdog: add new driver for STMP3xxx and i.MX23/28
  rtc: stmp3xxx: add wdt-accessor function
  watchdog: introduce retu_wdt driver
  watchdog: intel_scu_watchdog: fix Kconfig dependency
  ...

8 years agoMerge branch 'next' of git://git.infradead.org/users/vkoul/slave-dma
Linus Torvalds [Sun, 3 Mar 2013 18:20:22 +0000 (10:20 -0800)]
Merge branch 'next' of git://git.infradead.org/users/vkoul/slave-dma

Pull second set of slave-dmaengine updates from Vinod Koul:
 "Arnd's patch moves the dw_dmac to use generic DMA binding.  I agreed
  to merge this late as it will avoid the conflicts between trees.

  The second patch from Matt adding a dma_request_slave_channel_compat
  API was supposed to be picked up, but somehow never got picked up.
  Some patches dependent on this are already in -next :("

* 'next' of git://git.infradead.org/users/vkoul/slave-dma:
  dmaengine: dw_dmac: move to generic DMA binding
  dmaengine: add dma_request_slave_channel_compat()

8 years agoMerge branch 'for_linus' of git://cavan.codon.org.uk/platform-drivers-x86
Linus Torvalds [Sun, 3 Mar 2013 18:16:19 +0000 (10:16 -0800)]
Merge branch 'for_linus' of git://cavan.codon.org.uk/platform-drivers-x86

Pull x86 platform driver updates from Matthew Garrett:
 "Mostly relatively small updates, along with some hardware enablement
  for Sony hardware and a pile of updates to Google's Chromebook driver"

* 'for_linus' of git://cavan.codon.org.uk/platform-drivers-x86: (49 commits)
  ideapad-laptop: Depend on BACKLIGHT_CLASS_DEVICE instead of selecting it
  ideapad: depends on backlight subsystem and update comment
  Platform: x86: chromeos_laptop - add i915 gmbuses to adapter names
  Platform: x86: chromeos_laptop - Add isl light sensor for Pixel
  Platform: x86: chromeos_laptop - Add a more general add_i2c_device
  Platform: x86: chromeos_laptop - Add Pixel Touchscreen
  Platform: x86: chromeos_laptop - Add support for probing devices
  Platform: x86: chromeos_laptop - Add Pixel Trackpad
  hp-wmi: fix handling of platform device
  sony-laptop: leak in error handling sony_nc_lid_resume_setup()
  hp-wmi: Add support for SMBus hotkeys
  asus-wmi: Fix unused function build warning
  acer-wmi: avoid the warning of 'devices' may be used uninitialized
  drivers/platform/x86/thinkpad_acpi.c: Handle HKEY event 0x6040
  Platform: x86: chromeos_laptop - Add HP Pavilion 14
  Platform: x86: chromeos_laptop - Add Taos tsl2583 device
  Platform: x86: chromeos_laptop - Add Taos tsl2563 device
  Platform: x86: chromeos_laptop - Add Acer C7 trackpad
  Platform: x86: chromeos_laptop - Rename setup_lumpy_tp to setup_cyapa_smbus_tp
  asus-laptop: always report brightness key events
  ...

8 years agobtrfs/raid56: Add missing #include <linux/vmalloc.h>
Geert Uytterhoeven [Sun, 3 Mar 2013 11:44:41 +0000 (04:44 -0700)]
btrfs/raid56: Add missing #include <linux/vmalloc.h>

tilegx_defconfig:

fs/btrfs/raid56.c: In function 'btrfs_alloc_stripe_hash_table':
fs/btrfs/raid56.c:206:3: error: implicit declaration of function 'vzalloc' [-Werror=implicit-function-declaration]
fs/btrfs/raid56.c:206:9: warning: assignment makes pointer from integer without a cast [enabled by default]
fs/btrfs/raid56.c:226:4: error: implicit declaration of function 'vfree' [-Werror=implicit-function-declaration]

Signed-off-by: Geert Uytterhoeven <geert@linux-m68k.org>
Signed-off-by: Chris Mason <chris.mason@fusionio.com>
8 years agoMAINTAINERS: remove eexpress
Cesar Eduardo Barros [Sat, 2 Mar 2013 15:53:45 +0000 (15:53 +0000)]
MAINTAINERS: remove eexpress

This driver was removed by commit f84932d (drivers/net: delete ISA intel
eexpress and eepro i825xx drivers).

Cc: Paul Gortmaker <paul.gortmaker@windriver.com>
Cc: Philip Blundell <philb@gnu.org>
Cc: netdev@vger.kernel.org
Signed-off-by: Cesar Eduardo Barros <cesarb@cesarb.net>
Signed-off-by: David S. Miller <davem@davemloft.net>
8 years agoMAINTAINERS: remove drivers/net/wan/cycx*
Cesar Eduardo Barros [Sat, 2 Mar 2013 15:53:43 +0000 (15:53 +0000)]
MAINTAINERS: remove drivers/net/wan/cycx*

This driver was removed by commit 6fcdf4f (wanrouter: delete now
orphaned header content, files/drivers).

Cc: Paul Gortmaker <paul.gortmaker@windriver.com>
Cc: Arnaldo Carvalho de Melo <acme@redhat.com>
Cc: netdev@vger.kernel.org
Signed-off-by: Cesar Eduardo Barros <cesarb@cesarb.net>
Signed-off-by: David S. Miller <davem@davemloft.net>
8 years agoMAINTAINERS: remove 3c505
Cesar Eduardo Barros [Sat, 2 Mar 2013 15:53:39 +0000 (15:53 +0000)]
MAINTAINERS: remove 3c505

This driver was removed by commit 0e245db (drivers/net: delete the 3Com
3c505/3c507 intel i825xx support).

Cc: Paul Gortmaker <paul.gortmaker@windriver.com>
Cc: Philip Blundell <philb@gnu.org>
Cc: netdev@vger.kernel.org
Signed-off-by: Cesar Eduardo Barros <cesarb@cesarb.net>
Signed-off-by: David S. Miller <davem@davemloft.net>
8 years agocaif_dev: fix sparse warnings for caif_flow_cb
Silviu-Mihai Popescu [Sat, 2 Mar 2013 09:45:19 +0000 (09:45 +0000)]
caif_dev: fix sparse warnings for caif_flow_cb

This fixed the following sparse warning:
net/caif/caif_dev.c:121:6: warning: symbol 'caif_flow_cb' was not
declared. Should it be static?

Signed-off-by: Silviu-Mihai Popescu <silviupopescu1990@gmail.com>
Signed-off-by: David S. Miller <davem@davemloft.net>
8 years agoax88179_178a: ASIX AX88179_178A USB 3.0/2.0 to gigabit ethernet adapter driver
Freddy Xin [Sat, 2 Mar 2013 00:41:11 +0000 (00:41 +0000)]
ax88179_178a: ASIX AX88179_178A USB 3.0/2.0 to gigabit ethernet adapter driver

This is a resubmission.
Added kfree() in ax88179_get_eeprom to prevent memory leakage.
Modified "__le16 rxctl" to "u16 rxctl" in "struct ax88179_data" and removed pointless casts.
Removed asix_init and asix_exit functions and added "module_usb_driver(ax88179_178a_driver)".
Fixed endianness issue on big endian systems and verified this driver on iBook G4.
Removed steps that change net->features in ax88179_set_features function.
Added "const" to ethtool_ops structure and fixed the coding style of AX88179_BULKIN_SIZE array.
Fixed the issue that the default MTU is not 1500.
Added ax88179_change_mtu function and enabled the hardware jumbo frame function to support an
MTU higher than 1500.
Fixed indentation and empty line coding style errors.
The _nopm version usb functions were added to access register in suspend and resume functions.
Serveral variables allocted dynamically were removed and replaced by stack variables.
ax88179_get_eeprom were modified from asix_get_eeprom in asix_common.

This patch adds a driver for ASIX's AX88179 family of USB 3.0/2.0
to gigabit ethernet adapters. It's based on the AX88xxx driver but
the usb commands used to access registers for AX88179 are completely different.
This driver had been verified on x86 system with AX88179/AX88178A and
Sitcomm LN-032 USB dongles.

Signed-off-by: Freddy Xin <freddy@asix.com.tw>
Signed-off-by: David S. Miller <davem@davemloft.net>
8 years agoMerge tag 'ext4_for_linus' of git://git.kernel.org/pub/scm/linux/kernel/git/tytso...
Linus Torvalds [Sun, 3 Mar 2013 03:33:21 +0000 (19:33 -0800)]
Merge tag 'ext4_for_linus' of git://git./linux/kernel/git/tytso/ext4

Pull ext4 bug fixes from Ted Ts'o:
 "Various bug fixes for ext4.  The most important is a fix for the new
  extent cache's slab shrinker which can cause significant, user-visible
  pauses when the system is under memory pressure."

* tag 'ext4_for_linus' of git://git.kernel.org/pub/scm/linux/kernel/git/tytso/ext4:
  ext4: enable quotas before orphan cleanup
  ext4: don't allow quota mount options when quota feature enabled
  ext4: fix a warning from sparse check for ext4_dir_llseek
  ext4: convert number of blocks to clusters properly
  ext4: fix possible memory leak in ext4_remount()
  jbd2: fix ERR_PTR dereference in jbd2__journal_start
  ext4: use percpu counter for extent cache count
  ext4: optimize ext4_es_shrink()

8 years agoMerge branch 'for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/viro/signal
Linus Torvalds [Sun, 3 Mar 2013 03:32:06 +0000 (19:32 -0800)]
Merge branch 'for-linus' of git://git./linux/kernel/git/viro/signal

Pull sigprocmask compat fix from Al Viro:
 "generic compat_sys_rt_sigprocmask() had a very dumb braino; I'd spent
  quite a while staring at the offending commit before finally managing
  to spot the idiocy ;-/"

* 'for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/viro/signal:
  fix compat_sys_rt_sigprocmask()

8 years agofix compat_sys_rt_sigprocmask()
Al Viro [Sun, 3 Mar 2013 01:39:15 +0000 (20:39 -0500)]
fix compat_sys_rt_sigprocmask()

Converting bitmask to 32bit granularity is fine, but we'd better
_do_ something with the result.  Such as "copy it to userland"...

Signed-off-by: Al Viro <viro@zeniv.linux.org.uk>
8 years agoMerge tag 'nfs-for-3.9-2' of git://git.linux-nfs.org/projects/trondmy/linux-nfs
Linus Torvalds [Sun, 3 Mar 2013 00:46:07 +0000 (16:46 -0800)]
Merge tag 'nfs-for-3.9-2' of git://git.linux-nfs.org/projects/trondmy/linux-nfs

Pull NFS client bugfixes from Trond Myklebust:
 "We've just concluded another Connectathon interoperability testing
  week, and so here are the fixes for the bugs that were discovered:

   - Don't allow NFS silly-renamed files to be deleted
   - Don't start the retransmission timer when out of socket space
   - Fix a couple of pnfs-related Oopses.
   - Fix one more NFSv4 state recovery deadlock
   - Don't loop forever when LAYOUTGET returns NFS4ERR_LAYOUTTRYLATER"

* tag 'nfs-for-3.9-2' of git://git.linux-nfs.org/projects/trondmy/linux-nfs:
  SUNRPC: One line comment fix
  NFSv4.1: LAYOUTGET EDELAY loops timeout to the MDS
  SUNRPC: add call to get configured timeout
  PNFS: set the default DS timeout to 60 seconds
  NFSv4: Fix another open/open_recovery deadlock
  nfs: don't allow nfs_find_actor to match inodes of the wrong type
  NFSv4.1: Hold reference to layout hdr in layoutget
  pnfs: fix resend_to_mds for directio
  SUNRPC: Don't start the retransmission timer when out of socket space
  NFS: Don't allow NFS silly-renamed files to be deleted, no signal

8 years agoMerge branch 'for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/mason/linux...
Linus Torvalds [Sun, 3 Mar 2013 00:41:54 +0000 (16:41 -0800)]
Merge branch 'for-linus' of git://git./linux/kernel/git/mason/linux-btrfs

Pull btrfs update from Chris Mason:
 "The biggest feature in the pull is the new (and still experimental)
  raid56 code that David Woodhouse started long ago.  I'm still working
  on the parity logging setup that will avoid inconsistent parity after
  a crash, so this is only for testing right now.  But, I'd really like
  to get it out to a broader audience to hammer out any performance
  issues or other problems.

  scrub does not yet correct errors on raid5/6 either.

  Josef has another pass at fsync performance.  The big change here is
  to combine waiting for metadata with waiting for data, which is a big
  latency win.  It is also step one toward using atomics from the
  hardware during a commit.

  Mark Fasheh has a new way to use btrfs send/receive to send only the
  metadata changes.  SUSE is using this to make snapper more efficient
  at finding changes between snapshosts.

  Snapshot-aware defrag is also included.

  Otherwise we have a large number of fixes and cleanups.  Eric Sandeen
  wins the award for removing the most lines, and I'm hoping we steal
  this idea from XFS over and over again."

* 'for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/mason/linux-btrfs: (118 commits)
  btrfs: fixup/remove module.h usage as required
  Btrfs: delete inline extents when we find them during logging
  btrfs: try harder to allocate raid56 stripe cache
  Btrfs: cleanup to make the function btrfs_delalloc_reserve_metadata more logic
  Btrfs: don't call btrfs_qgroup_free if just btrfs_qgroup_reserve fails
  Btrfs: remove reduplicate check about root in the function btrfs_clean_quota_tree
  Btrfs: return ENOMEM rather than use BUG_ON when btrfs_alloc_path fails
  Btrfs: fix missing deleted items in btrfs_clean_quota_tree
  btrfs: use only inline_pages from extent buffer
  Btrfs: fix wrong reserved space when deleting a snapshot/subvolume
  Btrfs: fix wrong reserved space in qgroup during snap/subv creation
  Btrfs: remove unnecessary dget_parent/dput when creating the pending snapshot
  btrfs: remove a printk from scan_one_device
  Btrfs: fix NULL pointer after aborting a transaction
  Btrfs: fix memory leak of log roots
  Btrfs: copy everything if we've created an inline extent
  btrfs: cleanup for open-coded alignment
  Btrfs: do not change inode flags in rename
  Btrfs: use reserved space for creating a snapshot
  clear chunk_alloc flag on retryable failure
  ...

8 years agoMerge tag 'for-linus-20130301' of git://git.infradead.org/linux-mtd
Linus Torvalds [Sun, 3 Mar 2013 00:33:54 +0000 (16:33 -0800)]
Merge tag 'for-linus-20130301' of git://git.infradead.org/linux-mtd

Pull MTD update from David Woodhouse:
 "Fairly unexciting MTD merge for 3.9:

   - misc clean-ups in the MTD command-line partitioning parser
     (cmdlinepart)
   - add flash locking support for STmicro chips serial flash chips, as
     well as for CFI command set 2 chips.
   - new driver for the ELM error correction HW module found in various
     TI chips, enable the OMAP NAND driver to use the ELM HW error
     correction
   - added number of new serial flash IDs
   - various fixes and improvements in the gpmi NAND driver
   - bcm47xx NAND driver improvements
   - make the mtdpart module actually removable"

* tag 'for-linus-20130301' of git://git.infradead.org/linux-mtd: (45 commits)
  mtd: map: BUG() in non handled cases
  mtd: bcm47xxnflash: use pr_fmt for module prefix in messages
  mtd: davinci_nand: Use managed resources
  mtd: mtd_torturetest can cause stack overflows
  mtd: physmap_of: Convert device allocation to managed devm_kzalloc()
  mtd: at91: atmel_nand: for PMECC, add code to check the ONFI parameter ECC requirement.
  mtd: atmel_nand: make pmecc-cap, pmecc-sector-size in dts is optional.
  mtd: atmel_nand: avoid to report an error when lookup table offset is 0.
  mtd: bcm47xxsflash: adjust names of bus-specific functions
  mtd: bcm47xxpart: improve probing of nvram partition
  mtd: bcm47xxpart: add support for other erase sizes
  mtd: bcm47xxnflash: register this as normal driver
  mtd: bcm47xxnflash: fix message
  mtd: bcm47xxsflash: register this as normal driver
  mtd: bcm47xxsflash: write number of written bytes
  mtd: gpmi: add sanity check for the ECC
  mtd: gpmi: set the Golois Field bit for mx6q's BCH
  mtd: devices: elm: Removes <xx> literals in elm DT node
  mtd: gpmi: fix a dereferencing freed memory error
  mtd: fix the wrong timeo for panic_nand_wait()
  ...

8 years agoMerge branches 'devel-stable', 'fixes' and 'mmci' into for-linus
Russell King [Sun, 3 Mar 2013 00:32:50 +0000 (00:32 +0000)]
Merge branches 'devel-stable', 'fixes' and 'mmci' into for-linus

8 years agoSUNRPC: One line comment fix
Trond Myklebust [Sat, 2 Mar 2013 23:54:11 +0000 (15:54 -0800)]
SUNRPC: One line comment fix

Reported-by: Weston Andros Adamson <dros@netapp.com>
Signed-off-by: Trond Myklebust <Trond.Myklebust@netapp.com>
8 years agoext4: enable quotas before orphan cleanup
Jan Kara [Sat, 2 Mar 2013 23:22:38 +0000 (18:22 -0500)]
ext4: enable quotas before orphan cleanup

When using quota feature we need to enable quotas before orphan cleanup
so that changes happening during it are properly reflected in quota
accounting.

Signed-off-by: Jan Kara <jack@suse.cz>
Signed-off-by: "Theodore Ts'o" <tytso@mit.edu>
8 years agoext4: don't allow quota mount options when quota feature enabled
Jan Kara [Sat, 2 Mar 2013 22:57:08 +0000 (17:57 -0500)]
ext4: don't allow quota mount options when quota feature enabled

So far we silently ignored when quota mount options were set while quota
feature was enabled.  But this can create confusion in userspace when
mount options are set but silently ignored and also creates opportunities
for bugs when we don't properly test all quota types.  Actually
ext4_mark_dquot_dirty() forgets to test for quota feature so it was
dependent on journaled quota options being set.  OTOH ext4_orphan_cleanup()
tries to enable journaled quota when quota options are specified which is
wrong when quota feature is enabled.

Signed-off-by: Jan Kara <jack@suse.cz>
Signed-off-by: "Theodore Ts'o" <tytso@mit.edu>
8 years agoext4: fix a warning from sparse check for ext4_dir_llseek
Zheng Liu [Sat, 2 Mar 2013 22:24:05 +0000 (17:24 -0500)]
ext4: fix a warning from sparse check for ext4_dir_llseek

ext4_dir_llseek is only used as a callback function, and no one calls
it directly.  So make it as a static function in order to remove a
warning message from sparse check.

Signed-off-by: Zheng Liu <wenqing.lz@taobao.com>
Signed-off-by: "Theodore Ts'o" <tytso@mit.edu>
8 years agoext4: convert number of blocks to clusters properly
Lukas Czerner [Sat, 2 Mar 2013 22:18:58 +0000 (17:18 -0500)]
ext4: convert number of blocks to clusters properly

We're using macro EXT4_B2C() to convert number of blocks to number of
clusters for bigalloc file systems.  However, we should be using
EXT4_NUM_B2C().

Signed-off-by: Lukas Czerner <lczerner@redhat.com>
Signed-off-by: "Theodore Ts'o" <tytso@mit.edu>
Cc: stable@vger.kernel.org
8 years agoext4: fix possible memory leak in ext4_remount()
Wei Yongjun [Sat, 2 Mar 2013 22:13:55 +0000 (17:13 -0500)]
ext4: fix possible memory leak in ext4_remount()

'orig_data' is malloced in ext4_remount() and should be freed
before leaving from the error handling cases, otherwise it will
cause memory leak.

Signed-off-by: Wei Yongjun <yongjun_wei@trendmicro.com.cn>
Signed-off-by: "Theodore Ts'o" <tytso@mit.edu>
Reviewed-by: Lukas Czerner <lczerner@redhat.com>
Cc: stable@vger.kernel.org
8 years agojbd2: fix ERR_PTR dereference in jbd2__journal_start
Dmitry Monakhov [Sat, 2 Mar 2013 22:08:46 +0000 (17:08 -0500)]
jbd2: fix ERR_PTR dereference in jbd2__journal_start

If start_this_handle() failed handle will be initialized
to ERR_PTR() and can not be dereferenced.

paging request at fffffffffffffff6
IP: [<ffffffff813c073f>] jbd2__journal_start+0x18f/0x290
PGD 200e067 PUD 200f067 PMD 0
Oops: 0000 [#1] SMP
Modules linked in: cpufreq_ondemand acpi_cpufreq freq_table mperf coretemp kvm_intel kvm crc32c_intel ghash_clmulni_intel microcode sg xhci_hcd button sd_mod crc_t10dif aesni_intel ablk_helper cryptd lrw aes_x86_64 xts gf128mul ahci libahci pata_acpi ata_generic dm_mirror dm_region_hash dm_log dm_mod
CPU 0 journal commit I/O error

Pid: 2694, comm: fio Not tainted 3.8.0-rc3+ #79                  /DQ67SW
RIP: 0010:[<ffffffff813c073f>]  [<ffffffff813c073f>] jbd2__journal_start+0x18f/0x290
RSP: 0018:ffff880233b8ba58  EFLAGS: 00010292
RAX: 00000000ffffffe2 RBX: ffffffffffffffe2 RCX: 0000000000000006
RDX: 0000000000000000 RSI: 0000000000000000 RDI: ffffffff82128f48
RBP: ffff880233b8ba98 R08: 0000000000000000 R09: ffff88021440a6e0

Signed-off-by: Dmitry Monakhov <dmonakhov@openvz.org>
Signed-off-by: "Theodore Ts'o" <tytso@mit.edu>
8 years agometag: Provide dma_get_sgtable()
James Hogan [Tue, 19 Feb 2013 13:25:46 +0000 (13:25 +0000)]
metag: Provide dma_get_sgtable()

metag/allmodconfig:

drivers/media/v4l2-core/videobuf2-dma-contig.c: In function 'vb2_dc_get_base_sgt':
drivers/media/v4l2-core/videobuf2-dma-contig.c:387: error: implicit declaration of function 'dma_get_sgtable'

For architectures using dma_map_ops, dma_get_sgtable() is provided in
<asm-generic/dma-mapping-common.h>.

Metag does not use dma_map_ops yet, hence it should implement it as an
inline stub using dma_common_get_sgtable().

Signed-off-by: James Hogan <james.hogan@imgtec.com>
Cc: Geert Uytterhoeven <geert@linux-m68k.org>
Acked-by: Marek Szyprowski <m.szyprowski@samsung.com>
8 years agometag: prom.h: remove declaration of metag_dt_memblock_reserve()
James Hogan [Wed, 20 Feb 2013 14:19:54 +0000 (14:19 +0000)]
metag: prom.h: remove declaration of metag_dt_memblock_reserve()

Metag doesn't have a metag_dt_memblock_reserve() function so remove the
declaration from asm/prom.h.

Signed-off-by: James Hogan <james.hogan@imgtec.com>
8 years agometag: copy devicetree to non-init memory
James Hogan [Wed, 20 Feb 2013 13:59:13 +0000 (13:59 +0000)]
metag: copy devicetree to non-init memory

Make a copy of the device tree blob in non-init memory. It is required
when using built-in device tree files that the platform code copies the
blob to non-init memory prior to calling unflatten_device_tree(),
otherwise the strings that the device tree refer to will get poisoned
and potentially reused, breaking later reading of the device tree
post-init (such as compatible matching in modules, debugfs, and the
procfs interface).

Signed-off-by: James Hogan <james.hogan@imgtec.com>
Reviewed-by: Vineet Gupta <vgupta@synopsys.com>
8 years agometag: cleanup metag_ksyms.c includes
James Hogan [Wed, 13 Feb 2013 13:30:15 +0000 (13:30 +0000)]
metag: cleanup metag_ksyms.c includes

Minimise metag_ksyms.c includes to directly include the <asm/*.h> files
that declare a particular symbol, and not include any unnecessary ones.

Signed-off-by: James Hogan <james.hogan@imgtec.com>
8 years agometag: move mm/init.c exports out of metag_ksyms.c
James Hogan [Wed, 13 Feb 2013 13:19:15 +0000 (13:19 +0000)]
metag: move mm/init.c exports out of metag_ksyms.c

It's less error prone to have function symbols exported immediately
after the function rather than in metag_ksyms.c. Move each EXPORT_SYMBOL
in metag_ksyms.c for symbols defined in mm/init.c into mm/init.c.

Signed-off-by: James Hogan <james.hogan@imgtec.com>
8 years agometag: move usercopy.c exports out of metag_ksyms.c
James Hogan [Wed, 13 Feb 2013 12:57:10 +0000 (12:57 +0000)]
metag: move usercopy.c exports out of metag_ksyms.c

It's less error prone to have function symbols exported immediately
after the function rather than in metag_ksyms.c. Move each EXPORT_SYMBOL
in metag_ksyms.c for symbols defined in usercopy.c into usercopy.c

Signed-off-by: James Hogan <james.hogan@imgtec.com>
8 years agometag: move setup.c exports out of metag_ksyms.c
James Hogan [Wed, 13 Feb 2013 12:55:51 +0000 (12:55 +0000)]
metag: move setup.c exports out of metag_ksyms.c

It's less error prone to have function symbols exported immediately
after the function rather than in metag_ksyms.c. Move each EXPORT_SYMBOL
in metag_ksyms.c for symbols defined in setup.c into setup.c

Signed-off-by: James Hogan <james.hogan@imgtec.com>
8 years agometag: move kick.c exports out of metag_ksyms.c
James Hogan [Wed, 13 Feb 2013 13:01:55 +0000 (13:01 +0000)]
metag: move kick.c exports out of metag_ksyms.c

It's less error prone to have function symbols exported immediately
after the function rather than in metag_ksyms.c. Move each EXPORT_SYMBOL
in metag_ksyms.c for symbols defined in kick.c into kick.c

Signed-off-by: James Hogan <james.hogan@imgtec.com>
8 years agometag: move traps.c exports out of metag_ksyms.c
James Hogan [Wed, 13 Feb 2013 12:19:03 +0000 (12:19 +0000)]
metag: move traps.c exports out of metag_ksyms.c

It's less error prone to have function symbols exported immediately
after the function rather than in metag_ksyms.c. Move each EXPORT_SYMBOL
in metag_ksyms.c for symbols defined in traps.c into traps.c

Signed-off-by: James Hogan <james.hogan@imgtec.com>
8 years agometag: move irq enable out of irqflags.h on SMP
James Hogan [Tue, 12 Feb 2013 16:04:53 +0000 (16:04 +0000)]
metag: move irq enable out of irqflags.h on SMP

The SMP version of arch_local_irq_enable() uses preempt_disable(), but
<asm/irqflags.h> doesn't include <linux/preempt.h> causing the following
errors on SMP when pstore/ftrace is enabled (caught by buildbot smp
allyesconfig):

In file included from include/linux/irqflags.h:15,
                 from fs/pstore/ftrace.c:16:
arch/metag/include/asm/irqflags.h: In function 'arch_local_irq_enable':
arch/metag/include/asm/irqflags.h:84: error: implicit declaration of function 'preempt_disable'
arch/metag/include/asm/irqflags.h:86: error: implicit declaration of function 'preempt_enable_no_resched'

However <linux/preempt.h> cannot be easily included from
<asm/irqflags.h> as it can cause circular include dependencies in the
!SMP case, and potentially in the SMP case in the future. Therefore move
the SMP implementation of arch_local_irq_enable() into traps.c and use
an inline version of get_trigger_mask() which is also defined in traps.c
for SMP.

This adds an extra layer of function call / stack push when
preempt_disable needs to call other functions, however in the
non-preemptive SMP case it should be about as fast, as it was already
calling the get_trigger_mask() function which is now used inline.

Signed-off-by: James Hogan <james.hogan@imgtec.com>
8 years agogenksyms: fix metag symbol prefix on crc symbols
James Hogan [Mon, 11 Feb 2013 15:40:24 +0000 (15:40 +0000)]
genksyms: fix metag symbol prefix on crc symbols

Meta uses symbol prefixes, so add "metag" to the list of architectures
to set the mod_prefix to "_" for. This fixes __crc_* symbols to add the
extra underscore to match _CRC_SYMBOL macro in <linux/export.h> and so
that modpost finds them.

Signed-off-by: James Hogan <james.hogan@imgtec.com>
8 years agometag: hugetlb: convert to vm_unmapped_area()
James Hogan [Mon, 11 Feb 2013 17:28:10 +0000 (17:28 +0000)]
metag: hugetlb: convert to vm_unmapped_area()

Convert hugetlb_get_unmapped_area_new_pmd() to use vm_unmapped_area()
rather than searching the virtual address space itself. This fixes the
following errors in linux-next due to the specified members being
removed after other architectures have already been converted:

arch/metag/mm/hugetlbpage.c: In function 'hugetlb_get_unmapped_area_new_pmd':
arch/metag/mm/hugetlbpage.c:199: error: 'struct mm_struct' has no member named 'cached_hole_size'
arch/metag/mm/hugetlbpage.c:200: error: 'struct mm_struct' has no member named 'free_area_cache'
arch/metag/mm/hugetlbpage.c:215: error: 'struct mm_struct' has no member named 'cached_hole_size'

Signed-off-by: James Hogan <james.hogan@imgtec.com>
Acked-by: Michel Lespinasse <walken@google.com>
8 years agometag: export clear_page and copy_page
James Hogan [Mon, 11 Feb 2013 11:47:02 +0000 (11:47 +0000)]
metag: export clear_page and copy_page

Various file systems use clear_page() and copy_page(), so when they're
built as modules we get build errors like the following:

ERROR: "clear_page" [fs/ntfs/ntfs.ko] undefined!
ERROR: "copy_page" [fs/nilfs2/nilfs2.ko] undefined!

Therefore export these functions to modules from metag_ksyms.c to fix
the errors. This was hit by a randconfig build.

Signed-off-by: James Hogan <james.hogan@imgtec.com>
8 years agometag: export metag_code_cache_flush_all
James Hogan [Mon, 11 Feb 2013 11:43:20 +0000 (11:43 +0000)]
metag: export metag_code_cache_flush_all

Various file systems indirectly use metag_code_cache_flush_all(), so
when they're built as modules we get build errors like the following:

ERROR: "metag_code_cache_flush_all" [fs/xfs/xfs.ko] undefined!

Therefore export this function to modules to fix the errors. This was
hit by a randconfig build.

Signed-off-by: James Hogan <james.hogan@imgtec.com>
8 years agometag: protect more non-MMU memory regions
James Hogan [Thu, 31 Jan 2013 13:42:03 +0000 (13:42 +0000)]
metag: protect more non-MMU memory regions

Rename setup_txprivext() to setup_priv() and add initialisation of some
more per-thread privilege protection registers:

 - TxPRIVSYSR: 0x04400000-0x047fffff
               0x05000000-0x07ffffff
               0x84000000-0x87ffffff
 - TxPIOREG:   0x02000000-0x02ffffff
               0x04800000-0x048fffff
 - TxSYREG:    0x04000000-0x04000fff (except write fetch system event)

Signed-off-by: James Hogan <james.hogan@imgtec.com>
8 years agometag: make TXPRIVEXT bits explicit
James Hogan [Thu, 31 Jan 2013 13:27:35 +0000 (13:27 +0000)]
metag: make TXPRIVEXT bits explicit

Define PRIV_BITS using explicit constants from <asm/metag_regs.h> rather
than with a hard coded value. This also adds a couple of missing
definitions for the TXPRIVEXT priv bits for protecting writes to TXTIMER
and the trace registers.

Signed-off-by: James Hogan <james.hogan@imgtec.com>
8 years agometag: kernel/setup.c: sort includes
James Hogan [Thu, 31 Jan 2013 13:38:48 +0000 (13:38 +0000)]
metag: kernel/setup.c: sort includes

Sort includes in kernel/setup.c.

Signed-off-by: James Hogan <james.hogan@imgtec.com>
8 years agoperf: Enable building perf tools for Meta
James Hogan [Thu, 31 Jan 2013 12:22:37 +0000 (12:22 +0000)]
perf: Enable building perf tools for Meta

Define rmb(), cpu_relax(), and CPUINFO_PROC for Meta so that the perf
tools can be built for Meta.

Signed-off-by: James Hogan <james.hogan@imgtec.com>
Cc: Peter Zijlstra <a.p.zijlstra@chello.nl>
Cc: Paul Mackerras <paulus@samba.org>
Cc: Ingo Molnar <mingo@redhat.com>
Cc: Arnaldo Carvalho de Melo <acme@ghostprotocols.net>
8 years agometag: add boot time LNKGET/LNKSET check
James Hogan [Thu, 31 Jan 2013 11:06:03 +0000 (11:06 +0000)]
metag: add boot time LNKGET/LNKSET check

Add boot time check for whether LNKGET/LNKSET go through or around the
cache. Depending on the configuration an info message (no harm), warning
(technically wrong but no harm), or big WARN (expect failure in either
kernel or userland) may be emitted if the behaviour is not as expected:

Configuration                                Hardware   Response
------------------------------------------   --------   --------
AROUND_CACHE                                 through    pr_info
!AROUND_CACHE && ATOMICITY_LNKGET            around     WARN (kernel)
     "        && !ATOMICITY_LNKGET && SMP    around     WARN (user)
     "                   "         && !SMP   around     pr_warn

Signed-off-by: James Hogan <james.hogan@imgtec.com>
8 years agometag: add __init to metag_cache_probe()
James Hogan [Thu, 31 Jan 2013 11:04:49 +0000 (11:04 +0000)]
metag: add __init to metag_cache_probe()

metag_cache_probe() is only called from setup_arch(), so add the __init
attribute to it.

Signed-off-by: James Hogan <james.hogan@imgtec.com>
8 years agometag: Add JTAG Debug Adapter (DA) support
James Hogan [Fri, 21 Sep 2012 16:38:15 +0000 (17:38 +0100)]
metag: Add JTAG Debug Adapter (DA) support

Add basic JTAG Debug Adapter (DA) support so that drivers which
communicate with the DA can detect whether one is actually present
(otherwise the target will halt indefinitely).

This allows the metag_da TTY driver and imgdafs filesystem driver to be
built, updates defconfigs, and sets up the metag_da console early if
it's configured in.

Signed-off-by: James Hogan <james.hogan@imgtec.com>
8 years agoscripts/checkstack.pl: Add metag support
James Hogan [Wed, 17 Oct 2012 14:21:13 +0000 (15:21 +0100)]
scripts/checkstack.pl: Add metag support

Adapt checkstack.pl so that it works for metag.

Signed-off-by: James Hogan <james.hogan@imgtec.com>
8 years agometag: ftrace support
James Hogan [Fri, 5 Oct 2012 15:27:31 +0000 (16:27 +0100)]
metag: ftrace support

Add ftrace support for metag.

Signed-off-by: James Hogan <james.hogan@imgtec.com>
Cc: Frederic Weisbecker <fweisbec@gmail.com>
Cc: Ingo Molnar <mingo@redhat.com>
Reviewed-by: Steven Rostedt <rostedt@goodmis.org>
8 years agometag: Perf
James Hogan [Fri, 5 Oct 2012 15:54:55 +0000 (16:54 +0100)]
metag: Perf

Add Perf support for metag.

Signed-off-by: James Hogan <james.hogan@imgtec.com>
Cc: Peter Zijlstra <a.p.zijlstra@chello.nl>
Cc: Paul Mackerras <paulus@samba.org>
Cc: Ingo Molnar <mingo@redhat.com>
Cc: Arnaldo Carvalho de Melo <acme@ghostprotocols.net>
8 years agometag: Build infrastructure
James Hogan [Tue, 9 Oct 2012 09:54:32 +0000 (10:54 +0100)]
metag: Build infrastructure

Add metag build infrastructure.

Signed-off-by: James Hogan <james.hogan@imgtec.com>
8 years agoKconfig.debug: add METAG to dependency lists
James Hogan [Wed, 5 Dec 2012 11:34:13 +0000 (11:34 +0000)]
Kconfig.debug: add METAG to dependency lists

Add [!]METAG to a couple of Kconfig dependencies in lib/Kconfig.debug.
Don't allow stack utilization instrumentation on metag, and allow
building with frame pointers.

Signed-off-by: James Hogan <james.hogan@imgtec.com>
Cc: Andrew Morton <akpm@linux-foundation.org>
Cc: "Paul E. McKenney" <paul.mckenney@linaro.org>
Cc: Akinobu Mita <akinobu.mita@gmail.com>
Cc: Michel Lespinasse <walken@google.com>
Cc: Catalin Marinas <catalin.marinas@arm.com>
8 years agomm: define VM_GROWSUP for CONFIG_METAG
James Hogan [Tue, 16 Oct 2012 09:16:14 +0000 (10:16 +0100)]
mm: define VM_GROWSUP for CONFIG_METAG

Commit cc2383ec06be093789469852e1fe96e1148e9a2c ("mm: introduce
arch-specific vma flag VM_ARCH_1") merged in v3.7-rc1.

The above commit combined several arch-specific vma flags into one, and
in the process it changed the VM_GROWSUP definition to depend on
specific architectures rather than CONFIG_STACK_GROWSUP. Therefore add
an ifdef for CONFIG_METAG to also set VM_GROWSUP.

Signed-off-by: James Hogan <james.hogan@imgtec.com>
Cc: Konstantin Khlebnikov <khlebnikov@openvz.org>
Cc: Andrew Morton <akpm@linux-foundation.org>
Cc: Mel Gorman <mgorman@suse.de>
Cc: Michel Lespinasse <walken@google.com>
Cc: Al Viro <viro@zeniv.linux.org.uk>
Cc: linux-mm@kvack.org
8 years agometag: Various other headers
James Hogan [Fri, 5 Oct 2012 15:22:14 +0000 (16:22 +0100)]
metag: Various other headers

Add the remaining metag header files:
 - byteorder.h, swab.h (byte order and swapping)
 - barrier.h, cpu.h. hwthread.h, processor.h (hardware thread related)
 - bug.h, elf.h, gpio.h, linkage.h, resource.h (other)

Signed-off-by: James Hogan <james.hogan@imgtec.com>
8 years agometag: Stack unwinding
James Hogan [Fri, 5 Oct 2012 16:01:38 +0000 (17:01 +0100)]
metag: Stack unwinding

Add stack unwinding support for metag.

Signed-off-by: James Hogan <james.hogan@imgtec.com>
8 years agometag: Optimised library functions
James Hogan [Fri, 5 Oct 2012 16:02:09 +0000 (17:02 +0100)]
metag: Optimised library functions

Add optimised library functions for metag.

Signed-off-by: James Hogan <james.hogan@imgtec.com>
8 years agometag: DMA
James Hogan [Fri, 5 Oct 2012 15:27:03 +0000 (16:27 +0100)]
metag: DMA

Add DMA mapping code.

Signed-off-by: James Hogan <james.hogan@imgtec.com>
8 years agometag: SMP support
James Hogan [Fri, 5 Oct 2012 15:56:56 +0000 (16:56 +0100)]
metag: SMP support

Add SMP support for metag. This allows Linux to take control of multiple
hardware threads on a single Meta core, treating them as separate Linux
CPUs.

Signed-off-by: James Hogan <james.hogan@imgtec.com>
8 years agometag: Basic documentation
James Hogan [Tue, 9 Oct 2012 10:00:27 +0000 (11:00 +0100)]
metag: Basic documentation

Add basic metag documentation. This includes an outline description of
the ABIs (including syscall ABI) and calling conventions, similar to the
one in Documentation/frv/.

Signed-off-by: James Hogan <james.hogan@imgtec.com>
Cc: Rob Landley <rob@landley.net>
Cc: Al Viro <viro@ZenIV.linux.org.uk>
Cc: linux-doc@vger.kernel.org
8 years agometag: Atomics, locks and bitops
James Hogan [Tue, 9 Oct 2012 10:00:24 +0000 (11:00 +0100)]
metag: Atomics, locks and bitops

Add header files to implement Meta hardware thread locks (used by some
other atomic operations), atomics, spinlocks, and bitops.

There are 2 main types of atomic primitives for metag (in addition to
IRQs off on UP):
 - LOCK instructions provide locking between hardware threads.
 - LNKGET/LNKSET instructions provide load-linked/store-conditional
   operations allowing for lighter weight atomics on Meta2

LOCK instructions allow for hardware threads to acquire voluntary or
exclusive hardware thread locks:
 - LOCK0 releases exclusive and voluntary lock from the running hardware
   thread.
 - LOCK1 acquires the voluntary hardware lock, blocking until it becomes
   available.
 - LOCK2 implies LOCK1, and additionally acquires the exclusive hardware
   lock, blocking all other hardware threads from executing.

Signed-off-by: James Hogan <james.hogan@imgtec.com>
8 years agometag: Module support
James Hogan [Tue, 9 Oct 2012 09:55:00 +0000 (10:55 +0100)]
metag: Module support

Signed-off-by: James Hogan <james.hogan@imgtec.com>
8 years agometag: Scheduling/Process management
James Hogan [Tue, 9 Oct 2012 09:54:54 +0000 (10:54 +0100)]
metag: Scheduling/Process management

Signed-off-by: James Hogan <james.hogan@imgtec.com>
8 years agometag: System Calls
James Hogan [Tue, 9 Oct 2012 09:54:51 +0000 (10:54 +0100)]
metag: System Calls

Add metag system call and gateway page interfaces. The metag
architecture port uses the generic system call numbers from
asm-generic/unistd.h, as well as a user gateway page mapped at
0x6ffff000 which contains fast atomic primitives (depending on SMP) and
a fast method of accessing TLS data.

System calls use the SWITCH instruction with the immediate 0x440001 to
signal a system call.

Signed-off-by: James Hogan <james.hogan@imgtec.com>
8 years agometag: Internal and external irqchips
James Hogan [Tue, 9 Oct 2012 09:54:47 +0000 (10:54 +0100)]
metag: Internal and external irqchips

Meta core internal interrupts (from HWSTATMETA and friends) are vectored
onto the TR1 core trigger for the current thread. This is demultiplexed
in irq-metag.c to individual Linux IRQs for each internal interrupt.

External SoC interrupts (from HWSTATEXT and friends) are vectored onto
the TR2 core trigger for the current thread. This is demultiplexed in
irq-metag-ext.c to individual Linux IRQs for each external SoC interrupt.
The external irqchip has devicetree bindings for configuring the number
of irq banks and the type of masking available.

Signed-off-by: James Hogan <james.hogan@imgtec.com>
Cc: Arnd Bergmann <arnd@arndb.de>
Cc: Grant Likely <grant.likely@secretlab.ca>
Cc: Rob Herring <rob.herring@calxeda.com>
Cc: Rob Landley <rob@landley.net>
Cc: Dom Cobley <popcornmix@gmail.com>
Cc: Simon Arlott <simon@fire.lp0.eu>
Cc: Viresh Kumar <viresh.kumar@linaro.org>
Cc: Maxime Ripard <maxime.ripard@free-electrons.com>
Cc: devicetree-discuss@lists.ozlabs.org
Cc: linux-doc@vger.kernel.org
8 years agometag: IRQ handling
James Hogan [Tue, 9 Oct 2012 09:54:47 +0000 (10:54 +0100)]
metag: IRQ handling

Add core IRQ handling for metag. The code in irq.c exposes the TBX
signal numbers as Linux IRQs.

Signed-off-by: James Hogan <james.hogan@imgtec.com>
8 years agometag: Traps
James Hogan [Tue, 9 Oct 2012 09:54:43 +0000 (10:54 +0100)]
metag: Traps

Add trap code for metag. At the lowest level Meta traps (and return from
interrupt instruction - RTI) simply swap the PC and PCX registers and
optionally toggle the interrupt status bit (ISTAT). Low level TBX code
in tbipcx.S handles the core context save, determine the TBX signal
number based on the core trigger that fired (using the TXSTATI status
register), and call TBX signal handlers (mostly in traps.c) via a vector
table.

Signed-off-by: James Hogan <james.hogan@imgtec.com>
Cc: Al Viro <viro@zeniv.linux.org.uk>
8 years agometag: Time keeping
James Hogan [Tue, 9 Oct 2012 09:54:39 +0000 (10:54 +0100)]
metag: Time keeping

Add time keeping code for metag. Meta hardware threads have 2 timers.
The background timer (TXTIMER) is used as a free-running time base, and
the interrupt timer (TXTIMERI) is used for the timer interrupt. Both
counters traditionally count at approximately 1MHz.

Signed-off-by: James Hogan <james.hogan@imgtec.com>
Cc: John Stultz <johnstul@us.ibm.com>
Cc: Thomas Gleixner <tglx@linutronix.de>