gator: Move README to top directory
[android-sdk/arm-ds5-gator.git] / README_Streamline.txt
2 *** Purpose ***
4 Instructions on setting up ARM Streamline on the target.
5 The gator driver and gator daemon are required to run on the ARM linux target in order for ARM Streamline to operate.
6 The driver should be built as a module and the daemon must run with root permissions on the target.
8 *** Introduction ***
10 A linux development environment with cross compiling tools is most likely required, depending on what is already created and provided.
11 -For users, the ideal environment is to be given a BSP with gatord and gator.ko already running on a properly configured kernel. In such a scenario, a development environment is not needed, root permission may or may not be needed (gatord must be executed with root permissions but can be automatically started, see below), and the user can run Streamline and profile the system without any setup.
12 -The ideal development environment has the kernel source code available to be rebuilt and executed on the target. This environment allows the greatest flexibility in configuring the kernel and building the gator driver module.
13 -However, it is possible that a user/developer has a kernel but does not have the source code. In this scenario it may or may not be possible to obtain a valid profile.
14         -First, check if the kernel has the proper configuration options (see below). Profiling cannot occur using a kernel that is not configured properly, a new kernel must be created.
15         -Second, given a properly configured kernel, check if the filesystem contains the kernel source/headers, which can be used to re-create the gator driver.
16         -If the kernel is not properly configured or sources/headers are not available, the developer is on their own and kernel creation is beyond the scope of this document. Note: It is possible for a module to work when compiled against a similar kernel source code, though this is not guaranteed to work due to differences in kernel structures, exported symbols and incompatible configuration parameters.
18 *** Preparing and building the kernel ***
20 cd into the root source dir of the linux kernel
21 if your target has never been configured, choose the appropriate configuration for your target
22         make ARCH=arm CROSS_COMPILE=${CROSS_TOOLS}/bin/arm-none-linux-gnueabi- <platform_defconfig>
23 make ARCH=arm CROSS_COMPILE=${CROSS_TOOLS}/bin/arm-none-linux-gnueabi- menuconfig
25 Required Kernel Changes (depending on the kernel version, the location of these configuration settings within menuconfig may be different)
26 - General Setup
27   - [*] Profiling Support
28 - Kernel hacking
29   - [*] Tracers
30     - [*] Trace process context switches and events
31 - Kernel Features
32   - [*] High Resolution Timer Support
33   - [*] Use local timer interrupts (only required for SMP)
35 The "context switches and events" option will not be available if other trace configurations are enabled. Other trace configurations being enabled is sufficient to turn on context switches and events.
37 Optional Kernel Changes (depending on the kernel version, the location of these configuration settings within menuconfig may be different)
38 Note: Configurations may not be supported on all targets
39 - System Type
40   - [*] <SoC name> debugging peripherals (enable core performance counters on supported SoCs)  /* kernels before 2.6.35 */
42 make -j5 ARCH=arm CROSS_COMPILE=${CROSS_TOOLS}/bin/arm-none-linux-gnueabi- uImage
44 *** Checking the gator requirements ***
46 (optional) Use the hrtimer_module utility to validate the kernel High Resolution Timer requirement.
48 *** Building the gator module ***
50 To create the gator.ko module,
51         cd /path/to/gator/driver-src
52         tar xzf gator-driver.tar.gz
53         cd gator-driver
54         make -C <kernel_build_dir> M=`pwd` ARCH=arm CROSS_COMPILE=<...> modules
55 for example
56         make -C /home/username/kernel_2.6.32/ M=`pwd` ARCH=arm CROSS_COMPILE=/home/username/CodeSourcery/Sourcery_G++_Lite/bin/arm-none-linux-gnueabi- modules
57 If successful, a gator.ko module should be generated
59 *** Building the gator daemon ***
61 cd /path/to/gator/daemon-src
62 tar -xzf gator-daemon.tar.gz
63 For Linux,
64         build with 'make'
65 For Android,
66         mv gator-daemon jni
67         install the android ndk, see developer.android.com
68         /path/to/ndk/ndk-build
69         gatord should now be created and located in libs/armeabi
71 *** Running gator ***
73 Load the kernel onto the target and copy gatord and gator.ko into the target's filesystem.
74 Ensure gatord has execute permissions
75         chmod +x gatord
76 gator.ko must be located in the same directory as gatord on the target.
77 With root privileges, run the daemon
78         sudo ./gatord &
80 *** Compiling an application or shared library ***
82 Recommended compiler settings:
83         "-g": Debug symbols needed for best analysis results.
84         "-fno-inline": Speed improvement when processing the image files and most accurate analysis results.
85         "-fno-omit-frame-pointer": ARM EABI frame pointers (Code Sourcery cross compiler) allow the call stack to be recorded with each sample taken when in ARM state (i.e. not -mthumb).
87 *** Profiling the kernel (optional) ***
89 make ARCH=arm CROSS_COMPILE=$(CROSS_TOOLS}/bin/arm-none-linux-gnueabi- menuconfig
90 - Kernel Hacking
91   - [*] Compile the kernel with debug info
93 make -j5 ARCH=arm CROSS_COMPILE=${CROSS_TOOLS}/bin/arm-none-linux-gnueabi- uImage
94 Use vmlinux as the image for debug symbols in Streamline.
95 Drivers may be profiled using this method by statically linking the driver into the kernel image or adding the module as an image.
96 To perform kernel stack unwinding and module unwinding, edit the Makefile to enable GATOR_KERNEL_STACK_UNWINDING and rebuild gator.ko.
98 *** Automatically start gator on boot (optional) ***
100 cd /etc/init.d
101 vi rungator.sh
102         #!/bin/bash
103         /path/to/gatord &
104 update-rc.d rungator.sh defaults
106 *** GPL License ***
108 For license information, please see the file LICENSE after unzipping driver-src/gator-driver.tar.gz.