1 /**
2 * Copyright (C) ARM Limited 2010-2012. All rights reserved.
3 *
4 * This program is free software; you can redistribute it and/or modify
5 * it under the terms of the GNU General Public License version 2 as
6 * published by the Free Software Foundation.
7 */
9 #include <stdlib.h>
10 #include <string.h>
11 #include <signal.h>
12 #include <sys/syscall.h>
13 #include <sys/resource.h>
14 #include <unistd.h>
15 #include <sys/prctl.h>
16 #include "Logging.h"
17 #include "CapturedXML.h"
18 #include "SessionData.h"
19 #include "Child.h"
20 #include "LocalCapture.h"
21 #include "Collector.h"
22 #include "Sender.h"
23 #include "OlyUtility.h"
24 #include "StreamlineSetup.h"
25 #include "ConfigurationXML.h"
27 static sem_t haltPipeline, senderThreadStarted, startProfile; // Shared by Child and spawned threads
28 static Fifo* collectorFifo = NULL; // Shared by Child.cpp and spawned threads
29 static Sender* sender = NULL; // Shared by Child.cpp and spawned threads
30 Collector* collector = NULL;
31 Child* child = NULL; // shared by Child.cpp and main.cpp
33 extern void cleanUp();
34 void handleException() {
35 if (child && child->numExceptions++ > 0) {
36 // it is possible one of the below functions itself can cause an exception, thus allow only one exception
37 logg->logMessage("Received multiple exceptions, terminating the child");
38 exit(1);
39 }
40 fprintf(stderr, "%s", logg->getLastError());
42 if (child && child->socket) {
43 if (sender) {
44 // send the error, regardless of the command sent by Streamline
45 sender->writeData(logg->getLastError(), strlen(logg->getLastError()), RESPONSE_ERROR);
47 // cannot close the socket before Streamline issues the command, so wait for the command before exiting
48 if (gSessionData->mWaitingOnCommand) {
49 char discard;
50 child->socket->receiveNBytes(&discard, 1);
51 }
53 // this indirectly calls close socket which will ensure the data has been sent
54 delete sender;
55 }
56 }
58 if (gSessionData->mLocalCapture)
59 cleanUp();
61 exit(1);
62 }
64 // CTRL C Signal Handler for child process
65 void child_handler(int signum) {
66 static bool beenHere = false;
67 if (beenHere == true) {
68 logg->logMessage("Gator is being forced to shut down.");
69 exit(1);
70 }
71 beenHere = true;
72 logg->logMessage("Gator is shutting down.");
73 if (signum == SIGALRM || !collector) {
74 exit(1);
75 } else {
76 child->endSession();
77 alarm(5); // Safety net in case endSession does not complete within 5 seconds
78 }
79 }
81 void* durationThread(void* pVoid) {
82 prctl(PR_SET_NAME, (unsigned int)&"gatord-duration", 0, 0, 0);
83 sem_wait(&startProfile);
84 if (gSessionData->mSessionIsActive) {
85 // Time out after duration seconds
86 // Add a second for host-side filtering
87 sleep(gSessionData->mDuration + 1);
88 if (gSessionData->mSessionIsActive) {
89 logg->logMessage("Duration expired.");
90 child->endSession();
91 }
92 }
93 logg->logMessage("Exit duration thread");
94 return 0;
95 }
97 void* stopThread(void* pVoid) {
98 int length;
99 char type;
100 OlySocket* socket = child->socket;
102 prctl(PR_SET_NAME, (unsigned int)&"gatord-stopper", 0, 0, 0);
103 while (gSessionData->mSessionIsActive) {
104 // This thread will stall until the APC_STOP or PING command is received over the socket or the socket is disconnected
105 if (socket->receiveNBytes(&type, sizeof(type)) > 0) {
106 if ((type != COMMAND_APC_STOP) && (type != COMMAND_PING)) {
107 logg->logMessage("INVESTIGATE: Received unknown command type %d", type);
108 } else {
109 // verify a length of zero
110 if (socket->receiveNBytes((char*)&length, sizeof(length)) < 0) {
111 break;
112 }
114 if (length == 0) {
115 if (type == COMMAND_APC_STOP) {
116 logg->logMessage("Stop command received.");
117 child->endSession();
118 } else {
119 // Ping is used to make sure gator is alive and requires an ACK as the response
120 logg->logMessage("Ping command received.");
121 sender->writeData(NULL, 0, RESPONSE_ACK);
122 }
123 } else {
124 logg->logMessage("INVESTIGATE: Received stop command but with length = %d", length);
125 }
126 }
127 }
128 }
130 logg->logMessage("Exit stop thread");
131 return 0;
132 }
134 void* senderThread(void* pVoid) {
135 int length;
136 char* data;
138 sem_post(&senderThreadStarted);
139 prctl(PR_SET_NAME, (unsigned int)&"gatord-sender", 0, 0, 0);
140 sem_wait(&haltPipeline);
142 do {
143 data = collectorFifo->read(&length);
144 sender->writeData(data, length, RESPONSE_APC_DATA);
145 } while (length > 0);
146 logg->logMessage("Exit sender thread");
147 return 0;
148 }
150 Child::Child(char* path) {
151 initialization();
152 sessionXMLPath = path;
153 gSessionData->mLocalCapture = true;
154 }
156 Child::Child(OlySocket* sock, int conn) {
157 initialization();
158 socket = sock;
159 numConnections = conn;
160 }
162 Child::~Child() {
163 }
165 void Child::initialization() {
166 // Set up different handlers for signals
167 gSessionData->mSessionIsActive = true;
168 signal(SIGINT, child_handler);
169 signal(SIGTERM, child_handler);
170 signal(SIGABRT, child_handler);
171 signal(SIGALRM, child_handler);
172 socket = NULL;
173 numExceptions = 0;
174 numConnections = 0;
175 sessionXMLPath = 0;
177 // Initialize semaphores
178 sem_init(&senderThreadStarted, 0, 0);
179 sem_init(&startProfile, 0, 0);
180 }
182 void Child::endSession() {
183 gSessionData->mSessionIsActive = false;
184 collector->stop();
185 sem_post(&haltPipeline);
186 }
188 void Child::run() {
189 char* collectBuffer;
190 int bytesCollected = 0;
191 LocalCapture* localCapture = NULL;
193 prctl(PR_SET_NAME, (unsigned int)&"gatord-child", 0, 0, 0);
195 // Instantiate the Sender - must be done first, after which error messages can be sent
196 sender = new Sender(socket);
198 if (numConnections > 1) {
199 logg->logError(__FILE__, __LINE__, "Session already in progress");
200 handleException();
201 }
203 // Populate gSessionData with the configuration
204 new ConfigurationXML();
206 // Set up the driver; must be done after gSessionData->mPerfCounterType[] is populated
207 collector = new Collector();
209 // Start up and parse session xml
210 if (socket) {
211 // Respond to Streamline requests
212 StreamlineSetup ss(socket);
213 } else {
214 xmlString = util->readFromDisk(sessionXMLPath);
215 if (xmlString == 0) {
216 logg->logError(__FILE__, __LINE__, "Unable to read session xml file: %s", sessionXMLPath);
217 handleException();
218 }
219 gSessionData->parseSessionXML(xmlString);
220 localCapture = new LocalCapture();
221 localCapture->createAPCDirectory(gSessionData->target_path, gSessionData->title);
222 localCapture->copyImages(gSessionData->images);
223 localCapture->write(xmlString);
224 sender->createDataFile(gSessionData->apcDir);
225 delete xmlString;
226 }
228 // Write configuration into the driver
229 collector->enablePerfCounters();
231 // Create user-space buffers
232 int fifoBufferSize = collector->getBufferSize();
233 int numCollectorBuffers = (gSessionData->mTotalBufferSize * 1024 * 1024 + fifoBufferSize - 1) / fifoBufferSize;
234 numCollectorBuffers = (numCollectorBuffers < 4) ? 4 : numCollectorBuffers;
235 logg->logMessage("Created %d %d-byte collector buffers", numCollectorBuffers, fifoBufferSize);
236 collectorFifo = new Fifo(numCollectorBuffers, fifoBufferSize);
238 // Get the initial pointer to the collect buffer
239 collectBuffer = collectorFifo->start();
241 // Sender thread shall be halted until it is signaled for one shot mode
242 sem_init(&haltPipeline, 0, gSessionData->mOneShot ? 0 : 2);
244 // Create the duration, stop, and sender threads
245 bool thread_creation_success = true;
246 if (gSessionData->mDuration > 0 && pthread_create(&durationThreadID, NULL, durationThread, NULL))
247 thread_creation_success = false;
248 else if (socket && pthread_create(&stopThreadID, NULL, stopThread, NULL))
249 thread_creation_success = false;
250 else if (pthread_create(&senderThreadID, NULL, senderThread, NULL))
251 thread_creation_success = false;
252 if (!thread_creation_success) {
253 logg->logError(__FILE__, __LINE__, "Failed to create gator threads");
254 handleException();
255 }
257 // Wait until thread has started
258 sem_wait(&senderThreadStarted);
260 // Start profiling
261 logg->logMessage("********** Profiling started **********");
262 collector->start();
263 sem_post(&startProfile);
265 // Collect Data
266 do {
267 // This command will stall until data is received from the driver
268 bytesCollected = collector->collect(collectBuffer);
270 // In one shot mode, stop collection once all the buffers are filled
271 if (gSessionData->mOneShot && gSessionData->mSessionIsActive) {
272 // Depth minus 1 because write() has not yet been called
273 if ((bytesCollected == -1) || (collectorFifo->numWriteToReadBuffersFilled() == collectorFifo->depth() - 1)) {
274 logg->logMessage("One shot");
275 endSession();
276 }
277 }
278 collectBuffer = collectorFifo->write(bytesCollected);
279 } while (bytesCollected > 0);
280 logg->logMessage("Exit collect data loop");
282 // Wait for the other threads to exit
283 pthread_join(senderThreadID, NULL);
285 // Shutting down the connection should break the stop thread which is stalling on the socket recv() function
286 if (socket) {
287 logg->logMessage("Waiting on stop thread");
288 socket->shutdownConnection();
289 pthread_join(stopThreadID, NULL);
290 }
292 // Write the captured xml file
293 if (gSessionData->mLocalCapture) {
294 CapturedXML capturedXML;
295 capturedXML.write(gSessionData->apcDir);
296 }
298 logg->logMessage("Profiling ended.");
300 delete collectorFifo;
301 delete sender;
302 delete collector;
303 delete localCapture;
304 }