]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/arm-ds5-gator.git/blob - daemon/ConfigurationXML.cpp
gator-driver: Fix building on Linux 3.12
[android-sdk/arm-ds5-gator.git] / daemon / ConfigurationXML.cpp
1 /**
2  * Copyright (C) ARM Limited 2010-2013. All rights reserved.
3  *
4  * This program is free software; you can redistribute it and/or modify
5  * it under the terms of the GNU General Public License version 2 as
6  * published by the Free Software Foundation.
7  */
9 #include <string.h>
10 #include <stdlib.h>
11 #include <dirent.h>
12 #include "ConfigurationXML.h"
13 #include "Driver.h"
14 #include "Logging.h"
15 #include "OlyUtility.h"
16 #include "SessionData.h"
18 static const char* ATTR_COUNTER            = "counter";
19 static const char* ATTR_REVISION           = "revision";
20 static const char* ATTR_EVENT              = "event";
21 static const char* ATTR_COUNT              = "count";
23 ConfigurationXML::ConfigurationXML() {
24         const char * configuration_xml;
25         unsigned int configuration_xml_len;
26         getDefaultConfigurationXml(configuration_xml, configuration_xml_len);
27         
28         char path[PATH_MAX];
30         getPath(path);
31         mConfigurationXML = util->readFromDisk(path);
33         for (int retryCount = 0; retryCount < 2; ++retryCount) {
34                 if (mConfigurationXML == NULL) {
35                         logg->logMessage("Unable to locate configuration.xml, using default in binary");
36                         // null-terminate configuration_xml
37                         mConfigurationXML = (char*)malloc(configuration_xml_len + 1);
38                         memcpy(mConfigurationXML, (const void*)configuration_xml, configuration_xml_len);
39                         mConfigurationXML[configuration_xml_len] = 0;
40                 }
42                 int ret = parse(mConfigurationXML);
43                 if (ret == 1) {
44                         remove();
46                         // Free the current configuration and reload
47                         free((void*)mConfigurationXML);
48                         mConfigurationXML = NULL;
49                         continue;
50                 }
52                 break;
53         }
54         
55         validate();
56 }
58 ConfigurationXML::~ConfigurationXML() {
59         if (mConfigurationXML) {
60                 free((void*)mConfigurationXML);
61         }
62 }
64 int ConfigurationXML::parse(const char* configurationXML) {
65         mxml_node_t *tree, *node;
66         int ret;
68         // clear counter overflow
69         gSessionData->mCounterOverflow = 0;
70         mIndex = 0;
72         // disable all counters prior to parsing the configuration xml
73         for (int i = 0; i < MAX_PERFORMANCE_COUNTERS; i++) {
74                 gSessionData->mCounters[i].setEnabled(false);
75         }
77         tree = mxmlLoadString(NULL, configurationXML, MXML_NO_CALLBACK);
79         node = mxmlGetFirstChild(tree);
80         while (node && mxmlGetType(node) != MXML_ELEMENT)
81                 node = mxmlWalkNext(node, tree, MXML_NO_DESCEND);
82         
83         ret = configurationsTag(node);
85         node = mxmlGetFirstChild(node);
86         while (node) {
87                 if (mxmlGetType(node) != MXML_ELEMENT) {
88                         node = mxmlWalkNext(node, tree, MXML_NO_DESCEND);
89                         continue;
90                 }
91                 configurationTag(node);
92                 node = mxmlWalkNext(node, tree, MXML_NO_DESCEND);
93         }
95         mxmlDelete(tree);
97         return ret;
98 }
100 void ConfigurationXML::validate(void) {
101         for (int i = 0; i < MAX_PERFORMANCE_COUNTERS; i++) {
102                 const Counter & counter = gSessionData->mCounters[i];
103                 if (counter.isEnabled()) {
104                         if (strcmp(counter.getType(), "") == 0) {
105                                 logg->logError(__FILE__, __LINE__, "Invalid required attribute in configuration.xml:\n  counter=\"%s\"\n  event=%d\n", counter.getType(), counter.getEvent());
106                                 handleException();
107                         }
109                         // iterate through the remaining enabled performance counters
110                         for (int j = i + 1; j < MAX_PERFORMANCE_COUNTERS; j++) {
111                                 const Counter & counter2 = gSessionData->mCounters[j];
112                                 if (counter2.isEnabled()) {
113                                         // check if the types are the same
114                                         if (strcmp(counter.getType(), counter2.getType()) == 0) {
115                                                 logg->logError(__FILE__, __LINE__, "Duplicate performance counter type in configuration.xml: %s", counter.getType());
116                                                 handleException();
117                                         }
118                                 }
119                         }
120                 }
121         }
124 #define CONFIGURATION_REVISION 3
125 int ConfigurationXML::configurationsTag(mxml_node_t *node) {
126         const char* revision_string;
127         
128         revision_string = mxmlElementGetAttr(node, ATTR_REVISION);
129         if (!revision_string) {
130                 return 1; //revision issue;
131         }
133         int revision = strtol(revision_string, NULL, 10);
134         if (revision < CONFIGURATION_REVISION) {
135                 return 1; // revision issue
136         }
138         // A revision >= CONFIGURATION_REVISION is okay
139         // Greater than can occur when Streamline is newer than gator
141         return 0;
144 void ConfigurationXML::configurationTag(mxml_node_t *node) {
145         // handle all other performance counters
146         if (mIndex >= MAX_PERFORMANCE_COUNTERS) {
147                 mIndex++;
148                 gSessionData->mCounterOverflow = mIndex;
149                 return;
150         }
152         // read attributes
153         Counter & counter = gSessionData->mCounters[mIndex];
154         counter.clear();
155         if (mxmlElementGetAttr(node, ATTR_COUNTER)) counter.setType(mxmlElementGetAttr(node, ATTR_COUNTER));
156         if (mxmlElementGetAttr(node, ATTR_EVENT)) counter.setEvent(strtol(mxmlElementGetAttr(node, ATTR_EVENT), NULL, 16));
157         if (mxmlElementGetAttr(node, ATTR_COUNT)) counter.setCount(strtol(mxmlElementGetAttr(node, ATTR_COUNT), NULL, 10));
158         counter.setEnabled(true);
160         // Associate a driver with each counter
161         for (Driver *driver = Driver::getHead(); driver != NULL; driver = driver->getNext()) {
162                 if (driver->claimCounter(counter)) {
163                         if (counter.getDriver() != NULL) {
164                                 logg->logError(__FILE__, __LINE__, "More than one driver has claimed %s:%i", counter.getType(), counter.getEvent());
165                                 handleException();
166                         }
167                         counter.setDriver(driver);
168                 }
169         }
171         // If no driver is associated with the counter, disable it
172         if (counter.getDriver() == NULL) {
173                 logg->logMessage("No driver has claimed %s:%i", counter.getType(), counter.getEvent());
174                 counter.setEnabled(false);
175         }
177         if (counter.isEnabled()) {
178                 // update counter index
179                 mIndex++;
180         }
183 void ConfigurationXML::getDefaultConfigurationXml(const char * & xml, unsigned int & len) {
184 #include "configuration_xml.h" // defines and initializes char configuration_xml[] and int configuration_xml_len
185         xml = (const char *)configuration_xml;
186         len = configuration_xml_len;
189 void ConfigurationXML::getPath(char* path) {
190         if (gSessionData->mConfigurationXMLPath) {
191                 strncpy(path, gSessionData->mConfigurationXMLPath, PATH_MAX);
192         } else {
193                 if (util->getApplicationFullPath(path, PATH_MAX) != 0) {
194                         logg->logMessage("Unable to determine the full path of gatord, the cwd will be used");
195                 }
196                 strncat(path, "configuration.xml", PATH_MAX - strlen(path) - 1);
197         }
200 void ConfigurationXML::remove() {
201         char path[PATH_MAX];
202         getPath(path);
204         if (::remove(path) != 0) {
205                 logg->logError(__FILE__, __LINE__, "Invalid configuration.xml file detected and unable to delete it. To resolve, delete configuration.xml on disk");
206                 handleException();
207         }
208         logg->logMessage("Invalid configuration.xml file detected and removed");