]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/arm-ds5-gator.git/blob - daemon/LocalCapture.cpp
gator-driver: Handle task struct correctly
[android-sdk/arm-ds5-gator.git] / daemon / LocalCapture.cpp
1 /**
2  * Copyright (C) ARM Limited 2010-2013. All rights reserved.
3  *
4  * This program is free software; you can redistribute it and/or modify
5  * it under the terms of the GNU General Public License version 2 as
6  * published by the Free Software Foundation.
7  */
9 #include <sys/stat.h>
10 #include <sys/types.h>
11 #include <dirent.h>
12 #include <string.h>
13 #include <stdlib.h>
14 #include <unistd.h>
15 #include "LocalCapture.h"
16 #include "SessionData.h"
17 #include "Logging.h"
18 #include "OlyUtility.h"
19 #include "EventsXML.h"
21 LocalCapture::LocalCapture() {}
23 LocalCapture::~LocalCapture() {}
25 void LocalCapture::createAPCDirectory(char* target_path) {
26         gSessionData->mAPCDir = createUniqueDirectory(target_path, ".apc");
27         if ((removeDirAndAllContents(gSessionData->mAPCDir) != 0 || mkdir(gSessionData->mAPCDir, S_IRWXU | S_IRWXG | S_IROTH | S_IXOTH) != 0)) {
28                 logg->logError(__FILE__, __LINE__, "Unable to create directory %s", gSessionData->mAPCDir);
29                 handleException();
30         }
31 }
33 void LocalCapture::write(char* string) {
34         char file[PATH_MAX];
36         // Set full path
37         snprintf(file, PATH_MAX, "%s/session.xml", gSessionData->mAPCDir);
39         // Write the file
40         if (util->writeToDisk(file, string) < 0) {
41                 logg->logError(__FILE__, __LINE__, "Error writing %s\nPlease verify the path.", file);
42                 handleException();
43         }
45         // Write events XML
46         EventsXML eventsXML;
47         eventsXML.write(gSessionData->mAPCDir);
48 }
50 char* LocalCapture::createUniqueDirectory(const char* initialPath, const char* ending) {
51         char* output;
52         char path[PATH_MAX];
54         // Ensure the path is an absolute path, i.e. starts with a slash
55         if (initialPath == 0 || strlen(initialPath) == 0) {
56                 logg->logError(__FILE__, __LINE__, "Missing -o command line option required for a local capture.");
57                 handleException();
58         } else if (initialPath[0] != '/') {
59                 if (getcwd(path, PATH_MAX) == 0) {
60                         logg->logMessage("Unable to retrieve the current working directory");
61                 }
62                 strncat(path, "/", PATH_MAX - strlen(path) - 1);
63                 strncat(path, initialPath, PATH_MAX - strlen(path) - 1);
64         } else {
65                 strncpy(path, initialPath, PATH_MAX);
66                 path[PATH_MAX - 1] = 0; // strncpy does not guarantee a null-terminated string
67         }
69         // Add ending if it is not already there
70         if (strcmp(&path[strlen(path) - strlen(ending)], ending) != 0) {
71                 strncat(path, ending, PATH_MAX - strlen(path) - 1);
72         }
74         output = strdup(path);
76         return output;
77 }
79 int LocalCapture::removeDirAndAllContents(char* path) {
80         int error = 0;
81         struct stat mFileInfo;
82         // Does the path exist?
83         if (stat(path, &mFileInfo) == 0) {
84                 // Is it a directory?
85                 if (mFileInfo.st_mode & S_IFDIR) {
86                         DIR * dir = opendir(path);
87                         dirent* entry = readdir(dir);
88                         while (entry) {
89                                 if (strcmp(entry->d_name, ".") != 0 && strcmp(entry->d_name, "..") != 0) {
90                                         char* newpath = (char*)malloc(strlen(path) + strlen(entry->d_name) + 2);
91                                         sprintf(newpath, "%s/%s", path, entry->d_name);
92                                         error = removeDirAndAllContents(newpath);
93                                         free(newpath);
94                                         if (error) {
95                                                 break;
96                                         }
97                                 }
98                                 entry = readdir(dir);
99                         }
100                         closedir(dir);
101                         if (error == 0) {
102                                 error = rmdir(path);
103                         }
104                 } else {
105                         error = remove(path);
106                 }
107         }
108         return error;
111 void LocalCapture::copyImages(ImageLinkList* ptr) {
112         char dstfilename[PATH_MAX];
114         while (ptr) {
115                 strncpy(dstfilename, gSessionData->mAPCDir, PATH_MAX);
116                 dstfilename[PATH_MAX - 1] = 0; // strncpy does not guarantee a null-terminated string
117                 if (gSessionData->mAPCDir[strlen(gSessionData->mAPCDir) - 1] != '/') {
118                         strncat(dstfilename, "/", PATH_MAX - strlen(dstfilename) - 1);
119                 }
120                 strncat(dstfilename, util->getFilePart(ptr->path), PATH_MAX - strlen(dstfilename) - 1);
121                 if (util->copyFile(ptr->path, dstfilename)) {
122                         logg->logMessage("copied file %s to %s", ptr->path, dstfilename);
123                 } else {
124                         logg->logMessage("copy of file %s to %s failed", ptr->path, dstfilename);
125                 }
127                 ptr = ptr->next;
128         }