]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/arm-ds5-gator.git/blob - driver/gator_events_mmaped.c
Merge branch 'master' into android
[android-sdk/arm-ds5-gator.git] / driver / gator_events_mmaped.c
1 /*
2  * Example events provider
3  *
4  * Copyright (C) ARM Limited 2010-2012. All rights reserved.
5  *
6  * This program is free software; you can redistribute it and/or modify
7  * it under the terms of the GNU General Public License version 2 as
8  * published by the Free Software Foundation.
9  *
10  * Similar entries to those below must be present in the events.xml file.
11  * To add them to the events.xml, create an events-mmap.xml with the 
12  * following contents and rebuild gatord:
13  *
14  * <counter_set name="mmaped_cntX">
15  *   <counter name="mmaped_cnt0"/>
16  *   <counter name="mmaped_cnt1"/>
17  *   <counter name="mmaped_cnt2"/>
18  * </counter_set>
19  * <category name="mmaped" counter_set="mmaped_cntX" per_cpu="no">
20  *   <event event="0x0" title="Simulated" name="Sine" display="maximum" average_selection="yes" description="Sort-of-sine"/>
21  *   <event event="0x1" title="Simulated" name="Triangle" display="maximum" average_selection="yes" description="Triangular wave"/>
22  *   <event event="0x2" title="Simulated" name="PWM" display="maximum" average_selection="yes" description="PWM Signal"/>
23  * </category>
24  */
26 #include <linux/init.h>
27 #include <linux/io.h>
28 #include <linux/ratelimit.h>
30 #include "gator.h"
32 #define MMAPED_COUNTERS_NUM 3
34 static struct {
35         unsigned long enabled;
36         unsigned long event;
37         unsigned long key;
38 } mmaped_counters[MMAPED_COUNTERS_NUM];
40 static int mmaped_buffer[MMAPED_COUNTERS_NUM * 2];
42 #ifdef TODO
43 static void __iomem *mmaped_base;
44 #endif
46 #ifndef TODO
47 static s64 prev_time;
48 #endif
50 /* Adds mmaped_cntX directories and enabled, event, and key files to /dev/gator/events */
51 static int gator_events_mmaped_create_files(struct super_block *sb,
52                 struct dentry *root)
53 {
54         int i;
56         for (i = 0; i < MMAPED_COUNTERS_NUM; i++) {
57                 char buf[16];
58                 struct dentry *dir;
60                 snprintf(buf, sizeof(buf), "mmaped_cnt%d", i);
61                 dir = gatorfs_mkdir(sb, root, buf);
62                 if (WARN_ON(!dir))
63                         return -1;
64                 gatorfs_create_ulong(sb, dir, "enabled",
65                                 &mmaped_counters[i].enabled);
66                 gatorfs_create_ulong(sb, dir, "event",
67                                 &mmaped_counters[i].event);
68                 gatorfs_create_ro_ulong(sb, dir, "key",
69                                 &mmaped_counters[i].key);
70         }
72         return 0;
73 }
75 static int gator_events_mmaped_start(void)
76 {
77 #ifdef TODO
78         for (i = 0; i < MMAPED_COUNTERS_NUM; i++)
79                 writel(mmaped_counters[i].event,
80                                 mmaped_base + COUNTERS_CONFIG_OFFSET[i]);
82         writel(ENABLED, COUNTERS_CONTROL_OFFSET);
83 #endif
85 #ifndef TODO
86         struct timespec ts;
87         getnstimeofday(&ts);
88         prev_time = timespec_to_ns(&ts);
89 #endif
91         return 0;
92 }
94 static void gator_events_mmaped_stop(void)
95 {
96 #ifdef TODO
97         writel(DISABLED, COUNTERS_CONTROL_OFFSET);
98 #endif
99 }
101 #ifndef TODO
102 /* This function "simulates" counters, generating values of fancy
103  * functions like sine or triangle... */
104 static int mmaped_simulate(int counter, int delta_in_us)
106         int result = 0;
108         switch (counter) {
109         case 0: /* sort-of-sine */
110                 {
111                         static int t = 0;
112                         int x;
114                         t += delta_in_us;
115                         if (t > 2048000)
116                                 t = 0;
118                         if (t % 1024000 < 512000)
119                                 x = 512000 - (t % 512000);
120                         else
121                                 x = t % 512000;
123                         result = 32 * x / 512000;
124                         result = result * result;
126                         if (t < 1024000)
127                                 result = 1922 - result;
128                 }
129                 break;
130         case 1: /* triangle */
131                 {
132                         static int v, d = 1;
134                         v = v + d * delta_in_us;
135                         if (v < 0) {
136                                 v = 0;
137                                 d = 1;
138                         } else if (v > 1000000) {
139                                 v = 1000000;
140                                 d = -1;
141                         }
143                         result = v;
144                 }
145                 break;
146         case 2: /* PWM signal */
147                 {
148                         static int t, dc, x;
150                         t += delta_in_us;
151                         if (t > 1000000)
152                                 t = 0;
153                         if (x / 1000000 != (x + delta_in_us) / 1000000)
154                                 dc = (dc + 100000) % 1000000;
155                         x += delta_in_us;
156                         
157                         result = t < dc ? 0 : 10;
158                 }
159                 break;
160         }
162         return result;
164 #endif
166 static int gator_events_mmaped_read(int **buffer)
168         int i;
169         int len = 0;
170 #ifndef TODO
171         int delta_in_us;
172         struct timespec ts;
173         s64 time;
174 #endif
176         /* System wide counters - read from one core only */
177         if (smp_processor_id())
178                 return 0;
180 #ifndef TODO    
181         getnstimeofday(&ts);
182         time = timespec_to_ns(&ts);
183         delta_in_us = (int)(time - prev_time) / 1000;
184         prev_time = time;
185 #endif
187         for (i = 0; i < MMAPED_COUNTERS_NUM; i++) {
188                 if (mmaped_counters[i].enabled) {
189                         mmaped_buffer[len++] = mmaped_counters[i].key;
190 #ifdef TODO
191                         mmaped_buffer[len++] = readl(mmaped_base +
192                                         COUNTERS_VALUE_OFFSET[i]);
193 #else
194                         mmaped_buffer[len++] = mmaped_simulate(
195                                         mmaped_counters[i].event, delta_in_us);
196 #endif
197                 }
198         }
199         
200         if (buffer)
201                 *buffer = mmaped_buffer;
203         return len;
206 static struct gator_interface gator_events_mmaped_interface = {
207         .create_files = gator_events_mmaped_create_files,
208         .start = gator_events_mmaped_start,
209         .stop = gator_events_mmaped_stop,
210         .read = gator_events_mmaped_read,
211 };
213 /* Must not be static! */
214 int __init gator_events_mmaped_init(void)
216         int i;
218 #ifdef TODO
219         mmaped_base = ioremap(COUNTERS_PHYS_ADDR, SZ_4K);
220         if (!mmaped_base)
221                 return -ENOMEM; 
222 #endif
224         for (i = 0; i < MMAPED_COUNTERS_NUM; i++) {
225                 mmaped_counters[i].enabled = 0;
226                 mmaped_counters[i].key = gator_events_get_key();
227         }
229         return gator_events_install(&gator_events_mmaped_interface);
231 gator_events_init(gator_events_mmaped_init);