/** * Copyright (C) ARM Limited 2010-2012. All rights reserved. * * This program is free software; you can redistribute it and/or modify * it under the terms of the GNU General Public License version 2 as * published by the Free Software Foundation. */ #include #include #include #include "Fifo.h" #include "Logging.h" extern void handleException(); // bufferSize is the amount of data to be filled // singleBufferSize is the maximum size that may be filled during a single write // (bufferSize + singleBufferSize) will be allocated Fifo::Fifo(int singleBufferSize, int bufferSize) { mWrite = mRead = mReadCommit = mRaggedEnd = 0; mWrapThreshold = bufferSize; mSingleBufferSize = singleBufferSize; mBuffer = (char*)valloc(bufferSize + singleBufferSize); mEnd = false; if (mBuffer == NULL) { logg->logError(__FILE__, __LINE__, "failed to allocate %d bytes", bufferSize + singleBufferSize); handleException(); } if (sem_init(&mWaitForSpaceSem, 0, 0) || sem_init(&mWaitForDataSem, 0, 0)) { logg->logError(__FILE__, __LINE__, "sem_init() failed"); handleException(); } } Fifo::~Fifo() { free(mBuffer); } int Fifo::numBytesFilled() { return mWrite - mRead + mRaggedEnd; } char* Fifo::start() { return mBuffer; } bool Fifo::isEmpty() { return mRead == mWrite; } bool Fifo::isFull() { return willFill(0); } // Determines if the buffer will fill assuming 'additional' bytes will be added to the buffer // comparisons use '<', read and write pointers must never equal when not empty // 'full' means there is less than singleBufferSize bytes available; it does not mean there are zero bytes available bool Fifo::willFill(int additional) { if (mWrite > mRead) { if (numBytesFilled() + additional < mWrapThreshold) { return false; } } else { if (numBytesFilled() + additional < mWrapThreshold - mSingleBufferSize) { return false; } } return true; } // This function will stall until contiguous singleBufferSize bytes are available char* Fifo::write(int length) { if (length <= 0) { length = 0; mEnd = true; } // update the write pointer mWrite += length; // handle the wrap-around if (mWrite >= mWrapThreshold) { mRaggedEnd = mWrite; mWrite = 0; } // send a notification that data is ready sem_post(&mWaitForDataSem); // wait for space while (isFull()) { sem_wait(&mWaitForSpaceSem); } return &mBuffer[mWrite]; } // This function will stall until data is available char* Fifo::read(int* length) { // update the read pointer now that the data has been handled mRead = mReadCommit; // handle the wrap-around if (mRead >= mWrapThreshold) { mRaggedEnd = mRead = mReadCommit = 0; } // send a notification that data is free (space is available) sem_post(&mWaitForSpaceSem); // wait for data while (isEmpty() && !mEnd) { sem_wait(&mWaitForDataSem); } // obtain the length do { mReadCommit = mRaggedEnd ? mRaggedEnd : mWrite; *length = mReadCommit - mRead; } while (*length < 0); // plugs race condition without using semaphores return &mBuffer[mRead]; }