/** * Copyright (C) ARM Limited 2010-2012. All rights reserved. * * This program is free software; you can redistribute it and/or modify * it under the terms of the GNU General Public License version 2 as * published by the Free Software Foundation. */ #include #include #include #include #include #include #include #include #include #include #include #include "Child.h" #include "SessionData.h" #include "OlySocket.h" #include "Logging.h" #include "OlyUtility.h" #define DEBUG false extern Child* child; extern void handleException(); int shutdownFilesystem(); static pthread_mutex_t numSessions_mutex; static int numSessions = 0; static OlySocket* socket = NULL; static bool driverRunningAtStart = false; static bool driverMountedAtStart = false; struct cmdline_t { int port; char* module; }; void cleanUp() { if (shutdownFilesystem() == -1) { logg->logMessage("Error shutting down gator filesystem"); } delete socket; delete util; delete logg; } // CTRL C Signal Handler void handler(int signum) { logg->logMessage("Received signal %d, gator daemon exiting", signum); // Case 1: both child and parent receive the signal if (numSessions > 0) { // Arbitrary sleep of 1 second to give time for the child to exit; // if something bad happens, continue the shutdown process regardless sleep(1); } // Case 2: only the parent received the signal if (numSessions > 0) { // Kill child threads - the first signal exits gracefully logg->logMessage("Killing process group as %d child was running when signal was received", numSessions); kill(0, SIGINT); // Give time for the child to exit sleep(1); if (numSessions > 0) { // The second signal force kills the child logg->logMessage("Force kill the child"); kill(0, SIGINT); // Again, sleep for 1 second sleep(1); if (numSessions > 0) { // Something bad has really happened; the child is not exiting and therefore may hold the /dev/gator resource open printf("Unable to kill the gatord child process, thus gator.ko may still be loaded.\n"); } } } cleanUp(); exit(0); } // Child exit Signal Handler void child_exit(int signum) { int status; int pid = wait(&status); if (pid != -1) { pthread_mutex_lock(&numSessions_mutex); numSessions--; pthread_mutex_unlock(&numSessions_mutex); logg->logMessage("Child process %d exited with status %d", pid, status); } } // retval: -1 = failure; 0 = was already mounted; 1 = successfully mounted int mountGatorFS() { // If already mounted, if (access("/dev/gator/buffer", F_OK) == 0) { return 0; } // else, mount the filesystem mkdir("/dev/gator", S_IRWXU | S_IRWXG | S_IROTH | S_IXOTH); if (mount("nodev", "/dev/gator", "gatorfs", 0, NULL) != 0) { return -1; } else { return 1; } } int setupFilesystem(char* module) { int retval; // Verify root permissions uid_t euid = geteuid(); if (euid) { logg->logError(__FILE__, __LINE__, "gatord must be launched with root privileges"); handleException(); } if (module) { // unmount and rmmod if the module was specified on the commandline, i.e. ensure that the specified module is indeed running shutdownFilesystem(); // if still mounted if (access("/dev/gator/buffer", F_OK) == 0) { logg->logError(__FILE__, __LINE__, "Unable to remove the running gator.ko. Manually remove the module or use the running module by not specifying one on the commandline"); handleException(); } } retval = mountGatorFS(); if (retval == 1) { logg->logMessage("Driver already running at startup"); driverRunningAtStart = true; } else if (retval == 0) { logg->logMessage("Driver already mounted at startup"); driverRunningAtStart = driverMountedAtStart = true; } else { char command[256]; // arbitrarily large amount char location[256]; // arbitrarily large amount if (module) { strncpy(location, module, sizeof(location)); } else { // Is the driver co-located in the same directory? if (util->getApplicationFullPath(location, sizeof(location)) != 0) { // allow some buffer space logg->logMessage("Unable to determine the full path of gatord, the cwd will be used"); } strncat(location, "gator.ko", sizeof(location) - strlen(location) - 1); } if (access(location, F_OK) == -1) { logg->logError(__FILE__, __LINE__, "Unable to locate gator.ko driver:\n >>> gator.ko should be co-located with gatord in the same directory\n >>> OR insmod gator.ko prior to launching gatord\n >>> OR specify the location of gator.ko on the command line"); handleException(); } // Load driver snprintf(command, sizeof(command), "insmod %s >/dev/null 2>&1", location); if (system(command) != 0) { logg->logMessage("Unable to load gator.ko driver with command: %s", command); logg->logError(__FILE__, __LINE__, "Unable to load (insmod) gator.ko driver:\n >>> gator.ko must be built against the current kernel version & configuration\n >>> See dmesg for more details"); handleException(); } if (mountGatorFS() == -1) { logg->logError(__FILE__, __LINE__, "Unable to mount the gator filesystem needed for profiling."); handleException(); } } return 0; } int shutdownFilesystem() { if (driverMountedAtStart == false) { umount("/dev/gator"); } if (driverRunningAtStart == false) { if (system("rmmod gator >/dev/null 2>&1") != 0) { return -1; } } return 0; // success } struct cmdline_t parseCommandLine(int argc, char** argv) { struct cmdline_t cmdline; cmdline.port = 8080; cmdline.module = NULL; char version_string[256]; // arbitrary length to hold the version information int c; // build the version string if (PROTOCOL_VERSION < PROTOCOL_DEV) { snprintf(version_string, sizeof(version_string), "Streamline gatord version %d (DS-5 v5.%d)", PROTOCOL_VERSION, PROTOCOL_VERSION + 1); } else { snprintf(version_string, sizeof(version_string), "Streamline gatord development version %d", PROTOCOL_VERSION); } while ((c = getopt(argc, argv, "hvp:s:c:e:m:")) != -1) { switch(c) { case 'c': gSessionData->mConfigurationXMLPath = optarg; break; case 'e': gSessionData->mEventsXMLPath = optarg; break; case 'm': cmdline.module = optarg; break; case 'p': cmdline.port = strtol(optarg, NULL, 10); break; case 's': gSessionData->mSessionXMLPath = optarg; break; case 'h': case '?': logg->logError(__FILE__, __LINE__, "%s. All parameters are optional:\n" "-c config_xml path and filename of the configuration.xml to use\n" "-e events_xml path and filename of the events.xml to use\n" "-h this help page\n" "-m module path and filename of gator.ko\n" "-p port_number port upon which the server listens; default is 8080\n" "-s session_xml path and filename of a session xml used for local capture\n" "-v version information\n" , version_string); handleException(); break; case 'v': logg->logError(__FILE__, __LINE__, version_string); handleException(); break; } } // Error checking if (cmdline.port != 8080 && gSessionData->mSessionXMLPath != NULL) { logg->logError(__FILE__, __LINE__, "Only a port or a session xml can be specified, not both"); handleException(); } if (optind < argc) { logg->logError(__FILE__, __LINE__, "Unknown argument: %s. Use '-h' for help.", argv[optind]); handleException(); } return cmdline; } // Gator data flow: collector -> collector fifo -> sender int main(int argc, char** argv, char* envp[]) { gSessionData = new SessionData(); // Global data class logg = new Logging(DEBUG); // Set up global thread-safe logging util = new OlyUtility(); // Set up global utility class prctl(PR_SET_NAME, (unsigned long)&"gatord-main", 0, 0, 0); pthread_mutex_init(&numSessions_mutex, NULL); signal(SIGINT, handler); signal(SIGTERM, handler); signal(SIGABRT, handler); // Set to high priority if (setpriority(PRIO_PROCESS, syscall(__NR_gettid), -19) == -1) { logg->logMessage("setpriority() failed"); } // Initialize session data gSessionData->initialize(); // Parse the command line parameters struct cmdline_t cmdline = parseCommandLine(argc, argv); // Call before setting up the SIGCHLD handler, as system() spawns child processes setupFilesystem(cmdline.module); // Handle child exit codes signal(SIGCHLD, child_exit); // Ignore the SIGPIPE signal so that any send to a broken socket will return an error code instead of asserting a signal // Handling the error at the send function call is much easier than trying to do anything intelligent in the sig handler signal(SIGPIPE, SIG_IGN); // If the command line argument is a session xml file, no need to open a socket if (gSessionData->mSessionXMLPath) { child = new Child(); child->run(); delete child; } else { socket = new OlySocket(cmdline.port, true); // Forever loop, can be exited via a signal or exception while (1) { logg->logMessage("Waiting on connection..."); socket->acceptConnection(); int pid = fork(); if (pid < 0) { // Error logg->logError(__FILE__, __LINE__, "Fork process failed. Please power cycle the target device if this error persists."); } else if (pid == 0) { // Child socket->closeServerSocket(); child = new Child(socket, numSessions + 1); child->run(); delete child; exit(0); } else { // Parent socket->closeSocket(); pthread_mutex_lock(&numSessions_mutex); numSessions++; pthread_mutex_unlock(&numSessions_mutex); // Maximum number of connections is 2 int wait = 0; while (numSessions > 1) { // Throttle until one of the children exits before continuing to accept another socket connection logg->logMessage("%d sessions active!", numSessions); if (wait++ >= 10) { // Wait no more than 10 seconds // Kill last created child kill(pid, SIGALRM); break; } sleep(1); } } } } cleanUp(); return 0; }