/** * Copyright (C) ARM Limited 2010-2012. All rights reserved. * * This program is free software; you can redistribute it and/or modify * it under the terms of the GNU General Public License version 2 as * published by the Free Software Foundation. */ #ifndef GATOR_H_ #define GATOR_H_ #include #include #include #include #define GATOR_PERF_SUPPORT LINUX_VERSION_CODE >= KERNEL_VERSION(3, 0, 0) #define GATOR_PERF_PMU_SUPPORT GATOR_PERF_SUPPORT && defined(CONFIG_PERF_EVENTS) && (!(defined(__arm__) || defined(__aarch64__)) || defined(CONFIG_HW_PERF_EVENTS)) #define GATOR_NO_PERF_SUPPORT (!(GATOR_PERF_SUPPORT)) #define GATOR_CPU_FREQ_SUPPORT (LINUX_VERSION_CODE >= KERNEL_VERSION(2, 6, 38)) && defined(CONFIG_CPU_FREQ) // cpu ids #define ARM1136 0xb36 #define ARM1156 0xb56 #define ARM1176 0xb76 #define ARM11MPCORE 0xb02 #define CORTEX_A5 0xc05 #define CORTEX_A7 0xc07 #define CORTEX_A8 0xc08 #define CORTEX_A9 0xc09 #define CORTEX_A15 0xc0f #define SCORPION 0x00f #define SCORPIONMP 0x02d #define KRAITSIM 0x049 #define KRAIT 0x04d #define KRAIT_S4_PRO 0x06f #define CORTEX_A53 0xd03 #define CORTEX_A57 0xd07 #define AARCH64 0xd0f #define OTHER 0xfff #define MAXSIZE_CORE_NAME 32 struct gator_cpu { const int cpuid; const char core_name[MAXSIZE_CORE_NAME]; const char * const pmnc_name; const int pmnc_counters; const int ccnt; }; extern struct gator_cpu gator_cpus[]; /****************************************************************************** * Filesystem ******************************************************************************/ int gatorfs_create_file_perm(struct super_block *sb, struct dentry *root, char const *name, const struct file_operations *fops, int perm); struct dentry *gatorfs_mkdir(struct super_block *sb, struct dentry *root, char const *name); int gatorfs_create_ulong(struct super_block *sb, struct dentry *root, char const *name, unsigned long *val); int gatorfs_create_ro_ulong(struct super_block *sb, struct dentry *root, char const *name, unsigned long *val); void gator_op_create_files(struct super_block *sb, struct dentry *root); /****************************************************************************** * Tracepoints ******************************************************************************/ #if LINUX_VERSION_CODE < KERNEL_VERSION(2, 6, 32) # error Kernels prior to 2.6.32 not supported #elif LINUX_VERSION_CODE < KERNEL_VERSION(2, 6, 35) # define GATOR_DEFINE_PROBE(probe_name, proto) \ static void probe_##probe_name(PARAMS(proto)) # define GATOR_REGISTER_TRACE(probe_name) \ register_trace_##probe_name(probe_##probe_name) # define GATOR_UNREGISTER_TRACE(probe_name) \ unregister_trace_##probe_name(probe_##probe_name) #else # define GATOR_DEFINE_PROBE(probe_name, proto) \ static void probe_##probe_name(void *data, PARAMS(proto)) # define GATOR_REGISTER_TRACE(probe_name) \ register_trace_##probe_name(probe_##probe_name, NULL) # define GATOR_UNREGISTER_TRACE(probe_name) \ unregister_trace_##probe_name(probe_##probe_name, NULL) #endif /****************************************************************************** * Events ******************************************************************************/ struct gator_interface { void (*shutdown)(void); // Complementary function to init int (*create_files)(struct super_block *sb, struct dentry *root); int (*start)(void); void (*stop)(void); // Complementary function to start int (*online)(int **buffer); int (*offline)(int **buffer); void (*online_dispatch)(int cpu); // called in process context but may not be running on core 'cpu' void (*offline_dispatch)(int cpu); // called in process context but may not be running on core 'cpu' int (*read)(int **buffer); int (*read64)(long long **buffer); struct list_head list; }; // gator_events_init is used as a search term in gator_events.sh #define gator_events_init(initfn) \ static inline int __gator_events_init_test(void) \ { return initfn(); } int gator_events_install(struct gator_interface *interface); int gator_events_get_key(void); u32 gator_cpuid(void); void gator_backtrace_handler(struct pt_regs *const regs); #endif // GATOR_H_