/** * Copyright (C) ARM Limited 2010-2014. All rights reserved. * * This program is free software; you can redistribute it and/or modify * it under the terms of the GNU General Public License version 2 as * published by the Free Software Foundation. * */ #define COOKIEMAP_ENTRIES 1024 /* must be power of 2 */ #define TRANSLATE_BUFFER_SIZE 512 // must be a power of 2 - 512/4 = 128 entries #define TRANSLATE_TEXT_SIZE 256 #define MAX_COLLISIONS 2 static uint32_t *gator_crc32_table; static unsigned int translate_buffer_mask; struct cookie_args { struct task_struct *task; const char *text; }; static DEFINE_PER_CPU(char *, translate_text); static DEFINE_PER_CPU(uint32_t, cookie_next_key); static DEFINE_PER_CPU(uint64_t *, cookie_keys); static DEFINE_PER_CPU(uint32_t *, cookie_values); static DEFINE_PER_CPU(int, translate_buffer_read); static DEFINE_PER_CPU(int, translate_buffer_write); static DEFINE_PER_CPU(struct cookie_args *, translate_buffer); static uint32_t get_cookie(int cpu, struct task_struct *task, const char *text, bool from_wq); static void wq_cookie_handler(struct work_struct *unused); static DECLARE_WORK(cookie_work, wq_cookie_handler); static struct timer_list app_process_wake_up_timer; static void app_process_wake_up_handler(unsigned long unused_data); static uint32_t cookiemap_code(uint64_t value64) { uint32_t value = (uint32_t)((value64 >> 32) + value64); uint32_t cookiecode = (value >> 24) & 0xff; cookiecode = cookiecode * 31 + ((value >> 16) & 0xff); cookiecode = cookiecode * 31 + ((value >> 8) & 0xff); cookiecode = cookiecode * 31 + ((value >> 0) & 0xff); cookiecode &= (COOKIEMAP_ENTRIES - 1); return cookiecode * MAX_COLLISIONS; } static uint32_t gator_chksum_crc32(const char *data) { register unsigned long crc; const unsigned char *block = data; int i, length = strlen(data); crc = 0xFFFFFFFF; for (i = 0; i < length; i++) { crc = ((crc >> 8) & 0x00FFFFFF) ^ gator_crc32_table[(crc ^ *block++) & 0xFF]; } return (crc ^ 0xFFFFFFFF); } /* * Exists * Pre: [0][1][v][3]..[n-1] * Post: [v][0][1][3]..[n-1] */ static uint32_t cookiemap_exists(uint64_t key) { unsigned long x, flags, retval = 0; int cpu = get_physical_cpu(); uint32_t cookiecode = cookiemap_code(key); uint64_t *keys = &(per_cpu(cookie_keys, cpu)[cookiecode]); uint32_t *values = &(per_cpu(cookie_values, cpu)[cookiecode]); // Can be called from interrupt handler or from work queue local_irq_save(flags); for (x = 0; x < MAX_COLLISIONS; x++) { if (keys[x] == key) { uint32_t value = values[x]; for (; x > 0; x--) { keys[x] = keys[x - 1]; values[x] = values[x - 1]; } keys[0] = key; values[0] = value; retval = value; break; } } local_irq_restore(flags); return retval; } /* * Add * Pre: [0][1][2][3]..[n-1] * Post: [v][0][1][2]..[n-2] */ static void cookiemap_add(uint64_t key, uint32_t value) { int cpu = get_physical_cpu(); int cookiecode = cookiemap_code(key); uint64_t *keys = &(per_cpu(cookie_keys, cpu)[cookiecode]); uint32_t *values = &(per_cpu(cookie_values, cpu)[cookiecode]); int x; for (x = MAX_COLLISIONS - 1; x > 0; x--) { keys[x] = keys[x - 1]; values[x] = values[x - 1]; } keys[0] = key; values[0] = value; } #ifndef CONFIG_PREEMPT_RT_FULL static void translate_buffer_write_args(int cpu, struct task_struct *task, const char *text) { unsigned long flags; int write; int next_write; struct cookie_args *args; local_irq_save(flags); write = per_cpu(translate_buffer_write, cpu); next_write = (write + 1) & translate_buffer_mask; // At least one entry must always remain available as when read == write, the queue is empty not full if (next_write != per_cpu(translate_buffer_read, cpu)) { args = &per_cpu(translate_buffer, cpu)[write]; args->task = task; args->text = text; #if LINUX_VERSION_CODE >= KERNEL_VERSION(2, 6, 39) get_task_struct(task); #endif per_cpu(translate_buffer_write, cpu) = next_write; } local_irq_restore(flags); } #endif static void translate_buffer_read_args(int cpu, struct cookie_args *args) { unsigned long flags; int read; local_irq_save(flags); read = per_cpu(translate_buffer_read, cpu); *args = per_cpu(translate_buffer, cpu)[read]; per_cpu(translate_buffer_read, cpu) = (read + 1) & translate_buffer_mask; local_irq_restore(flags); } static void wq_cookie_handler(struct work_struct *unused) { struct cookie_args args; int cpu = get_physical_cpu(), cookie; mutex_lock(&start_mutex); if (gator_started != 0) { while (per_cpu(translate_buffer_read, cpu) != per_cpu(translate_buffer_write, cpu)) { translate_buffer_read_args(cpu, &args); cookie = get_cookie(cpu, args.task, args.text, true); marshal_link(cookie, args.task->tgid, args.task->pid); #if LINUX_VERSION_CODE >= KERNEL_VERSION(2, 6, 39) put_task_struct(args.task); #endif } } mutex_unlock(&start_mutex); } static void app_process_wake_up_handler(unsigned long unused_data) { // had to delay scheduling work as attempting to schedule work during the context switch is illegal in kernel versions 3.5 and greater schedule_work(&cookie_work); } // Retrieve full name from proc/pid/cmdline for java processes on Android static int translate_app_process(const char **text, int cpu, struct task_struct *task, bool from_wq) { void *maddr; unsigned int len; unsigned long addr; struct mm_struct *mm; struct page *page = NULL; struct vm_area_struct *page_vma; int bytes, offset, retval = 0; char *buf = per_cpu(translate_text, cpu); #ifndef CONFIG_PREEMPT_RT_FULL // Push work into a work queue if in atomic context as the kernel functions below might sleep // Rely on the in_interrupt variable rather than in_irq() or in_interrupt() kernel functions, as the value of these functions seems // inconsistent during a context switch between android/linux versions if (!from_wq) { // Check if already in buffer int pos = per_cpu(translate_buffer_read, cpu); while (pos != per_cpu(translate_buffer_write, cpu)) { if (per_cpu(translate_buffer, cpu)[pos].task == task) goto out; pos = (pos + 1) & translate_buffer_mask; } translate_buffer_write_args(cpu, task, *text); // Not safe to call in RT-Preempt full in schedule switch context mod_timer(&app_process_wake_up_timer, jiffies + 1); goto out; } #endif mm = get_task_mm(task); if (!mm) goto out; if (!mm->arg_end) goto outmm; addr = mm->arg_start; len = mm->arg_end - mm->arg_start; if (len > TRANSLATE_TEXT_SIZE) len = TRANSLATE_TEXT_SIZE; down_read(&mm->mmap_sem); while (len) { if (get_user_pages(task, mm, addr, 1, 0, 1, &page, &page_vma) <= 0) goto outsem; maddr = kmap(page); offset = addr & (PAGE_SIZE - 1); bytes = len; if (bytes > PAGE_SIZE - offset) bytes = PAGE_SIZE - offset; copy_from_user_page(page_vma, page, addr, buf, maddr + offset, bytes); kunmap(page); // release page allocated by get_user_pages() page_cache_release(page); len -= bytes; buf += bytes; addr += bytes; *text = per_cpu(translate_text, cpu); retval = 1; } // On app_process startup, /proc/pid/cmdline is initially "zygote" then "" but changes after an initial startup period if (strcmp(*text, "zygote") == 0 || strcmp(*text, "") == 0) retval = 0; outsem: up_read(&mm->mmap_sem); outmm: mmput(mm); out: return retval; } static uint32_t get_cookie(int cpu, struct task_struct *task, const char *text, bool from_wq) { unsigned long flags, cookie; uint64_t key; key = gator_chksum_crc32(text); key = (key << 32) | (uint32_t)task->tgid; cookie = cookiemap_exists(key); if (cookie) { return cookie; } if (strcmp(text, "app_process") == 0) { if (!translate_app_process(&text, cpu, task, from_wq)) return UNRESOLVED_COOKIE; } // Can be called from interrupt handler or from work queue or from scheduler trace local_irq_save(flags); cookie = UNRESOLVED_COOKIE; if (marshal_cookie_header(text)) { cookie = per_cpu(cookie_next_key, cpu) += nr_cpu_ids; cookiemap_add(key, cookie); marshal_cookie(cookie, text); } local_irq_restore(flags); return cookie; } static int get_exec_cookie(int cpu, struct task_struct *task) { struct mm_struct *mm = task->mm; const char *text; // kernel threads have no address space if (!mm) return NO_COOKIE; if (task && task->mm && task->mm->exe_file) { text = task->mm->exe_file->f_path.dentry->d_name.name; return get_cookie(cpu, task, text, false); } return UNRESOLVED_COOKIE; } static unsigned long get_address_cookie(int cpu, struct task_struct *task, unsigned long addr, off_t *offset) { unsigned long cookie = NO_COOKIE; struct mm_struct *mm = task->mm; struct vm_area_struct *vma; const char *text; if (!mm) return cookie; for (vma = find_vma(mm, addr); vma; vma = vma->vm_next) { if (addr < vma->vm_start || addr >= vma->vm_end) continue; if (vma->vm_file) { text = vma->vm_file->f_path.dentry->d_name.name; cookie = get_cookie(cpu, task, text, false); *offset = (vma->vm_pgoff << PAGE_SHIFT) + addr - vma->vm_start; } else { /* must be an anonymous map */ *offset = addr; } break; } if (!vma) cookie = UNRESOLVED_COOKIE; return cookie; } static int cookies_initialize(void) { uint32_t crc, poly; int i, j, cpu, size, err = 0; translate_buffer_mask = TRANSLATE_BUFFER_SIZE / sizeof(per_cpu(translate_buffer, 0)[0]) - 1; for_each_present_cpu(cpu) { per_cpu(cookie_next_key, cpu) = nr_cpu_ids + cpu; size = COOKIEMAP_ENTRIES * MAX_COLLISIONS * sizeof(uint64_t); per_cpu(cookie_keys, cpu) = (uint64_t *)kmalloc(size, GFP_KERNEL); if (!per_cpu(cookie_keys, cpu)) { err = -ENOMEM; goto cookie_setup_error; } memset(per_cpu(cookie_keys, cpu), 0, size); size = COOKIEMAP_ENTRIES * MAX_COLLISIONS * sizeof(uint32_t); per_cpu(cookie_values, cpu) = (uint32_t *)kmalloc(size, GFP_KERNEL); if (!per_cpu(cookie_values, cpu)) { err = -ENOMEM; goto cookie_setup_error; } memset(per_cpu(cookie_values, cpu), 0, size); per_cpu(translate_buffer, cpu) = (struct cookie_args *)kmalloc(TRANSLATE_BUFFER_SIZE, GFP_KERNEL); if (!per_cpu(translate_buffer, cpu)) { err = -ENOMEM; goto cookie_setup_error; } per_cpu(translate_buffer_write, cpu) = 0; per_cpu(translate_buffer_read, cpu) = 0; per_cpu(translate_text, cpu) = (char *)kmalloc(TRANSLATE_TEXT_SIZE, GFP_KERNEL); if (!per_cpu(translate_text, cpu)) { err = -ENOMEM; goto cookie_setup_error; } } // build CRC32 table poly = 0x04c11db7; gator_crc32_table = (uint32_t *)kmalloc(256 * sizeof(uint32_t), GFP_KERNEL); if (!gator_crc32_table) { err = -ENOMEM; goto cookie_setup_error; } for (i = 0; i < 256; i++) { crc = i; for (j = 8; j > 0; j--) { if (crc & 1) { crc = (crc >> 1) ^ poly; } else { crc >>= 1; } } gator_crc32_table[i] = crc; } setup_timer(&app_process_wake_up_timer, app_process_wake_up_handler, 0); cookie_setup_error: return err; } static void cookies_release(void) { int cpu; for_each_present_cpu(cpu) { kfree(per_cpu(cookie_keys, cpu)); per_cpu(cookie_keys, cpu) = NULL; kfree(per_cpu(cookie_values, cpu)); per_cpu(cookie_values, cpu) = NULL; kfree(per_cpu(translate_buffer, cpu)); per_cpu(translate_buffer, cpu) = NULL; per_cpu(translate_buffer_read, cpu) = 0; per_cpu(translate_buffer_write, cpu) = 0; kfree(per_cpu(translate_text, cpu)); per_cpu(translate_text, cpu) = NULL; } del_timer_sync(&app_process_wake_up_timer); kfree(gator_crc32_table); gator_crc32_table = NULL; }