/** * Copyright (C) ARM Limited 2010-2011. All rights reserved. * * This program is free software; you can redistribute it and/or modify * it under the terms of the GNU General Public License version 2 as * published by the Free Software Foundation. * */ #include "gator.h" #include #define HARDIRQ 0 #define SOFTIRQ 1 #define TOTALIRQ (SOFTIRQ+1) static ulong hardirq_enabled; static ulong softirq_enabled; static ulong hardirq_key; static ulong softirq_key; static DEFINE_PER_CPU(int[TOTALIRQ], irqCnt); static DEFINE_PER_CPU(int[TOTALIRQ], irqPrev); static DEFINE_PER_CPU(int[TOTALIRQ * 2], irqGet); GATOR_DEFINE_PROBE(irq_handler_exit, TP_PROTO(int irq, struct irqaction *action, int ret)) { unsigned long flags; // disable interrupts to synchronize with gator_events_irq_read() // spinlocks not needed since percpu buffers are used local_irq_save(flags); per_cpu(irqCnt, smp_processor_id())[HARDIRQ]++; local_irq_restore(flags); } #if LINUX_VERSION_CODE < KERNEL_VERSION(2, 6, 37) GATOR_DEFINE_PROBE(softirq_exit, TP_PROTO(struct softirq_action *h, struct softirq_action *vec)) #else GATOR_DEFINE_PROBE(softirq_exit, TP_PROTO(unsigned int vec_nr)) #endif { unsigned long flags; // disable interrupts to synchronize with gator_events_irq_read() // spinlocks not needed since percpu buffers are used local_irq_save(flags); per_cpu(irqCnt, smp_processor_id())[SOFTIRQ]++; local_irq_restore(flags); } static int gator_events_irq_create_files(struct super_block *sb, struct dentry *root) { struct dentry *dir; /* irq */ dir = gatorfs_mkdir(sb, root, "Linux_irq_irq"); if (!dir) { return -1; } gatorfs_create_ulong(sb, dir, "enabled", &hardirq_enabled); gatorfs_create_ro_ulong(sb, dir, "key", &hardirq_key); /* soft irq */ dir = gatorfs_mkdir(sb, root, "Linux_irq_softirq"); if (!dir) { return -1; } gatorfs_create_ulong(sb, dir, "enabled", &softirq_enabled); gatorfs_create_ro_ulong(sb, dir, "key", &softirq_key); return 0; } static int gator_events_irq_start(void) { int cpu, i; for_each_present_cpu(cpu) { for (i = 0; i < TOTALIRQ; i++) per_cpu(irqPrev, cpu)[i] = 0; } // register tracepoints if (hardirq_enabled) if (GATOR_REGISTER_TRACE(irq_handler_exit)) goto fail_hardirq_exit; if (softirq_enabled) if (GATOR_REGISTER_TRACE(softirq_exit)) goto fail_softirq_exit; pr_debug("gator: registered irq tracepoints\n"); return 0; // unregister tracepoints on error fail_softirq_exit: if (hardirq_enabled) GATOR_UNREGISTER_TRACE(irq_handler_exit); fail_hardirq_exit: pr_err("gator: irq tracepoints failed to activate, please verify that tracepoints are enabled in the linux kernel\n"); return -1; } static void gator_events_irq_stop(void) { if (hardirq_enabled) GATOR_UNREGISTER_TRACE(irq_handler_exit); if (softirq_enabled) GATOR_UNREGISTER_TRACE(softirq_exit); pr_debug("gator: unregistered irq tracepoints\n"); hardirq_enabled = 0; softirq_enabled = 0; } static int gator_events_irq_read(int **buffer) { unsigned long flags; int len, value; int cpu = smp_processor_id(); len = 0; if (hardirq_enabled) { local_irq_save(flags); value = per_cpu(irqCnt, cpu)[HARDIRQ]; per_cpu(irqCnt, cpu)[HARDIRQ] = 0; local_irq_restore(flags); if (value != per_cpu(irqPrev, cpu)[HARDIRQ]) { per_cpu(irqPrev, cpu)[HARDIRQ] = value; per_cpu(irqGet, cpu)[len++] = hardirq_key; per_cpu(irqGet, cpu)[len++] = value; } } if (softirq_enabled) { local_irq_save(flags); value = per_cpu(irqCnt, cpu)[SOFTIRQ]; per_cpu(irqCnt, cpu)[SOFTIRQ] = 0; local_irq_restore(flags); if (value != per_cpu(irqPrev, cpu)[SOFTIRQ]) { per_cpu(irqPrev, cpu)[SOFTIRQ] = value; per_cpu(irqGet, cpu)[len++] = softirq_key; per_cpu(irqGet, cpu)[len++] = value; } } if (buffer) *buffer = per_cpu(irqGet, cpu); return len; } static struct gator_interface gator_events_irq_interface = { .create_files = gator_events_irq_create_files, .start = gator_events_irq_start, .stop = gator_events_irq_stop, .read = gator_events_irq_read, }; int gator_events_irq_init(void) { hardirq_key = gator_events_get_key(); softirq_key = gator_events_get_key(); hardirq_enabled = 0; softirq_enabled = 0; return gator_events_install(&gator_events_irq_interface); } gator_events_init(gator_events_irq_init);