/** * Copyright (C) ARM Limited 2010-2012. All rights reserved. * * This program is free software; you can redistribute it and/or modify * it under the terms of the GNU General Public License version 2 as * published by the Free Software Foundation. * */ #include "gator.h" #include #define SCHED_SWITCH 0 #define SCHED_TOTAL (SCHED_SWITCH+1) static ulong sched_switch_enabled; static ulong sched_switch_key; static DEFINE_PER_CPU(int[SCHED_TOTAL], schedCnt); static DEFINE_PER_CPU(int[SCHED_TOTAL * 2], schedGet); #if LINUX_VERSION_CODE < KERNEL_VERSION(2, 6, 35) GATOR_DEFINE_PROBE(sched_switch, TP_PROTO(struct rq *rq, struct task_struct *prev, struct task_struct *next)) #else GATOR_DEFINE_PROBE(sched_switch, TP_PROTO(struct task_struct *prev, struct task_struct *next)) #endif { unsigned long flags; // disable interrupts to synchronize with gator_events_sched_read() // spinlocks not needed since percpu buffers are used local_irq_save(flags); per_cpu(schedCnt, smp_processor_id())[SCHED_SWITCH]++; local_irq_restore(flags); } static int gator_events_sched_create_files(struct super_block *sb, struct dentry *root) { struct dentry *dir; /* switch */ dir = gatorfs_mkdir(sb, root, "Linux_sched_switch"); if (!dir) { return -1; } gatorfs_create_ulong(sb, dir, "enabled", &sched_switch_enabled); gatorfs_create_ro_ulong(sb, dir, "key", &sched_switch_key); return 0; } static int gator_events_sched_start(void) { // register tracepoints if (sched_switch_enabled) if (GATOR_REGISTER_TRACE(sched_switch)) goto sched_switch_exit; pr_debug("gator: registered scheduler event tracepoints\n"); return 0; // unregister tracepoints on error sched_switch_exit: pr_err("gator: scheduler event tracepoints failed to activate, please verify that tracepoints are enabled in the linux kernel\n"); return -1; } static void gator_events_sched_stop(void) { if (sched_switch_enabled) GATOR_UNREGISTER_TRACE(sched_switch); pr_debug("gator: unregistered scheduler event tracepoints\n"); sched_switch_enabled = 0; } static int gator_events_sched_read(int **buffer) { unsigned long flags; int len, value; int cpu = smp_processor_id(); len = 0; if (sched_switch_enabled) { local_irq_save(flags); value = per_cpu(schedCnt, cpu)[SCHED_SWITCH]; per_cpu(schedCnt, cpu)[SCHED_SWITCH] = 0; local_irq_restore(flags); per_cpu(schedGet, cpu)[len++] = sched_switch_key; per_cpu(schedGet, cpu)[len++] = value; } if (buffer) *buffer = per_cpu(schedGet, cpu); return len; } static struct gator_interface gator_events_sched_interface = { .create_files = gator_events_sched_create_files, .start = gator_events_sched_start, .stop = gator_events_sched_stop, .read = gator_events_sched_read, }; int gator_events_sched_init(void) { sched_switch_enabled = 0; sched_switch_key = gator_events_get_key(); return gator_events_install(&gator_events_sched_interface); } gator_events_init(gator_events_sched_init);