/** * Copyright (C) ARM Limited 2010-2012. All rights reserved. * * This program is free software; you can redistribute it and/or modify * it under the terms of the GNU General Public License version 2 as * published by the Free Software Foundation. * */ #include #include "gator.h" #define SCHED_SWITCH 1 #define SCHED_PROCESS_EXIT 2 #define TASK_MAP_ENTRIES 1024 /* must be power of 2 */ #define TASK_MAX_COLLISIONS 2 static DEFINE_PER_CPU(uint64_t *, taskname_keys); static DEFINE_PER_CPU(int, collecting); enum { STATE_WAIT_ON_OTHER = 0, STATE_CONTENTION, STATE_WAIT_ON_IO, STATE_WAIT_ON_MUTEX, }; void emit_pid_name(struct task_struct* task) { bool found = false; char taskcomm[TASK_COMM_LEN + 3]; unsigned long x, cpu = smp_processor_id(); uint64_t *keys = &(per_cpu(taskname_keys, cpu)[(task->pid & 0xFF) * TASK_MAX_COLLISIONS]); uint64_t value; value = gator_chksum_crc32(task->comm); value = (value << 32) | (uint32_t)task->pid; // determine if the thread name was emitted already for (x = 0; x < TASK_MAX_COLLISIONS; x++) { if (keys[x] == value) { found = true; break; } } if (!found) { // shift values, new value always in front uint64_t oldv, newv = value; for (x = 0; x < TASK_MAX_COLLISIONS; x++) { oldv = keys[x]; keys[x] = newv; newv = oldv; } // emit pid names, cannot use get_task_comm, as it's not exported on all kernel versions if (strlcpy(taskcomm, task->comm, TASK_COMM_LEN) == TASK_COMM_LEN - 1) { // append ellipses if task->comm has length of TASK_COMM_LEN - 1 strcat(taskcomm, "..."); } marshal_thread_name(task->pid, taskcomm); } } static void collect_counters(void) { int *buffer, len; long long *buffer64; struct gator_interface *gi; if (marshal_event_header()) { list_for_each_entry(gi, &gator_events, list) { if (gi->read) { len = gi->read(&buffer); marshal_event(len, buffer); } else if (gi->read64) { len = gi->read64(&buffer64); marshal_event64(len, buffer64); } } } } static void probe_sched_write(int type, struct task_struct* task, struct task_struct* old_task) { int cookie = 0, state = 0; int cpu = smp_processor_id(); int tgid = task->tgid; int pid = task->pid; if (type == SCHED_SWITCH) { // do as much work as possible before disabling interrupts cookie = get_exec_cookie(cpu, task); emit_pid_name(task); if (old_task->state == TASK_RUNNING) { state = STATE_CONTENTION; } else if (old_task->in_iowait) { state = STATE_WAIT_ON_IO; #ifdef CONFIG_DEBUG_MUTEXES } else if (old_task->blocked_on) { state = STATE_WAIT_ON_MUTEX; #endif } else { state = STATE_WAIT_ON_OTHER; } per_cpu(collecting, cpu) = 1; collect_counters(); per_cpu(collecting, cpu) = 0; } // marshal_sched_trace() disables interrupts as the free may trigger while switch is writing to the buffer; disabling preemption is not sufficient // is disable interrupts necessary now that exit is used instead of free? if (type == SCHED_SWITCH) { marshal_sched_trace_switch(tgid, pid, cookie, state); } else { marshal_sched_trace_exit(tgid, pid); } } // special case used during a suspend of the system static void trace_sched_insert_idle(void) { marshal_sched_trace_switch(0, 0, 0, 0); } #if LINUX_VERSION_CODE < KERNEL_VERSION(2, 6, 35) GATOR_DEFINE_PROBE(sched_switch, TP_PROTO(struct rq *rq, struct task_struct *prev, struct task_struct *next)) #else GATOR_DEFINE_PROBE(sched_switch, TP_PROTO(struct task_struct *prev, struct task_struct *next)) #endif { probe_sched_write(SCHED_SWITCH, next, prev); } GATOR_DEFINE_PROBE(sched_process_exit, TP_PROTO(struct task_struct *p)) { probe_sched_write(SCHED_PROCESS_EXIT, p, 0); } static int register_scheduler_tracepoints(void) { // register tracepoints if (GATOR_REGISTER_TRACE(sched_switch)) goto fail_sched_switch; if (GATOR_REGISTER_TRACE(sched_process_exit)) goto fail_sched_process_exit; pr_debug("gator: registered tracepoints\n"); return 0; // unregister tracepoints on error fail_sched_process_exit: GATOR_UNREGISTER_TRACE(sched_switch); fail_sched_switch: pr_err("gator: tracepoints failed to activate, please verify that tracepoints are enabled in the linux kernel\n"); return -1; } int gator_trace_sched_start(void) { int cpu, size; for_each_present_cpu(cpu) { size = TASK_MAP_ENTRIES * TASK_MAX_COLLISIONS * sizeof(uint64_t); per_cpu(taskname_keys, cpu) = (uint64_t*)kmalloc(size, GFP_KERNEL); if (!per_cpu(taskname_keys, cpu)) return -1; memset(per_cpu(taskname_keys, cpu), 0, size); } return register_scheduler_tracepoints(); } void gator_trace_sched_offline(void) { trace_sched_insert_idle(); } static void unregister_scheduler_tracepoints(void) { GATOR_UNREGISTER_TRACE(sched_switch); GATOR_UNREGISTER_TRACE(sched_process_exit); pr_debug("gator: unregistered tracepoints\n"); } void gator_trace_sched_stop(void) { int cpu; unregister_scheduler_tracepoints(); for_each_present_cpu(cpu) { kfree(per_cpu(taskname_keys, cpu)); } }