diff --git a/daemon/OlySocket.cpp b/daemon/OlySocket.cpp
index ab5c3c2c89383d5b26ab916c2508134bd34629f7..26e4768f39342440d0c25a81a2bdd8c579d352a6 100644 (file)
--- a/daemon/OlySocket.cpp
+++ b/daemon/OlySocket.cpp
/**
- * Copyright (C) ARM Limited 2010-2013. All rights reserved.
+ * Copyright (C) ARM Limited 2010-2014. All rights reserved.
*
* This program is free software; you can redistribute it and/or modify
* it under the terms of the GNU General Public License version 2 as
#else
#include <netinet/in.h>
#include <sys/socket.h>
+#include <sys/un.h>
#include <unistd.h>
#include <netdb.h>
#endif
#define SHUTDOWN_RX_TX SHUT_RDWR
#endif
-OlySocket::OlySocket(int port, bool multiple) {
+OlyServerSocket::OlyServerSocket(int port) {
#ifdef WIN32
WSADATA wsaData;
if (WSAStartup(0x0202, &wsaData) != 0) {
}
#endif
- if (multiple) {
- createServerSocket(port);
- } else {
- createSingleServerConnection(port);
- }
+ createServerSocket(port);
}
-OlySocket::OlySocket(int port, char* host) {
- mFDServer = 0;
+OlySocket::OlySocket(int port, const char* host) {
createClientSocket(host, port);
}
+OlySocket::OlySocket(int socketID) : mSocketID(socketID) {
+}
+
+#ifndef WIN32
+
+OlyServerSocket::OlyServerSocket(const char* path) {
+ // Create socket
+ mFDServer = socket(PF_UNIX, SOCK_STREAM, 0);
+ if (mFDServer < 0) {
+ logg->logError(__FILE__, __LINE__, "Error creating server socket");
+ handleException();
+ }
+
+ unlink(path);
+
+ // Create sockaddr_in structure, ensuring non-populated fields are zero
+ struct sockaddr_un sockaddr;
+ memset((void*)&sockaddr, 0, sizeof(sockaddr));
+ sockaddr.sun_family = AF_UNIX;
+ strncpy(sockaddr.sun_path, path, sizeof(sockaddr.sun_path) - 1);
+ sockaddr.sun_path[sizeof(sockaddr.sun_path) - 1] = '\0';
+
+ // Bind the socket to an address
+ if (bind(mFDServer, (const struct sockaddr*)&sockaddr, sizeof(sockaddr)) < 0) {
+ logg->logError(__FILE__, __LINE__, "Binding of server socket failed.");
+ handleException();
+ }
+
+ // Listen for connections on this socket
+ if (listen(mFDServer, 1) < 0) {
+ logg->logError(__FILE__, __LINE__, "Listening of server socket failed");
+ handleException();
+ }
+}
+
+OlySocket::OlySocket(const char* path) {
+ mSocketID = socket(PF_UNIX, SOCK_STREAM, 0);
+ if (mSocketID < 0) {
+ return;
+ }
+
+ // Create sockaddr_in structure, ensuring non-populated fields are zero
+ struct sockaddr_un sockaddr;
+ memset((void*)&sockaddr, 0, sizeof(sockaddr));
+ sockaddr.sun_family = AF_UNIX;
+ strncpy(sockaddr.sun_path, path, sizeof(sockaddr.sun_path) - 1);
+ sockaddr.sun_path[sizeof(sockaddr.sun_path) - 1] = '\0';
+
+ if (connect(mSocketID, (const struct sockaddr*)&sockaddr, sizeof(sockaddr)) < 0) {
+ close(mSocketID);
+ mSocketID = -1;
+ return;
+ }
+}
+
+#endif
+
OlySocket::~OlySocket() {
if (mSocketID > 0) {
CLOSE_SOCKET(mSocketID);
}
}
+OlyServerSocket::~OlyServerSocket() {
+ if (mFDServer > 0) {
+ CLOSE_SOCKET(mFDServer);
+ }
+}
+
void OlySocket::shutdownConnection() {
// Shutdown is primarily used to unblock other threads that are blocking on send/receive functions
shutdown(mSocketID, SHUTDOWN_RX_TX);
}
}
-void OlySocket::closeServerSocket() {
+void OlyServerSocket::closeServerSocket() {
if (CLOSE_SOCKET(mFDServer) != 0) {
logg->logError(__FILE__, __LINE__, "Failed to close server socket.");
handleException();
mFDServer = 0;
}
-void OlySocket::createClientSocket(char* hostname, int portno) {
+void OlySocket::createClientSocket(const char* hostname, int portno) {
#ifdef WIN32
// TODO: Implement for Windows
#else
#endif
}
-void OlySocket::createSingleServerConnection(int port) {
- createServerSocket(port);
-
- mSocketID = acceptConnection();
- closeServerSocket();
-}
-
-void OlySocket::createServerSocket(int port) {
+void OlyServerSocket::createServerSocket(int port) {
int family = AF_INET6;
// Create socket
// mSocketID is always set to the most recently accepted connection
// The user of this class should maintain the different socket connections, e.g. by forking the process
-int OlySocket::acceptConnection() {
+int OlyServerSocket::acceptConnection() {
+ int socketID;
if (mFDServer <= 0) {
logg->logError(__FILE__, __LINE__, "Attempting multiple connections on a single connection server socket or attempting to accept on a client socket");
handleException();
}
// Accept a connection, note that this call blocks until a client connects
- mSocketID = accept(mFDServer, NULL, NULL);
- if (mSocketID < 0) {
+ socketID = accept(mFDServer, NULL, NULL);
+ if (socketID < 0) {
logg->logError(__FILE__, __LINE__, "Socket acceptance failed");
handleException();
}
- return mSocketID;
+ return socketID;
}
-void OlySocket::send(char* buffer, int size) {
+void OlySocket::send(const char* buffer, int size) {
if (size <= 0 || buffer == NULL) {
return;
}