diff --git a/daemon/main.cpp b/daemon/main.cpp
--- /dev/null
+++ b/daemon/main.cpp
@@ -0,0 +1,252 @@
+/**
+ * Copyright (C) ARM Limited 2010-2011. All rights reserved.
+ *
+ * This program is free software; you can redistribute it and/or modify
+ * it under the terms of the GNU General Public License version 2 as
+ * published by the Free Software Foundation.
+ */
+
+typedef unsigned long long uint64_t;
+#include <stdint.h>
+#include <stdlib.h>
+#include <signal.h>
+#include <ctype.h>
+#include <sys/wait.h>
+#include <unistd.h>
+#include <sys/syscall.h>
+#include <sys/prctl.h>
+#include <sys/types.h>
+#include <sys/stat.h>
+#include <sys/mount.h>
+#include "Child.h"
+#include "SessionData.h"
+#include "OlySocket.h"
+#include "Logging.h"
+#include "OlyUtility.h"
+
+#define DEBUG false
+
+extern Child* child;
+extern void handleException();
+int shutdownFilesystem();
+static pthread_mutex_t numSessions_mutex;
+static int numSessions = 0;
+static OlySocket* socket = NULL;
+static bool driverRunningAtStart = false;
+
+struct cmdline_t {
+ int port;
+ char* sessionXML;
+};
+
+void cleanUp() {
+ if (shutdownFilesystem() == -1) {
+ logg->logMessage("Error shutting down gator filesystem");
+ }
+ delete socket;
+ delete util;
+ delete logg;
+}
+
+// CTRL C Signal Handler
+void handler(int signum) {
+ logg->logMessage("Received signal %d, gator daemon exiting", signum);
+ if (numSessions > 0) {
+ // Kill child threads
+ logg->logMessage("Killing process group as %d child was running when signal was received", numSessions);
+ kill(0, SIGINT);
+ }
+
+ cleanUp();
+ exit(0);
+}
+
+// Child exit Signal Handler
+void child_exit(int signum) {
+ int status;
+ int pid = wait(&status);
+ if (pid != -1) {
+ pthread_mutex_lock(&numSessions_mutex);
+ numSessions--;
+ pthread_mutex_unlock(&numSessions_mutex);
+ logg->logMessage("Child process %d exited with status %d", pid, status);
+ }
+}
+
+// retval: -1 = failure; 0 = was already mounted; 1 = successfully mounted
+int mountGatorFS() {
+ // If already mounted,
+ if (access("/dev/gator/buffer", F_OK) != -1)
+ return 0;
+
+ // else, mount the filesystem
+ mkdir("/dev/gator", S_IRWXU | S_IRWXG | S_IROTH | S_IXOTH);
+ if (mount("nodev", "/dev/gator", "gatorfs", 0, NULL) != 0)
+ return -1;
+ else
+ return 1;
+}
+
+int setupFilesystem() {
+ // Verify root permissions
+ uid_t euid = geteuid();
+ if (euid) {
+ logg->logError(__FILE__, __LINE__, "gatord must be launched with root privileges");
+ handleException();
+ }
+
+ if (mountGatorFS() >= 0) {
+ logg->logMessage("Driver already running at startup");
+ driverRunningAtStart = true;
+ } else {
+ // Load driver
+ char command[512];
+ strcpy(command, "insmod ");
+ if (util->getApplicationFullPath(&command[7], sizeof(command) - 64) != 0) {
+ logg->logMessage("Unable to determine the full path of gatord, the cwd will be used");
+ }
+ strcat(command, "gator.ko >/dev/null 2>&1");
+ if (system(command) != 0) {
+ logg->logMessage("Unable to load gator.ko driver with command: %s", command);
+ logg->logError(__FILE__, __LINE__, "Unable to load (insmod) gator.ko driver. %s", DRIVER_ERROR);
+ handleException();
+ }
+
+ if (mountGatorFS() == -1) {
+ logg->logError(__FILE__, __LINE__, "Unable to mount the gator filesystem needed for profiling.");
+ handleException();
+ }
+ }
+
+ return 0;
+}
+
+int shutdownFilesystem() {
+ umount("/dev/gator");
+ if (driverRunningAtStart == true || system("rmmod gator >/dev/null 2>&1") == 0) {
+ return 0;
+ }
+
+ return -1;
+}
+
+struct cmdline_t parseCommandLine(int argc, char** argv) {
+ struct cmdline_t cmdline;
+ cmdline.port = 8080;
+ cmdline.sessionXML = NULL;
+
+ for (int i = 1; i < argc; i++) {
+ // Is the argument a number?
+ if (atoi(argv[i]) > 0) {
+ cmdline.port = atoi(argv[i]);
+ continue;
+ }
+
+ if (strcmp(argv[i], "-h") == 0 || strcmp(argv[i], "-?") == 0 || strcmp(argv[i], "--help") == 0) {
+ logg->logError(__FILE__, __LINE__,
+ "Streamline gatord version %d. All parameters are optional:\n"
+ "port_number\tport upon which the server listens; default is 8080\n"
+ "session_xml\tfilename of a session xml used for local capture\n"
+ "-v/--version\tversion information\n"
+ "-h/--help\tthis help page\n", PROTOCOL_VERSION);
+ handleException();
+ } else if (strcmp(argv[i], "-v") == 0 || strcmp(argv[i], "--version") == 0) {
+ logg->logError(__FILE__, __LINE__, "Streamline gatord version %d", PROTOCOL_VERSION);
+ handleException();
+ } else {
+ // Assume it is an .xml file
+ cmdline.sessionXML = argv[i];
+ }
+ }
+
+ // Error checking
+ if (cmdline.port != 8080 && cmdline.sessionXML != NULL) {
+ logg->logError(__FILE__, __LINE__, "Only a port or a session xml can be specified, not both");
+ handleException();
+ }
+
+ return cmdline;
+}
+
+// Gator data flow: collector -> collector fifo -> sender
+int main(int argc, char** argv, char *envp[]) {
+ logg = new Logging(DEBUG); // Set up global thread-safe logging
+ util = new OlyUtility(); // Set up global utility class
+
+ prctl(PR_SET_NAME, (unsigned int)&"gatord-main", 0, 0, 0);
+ pthread_mutex_init(&numSessions_mutex, NULL);
+
+ signal(SIGINT, handler);
+ signal(SIGTERM, handler);
+ signal(SIGABRT, handler);
+
+ // Set to high priority
+ setpriority(PRIO_PROCESS, syscall(__NR_gettid), -19);
+
+ // Initialize session data
+ gSessionData.initialize();
+
+ // Parse the command line parameters
+ struct cmdline_t cmdline = parseCommandLine(argc, argv);
+
+ // Call before setting up the SIGCHLD handler, as system() spawns child processes
+ setupFilesystem();
+
+ // Handle child exit codes
+ signal(SIGCHLD, child_exit);
+
+ // Ignore the SIGPIPE signal so that any send to a broken socket will return an error code instead of asserting a signal
+ // Handling the error at the send function call is much easier than trying to do anything intelligent in the sig handler
+ signal(SIGPIPE, SIG_IGN);
+
+ // If the command line argument is a session xml file, no need to open a socket
+ if (cmdline.sessionXML) {
+ child = new Child(cmdline.sessionXML);
+ child->run();
+ delete child;
+ } else {
+ socket = new OlySocket(cmdline.port, true);
+ // Forever loop, can be exited via a signal or exception
+ while (1) {
+ logg->logMessage("Waiting on connection...");
+ socket->acceptConnection();
+
+ int pid = fork();
+ if (pid < 0) {
+ // Error
+ logg->logError(__FILE__, __LINE__, "Fork process failed. Please power cycle the target device if this error persists.");
+ } else if (pid == 0) {
+ // Child
+ strncpy(argv[0],"gatorc",strlen(argv[0])); // rename command line name to gatorc
+ socket->closeServerSocket();
+ child = new Child(socket, numSessions + 1);
+ child->run();
+ delete child;
+ exit(0);
+ } else {
+ // Parent
+ socket->closeSocket();
+
+ pthread_mutex_lock(&numSessions_mutex);
+ numSessions++;
+ pthread_mutex_unlock(&numSessions_mutex);
+
+ // Maximum number of connections is 2
+ int wait = 0;
+ while (numSessions > 1) {
+ // Throttle until one of the children exits before continuing to accept another socket connection
+ logg->logMessage("%d sessions active!", numSessions);
+ if (wait++ >= 10) { // Wait no more than 10 seconds
+ // Kill last created child
+ kill(pid, SIGALRM);
+ break;
+ }
+ sleep(1);
+ }
+ }
+ }
+ }
+
+ cleanUp();
+ return 0;
+}