diff --git a/driver/gator_main.c b/driver/gator_main.c
index a2d8ef02ce9a8b3224d51a041a5bec42b3185853..5eab03456ce67060b0828dc82247aec3ba91be85 100644 (file)
--- a/driver/gator_main.c
+++ b/driver/gator_main.c
/**
- * Copyright (C) ARM Limited 2010-2012. All rights reserved.
+ * Copyright (C) ARM Limited 2010-2013. All rights reserved.
*
* This program is free software; you can redistribute it and/or modify
* it under the terms of the GNU General Public License version 2 as
*
*/
-static unsigned long gator_protocol_version = 11;
+// This version must match the gator daemon version
+static unsigned long gator_protocol_version = 14;
#include <linux/slab.h>
#include <linux/cpu.h>
#include <linux/suspend.h>
#include <linux/module.h>
#include <linux/perf_event.h>
+#include <linux/utsname.h>
#include <asm/stacktrace.h>
#include <asm/uaccess.h>
#define SUMMARY_BUFFER_SIZE (1*1024)
#define BACKTRACE_BUFFER_SIZE (128*1024)
#define NAME_BUFFER_SIZE (64*1024)
-#define COUNTER_BUFFER_SIZE (64*1024) // counters have the core as part of the data and the core value in the frame header may be discarded
+#define COUNTER_BUFFER_SIZE (64*1024) // counters have the core as part of the data and the core value in the frame header may be discarded
#define BLOCK_COUNTER_BUFFER_SIZE (128*1024)
-#define ANNOTATE_BUFFER_SIZE (64*1024) // annotate counters have the core as part of the data and the core value in the frame header may be discarded
+#define ANNOTATE_BUFFER_SIZE (64*1024) // annotate counters have the core as part of the data and the core value in the frame header may be discarded
#define SCHED_TRACE_BUFFER_SIZE (128*1024)
-#define GPU_TRACE_BUFFER_SIZE (64*1024) // gpu trace counters have the core as part of the data and the core value in the frame header may be discarded
-#define IDLE_BUFFER_SIZE (32*1024) // idle counters have the core as part of the data and the core value in the frame header may be discarded
+#define GPU_TRACE_BUFFER_SIZE (64*1024) // gpu trace counters have the core as part of the data and the core value in the frame header may be discarded
+#define IDLE_BUFFER_SIZE (32*1024) // idle counters have the core as part of the data and the core value in the frame header may be discarded
#define NO_COOKIE 0U
#define INVALID_COOKIE ~0U
#define MESSAGE_SCHED_SWITCH 1
#define MESSAGE_SCHED_EXIT 2
+#define MESSAGE_IDLE_ENTER 1
+#define MESSAGE_IDLE_EXIT 2
+
#define MAXSIZE_PACK32 5
#define MAXSIZE_PACK64 10
-#define MAXSIZE_CORE_NAME 32
+
+#define FRAME_HEADER_SIZE 3
#if defined(__arm__)
#define PC_REG regs->ARM_pc
* Globals
******************************************************************************/
static unsigned long gator_cpu_cores;
+// Size of the largest buffer. Effectively constant, set in gator_op_create_files
static unsigned long userspace_buffer_size;
static unsigned long gator_backtrace_depth;
+// How often to commit the buffers for live in nanoseconds
+static u64 gator_live_rate;
static unsigned long gator_started;
-static uint64_t monotonic_started;
+static u64 gator_monotonic_started;
static unsigned long gator_buffer_opened;
static unsigned long gator_timer_count;
static unsigned long gator_response_type;
static DEFINE_MUTEX(start_mutex);
static DEFINE_MUTEX(gator_buffer_mutex);
+bool event_based_sampling;
+
static DECLARE_WAIT_QUEUE_HEAD(gator_buffer_wait);
+static DECLARE_WAIT_QUEUE_HEAD(gator_annotate_wait);
static struct timer_list gator_buffer_wake_up_timer;
static LIST_HEAD(gator_events);
+static DEFINE_PER_CPU(u64, last_timestamp);
+
+static bool printed_monotonic_warning;
+
+static bool sent_core_name[NR_CPUS];
+
/******************************************************************************
* Prototypes
******************************************************************************/
-static void buffer_check(int cpu, int buftype);
+static void buffer_check(int cpu, int buftype, u64 time);
+static void gator_commit_buffer(int cpu, int buftype, u64 time);
static int buffer_bytes_available(int cpu, int buftype);
static bool buffer_check_space(int cpu, int buftype, int bytes);
static int contiguous_space_available(int cpu, int bufytpe);
-static void gator_buffer_write_packed_int(int cpu, int buftype, unsigned int x);
-static void gator_buffer_write_packed_int64(int cpu, int buftype, unsigned long long x);
+static void gator_buffer_write_packed_int(int cpu, int buftype, int x);
+static void gator_buffer_write_packed_int64(int cpu, int buftype, long long x);
static void gator_buffer_write_bytes(int cpu, int buftype, const char *x, int len);
static void gator_buffer_write_string(int cpu, int buftype, const char *x);
static void gator_add_trace(int cpu, unsigned long address);
-static void gator_add_sample(int cpu, struct pt_regs * const regs);
-static uint64_t gator_get_time(void);
+static void gator_add_sample(int cpu, struct pt_regs *const regs);
+static u64 gator_get_time(void);
+// Size of the buffer, must be a power of 2. Effectively constant, set in gator_op_setup.
static uint32_t gator_buffer_size[NUM_GATOR_BUFS];
+// gator_buffer_size - 1, bitwise and with pos to get offset into the array. Effectively constant, set in gator_op_setup.
static uint32_t gator_buffer_mask[NUM_GATOR_BUFS];
+// Read position in the buffer. Initialized to zero in gator_op_setup and incremented after bytes are read by userspace in userspace_buffer_read
static DEFINE_PER_CPU(int[NUM_GATOR_BUFS], gator_buffer_read);
+// Write position in the buffer. Initialized to zero in gator_op_setup and incremented after bytes are written to the buffer
static DEFINE_PER_CPU(int[NUM_GATOR_BUFS], gator_buffer_write);
+// Commit position in the buffer. Initialized to zero in gator_op_setup and incremented after a frame is ready to be read by userspace
static DEFINE_PER_CPU(int[NUM_GATOR_BUFS], gator_buffer_commit);
+// If set to false, decreases the number of bytes returned by buffer_bytes_available. Set in buffer_check_space if no space is remaining. Initialized to true in gator_op_setup
+// This means that if we run out of space, continue to report that no space is available until bytes are read by userspace
static DEFINE_PER_CPU(int[NUM_GATOR_BUFS], buffer_space_available);
+// The buffer. Allocated in gator_op_setup
static DEFINE_PER_CPU(char *[NUM_GATOR_BUFS], gator_buffer);
+#if GATOR_LIVE
+// The time after which the buffer should be committed for live display
+static DEFINE_PER_CPU(u64, gator_buffer_commit_time);
+#endif
+
/******************************************************************************
* Application Includes
******************************************************************************/
/******************************************************************************
* Misc
******************************************************************************/
-#if defined(__arm__) || defined(__aarch64__)
+
+const struct gator_cpu gator_cpus[] = {
+ {
+ .cpuid = ARM1136,
+ .core_name = "ARM1136",
+ .pmnc_name = "ARM_ARM11",
+ .pmnc_counters = 3,
+ },
+ {
+ .cpuid = ARM1156,
+ .core_name = "ARM1156",
+ .pmnc_name = "ARM_ARM11",
+ .pmnc_counters = 3,
+ },
+ {
+ .cpuid = ARM1176,
+ .core_name = "ARM1176",
+ .pmnc_name = "ARM_ARM11",
+ .pmnc_counters = 3,
+ },
+ {
+ .cpuid = ARM11MPCORE,
+ .core_name = "ARM11MPCore",
+ .pmnc_name = "ARM_ARM11MPCore",
+ .pmnc_counters = 3,
+ },
+ {
+ .cpuid = CORTEX_A5,
+ .core_name = "Cortex-A5",
+ .pmu_name = "ARMv7_Cortex_A5",
+ .pmnc_name = "ARM_Cortex-A5",
+ .pmnc_counters = 2,
+ },
+ {
+ .cpuid = CORTEX_A7,
+ .core_name = "Cortex-A7",
+ .pmu_name = "ARMv7_Cortex_A7",
+ .pmnc_name = "ARM_Cortex-A7",
+ .pmnc_counters = 4,
+ },
+ {
+ .cpuid = CORTEX_A8,
+ .core_name = "Cortex-A8",
+ .pmu_name = "ARMv7_Cortex_A8",
+ .pmnc_name = "ARM_Cortex-A8",
+ .pmnc_counters = 4,
+ },
+ {
+ .cpuid = CORTEX_A9,
+ .core_name = "Cortex-A9",
+ .pmu_name = "ARMv7_Cortex_A9",
+ .pmnc_name = "ARM_Cortex-A9",
+ .pmnc_counters = 6,
+ },
+ {
+ .cpuid = CORTEX_A15,
+ .core_name = "Cortex-A15",
+ .pmu_name = "ARMv7_Cortex_A15",
+ .pmnc_name = "ARM_Cortex-A15",
+ .pmnc_counters = 6,
+ },
+ {
+ .cpuid = SCORPION,
+ .core_name = "Scorpion",
+ .pmnc_name = "Scorpion",
+ .pmnc_counters = 4,
+ },
+ {
+ .cpuid = SCORPIONMP,
+ .core_name = "ScorpionMP",
+ .pmnc_name = "ScorpionMP",
+ .pmnc_counters = 4,
+ },
+ {
+ .cpuid = KRAITSIM,
+ .core_name = "KraitSIM",
+ .pmnc_name = "Krait",
+ .pmnc_counters = 4,
+ },
+ {
+ .cpuid = KRAIT,
+ .core_name = "Krait",
+ .pmnc_name = "Krait",
+ .pmnc_counters = 4,
+ },
+ {
+ .cpuid = KRAIT_S4_PRO,
+ .core_name = "Krait S4 Pro",
+ .pmnc_name = "Krait",
+ .pmnc_counters = 4,
+ },
+ {
+ .cpuid = CORTEX_A53,
+ .core_name = "Cortex-A53",
+ .pmnc_name = "ARM_Cortex-A53",
+ .pmnc_counters = 6,
+ },
+ {
+ .cpuid = CORTEX_A57,
+ .core_name = "Cortex-A57",
+ .pmnc_name = "ARM_Cortex-A57",
+ .pmnc_counters = 6,
+ },
+ {
+ .cpuid = AARCH64,
+ .core_name = "AArch64",
+ .pmnc_name = "ARM_AArch64",
+ .pmnc_counters = 6,
+ },
+ {
+ .cpuid = OTHER,
+ .core_name = "Other",
+ .pmnc_name = "Other",
+ .pmnc_counters = 6,
+ },
+ {}
+};
+
+const struct gator_cpu *gator_find_cpu_by_cpuid(const u32 cpuid)
+{
+ int i;
+
+ for (i = 0; gator_cpus[i].cpuid != 0; ++i) {
+ const struct gator_cpu *const gator_cpu = &gator_cpus[i];
+ if (gator_cpu->cpuid == cpuid) {
+ return gator_cpu;
+ }
+ }
+
+ return NULL;
+}
+
+const struct gator_cpu *gator_find_cpu_by_pmu_name(const char *const name)
+{
+ int i;
+
+ for (i = 0; gator_cpus[i].cpuid != 0; ++i) {
+ const struct gator_cpu *const gator_cpu = &gator_cpus[i];
+ if (gator_cpu->pmu_name != NULL && strcmp(gator_cpu->pmu_name, name) == 0) {
+ return gator_cpu;
+ }
+ }
+
+ return NULL;
+}
+
u32 gator_cpuid(void)
{
+#if defined(__arm__) || defined(__aarch64__)
u32 val;
#if !defined(__aarch64__)
asm volatile("mrc p15, 0, %0, c0, c0, 0" : "=r" (val));
asm volatile("mrs %0, midr_el1" : "=r" (val));
#endif
return (val >> 4) & 0xfff;
-}
+#else
+ return OTHER;
#endif
+}
static void gator_buffer_wake_up(unsigned long data)
{
/******************************************************************************
* Commit interface
******************************************************************************/
-static bool buffer_commit_ready(int* cpu, int* buftype)
+static bool buffer_commit_ready(int *cpu, int *buftype)
{
int cpu_x, x;
for_each_present_cpu(cpu_x) {
return true;
}
}
+ *cpu = -1;
+ *buftype = -1;
return false;
}
@@ -265,7 +447,7 @@ static void gator_buffer_write_bytes(int cpu, int buftype, const char *x, int le
int i;
u32 write = per_cpu(gator_buffer_write, cpu)[buftype];
u32 mask = gator_buffer_mask[buftype];
- char* buffer = per_cpu(gator_buffer, cpu)[buftype];
+ char *buffer = per_cpu(gator_buffer, cpu)[buftype];
for (i = 0; i < len; i++) {
buffer[write] = x[i];
gator_buffer_write_bytes(cpu, buftype, x, len);
}
-static void gator_buffer_header(int cpu, int buftype)
+static void gator_commit_buffer(int cpu, int buftype, u64 time)
{
- int frame;
+ int type_length, commit, length, byte;
- switch (buftype) {
- case SUMMARY_BUF:
- frame = FRAME_SUMMARY;
- break;
- case BACKTRACE_BUF:
- frame = FRAME_BACKTRACE;
- break;
- case NAME_BUF:
- frame = FRAME_NAME;
- break;
- case COUNTER_BUF:
- frame = FRAME_COUNTER;
- break;
- case BLOCK_COUNTER_BUF:
- frame = FRAME_BLOCK_COUNTER;
- break;
- case ANNOTATE_BUF:
- frame = FRAME_ANNOTATE;
- break;
- case SCHED_TRACE_BUF:
- frame = FRAME_SCHED_TRACE;
- break;
- case GPU_TRACE_BUF:
- frame = FRAME_GPU_TRACE;
- break;
- case IDLE_BUF:
- frame = FRAME_IDLE;
- break;
- default:
- frame = -1;
- break;
- }
+ if (!per_cpu(gator_buffer, cpu)[buftype])
+ return;
- if (per_cpu(gator_buffer, cpu)[buftype]) {
- marshal_frame(cpu, buftype, frame);
+ // post-populate the length, which does not include the response type length nor the length itself, i.e. only the length of the payload
+ type_length = gator_response_type ? 1 : 0;
+ commit = per_cpu(gator_buffer_commit, cpu)[buftype];
+ length = per_cpu(gator_buffer_write, cpu)[buftype] - commit;
+ if (length < 0) {
+ length += gator_buffer_size[buftype];
}
-}
+ length = length - type_length - sizeof(s32);
-static void gator_commit_buffer(int cpu, int buftype)
-{
- if (!per_cpu(gator_buffer, cpu)[buftype])
+ if (length <= FRAME_HEADER_SIZE) {
+ // Nothing to write, only the frame header is present
return;
+ }
+
+ for (byte = 0; byte < sizeof(s32); byte++) {
+ per_cpu(gator_buffer, cpu)[buftype][(commit + type_length + byte) & gator_buffer_mask[buftype]] = (length >> byte * 8) & 0xFF;
+ }
per_cpu(gator_buffer_commit, cpu)[buftype] = per_cpu(gator_buffer_write, cpu)[buftype];
- gator_buffer_header(cpu, buftype);
+
+#if GATOR_LIVE
+ if (gator_live_rate > 0) {
+ while (time > per_cpu(gator_buffer_commit_time, cpu)) {
+ per_cpu(gator_buffer_commit_time, cpu) += gator_live_rate;
+ }
+ }
+#endif
+
+ marshal_frame(cpu, buftype);
// had to delay scheduling work as attempting to schedule work during the context switch is illegal in kernel versions 3.5 and greater
mod_timer(&gator_buffer_wake_up_timer, jiffies + 1);
}
-static void buffer_check(int cpu, int buftype)
+static void buffer_check(int cpu, int buftype, u64 time)
{
int filled = per_cpu(gator_buffer_write, cpu)[buftype] - per_cpu(gator_buffer_commit, cpu)[buftype];
if (filled < 0) {
filled += gator_buffer_size[buftype];
}
if (filled >= ((gator_buffer_size[buftype] * 3) / 4)) {
- gator_commit_buffer(cpu, buftype);
+ gator_commit_buffer(cpu, buftype, time);
}
}
marshal_backtrace(offset & ~1, cookie);
}
-static void gator_add_sample(int cpu, struct pt_regs * const regs)
+static void gator_add_sample(int cpu, struct pt_regs *const regs)
{
bool inKernel;
unsigned long exec_cookie;
******************************************************************************/
static void gator_timer_interrupt(void)
{
- struct pt_regs * const regs = get_irq_regs();
+ struct pt_regs *const regs = get_irq_regs();
gator_backtrace_handler(regs);
}
-void gator_backtrace_handler(struct pt_regs * const regs)
+void gator_backtrace_handler(struct pt_regs *const regs)
{
- int cpu = smp_processor_id();
+ int cpu = get_physical_cpu();
// Output backtrace
gator_add_sample(cpu, regs);
static int gator_running;
// This function runs in interrupt context and on the appropriate core
-static void gator_timer_offline(void* unused)
+static void gator_timer_offline(void *migrate)
{
struct gator_interface *gi;
- int i, len, cpu = smp_processor_id();
- int* buffer;
+ int i, len, cpu = get_physical_cpu();
+ int *buffer;
+ u64 time;
gator_trace_sched_offline();
gator_trace_power_offline();
- gator_hrtimer_offline(cpu);
+ if (!migrate) {
+ gator_hrtimer_offline();
+ }
// Offline any events and output counters
- if (marshal_event_header()) {
+ time = gator_get_time();
+ if (marshal_event_header(time)) {
list_for_each_entry(gi, &gator_events, list) {
if (gi->offline) {
- len = gi->offline(&buffer);
+ len = gi->offline(&buffer, migrate);
marshal_event(len, buffer);
}
}
+ // Only check after writing all counters so that time and corresponding counters appear in the same frame
+ buffer_check(cpu, BLOCK_COUNTER_BUF, time);
}
// Flush all buffers on this core
for (i = 0; i < NUM_GATOR_BUFS; i++)
- gator_commit_buffer(cpu, i);
+ gator_commit_buffer(cpu, i, time);
}
-// This function runs in process context and may be running on a core other than core 'cpu'
-static void gator_timer_offline_dispatch(int cpu)
+// This function runs in interrupt context and may be running on a core other than core 'cpu'
+static void gator_timer_offline_dispatch(int cpu, bool migrate)
{
struct gator_interface *gi;
- list_for_each_entry(gi, &gator_events, list)
- if (gi->offline_dispatch)
- gi->offline_dispatch(cpu);
+ list_for_each_entry(gi, &gator_events, list) {
+ if (gi->offline_dispatch) {
+ gi->offline_dispatch(cpu, migrate);
+ }
+ }
}
static void gator_timer_stop(void)
if (gator_running) {
on_each_cpu(gator_timer_offline, NULL, 1);
for_each_online_cpu(cpu) {
- gator_timer_offline_dispatch(cpu);
+ gator_timer_offline_dispatch(lcpu_to_pcpu(cpu), false);
}
gator_running = 0;
}
// This function runs in interrupt context and on the appropriate core
-static void gator_timer_online(void* unused)
+static void gator_timer_online(void *migrate)
{
struct gator_interface *gi;
- int len, cpu = smp_processor_id();
- int* buffer;
+ int len, cpu = get_physical_cpu();
+ int *buffer;
+ u64 time;
gator_trace_power_online();
// online any events and output counters
- if (marshal_event_header()) {
+ time = gator_get_time();
+ if (marshal_event_header(time)) {
list_for_each_entry(gi, &gator_events, list) {
if (gi->online) {
- len = gi->online(&buffer);
+ len = gi->online(&buffer, migrate);
marshal_event(len, buffer);
}
}
+ // Only check after writing all counters so that time and corresponding counters appear in the same frame
+ buffer_check(cpu, BLOCK_COUNTER_BUF, time);
+ }
+
+ if (!migrate) {
+ gator_hrtimer_online();
}
- gator_hrtimer_online(cpu);
#if defined(__arm__) || defined(__aarch64__)
- {
- const char * core_name = NULL;
-
- // String lengths must be less than MAXSIZE_CORE_NAME
- switch (gator_cpuid()) {
- case ARM1136: core_name = "ARM1136"; break;
- case ARM1156: core_name = "ARM1156"; break;
- case ARM1176: core_name = "ARM1176"; break;
- case ARM11MPCORE: core_name = "ARM11MPCore"; break;
- case CORTEX_A5: core_name = "Cortex-A5"; break;
- case CORTEX_A7: core_name = "Cortex-A7"; break;
- case CORTEX_A8: core_name = "Cortex-A8"; break;
- case CORTEX_A9: core_name = "Cortex-A9"; break;
- case CORTEX_A15: core_name = "Cortex-A15"; break;
- case SCORPION: core_name = "Scorpion"; break;
- case SCORPIONMP: core_name = "ScorpionMP"; break;
- case KRAITSIM: core_name = "KraitSIM"; break;
- case KRAIT: core_name = "Krait"; break;
- case AARCH64: core_name = "AArch64"; break;
- default: core_name = "Unknown"; break;
+ if (!sent_core_name[cpu]) {
+ const char *core_name = NULL;
+ const u32 cpuid = gator_cpuid();
+ const struct gator_cpu *const gator_cpu = gator_find_cpu_by_cpuid(cpuid);
+ char core_name_buf[32];
+
+ if (gator_cpu != NULL) {
+ core_name = gator_cpu->core_name;
+ } else {
+ snprintf(core_name_buf, sizeof(core_name_buf), "Unknown (0x%.3x)", cpuid);
+ core_name = core_name_buf;
}
- marshal_core_name(core_name);
+ marshal_core_name(cpuid, core_name);
+ sent_core_name[cpu] = true;
}
#endif
}
// This function runs in interrupt context and may be running on a core other than core 'cpu'
-static void gator_timer_online_dispatch(int cpu)
+static void gator_timer_online_dispatch(int cpu, bool migrate)
{
struct gator_interface *gi;
- list_for_each_entry(gi, &gator_events, list)
- if (gi->online_dispatch)
- gi->online_dispatch(cpu);
+ list_for_each_entry(gi, &gator_events, list) {
+ if (gi->online_dispatch) {
+ gi->online_dispatch(cpu, migrate);
+ }
+ }
}
int gator_timer_start(unsigned long sample_rate)
gator_running = 1;
+ // event based sampling trumps hr timer based sampling
+ if (event_based_sampling) {
+ sample_rate = 0;
+ }
+
if (gator_hrtimer_init(sample_rate, gator_timer_interrupt) == -1)
return -1;
for_each_online_cpu(cpu) {
- gator_timer_online_dispatch(cpu);
+ gator_timer_online_dispatch(lcpu_to_pcpu(cpu), false);
}
on_each_cpu(gator_timer_online, NULL, 1);
return 0;
}
-static uint64_t gator_get_time(void)
+static u64 gator_get_time(void)
{
struct timespec ts;
- uint64_t timestamp;
+ u64 timestamp;
+ u64 prev_timestamp;
+ u64 delta;
+ int cpu = smp_processor_id();
- //getnstimeofday(&ts);
- do_posix_clock_monotonic_gettime(&ts);
- timestamp = timespec_to_ns(&ts) - monotonic_started;
+ // Match clock_gettime(CLOCK_MONOTONIC_RAW, &ts) from userspace
+ getrawmonotonic(&ts);
+ timestamp = timespec_to_ns(&ts);
- return timestamp;
+ // getrawmonotonic is not monotonic on all systems. Detect and attempt to correct these cases.
+ // up to 0.5ms delta has been seen on some systems, which can skew Streamline data when viewing at high resolution.
+ prev_timestamp = per_cpu(last_timestamp, cpu);
+ if (prev_timestamp <= timestamp) {
+ per_cpu(last_timestamp, cpu) = timestamp;
+ } else {
+ delta = prev_timestamp - timestamp;
+ // Log the error once
+ if (!printed_monotonic_warning && delta > 500000) {
+ printk(KERN_ERR "%s: getrawmonotonic is not monotonic cpu: %i delta: %lli\nSkew in Streamline data may be present at the fine zoom levels\n", __FUNCTION__, cpu, delta);
+ printed_monotonic_warning = true;
+ }
+ timestamp = prev_timestamp;
+ }
+
+ return timestamp - gator_monotonic_started;
}
/******************************************************************************
* cpu hotplug and pm notifiers
******************************************************************************/
+#include "gator_iks.c"
+
static int __cpuinit gator_hotcpu_notify(struct notifier_block *self, unsigned long action, void *hcpu)
{
- long cpu = (long)hcpu;
+ int cpu = lcpu_to_pcpu((long)hcpu);
switch (action) {
- case CPU_DOWN_PREPARE:
- case CPU_DOWN_PREPARE_FROZEN:
- smp_call_function_single(cpu, gator_timer_offline, NULL, 1);
- gator_timer_offline_dispatch(cpu);
- break;
- case CPU_ONLINE:
- case CPU_ONLINE_FROZEN:
- gator_timer_online_dispatch(cpu);
- smp_call_function_single(cpu, gator_timer_online, NULL, 1);
- break;
+ case CPU_DOWN_PREPARE:
+ case CPU_DOWN_PREPARE_FROZEN:
+ smp_call_function_single(cpu, gator_timer_offline, NULL, 1);
+ gator_timer_offline_dispatch(cpu, false);
+ break;
+ case CPU_ONLINE:
+ case CPU_ONLINE_FROZEN:
+ gator_timer_online_dispatch(cpu, false);
+ smp_call_function_single(cpu, gator_timer_online, NULL, 1);
+ break;
}
return NOTIFY_OK;
@@ -589,24 +792,24 @@ static int gator_pm_notify(struct notifier_block *nb, unsigned long event, void
int cpu;
switch (event) {
- case PM_HIBERNATION_PREPARE:
- case PM_SUSPEND_PREPARE:
- unregister_hotcpu_notifier(&gator_hotcpu_notifier);
- unregister_scheduler_tracepoints();
- on_each_cpu(gator_timer_offline, NULL, 1);
- for_each_online_cpu(cpu) {
- gator_timer_offline_dispatch(cpu);
- }
- break;
- case PM_POST_HIBERNATION:
- case PM_POST_SUSPEND:
- for_each_online_cpu(cpu) {
- gator_timer_online_dispatch(cpu);
- }
- on_each_cpu(gator_timer_online, NULL, 1);
- register_scheduler_tracepoints();
- register_hotcpu_notifier(&gator_hotcpu_notifier);
- break;
+ case PM_HIBERNATION_PREPARE:
+ case PM_SUSPEND_PREPARE:
+ unregister_hotcpu_notifier(&gator_hotcpu_notifier);
+ unregister_scheduler_tracepoints();
+ on_each_cpu(gator_timer_offline, NULL, 1);
+ for_each_online_cpu(cpu) {
+ gator_timer_offline_dispatch(lcpu_to_pcpu(cpu), false);
+ }
+ break;
+ case PM_POST_HIBERNATION:
+ case PM_POST_SUSPEND:
+ for_each_online_cpu(cpu) {
+ gator_timer_online_dispatch(lcpu_to_pcpu(cpu), false);
+ }
+ on_each_cpu(gator_timer_online, NULL, 1);
+ register_scheduler_tracepoints();
+ register_hotcpu_notifier(&gator_hotcpu_notifier);
+ break;
}
return NOTIFY_OK;
******************************************************************************/
static void gator_summary(void)
{
- uint64_t timestamp;
- struct timespec uptime_ts;
+ u64 timestamp, uptime;
+ struct timespec ts;
+ char uname_buf[512];
+ void (*m2b)(struct timespec *ts);
+ unsigned long flags;
+
+ snprintf(uname_buf, sizeof(uname_buf), "%s %s %s %s %s GNU/Linux", utsname()->sysname, utsname()->nodename, utsname()->release, utsname()->version, utsname()->machine);
+
+ getnstimeofday(&ts);
+ timestamp = timespec_to_ns(&ts);
- timestamp = gator_get_time();
+ do_posix_clock_monotonic_gettime(&ts);
+ // monotonic_to_bootbased is not defined for some versions of Android
+ m2b = symbol_get(monotonic_to_bootbased);
+ if (m2b) {
+ m2b(&ts);
+ }
+ uptime = timespec_to_ns(&ts);
- do_posix_clock_monotonic_gettime(&uptime_ts);
- monotonic_started = timespec_to_ns(&uptime_ts);
+ // Disable interrupts as gator_get_time calls smp_processor_id to verify time is monotonic
+ local_irq_save(flags);
+ // Set monotonic_started to zero as gator_get_time is uptime minus monotonic_started
+ gator_monotonic_started = 0;
+ gator_monotonic_started = gator_get_time();
+ local_irq_restore(flags);
- marshal_summary(timestamp, monotonic_started);
+ marshal_summary(timestamp, uptime, uname_buf);
}
int gator_events_install(struct gator_interface *interface)
// key of zero is reserved as a timestamp
static int key = 1;
- return key++;
+ const int ret = key;
+ key += 2;
+ return ret;
}
static int gator_init(void)
{
int i;
+ calc_first_cluster_size();
+
// events sources (gator_events.h, generated by gator_events.sh)
for (i = 0; i < ARRAY_SIZE(gator_events_list); i++)
if (gator_events_list[i])
gator_events_list[i]();
+ gator_trace_sched_init();
gator_trace_power_init();
return 0;
}
+static void gator_exit(void)
+{
+ struct gator_interface *gi;
+
+ list_for_each_entry(gi, &gator_events, list)
+ if (gi->shutdown)
+ gi->shutdown();
+}
+
static int gator_start(void)
{
unsigned long cpu, i;
struct gator_interface *gi;
+ if (gator_migrate_start())
+ goto migrate_failure;
+
// Initialize the buffer with the frame type and core
for_each_present_cpu(cpu) {
for (i = 0; i < NUM_GATOR_BUFS; i++) {
- gator_buffer_header(cpu, i);
+ marshal_frame(cpu, i);
}
+ per_cpu(last_timestamp, cpu) = 0;
}
+ printed_monotonic_warning = false;
- // Capture the start time
+ // Capture the start time
gator_summary();
// start all events
if (gi->stop)
gi->stop();
events_failure:
+ gator_migrate_stop();
+migrate_failure:
return -1;
}
gator_trace_gpu_stop();
// stop all interrupt callback reads before tearing down other interfaces
- gator_notifier_stop(); // should be called before gator_timer_stop to avoid re-enabling the hrtimer after it has been offlined
+ gator_notifier_stop(); // should be called before gator_timer_stop to avoid re-enabling the hrtimer after it has been offlined
gator_timer_stop();
// stop all events
list_for_each_entry(gi, &gator_events, list)
if (gi->stop)
gi->stop();
+
+ gator_migrate_stop();
}
/******************************************************************************
per_cpu(gator_buffer_write, cpu)[i] = 0;
per_cpu(gator_buffer_commit, cpu)[i] = 0;
per_cpu(buffer_space_available, cpu)[i] = true;
+#if GATOR_LIVE
+ per_cpu(gator_buffer_commit_time, cpu) = gator_live_rate;
+#endif
// Annotation is a special case that only uses a single buffer
if (cpu > 0 && i == ANNOTATE_BUF) {
mutex_lock(&gator_buffer_mutex);
gator_started = 0;
+ gator_monotonic_started = 0;
cookies_release();
wake_up(&gator_buffer_wait);
per_cpu(gator_buffer_write, cpu)[i] = 0;
per_cpu(gator_buffer_commit, cpu)[i] = 0;
per_cpu(buffer_space_available, cpu)[i] = true;
+#if GATOR_LIVE
+ per_cpu(gator_buffer_commit_time, cpu) = 0;
+#endif
}
mutex_unlock(&gator_buffer_mutex);
}
+ memset(&sent_core_name, 0, sizeof(sent_core_name));
+
mutex_unlock(&start_mutex);
}
@@ -941,8 +1194,8 @@ static ssize_t enable_write(struct file *file, char const __user *buf, size_t co
}
static const struct file_operations enable_fops = {
- .read = enable_read,
- .write = enable_write,
+ .read = enable_read,
+ .write = enable_write,
};
static int userspace_buffer_open(struct inode *inode, struct file *file)
return 0;
}
-static ssize_t userspace_buffer_read(struct file *file, char __user *buf,
- size_t count, loff_t *offset)
+static ssize_t userspace_buffer_read(struct file *file, char __user *buf, size_t count, loff_t *offset)
{
- int retval = -EINVAL;
- int commit = 0, length, length1, length2, read, byte, type_length;
+ int commit, length1, length2, read;
char *buffer1;
- char *buffer2 = NULL;
+ char *buffer2;
int cpu, buftype;
+ int written = 0;
- /* do not handle partial reads */
- if (count != userspace_buffer_size || *offset)
+ // ensure there is enough space for a whole frame
+ if (count < userspace_buffer_size || *offset) {
return -EINVAL;
+ }
// sleep until the condition is true or a signal is received
// the condition is checked each time gator_buffer_wait is woken up
- buftype = cpu = -1;
wait_event_interruptible(gator_buffer_wait, buffer_commit_ready(&cpu, &buftype) || !gator_started);
- if (signal_pending(current))
+ if (signal_pending(current)) {
return -EINTR;
+ }
- length2 = 0;
- retval = -EFAULT;
+ if (buftype == -1 || cpu == -1) {
+ return 0;
+ }
mutex_lock(&gator_buffer_mutex);
- if (buftype == -1 || cpu == -1) {
- retval = 0;
- goto out;
- }
+ do {
+ read = per_cpu(gator_buffer_read, cpu)[buftype];
+ commit = per_cpu(gator_buffer_commit, cpu)[buftype];
- read = per_cpu(gator_buffer_read, cpu)[buftype];
- commit = per_cpu(gator_buffer_commit, cpu)[buftype];
+ // May happen if the buffer is freed during pending reads.
+ if (!per_cpu(gator_buffer, cpu)[buftype]) {
+ break;
+ }
- /* May happen if the buffer is freed during pending reads. */
- if (!per_cpu(gator_buffer, cpu)[buftype]) {
- retval = -EFAULT;
- goto out;
- }
+ // determine the size of two halves
+ length1 = commit - read;
+ length2 = 0;
+ buffer1 = &(per_cpu(gator_buffer, cpu)[buftype][read]);
+ buffer2 = &(per_cpu(gator_buffer, cpu)[buftype][0]);
+ if (length1 < 0) {
+ length1 = gator_buffer_size[buftype] - read;
+ length2 = commit;
+ }
- /* determine the size of two halves */
- length1 = commit - read;
- buffer1 = &(per_cpu(gator_buffer, cpu)[buftype][read]);
- buffer2 = &(per_cpu(gator_buffer, cpu)[buftype][0]);
- if (length1 < 0) {
- length1 = gator_buffer_size[buftype] - read;
- length2 = commit;
- }
+ if (length1 + length2 > count - written) {
+ break;
+ }
- // post-populate the length, which does not include the response type length nor the length itself, i.e. only the length of the payload
- type_length = gator_response_type ? 1 : 0;
- length = length1 + length2 - type_length - sizeof(int);
- for (byte = 0; byte < sizeof(int); byte++) {
- per_cpu(gator_buffer, cpu)[buftype][(read + type_length + byte) & gator_buffer_mask[buftype]] = (length >> byte * 8) & 0xFF;
- }
+ // start, middle or end
+ if (length1 > 0 && copy_to_user(&buf[written], buffer1, length1)) {
+ break;
+ }
- /* start, middle or end */
- if (length1 > 0) {
- if (copy_to_user(&buf[0], buffer1, length1)) {
- goto out;
+ // possible wrap around
+ if (length2 > 0 && copy_to_user(&buf[written + length1], buffer2, length2)) {
+ break;
}
- }
- /* possible wrap around */
- if (length2 > 0) {
- if (copy_to_user(&buf[length1], buffer2, length2)) {
- goto out;
+ per_cpu(gator_buffer_read, cpu)[buftype] = commit;
+ written += length1 + length2;
+
+ // Wake up annotate_write if more space is available
+ if (buftype == ANNOTATE_BUF) {
+ wake_up(&gator_annotate_wait);
}
- }
+ } while (buffer_commit_ready(&cpu, &buftype));
- per_cpu(gator_buffer_read, cpu)[buftype] = commit;
- retval = length1 + length2;
+ mutex_unlock(&gator_buffer_mutex);
- /* kick just in case we've lost an SMP event */
+ // kick just in case we've lost an SMP event
wake_up(&gator_buffer_wait);
-out:
- mutex_unlock(&gator_buffer_mutex);
- return retval;
+ return written > 0 ? written : -EFAULT;
}
const struct file_operations gator_event_buffer_fops = {
- .open = userspace_buffer_open,
- .release = userspace_buffer_release,
- .read = userspace_buffer_read,
+ .open = userspace_buffer_open,
+ .release = userspace_buffer_release,
+ .read = userspace_buffer_read,
};
static ssize_t depth_read(struct file *file, char __user *buf, size_t count, loff_t *offset)
{
- return gatorfs_ulong_to_user(gator_backtrace_depth, buf, count,
- offset);
+ return gatorfs_ulong_to_user(gator_backtrace_depth, buf, count, offset);
}
static ssize_t depth_write(struct file *file, char const __user *buf, size_t count, loff_t *offset)
@@ -1090,8 +1338,8 @@ static ssize_t depth_write(struct file *file, char const __user *buf, size_t cou
}
static const struct file_operations depth_fops = {
- .read = depth_read,
- .write = depth_write
+ .read = depth_read,
+ .write = depth_write
};
void gator_op_create_files(struct super_block *sb, struct dentry *root)
for_each_present_cpu(cpu) {
gator_cpu_cores++;
}
- userspace_buffer_size = BACKTRACE_BUFFER_SIZE;
+ userspace_buffer_size = BACKTRACE_BUFFER_SIZE;
gator_response_type = 1;
+ gator_live_rate = 0;
gatorfs_create_file(sb, root, "enable", &enable_fops);
gatorfs_create_file(sb, root, "buffer", &gator_event_buffer_fops);
gatorfs_create_ulong(sb, root, "tick", &gator_timer_count);
gatorfs_create_ulong(sb, root, "response_type", &gator_response_type);
gatorfs_create_ro_ulong(sb, root, "version", &gator_protocol_version);
+ gatorfs_create_ro_u64(sb, root, "started", &gator_monotonic_started);
+ gatorfs_create_u64(sb, root, "live_rate", &gator_live_rate);
// Annotate interface
gator_annotate_create_files(sb, root);
if (gi->create_files)
gi->create_files(sb, dir);
+ // Sched Events
+ sched_trace_create_files(sb, dir);
+
// Power interface
gator_trace_power_create_files(sb, dir);
}
{
del_timer_sync(&gator_buffer_wake_up_timer);
tracepoint_synchronize_unregister();
+ gator_exit();
gatorfs_unregister();
}