]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android-sdk/device-ti-proprietary-open.git/log
android-sdk/device-ti-proprietary-open.git
11 years agoUpdated Ducati installation logic
James W. Mills [Thu, 12 Apr 2012 19:06:05 +0000 (14:06 -0500)]
Updated Ducati installation logic

This patch moves the ducati installation logic into the top-level
Android.mk for proprietary-open, and generalizes the procedure so that
new devices can be added easily.  Benefis include:

* Unpacking into an intermediate location

* Only unpacked if enabled for a specific device

* All devices can use the same PRODUCT_PACKAGE definition

* User-defined ducati TGZ location

Change-Id: I48314920b138230e73b3a56e1ff899ad82289b59
Signed-off-by: James W. Mills <jameswmills@ti.com>
11 years agoBT: Upgraded BT firmware to Service Pack 1.2
Shitiz Kumar [Thu, 23 Feb 2012 23:34:59 +0000 (17:34 -0600)]
BT: Upgraded BT firmware to Service Pack 1.2

    SP1.2 @TI_P1.38

Change-Id: I6cc49cb13752e1d430c022f51538b6bb5df3283a
Signed-off-by: Shitiz Kumar <shitiz_kumar@ti.com>
11 years agodevice:ti:proprietary-open: Add BT firmware script for COM8
Manjunatha Halli [Wed, 15 Feb 2012 18:13:27 +0000 (12:13 -0600)]
device:ti:proprietary-open: Add BT firmware script for COM8

Also this patch adds firmware scripts for FM TX on COM6 modules.

Should be merged with:  http://review.omapzoom.org/#/c/19195/

Change-Id: Ibb69f649a67e37fa8efee30889e3297e559bb540
Signed-off-by: Manjunatha Halli <x0130808@ti.com>
11 years agoSGX: DDK upgrade with NV12 texture fix on 1.8@796887
Hemant Hariyani [Tue, 21 Feb 2012 22:32:52 +0000 (16:32 -0600)]
SGX: DDK upgrade with NV12 texture fix on 1.8@796887

This upgrade fixes the problem where NV12 texture was not visible
when there was an RGB layer on top.

Change-Id: I206954e8e468f402e7ce19d779d5bf066578d339
Signed-off-by: Hemant Hariyani <hemanthariyani@ti.com>
11 years agoMerge "SGX: Upgrade SGX driver to version 1.8@796887" into ics-mr1
Jean Johnson [Thu, 16 Feb 2012 21:50:26 +0000 (15:50 -0600)]
Merge "SGX: Upgrade SGX driver to version 1.8@796887" into ics-mr1

11 years agoSGX: Upgrade SGX driver to version 1.8@796887
Hemant Hariyani [Thu, 16 Feb 2012 18:06:20 +0000 (12:06 -0600)]
SGX: Upgrade SGX driver to version 1.8@796887

SGX binaries for OMAP4. Version 1.8@796887.

Change-Id: I2b79d9c275a6519d1f9aea06fe6c6ae9d90b839a
Signed-off-by: Hemant Hariyani <hemanthariyani@ti.com>
11 years agodevice:ti:proprietary-open: add wpan firmware
Pavan Savoy [Thu, 2 Feb 2012 18:06:57 +0000 (12:06 -0600)]
device:ti:proprietary-open: add wpan firmware

Add the wpan.tgz firmware tarball which constitutes of the firmware and the
right LICENSE for them.
Also add in the line in Android.mk to untar them to the relevant folder from
where they will be picked up to be installed into the relevant folder on
/system/etc/firmware/.

Change-Id: Ie2a7af0febb072862bbeb45039625ba810923766
Signed-off-by: Pavan Savoy <pavan_savoy@ti.com>
Conflicts:

Android.mk

Signed-off-by: Pavan Savoy <pavan_savoy@ti.com>
11 years agoMerge "SGX: DDK update for 2D blit support" into ics-mr1
Jean Johnson [Sat, 28 Jan 2012 06:12:36 +0000 (00:12 -0600)]
Merge "SGX: DDK update for 2D blit support" into ics-mr1

11 years agoSGX: DDK update for 2D blit support
Tony Lofthouse [Sat, 28 Jan 2012 03:55:01 +0000 (21:55 -0600)]
SGX: DDK update for 2D blit support

From ti_ics_1.8 gerrit.ext.ti.com/img-ddk-linux-android

Commits:

d932e8d Merge "Gralloc: fb: Add a flag to force searching a free framebuffer if needed" into t

Change-Id: Ieb454b19c645b6a2ad77136b13f326d50f3f53d0
Signed-off-by: Tony Lofthouse <a0741364@ti.com>
11 years agoUpdate ducati mk files to use literal TARGET_PRODUCT values
James W. Mills [Fri, 27 Jan 2012 18:44:59 +0000 (12:44 -0600)]
Update ducati mk files to use literal TARGET_PRODUCT values

The build system sources ALL devices during the lunch command, and
this is causing it to look for ducati_$(TARGET_PRODUCT) files even
when there are not any.  Rewritten to be explicit about full_blaze and
blaze_tablet so that all devices behave as expected.

Change-Id: Ib73156f330b449682394e7fe7812d6f4e3a75a97
Signed-off-by: James W. Mills <jameswmills@ti.com>
11 years agoUpdated GFX for both 4430/60 and 4470
James W. Mills [Fri, 27 Jan 2012 00:23:04 +0000 (18:23 -0600)]
Updated GFX for both 4430/60 and 4470

These drivers should work for both 4430/4460 and 4470 boards

Change-Id: I67bf4d910ac776960aad6d043cd553cc6d545561
Signed-off-by: James W. Mills <jameswmills@ti.com>
11 years agoDucati binary fw and DCC files for Blaze
James W. Mills [Tue, 24 Jan 2012 20:53:48 +0000 (14:53 -0600)]
Ducati binary fw and DCC files for Blaze

This patch includes the files needed to install Ducati fw and DCC
files for the Blaze.

Versions of Ducati can be dropped in with an accompanying mk file, and
each device capable of using that version of ducati can include the
makefile at the device level.

Change-Id: I10a61dab74b18acc2de3d2af93094009770baba2
Signed-off-by: James W. Mills <jameswmills@ti.com>
11 years agoDucati binary fw and DCC files for Blaze Tablet
James W. Mills [Tue, 17 Jan 2012 20:25:14 +0000 (14:25 -0600)]
Ducati binary fw and DCC files for Blaze Tablet

This patch includes the files needed to install Ducati fw and DCC
files for the Blaze Tablet.

Versions of Ducati can be dropped in with an accompanying mk file, and
each device capable of using that version of ducati can include the
makefile at the device level

Change-Id: I1df3fb99eac48106032a404184f09668d0148cda
Signed-off-by: James W. Mills <jameswmills@ti.com>
11 years ago[proprietary-open] Update WLAN firmware file
Vishal Mahaveer [Thu, 12 Jan 2012 21:01:58 +0000 (15:01 -0600)]
[proprietary-open] Update WLAN firmware file

Updating WLAN firmware and plt files
  wl128x - 7.3.5.0.79 to 7.3.7.0.79
  wl127x - 6.3.5.0.79 to 6.3.7.0.79

Change-Id: I8fe5996bfcb26d517253f9e24ec43c73f878f7f9
Signed-off-by: Vishal Mahaveer <vishalm@ti.com>
11 years ago[proprietary-open] Update WLAN firmware file
Vishal Mahaveer [Mon, 9 Jan 2012 16:30:44 +0000 (10:30 -0600)]
[proprietary-open] Update WLAN firmware file

Updating WLAN firmware file for wl1283.

Change-Id: I4830c4a66057bd46cdcb2dc1094576f616dbcbe1
Signed-off-by: Vishal Mahaveer <vishalm@ti.com>
11 years agoproprietary-open - Update wl12xx/wlan firmware
Vishal Mahaveer [Mon, 19 Dec 2011 23:46:19 +0000 (17:46 -0600)]
proprietary-open - Update wl12xx/wlan firmware

Update WLAN firmware to R4_SP2 version

Change-Id: Ibb4eb34f113e93c4c21496d0a0f592b2d66c26b8
Signed-off-by: Vishal Mahaveer <vishalm@ti.com>
11 years agoUpdated DDK
James W. Mills [Wed, 21 Dec 2011 21:29:34 +0000 (15:29 -0600)]
Updated DDK

Change-Id: I3fa11aa320f825f5676f93875a44fb7c4957de34
Signed-off-by: James W. Mills <jameswmills@ti.com>
11 years agoNo longer force reinstallation on every build
James W. Mills [Tue, 20 Dec 2011 20:55:31 +0000 (14:55 -0600)]
No longer force reinstallation on every build

The tgz delivered content is no longer installed every time you run
make.  Instead, it adheres to normal Makefile rules.

Change-Id: Ia9f33f14b10b1706ad1f0e6d42fdeed4076b1414
Signed-off-by: James W. Mills <jameswmills@ti.com>
11 years agoMoved the ducati Android.mk into the filesystem, and updated the module name
James W. Mills [Thu, 15 Dec 2011 01:00:29 +0000 (19:00 -0600)]
Moved the ducati Android.mk into the filesystem, and updated the module name

Change-Id: I11fb179dc922118ba7e791621676d7bc6fe706ac
Signed-off-by: James W. Mills <jameswmills@ti.com>
11 years agoUpped the version of the DDK to match the kernel. I've also added the Android.mk...
James W. Mills [Wed, 14 Dec 2011 23:41:22 +0000 (17:41 -0600)]
Upped the version of the DDK to match the kernel. I've also added the Android.mk file from the update DDK so that the first pass make system picks it up as expected.

Change-Id: Ief0b0d770a90c9fc8f32556204cf7e11a78ecc78
Signed-off-by: James W. Mills <jameswmills@ti.com>
11 years agoLicensed ducati bundle
James W. Mills [Tue, 13 Dec 2011 20:39:52 +0000 (14:39 -0600)]
Licensed ducati bundle

Release a binary version of Ducati, complete with DCC files, all under
license.

Change-Id: I62f1784dfb1b815e8f58b69716b19bb53ca32b2e
Signed-off-by: James W. Mills <jameswmills@ti.com>
12 years agoMove licensed content to tgz archives
James W. Mills [Thu, 8 Dec 2011 19:11:06 +0000 (13:11 -0600)]
Move licensed content to tgz archives

This change allows all licensed material to be license-bound, and
prevents any single component from being downloaded without the proper
license agreement.

Change-Id: I353122644b1696438a7c7a33a26d43087e19440a
Signed-off-by: James W. Mills <jameswmills@ti.com>
12 years agoMerge "[proprietary-open] Upload WLAN firmware files" into ics-mr0
Jean Johnson [Sat, 3 Dec 2011 08:13:59 +0000 (02:13 -0600)]
Merge "[proprietary-open] Upload WLAN firmware files" into ics-mr0

12 years ago[proprietary-open] Upload WLAN firmware files
Vishal Mahaveer [Wed, 23 Nov 2011 15:21:57 +0000 (08:21 -0700)]
[proprietary-open] Upload WLAN firmware files

Upload WLAN firmware files to proprietary-open.

Change-Id: I11f99a79df511e792fa0e6d6cf5872b4b5ce7a27
Signed-off-by: Vishal Mahaveer <a0271468@ti.com>
12 years agoPRODUCT PACKAGES being overwritten again
Jean Johnson [Wed, 30 Nov 2011 15:48:22 +0000 (09:48 -0600)]
PRODUCT PACKAGES being overwritten again

The PRODUCT PACKAGES list was being overwritten due use of :=
instead of += in the PRODUCT_PACKAGES assignement.

Signed-off-by: Jean Johnson <jean-johnson@ti.com>
Change-Id: Icc6d7a53f5b56e6eb06201b6a7cfec7ca0eb06e0

12 years agoSGX-BIN: IMG DDK 1.8@550175 binaries for ICS
Hemant Hariyani [Wed, 23 Nov 2011 17:09:06 +0000 (11:09 -0600)]
SGX-BIN: IMG DDK 1.8@550175 binaries for ICS

IMG DDK 1.8@550175 binaries

Change-Id: I215a17b72d2b3a2e57e06546403a9f643cebee04
Signed-off-by: Hemant Hariyani <hemanthariyani@ti.com>
13 years agoInitial blank repo
Keith Deacon [Tue, 14 Sep 2010 06:29:08 +0000 (01:29 -0500)]
Initial blank repo