Merge branch 'drm-nouveau-fixes-3.8' of git://anongit.freedesktop.org/git/nouveau/linux-2.6 into drm-next Fixes for one major lockdep warning, one oops reported by a few people, and fix for a long hang on some gpu engines. * 'drm-nouveau-fixes-3.8' of git://anongit.freedesktop.org/git/nouveau/linux-2.6: drm/nouveau: add lockdep annotations drm/nv50/fb: Fix nullptr-deref on IGPs drm/nouveau: use different register to wait for secret scrubber
drm/nouveau: add lockdep annotations 1) Lockdep thinks all nouveau subdevs belong to the same class and can be locked in arbitrary order, which is not true (at least in general case). Tell it to distinguish subdevs by (o)class type. 2) DRM client can be locked under user client lock - tell lockdep to put DRM client lock in a separate class. Reported-by: Arend van Spriel <arend@broadcom.com> Reported-by: Peter Hurley <peter@hurleysoftware.com> Reported-by: Maarten Lankhorst <maarten.lankhorst@canonical.com> Reported-by: Daniel J Blueman <daniel@quora.org> Signed-off-by: Marcin Slusarz <marcin.slusarz@gmail.com> Cc: stable@vger.kernel.org [3.7, but needs s/const ofuncs/ofuncs/ to build] Signed-off-by: Ben Skeggs <bskeggs@redhat.com>
Merge branch 'drm-nouveau-fixes' of git://anongit.freedesktop.org/git/nouveau/linux-2.6 into drm-next Regression fixes since rework mostly. * 'drm-nouveau-fixes' of git://anongit.freedesktop.org/git/nouveau/linux-2.6: drm/nvc0/fb: fix crash when different mutex is used to protect same list drm/nouveau/clock: fix support for more than 2 monitors on nve0 drm/nv50/disp: fix selection of bios script for analog outputs drm/nv17-50: restore fence buffer on resume drm/nouveau: fix blank LVDS screen regression on pre-nv50 cards drm/nouveau: fix nouveau_client allocation failure path drm/nouveau: don't return freed object from nouveau_handle_create drm/nouveau/vm: fix memory corruption when pgt allocation fails drm/nouveau: add locking around instobj list operations drm/nouveau: do not forcibly power on lvds panels drm/nouveau/devinit: ensure legacy vga control is enabled during post
drm/nouveau: fix nouveau_client allocation failure path Depending on the point of failure, freed object would be returned or memory leak would happen. Signed-off-by: Marcin Slusarz <marcin.slusarz@gmail.com> Signed-off-by: Ben Skeggs <bskeggs@redhat.com>
Drivers: gpu: remove __dev* attributes. CONFIG_HOTPLUG is going away as an option. As a result, the __dev* markings need to be removed. This change removes the use of __devinit, __devexit_p, and __devexit from these drivers. Based on patches originally written by Bill Pemberton, but redone by me in order to handle some of the coding style issues better, by hand. Cc: Bill Pemberton <wfp5p@virginia.edu> Cc: David Airlie <airlied@linux.ie> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
Merge branch 'drm-next-3.8' of git://people.freedesktop.org/~agd5f/linux into drm-next Alex writes: Pretty minor -next pull request. We some additional new bits waiting internally for release. Hopefully Monday we can get at least some of them out. The others will probably take a few more weeks. Highlights of the current request: - ELD registers for passing audio information to the sound hardware - Handle GPUVM page faults more gracefully - Misc fixes Merge radeon test * 'drm-next-3.8' of git://people.freedesktop.org/~agd5f/linux: (483 commits) drm/radeon: bump driver version for new info ioctl requests drm/radeon: fix eDP clk and lane setup for scaled modes drm/radeon: add new INFO ioctl requests drm/radeon/dce32+: use fractional fb dividers for high clocks drm/radeon: use cached memory when evicting for vram on non agp drm/radeon: add a CS flag END_OF_FRAME drm/radeon: stop page faults from hanging the system (v2) drm/radeon/dce4/5: add registers for ELD handling drm/radeon/dce3.2: add registers for ELD handling radeon: fix pll/ctrc mapping on dce2 and dce3 hardware Linux 3.7-rc7 powerpc/eeh: Do not invalidate PE properly Revert "drm/i915: enable rc6 on ilk again" ALSA: hda - Fix build without CONFIG_PM of/address: sparc: Declare of_iomap as an extern function for sparc again PM / QoS: fix wrong error-checking condition bnx2x: remove redundant warning log vxlan: fix command usage in its doc 8139cp: revert "set ring address before enabling receiver" MPI: Fix compilation on MIPS with GCC 4.4 and newer ... Conflicts: drivers/gpu/drm/exynos/exynos_drm_encoder.c drivers/gpu/drm/exynos/exynos_drm_fbdev.c drivers/gpu/drm/nouveau/core/engine/disp/nv50.c
drm/nouveau: remove duplicate inclusion of nouveau_ttm.h nouveau_ttm.h was included twice. Signed-off-by: Sachin Kamat <sachin.kamat@linaro.org> Signed-off-by: Ben Skeggs <bskeggs@redhat.com>
drm/nve0: allow specification of channel engine type in abi16 call Previously, if either vram/gart handles were specified as ~0, the ioctl call would fail. In order to hack engine selection into the ioctl for kepler, we now define (fb_ctxdma_handle == ~0) to mean "engine mask is in tt_ctxdma_handle". This approach also allows new userspace to detect lack of support for non-PGRAPH channels on older kernels. Signed-off-by: Ben Skeggs <bskeggs@redhat.com>
drm/nouveau: convert to dev_pm_ops This is a precursor to dynamic power management support for nouveau, we need to use pm ops for that, so first convert the driver to using pm ops interfaces. Signed-off-by: Dave Airlie <airlied@redhat.com> Signed-off-by: Ben Skeggs <bskeggs@redhat.com>
drm/nouveau: use the correct fence implementation for nv50 Only compile time tested, noticed nv50_fence_create was never used, so fix this. This will probably fix vblank on nv50 cards. Hopefully this is still in time for 3.7 final release. Signed-off-by: Maarten Lankhorst <maarten.lankhorst@canonical.com> Signed-off-by: Ben Skeggs <bskeggs@redhat.com>
drm/nouveau: free memory allocated with alloc_apertures() Fix a memory leak by deallocating the memory we got from alloc_apertures(). Signed-off-by: Tommi Rantala <tt.rantala@gmail.com> Signed-off-by: Dave Airlie <airlied@redhat.com>
drm/nouveau: headless mode by default if pci class != vga display This is to prevent nouveau from taking over the console on headless boards such as Tesla. Signed-off-by: Ben Skeggs <bskeggs@redhat.com>
drm/nouveau: resurrect headless mode since rework Signed-off-by: Ben Skeggs <bskeggs@redhat.com>
Merge branch 'drm-next' of git://people.freedesktop.org/~airlied/linux Pull drm merge (part 1) from Dave Airlie: "So first of all my tree and uapi stuff has a conflict mess, its my fault as the nouveau stuff didn't hit -next as were trying to rebase regressions out of it before we merged. Highlights: - SH mobile modesetting driver and associated helpers - some DRM core documentation - i915 modesetting rework, haswell hdmi, haswell and vlv fixes, write combined pte writing, ilk rc6 support, - nouveau: major driver rework into a hw core driver, makes features like SLI a lot saner to implement, - psb: add eDP/DP support for Cedarview - radeon: 2 layer page tables, async VM pte updates, better PLL selection for > 2 screens, better ACPI interactions The rest is general grab bag of fixes. So why part 1? well I have the exynos pull req which came in a bit late but was waiting for me to do something they shouldn't have and it looks fairly safe, and David Howells has some more header cleanups he'd like me to pull, that seem like a good idea, but I'd like to get this merge out of the way so -next dosen't get blocked." Tons of conflicts mostly due to silly include line changes, but mostly mindless. A few other small semantic conflicts too, noted from Dave's pre-merged branch. * 'drm-next' of git://people.freedesktop.org/~airlied/linux: (447 commits) drm/nv98/crypt: fix fuc build with latest envyas drm/nouveau/devinit: fixup various issues with subdev ctor/init ordering drm/nv41/vm: fix and enable use of "real" pciegart drm/nv44/vm: fix and enable use of "real" pciegart drm/nv04/dmaobj: fixup vm target handling in preparation for nv4x pcie drm/nouveau: store supported dma mask in vmmgr drm/nvc0/ibus: initial implementation of subdev drm/nouveau/therm: add support for fan-control modes drm/nouveau/hwmon: rename pwm0* to pmw1* to follow hwmon's rules drm/nouveau/therm: calculate the pwm divisor on nv50+ drm/nouveau/fan: rewrite the fan tachometer driver to get more precision, faster drm/nouveau/therm: move thermal-related functions to the therm subdev drm/nouveau/bios: parse the pwm divisor from the perf table drm/nouveau/therm: use the EXTDEV table to detect i2c monitoring devices drm/nouveau/therm: rework thermal table parsing drm/nouveau/gpio: expose the PWM/TOGGLE parameter found in the gpio vbios table drm/nouveau: fix pm initialization order drm/nouveau/bios: check that fixed tvdac gpio data is valid before using it drm/nouveau: log channel debug/error messages from client object rather than drm client drm/nouveau: have drm debugging macros build on top of core macros ...
drm/nouveau/core: have client-id be a string, rather than an integer Can be somewhat more informative that way... Signed-off-by: Ben Skeggs <bskeggs@redhat.com>
drm/nouveau: quiet some static-related sparse noise Signed-off-by: Marcin Slusarz <marcin.slusarz@gmail.com> Signed-off-by: Ben Skeggs <bskeggs@redhat.com>
drm/nve0: use async copy engine for ttm buffer moves if available Kepler PFIFO lost the ability to address multiple engines from a single channel, so we need a separate one for the copy engine. v2: Marcin Slusarz <marcin.slusarz@gmail.com> - regression fix: restore hw accelerated buffer copies Signed-off-by: Ben Skeggs <bskeggs@redhat.com>
drm/nouveau: port remainder of drm code, and rip out compat layer v2: Ben Skeggs <bskeggs@redhat.com> - fill in nouveau_pm.dev to prevent oops - fix ppc issues (build + OF shadow) Signed-off-by: Ben Skeggs <bskeggs@redhat.com>
drm/nouveau: port all engines to new engine module format This is a HUGE commit, but it's not nearly as bad as it looks - any problems can be isolated to a particular chipset and engine combination. It was simply too difficult to port each one at a time, the compat layers are *already* ridiculous. Most of the changes here are simply to the glue, the process for each of the engine modules was to start with a standard skeleton and copy+paste the old code into the appropriate places, fixing up variable names etc as needed. v2: Marcin Slusarz <marcin.slusarz@gmail.com> - fix find/replace bug in license header v3: Ben Skeggs <bskeggs@redhat.com> - bump indirect pushbuf size to 8KiB, 4KiB barely enough for userspace and left no space for kernel's requirements during GEM pushbuf submission. - fix duplicate assignments noticed by clang v4: Marcin Slusarz <marcin.slusarz@gmail.com> - add sparse annotations to nv04_fifo_pause/nv04_fifo_start - use ioread32_native/iowrite32_native for fifo control registers v5: Ben Skeggs <bskeggs@redhat.com> - rebase on v3.6-rc4, modified to keep copy engine fix intact - nv10/fence: unmap fence bo before destroying - fixed fermi regression when using nvidia gr fuc - fixed typo in supported dma_mask checking Signed-off-by: Ben Skeggs <bskeggs@redhat.com>
drm/nouveau: implement devinit subdev, and new init table parser v2: - make sure not to execute display scripts unless resuming Signed-off-by: Ben Skeggs <bskeggs@redhat.com>